]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commitdiff
Remove the old coalescer algorithm.
authorJakob Stoklund Olesen <stoklund@2pi.dk>
Tue, 2 Oct 2012 22:45:03 +0000 (22:45 +0000)
committerJakob Stoklund Olesen <stoklund@2pi.dk>
Tue, 2 Oct 2012 22:45:03 +0000 (22:45 +0000)
The new algorithm has been enabled by default for almost a week now and
seems to be stable.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@165062 91177308-0d34-0410-b5e6-96231b3b80d8

lib/CodeGen/RegisterCoalescer.cpp

index ad1f5f4f125c49924fb2981e0950d16a6151556c..1b46256baf2b14ff1adc34e44a642a3cec42ba0d 100644 (file)
@@ -68,11 +68,6 @@ VerifyCoalescing("verify-coalescing",
          cl::desc("Verify machine instrs before and after register coalescing"),
          cl::Hidden);
 
-// Temporary option for testing new coalescer algo.
-static cl::opt<bool>
-NewCoalescer("new-coalescer", cl::Hidden, cl::init(true),
-             cl::desc("Use new coalescer algorithm"));
-
 namespace {
   class RegisterCoalescer : public MachineFunctionPass,
                             private LiveRangeEdit::Delegate {
@@ -1844,348 +1839,10 @@ bool RegisterCoalescer::joinVirtRegs(CoalescerPair &CP) {
   return true;
 }
 
-/// ComputeUltimateVN - Assuming we are going to join two live intervals,
-/// compute what the resultant value numbers for each value in the input two
-/// ranges will be.  This is complicated by copies between the two which can
-/// and will commonly cause multiple value numbers to be merged into one.
-///
-/// VN is the value number that we're trying to resolve.  InstDefiningValue
-/// keeps track of the new InstDefiningValue assignment for the result
-/// LiveInterval.  ThisFromOther/OtherFromThis are sets that keep track of
-/// whether a value in this or other is a copy from the opposite set.
-/// ThisValNoAssignments/OtherValNoAssignments keep track of value #'s that have
-/// already been assigned.
-///
-/// ThisFromOther[x] - If x is defined as a copy from the other interval, this
-/// contains the value number the copy is from.
-///
-static unsigned ComputeUltimateVN(VNInfo *VNI,
-                                  SmallVector<VNInfo*, 16> &NewVNInfo,
-                                  DenseMap<VNInfo*, VNInfo*> &ThisFromOther,
-                                  DenseMap<VNInfo*, VNInfo*> &OtherFromThis,
-                                  SmallVector<int, 16> &ThisValNoAssignments,
-                                  SmallVector<int, 16> &OtherValNoAssignments) {
-  unsigned VN = VNI->id;
-
-  // If the VN has already been computed, just return it.
-  if (ThisValNoAssignments[VN] >= 0)
-    return ThisValNoAssignments[VN];
-  assert(ThisValNoAssignments[VN] != -2 && "Cyclic value numbers");
-
-  // If this val is not a copy from the other val, then it must be a new value
-  // number in the destination.
-  DenseMap<VNInfo*, VNInfo*>::iterator I = ThisFromOther.find(VNI);
-  if (I == ThisFromOther.end()) {
-    NewVNInfo.push_back(VNI);
-    return ThisValNoAssignments[VN] = NewVNInfo.size()-1;
-  }
-  VNInfo *OtherValNo = I->second;
-
-  // Otherwise, this *is* a copy from the RHS.  If the other side has already
-  // been computed, return it.
-  if (OtherValNoAssignments[OtherValNo->id] >= 0)
-    return ThisValNoAssignments[VN] = OtherValNoAssignments[OtherValNo->id];
-
-  // Mark this value number as currently being computed, then ask what the
-  // ultimate value # of the other value is.
-  ThisValNoAssignments[VN] = -2;
-  unsigned UltimateVN =
-    ComputeUltimateVN(OtherValNo, NewVNInfo, OtherFromThis, ThisFromOther,
-                      OtherValNoAssignments, ThisValNoAssignments);
-  return ThisValNoAssignments[VN] = UltimateVN;
-}
-
-
-// Find out if we have something like
-// A = X
-// B = X
-// if so, we can pretend this is actually
-// A = X
-// B = A
-// which allows us to coalesce A and B.
-// VNI is the definition of B. LR is the life range of A that includes
-// the slot just before B. If we return true, we add "B = X" to DupCopies.
-// This implies that A dominates B.
-static bool RegistersDefinedFromSameValue(LiveIntervals &li,
-                                          const TargetRegisterInfo &tri,
-                                          CoalescerPair &CP,
-                                          VNInfo *VNI,
-                                          VNInfo *OtherVNI,
-                                     SmallVector<MachineInstr*, 8> &DupCopies) {
-  // FIXME: This is very conservative. For example, we don't handle
-  // physical registers.
-
-  MachineInstr *MI = li.getInstructionFromIndex(VNI->def);
-
-  if (!MI || CP.isPartial() || CP.isPhys())
-    return false;
-
-  unsigned A = CP.getDstReg();
-  if (!TargetRegisterInfo::isVirtualRegister(A))
-    return false;
-
-  unsigned B = CP.getSrcReg();
-  if (!TargetRegisterInfo::isVirtualRegister(B))
-    return false;
-
-  MachineInstr *OtherMI = li.getInstructionFromIndex(OtherVNI->def);
-  if (!OtherMI)
-    return false;
-
-  if (MI->isImplicitDef()) {
-    DupCopies.push_back(MI);
-    return true;
-  } else {
-    if (!MI->isFullCopy())
-      return false;
-    unsigned Src = MI->getOperand(1).getReg();
-    if (!TargetRegisterInfo::isVirtualRegister(Src))
-      return false;
-    if (!OtherMI->isFullCopy())
-      return false;
-    unsigned OtherSrc = OtherMI->getOperand(1).getReg();
-    if (!TargetRegisterInfo::isVirtualRegister(OtherSrc))
-      return false;
-
-    if (Src != OtherSrc)
-      return false;
-
-    // If the copies use two different value numbers of X, we cannot merge
-    // A and B.
-    LiveInterval &SrcInt = li.getInterval(Src);
-    // getVNInfoBefore returns NULL for undef copies. In this case, the
-    // optimization is still safe.
-    if (SrcInt.getVNInfoBefore(OtherVNI->def) !=
-        SrcInt.getVNInfoBefore(VNI->def))
-      return false;
-
-    DupCopies.push_back(MI);
-    return true;
-  }
-}
-
 /// joinIntervals - Attempt to join these two intervals.  On failure, this
 /// returns false.
 bool RegisterCoalescer::joinIntervals(CoalescerPair &CP) {
-  // Handle physreg joins separately.
-  if (CP.isPhys())
-    return joinReservedPhysReg(CP);
-
-  if (NewCoalescer)
-    return joinVirtRegs(CP);
-
-  LiveInterval &RHS = LIS->getInterval(CP.getSrcReg());
-  DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
-               << '\n');
-
-  // Compute the final value assignment, assuming that the live ranges can be
-  // coalesced.
-  SmallVector<int, 16> LHSValNoAssignments;
-  SmallVector<int, 16> RHSValNoAssignments;
-  DenseMap<VNInfo*, VNInfo*> LHSValsDefinedFromRHS;
-  DenseMap<VNInfo*, VNInfo*> RHSValsDefinedFromLHS;
-  SmallVector<VNInfo*, 16> NewVNInfo;
-
-  SmallVector<MachineInstr*, 8> DupCopies;
-  SmallVector<MachineInstr*, 8> DeadCopies;
-
-  LiveInterval &LHS = LIS->getOrCreateInterval(CP.getDstReg());
-  DEBUG(dbgs() << "\t\tLHS = " << PrintReg(CP.getDstReg(), TRI) << ' ' << LHS
-               << '\n');
-
-  // Loop over the value numbers of the LHS, seeing if any are defined from
-  // the RHS.
-  for (LiveInterval::vni_iterator i = LHS.vni_begin(), e = LHS.vni_end();
-       i != e; ++i) {
-    VNInfo *VNI = *i;
-    if (VNI->isUnused() || VNI->isPHIDef())
-      continue;
-    MachineInstr *MI = LIS->getInstructionFromIndex(VNI->def);
-    assert(MI && "Missing def");
-    if (!MI->isCopyLike() && !MI->isImplicitDef()) // Src not defined by a copy?
-      continue;
-
-    // Figure out the value # from the RHS.
-    VNInfo *OtherVNI = RHS.getVNInfoBefore(VNI->def);
-    // The copy could be to an aliased physreg.
-    if (!OtherVNI)
-      continue;
-
-    // DstReg is known to be a register in the LHS interval.  If the src is
-    // from the RHS interval, we can use its value #.
-    if (CP.isCoalescable(MI))
-      DeadCopies.push_back(MI);
-    else if (!RegistersDefinedFromSameValue(*LIS, *TRI, CP, VNI, OtherVNI,
-                                            DupCopies))
-      continue;
-
-    LHSValsDefinedFromRHS[VNI] = OtherVNI;
-  }
-
-  // Loop over the value numbers of the RHS, seeing if any are defined from
-  // the LHS.
-  for (LiveInterval::vni_iterator i = RHS.vni_begin(), e = RHS.vni_end();
-       i != e; ++i) {
-    VNInfo *VNI = *i;
-    if (VNI->isUnused() || VNI->isPHIDef())
-      continue;
-    MachineInstr *MI = LIS->getInstructionFromIndex(VNI->def);
-    assert(MI && "Missing def");
-    if (!MI->isCopyLike() && !MI->isImplicitDef()) // Src not defined by a copy?
-      continue;
-
-    // Figure out the value # from the LHS.
-    VNInfo *OtherVNI = LHS.getVNInfoBefore(VNI->def);
-    // The copy could be to an aliased physreg.
-    if (!OtherVNI)
-      continue;
-
-    // DstReg is known to be a register in the RHS interval.  If the src is
-    // from the LHS interval, we can use its value #.
-    if (CP.isCoalescable(MI))
-      DeadCopies.push_back(MI);
-    else if (!RegistersDefinedFromSameValue(*LIS, *TRI, CP, VNI, OtherVNI,
-                                            DupCopies))
-        continue;
-
-    RHSValsDefinedFromLHS[VNI] = OtherVNI;
-  }
-
-  LHSValNoAssignments.resize(LHS.getNumValNums(), -1);
-  RHSValNoAssignments.resize(RHS.getNumValNums(), -1);
-  NewVNInfo.reserve(LHS.getNumValNums() + RHS.getNumValNums());
-
-  for (LiveInterval::vni_iterator i = LHS.vni_begin(), e = LHS.vni_end();
-       i != e; ++i) {
-    VNInfo *VNI = *i;
-    unsigned VN = VNI->id;
-    if (LHSValNoAssignments[VN] >= 0 || VNI->isUnused())
-      continue;
-    ComputeUltimateVN(VNI, NewVNInfo,
-                      LHSValsDefinedFromRHS, RHSValsDefinedFromLHS,
-                      LHSValNoAssignments, RHSValNoAssignments);
-  }
-  for (LiveInterval::vni_iterator i = RHS.vni_begin(), e = RHS.vni_end();
-       i != e; ++i) {
-    VNInfo *VNI = *i;
-    unsigned VN = VNI->id;
-    if (RHSValNoAssignments[VN] >= 0 || VNI->isUnused())
-      continue;
-    // If this value number isn't a copy from the LHS, it's a new number.
-    if (RHSValsDefinedFromLHS.find(VNI) == RHSValsDefinedFromLHS.end()) {
-      NewVNInfo.push_back(VNI);
-      RHSValNoAssignments[VN] = NewVNInfo.size()-1;
-      continue;
-    }
-
-    ComputeUltimateVN(VNI, NewVNInfo,
-                      RHSValsDefinedFromLHS, LHSValsDefinedFromRHS,
-                      RHSValNoAssignments, LHSValNoAssignments);
-  }
-
-  // Armed with the mappings of LHS/RHS values to ultimate values, walk the
-  // interval lists to see if these intervals are coalescable.
-  LiveInterval::const_iterator I = LHS.begin();
-  LiveInterval::const_iterator IE = LHS.end();
-  LiveInterval::const_iterator J = RHS.begin();
-  LiveInterval::const_iterator JE = RHS.end();
-
-  // Collect interval end points that will no longer be kills.
-  SmallVector<MachineInstr*, 8> LHSOldKills;
-  SmallVector<MachineInstr*, 8> RHSOldKills;
-
-  // Skip ahead until the first place of potential sharing.
-  if (I != IE && J != JE) {
-    if (I->start < J->start) {
-      I = std::upper_bound(I, IE, J->start);
-      if (I != LHS.begin()) --I;
-    } else if (J->start < I->start) {
-      J = std::upper_bound(J, JE, I->start);
-      if (J != RHS.begin()) --J;
-    }
-  }
-
-  while (I != IE && J != JE) {
-    // Determine if these two live ranges overlap.
-    // If so, check value # info to determine if they are really different.
-    if (I->end > J->start && J->end > I->start) {
-      // If the live range overlap will map to the same value number in the
-      // result liverange, we can still coalesce them.  If not, we can't.
-      if (LHSValNoAssignments[I->valno->id] !=
-          RHSValNoAssignments[J->valno->id])
-        return false;
-
-      // Extended live ranges should no longer be killed.
-      if (!I->end.isBlock() && I->end < J->end)
-        if (MachineInstr *MI = LIS->getInstructionFromIndex(I->end))
-          LHSOldKills.push_back(MI);
-      if (!J->end.isBlock() && J->end < I->end)
-        if (MachineInstr *MI = LIS->getInstructionFromIndex(J->end))
-          RHSOldKills.push_back(MI);
-    }
-
-    if (I->end < J->end)
-      ++I;
-    else
-      ++J;
-  }
-
-  // Clear kill flags where live ranges are extended.
-  while (!LHSOldKills.empty())
-    LHSOldKills.pop_back_val()->clearRegisterKills(LHS.reg, TRI);
-  while (!RHSOldKills.empty())
-    RHSOldKills.pop_back_val()->clearRegisterKills(RHS.reg, TRI);
-
-  if (LHSValNoAssignments.empty())
-    LHSValNoAssignments.push_back(-1);
-  if (RHSValNoAssignments.empty())
-    RHSValNoAssignments.push_back(-1);
-
-  // Now erase all the redundant copies.
-  for (unsigned i = 0, e = DeadCopies.size(); i != e; ++i) {
-    MachineInstr *MI = DeadCopies[i];
-    if (!ErasedInstrs.insert(MI))
-      continue;
-    DEBUG(dbgs() << "\t\terased:\t" << LIS->getInstructionIndex(MI)
-                 << '\t' << *MI);
-    LIS->RemoveMachineInstrFromMaps(MI);
-    MI->eraseFromParent();
-  }
-
-  SmallVector<unsigned, 8> SourceRegisters;
-  for (SmallVector<MachineInstr*, 8>::iterator I = DupCopies.begin(),
-         E = DupCopies.end(); I != E; ++I) {
-    MachineInstr *MI = *I;
-    if (!ErasedInstrs.insert(MI))
-      continue;
-
-    // If MI is a copy, then we have pretended that the assignment to B in
-    // A = X
-    // B = X
-    // was actually a copy from A. Now that we decided to coalesce A and B,
-    // transform the code into
-    // A = X
-    // In the case of the implicit_def, we just have to remove it.
-    if (!MI->isImplicitDef()) {
-      unsigned Src = MI->getOperand(1).getReg();
-      SourceRegisters.push_back(Src);
-    }
-    LIS->RemoveMachineInstrFromMaps(MI);
-    MI->eraseFromParent();
-  }
-
-  // If B = X was the last use of X in a liverange, we have to shrink it now
-  // that B = X is gone.
-  for (SmallVector<unsigned, 8>::iterator I = SourceRegisters.begin(),
-         E = SourceRegisters.end(); I != E; ++I) {
-    LIS->shrinkToUses(&LIS->getInterval(*I));
-  }
-
-  // If we get here, we know that we can coalesce the live ranges.  Ask the
-  // intervals to coalesce themselves now.
-  LHS.join(RHS, &LHSValNoAssignments[0], &RHSValNoAssignments[0], NewVNInfo,
-           MRI);
-  return true;
+  return CP.isPhys() ? joinReservedPhysReg(CP) : joinVirtRegs(CP);
 }
 
 namespace {