summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2d1536a)
raw | patch | inline | side by side (parent: 2d1536a)
author | Matthias Braun <matze@braunis.de> | |
Wed, 10 Dec 2014 01:12:00 +0000 (01:12 +0000) | ||
committer | Matthias Braun <matze@braunis.de> | |
Wed, 10 Dec 2014 01:12:00 +0000 (01:12 +0000) |
This works like the composeSubRegisterIndices() function but transforms
a subregister lane mask instead of a subregister index.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@223874 91177308-0d34-0410-b5e6-96231b3b80d8
a subregister lane mask instead of a subregister index.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@223874 91177308-0d34-0410-b5e6-96231b3b80d8
index ad4fdbe39584a1c8d011d30aeb1b64406ac779d8..d5c048e010ecdbaf9beb23a3e226e43f50730932 100644 (file)
return composeSubRegIndicesImpl(a, b);
}
+ /// Transforms a LaneMask computed for one subregister to the lanemask that
+ /// would have been computed when composing the subsubregisters with IdxA
+ /// first. @sa composeSubRegIndices()
+ unsigned composeSubRegIndexLaneMask(unsigned IdxA, unsigned LaneMask) const {
+ if (!IdxA)
+ return LaneMask;
+ return composeSubRegIndexLaneMaskImpl(IdxA, LaneMask);
+ }
+
/// Debugging helper: dump register in human readable form to dbgs() stream.
static void dumpReg(unsigned Reg, unsigned SubRegIndex = 0,
const TargetRegisterInfo* TRI = nullptr);
llvm_unreachable("Target has no sub-registers");
}
+ /// Overridden by TableGen in targets that have sub-registers.
+ virtual unsigned
+ composeSubRegIndexLaneMaskImpl(unsigned, unsigned) const {
+ llvm_unreachable("Target has no sub-registers");
+ }
+
public:
/// getCommonSuperRegClass - Find a common super-register class if it exists.
///
index fdfdba4f20262b94dbafa8718a22c33426f6b644..f37c3aec1cac6163e684089fde3995f68375d97e 100644 (file)
}
}
+ // Compute transformation sequences for composeSubRegIndexLaneMask. The idea
+ // here is that for each possible target subregister we look at the leafs
+ // in the subregister graph that compose for this target and create
+ // transformation sequences for the lanemasks. Each step in the sequence
+ // consists of a bitmask and a bitrotate operation. As the rotation amounts
+ // are usually the same for many subregisters we can easily combine the steps
+ // by combining the masks.
+ for (const auto &Idx : SubRegIndices) {
+ const auto &Composites = Idx.getComposites();
+ auto &LaneTransforms = Idx.CompositionLaneMaskTransform;
+ // Go through all leaf subregisters and find the ones that compose with Idx.
+ // These make out all possible valid bits in the lane mask we want to
+ // transform. Looking only at the leafs ensure that only a single bit in
+ // the mask is set.
+ unsigned NextBit = 0;
+ for (auto &Idx2 : SubRegIndices) {
+ // Skip non-leaf subregisters.
+ if (!Idx2.getComposites().empty())
+ continue;
+ // Replicate the behaviour from the lane mask generation loop above.
+ unsigned SrcBit = NextBit;
+ unsigned SrcMask = 1u << SrcBit;
+ if (NextBit < 31)
+ ++NextBit;
+ assert(Idx2.LaneMask == SrcMask);
+
+ // Get the composed subregister if there is any.
+ auto C = Composites.find(&Idx2);
+ if (C == Composites.end())
+ continue;
+ const CodeGenSubRegIndex *Composite = C->second;
+ // The Composed subreg should be a leaf subreg too
+ assert(Composite->getComposites().empty());
+
+ // Create Mask+Rotate operation and merge with existing ops if possible.
+ unsigned DstBit = Log2_32(Composite->LaneMask);
+ int Shift = DstBit - SrcBit;
+ uint8_t RotateLeft = Shift >= 0 ? (uint8_t)Shift : 32+Shift;
+ for (auto &I : LaneTransforms) {
+ if (I.RotateLeft == RotateLeft) {
+ I.Mask |= SrcMask;
+ SrcMask = 0;
+ }
+ }
+ if (SrcMask != 0) {
+ MaskRolPair MaskRol = { SrcMask, RotateLeft };
+ LaneTransforms.push_back(MaskRol);
+ }
+ }
+ // Optimize if the transformation consists of one step only: Set mask to
+ // 0xffffffff (including some irrelevant invalid bits) so that it should
+ // merge with more entries later while compressing the table.
+ if (LaneTransforms.size() == 1)
+ LaneTransforms[0].Mask = ~0u;
+
+ // Further compression optimization: For invalid compositions resulting
+ // in a sequence with 0 entries we can just pick any other. Choose
+ // Mask 0xffffffff with Rotation 0.
+ if (LaneTransforms.size() == 0) {
+ MaskRolPair P = { ~0u, 0 };
+ LaneTransforms.push_back(P);
+ }
+ }
+
// FIXME: What if ad-hoc aliasing introduces overlaps that aren't represented
// by the sub-register graph? This doesn't occur in any known targets.
index 6baaa28d95ddc2f1e4e9caad96d4e128a70d5e63..d4668a05f332569f9221433548754a656fb1364c 100644 (file)
namespace llvm {
class CodeGenRegBank;
+ /// Used to encode a step in a register lane mask transformation.
+ /// Mask the bits specified in Mask, then rotate them Rol bits to the left
+ /// assuming a wraparound at 32bits.
+ struct MaskRolPair {
+ unsigned Mask;
+ uint8_t RotateLeft;
+ bool operator==(const MaskRolPair Other) {
+ return Mask == Other.Mask && RotateLeft == Other.RotateLeft;
+ }
+ bool operator!=(const MaskRolPair Other) {
+ return Mask != Other.Mask || RotateLeft != Other.RotateLeft;
+ }
+ };
+
/// CodeGenSubRegIndex - Represents a sub-register index.
class CodeGenSubRegIndex {
Record *const TheDef;
uint16_t Offset;
const unsigned EnumValue;
mutable unsigned LaneMask;
+ mutable SmallVector<MaskRolPair,1> CompositionLaneMaskTransform;
// Are all super-registers containing this SubRegIndex covered by their
// sub-registers?
index b7bd37b30a2395a85d2fd44f9257bfd0b1538fc0..bde6a174dd19ebb63c684de5c204c1bd1da4eac3 100644 (file)
const std::string &ClassName);
void emitComposeSubRegIndices(raw_ostream &OS, CodeGenRegBank &RegBank,
const std::string &ClassName);
+ void emitComposeSubRegIndexLaneMask(raw_ostream &OS, CodeGenRegBank &RegBank,
+ const std::string &ClassName);
};
} // End anonymous namespace
OS << "}\n\n";
}
+void
+RegisterInfoEmitter::emitComposeSubRegIndexLaneMask(raw_ostream &OS,
+ CodeGenRegBank &RegBank,
+ const std::string &ClName) {
+ // See the comments in computeSubRegLaneMasks() for our goal here.
+ const auto &SubRegIndices = RegBank.getSubRegIndices();
+
+ // Create a list of Mask+Rotate operations, with equivalent entries merged.
+ SmallVector<unsigned, 4> SubReg2SequenceIndexMap;
+ SmallVector<SmallVector<MaskRolPair, 1>, 4> Sequences;
+ for (const auto &Idx : SubRegIndices) {
+ const SmallVector<MaskRolPair, 1> &IdxSequence
+ = Idx.CompositionLaneMaskTransform;
+
+ unsigned Found = ~0u;
+ unsigned SIdx = 0;
+ unsigned NextSIdx;
+ for (size_t s = 0, se = Sequences.size(); s != se; ++s, SIdx = NextSIdx) {
+ SmallVectorImpl<MaskRolPair> &Sequence = Sequences[s];
+ NextSIdx = SIdx + Sequence.size() + 1;
+ if (Sequence.size() != IdxSequence.size())
+ continue;
+ bool Identical = true;
+ for (size_t o = 0, oe = Sequence.size(); o != oe; ++o) {
+ if (Sequence[o] != IdxSequence[o]) {
+ Identical = false;
+ break;
+ }
+ }
+ if (Identical) {
+ Found = SIdx;
+ break;
+ }
+ }
+ if (Found == ~0u) {
+ Sequences.push_back(IdxSequence);
+ Found = SIdx;
+ }
+ SubReg2SequenceIndexMap.push_back(Found);
+ }
+
+ OS << "unsigned " << ClName
+ << "::composeSubRegIndexLaneMaskImpl(unsigned IdxA, unsigned LaneMask)"
+ " const {\n";
+
+ OS << " struct MaskRolOp {\n"
+ " unsigned Mask;\n"
+ " uint8_t RotateLeft;\n"
+ " };\n"
+ " static const MaskRolOp Seqs[] = {\n";
+ unsigned Idx = 0;
+ for (size_t s = 0, se = Sequences.size(); s != se; ++s) {
+ OS << " ";
+ const SmallVectorImpl<MaskRolPair> &Sequence = Sequences[s];
+ for (size_t p = 0, pe = Sequence.size(); p != pe; ++p) {
+ const MaskRolPair &P = Sequence[p];
+ OS << format("{ 0x%08X, %2u }, ", P.Mask, P.RotateLeft);
+ }
+ OS << "{ 0, 0 }";
+ if (s+1 != se)
+ OS << ", ";
+ OS << " // Sequence " << Idx << "\n";
+ Idx += Sequence.size() + 1;
+ }
+ OS << " };\n"
+ " static const MaskRolOp *CompositeSequences[] = {\n";
+ for (size_t i = 0, e = SubRegIndices.size(); i != e; ++i) {
+ OS << " ";
+ unsigned Idx = SubReg2SequenceIndexMap[i];
+ OS << format("&Seqs[%u]", Idx);
+ if (i+1 != e)
+ OS << ",";
+ OS << " // to " << SubRegIndices[i].getName() << "\n";
+ }
+ OS << " };\n\n";
+
+ OS << " --IdxA; assert(IdxA < " << SubRegIndices.size()
+ << " && \"Subregister index out of bounds\");\n"
+ " unsigned Result = 0;\n"
+ " for (const MaskRolOp *Ops = CompositeSequences[IdxA]; Ops->Mask != 0; ++Ops)"
+ " {\n"
+ " unsigned Masked = LaneMask & Ops->Mask;\n"
+ " Result |= (Masked << Ops->RotateLeft) & 0xFFFFFFFF;\n"
+ " Result |= (Masked >> ((32 - Ops->RotateLeft) & 0x1F));\n"
+ " }\n"
+ " return Result;\n"
+ "}\n";
+}
+
//
// runMCDesc - Print out MC register descriptions.
//
<< " { return false; }\n";
if (!RegBank.getSubRegIndices().empty()) {
OS << " unsigned composeSubRegIndicesImpl"
+ << "(unsigned, unsigned) const override;\n"
+ << " unsigned composeSubRegIndexLaneMaskImpl"
<< "(unsigned, unsigned) const override;\n"
<< " const TargetRegisterClass *getSubClassWithSubReg"
<< "(const TargetRegisterClass*, unsigned) const override;\n";
auto SubRegIndicesSize =
std::distance(SubRegIndices.begin(), SubRegIndices.end());
- if (!SubRegIndices.empty())
+ if (!SubRegIndices.empty()) {
emitComposeSubRegIndices(OS, RegBank, ClassName);
+ emitComposeSubRegIndexLaneMask(OS, RegBank, ClassName);
+ }
// Emit getSubClassWithSubReg.
if (!SubRegIndices.empty()) {