summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b6adb42)
raw | patch | inline | side by side (parent: b6adb42)
author | Alexey Samsonov <samsonov@google.com> | |
Wed, 2 Oct 2013 15:31:34 +0000 (15:31 +0000) | ||
committer | Alexey Samsonov <samsonov@google.com> | |
Wed, 2 Oct 2013 15:31:34 +0000 (15:31 +0000) |
Summary:
As discussed in http://llvm-reviews.chandlerc.com/D1754,
this optimization isn't really valid for C, and fires too rarely anyway.
Reviewers: rafael, nicholas
Reviewed By: nicholas
CC: rnk, llvm-commits, nicholas
Differential Revision: http://llvm-reviews.chandlerc.com/D1769
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@191834 91177308-0d34-0410-b5e6-96231b3b80d8
As discussed in http://llvm-reviews.chandlerc.com/D1754,
this optimization isn't really valid for C, and fires too rarely anyway.
Reviewers: rafael, nicholas
Reviewed By: nicholas
CC: rnk, llvm-commits, nicholas
Differential Revision: http://llvm-reviews.chandlerc.com/D1769
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@191834 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/IPO/GlobalOpt.cpp | patch | blob | history | |
test/Transforms/GlobalOpt/metadata.ll | [deleted file] | patch | blob | history |
index cf15580b03920c9d628794d46fbabf12ca0daa8d..3129559fb99a0c2698b703f5610364533e15628c 100644 (file)
STATISTIC(NumDeleted , "Number of globals deleted");
STATISTIC(NumFnDeleted , "Number of functions deleted");
STATISTIC(NumGlobUses , "Number of global uses devirtualized");
-STATISTIC(NumLocalized , "Number of globals localized");
STATISTIC(NumShrunkToBool , "Number of global vars shrunk to booleans");
STATISTIC(NumFastCallFns , "Number of functions converted to fastcc");
STATISTIC(NumCtorsEvaluated, "Number of static ctors evaluated");
/// ever stored to this global, keep track of what value it is.
Value *StoredOnceValue;
- /// AccessingFunction/HasMultipleAccessingFunctions - These start out
- /// null/false. When the first accessing function is noticed, it is recorded.
- /// When a second different accessing function is noticed,
- /// HasMultipleAccessingFunctions is set to true.
- const Function *AccessingFunction;
- bool HasMultipleAccessingFunctions;
-
- /// HasNonInstructionUser - Set to true if this global has a user that is not
- /// an instruction (e.g. a constant expr or GV initializer).
- bool HasNonInstructionUser;
-
/// AtomicOrdering - Set to the strongest atomic ordering requirement.
AtomicOrdering Ordering;
- GlobalStatus() : isCompared(false), isLoaded(false), StoredType(NotStored),
- StoredOnceValue(0), AccessingFunction(0),
- HasMultipleAccessingFunctions(false),
- HasNonInstructionUser(false), Ordering(NotAtomic) {}
+ GlobalStatus()
+ : isCompared(false), isLoaded(false), StoredType(NotStored),
+ StoredOnceValue(0), Ordering(NotAtomic) {}
};
}
++UI) {
const User *U = *UI;
if (const ConstantExpr *CE = dyn_cast<ConstantExpr>(U)) {
- GS.HasNonInstructionUser = true;
-
// If the result of the constantexpr isn't pointer type, then we won't
// know to expect it in various places. Just reject early.
if (!isa<PointerType>(CE->getType())) return true;
if (AnalyzeGlobal(CE, GS, PHIUsers)) return true;
} else if (const Instruction *I = dyn_cast<Instruction>(U)) {
- if (!GS.HasMultipleAccessingFunctions) {
- const Function *F = I->getParent()->getParent();
- if (GS.AccessingFunction == 0)
- GS.AccessingFunction = F;
- else if (GS.AccessingFunction != F)
- GS.HasMultipleAccessingFunctions = true;
- }
if (const LoadInst *LI = dyn_cast<LoadInst>(I)) {
GS.isLoaded = true;
// Don't hack on volatile loads.
return true; // Any other non-load instruction might take address!
}
} else if (const Constant *C = dyn_cast<Constant>(U)) {
- GS.HasNonInstructionUser = true;
// We might have a dead and dangling constant hanging off of here.
if (!SafeToDestroyConstant(C))
return true;
} else {
- GS.HasNonInstructionUser = true;
// Otherwise must be some other user.
return true;
}
bool GlobalOpt::ProcessInternalGlobal(GlobalVariable *GV,
Module::global_iterator &GVI,
const GlobalStatus &GS) {
- // If this is a first class global and has only one accessing function
- // and this function is main (which we know is not recursive), we replace
- // the global with a local alloca in this function.
- //
- // NOTE: It doesn't make sense to promote non single-value types since we
- // are just replacing static memory to stack memory.
- //
- // If the global is in different address space, don't bring it to stack.
- if (!GS.HasMultipleAccessingFunctions &&
- GS.AccessingFunction && !GS.HasNonInstructionUser &&
- GV->getType()->getElementType()->isSingleValueType() &&
- GS.AccessingFunction->getName() == "main" &&
- GS.AccessingFunction->hasExternalLinkage() &&
- GV->getType()->getAddressSpace() == 0) {
- DEBUG(dbgs() << "LOCALIZING GLOBAL: " << *GV);
- Instruction &FirstI = const_cast<Instruction&>(*GS.AccessingFunction
- ->getEntryBlock().begin());
- Type *ElemTy = GV->getType()->getElementType();
- // FIXME: Pass Global's alignment when globals have alignment
- AllocaInst *Alloca = new AllocaInst(ElemTy, NULL, GV->getName(), &FirstI);
- if (!isa<UndefValue>(GV->getInitializer()))
- new StoreInst(GV->getInitializer(), Alloca, &FirstI);
-
- GV->replaceAllUsesWith(Alloca);
- GV->eraseFromParent();
- ++NumLocalized;
- return true;
- }
-
// If the global is never loaded (but may be stored to), it is dead.
// Delete it now.
if (!GS.isLoaded) {
diff --git a/test/Transforms/GlobalOpt/metadata.ll b/test/Transforms/GlobalOpt/metadata.ll
+++ /dev/null
@@ -1,26 +0,0 @@
-; RUN: opt -S -globalopt < %s | FileCheck %s
-
-; PR6112 - When globalopt does RAUW(@G, %G), the metadata reference should drop
-; to null. Function local metadata that references @G from a different function
-; to that containing %G should likewise drop to null.
-@G = internal global i8** null
-
-define i32 @main(i32 %argc, i8** %argv) {
-; CHECK-LABEL: @main(
-; CHECK: %G = alloca
- store i8** %argv, i8*** @G
- ret i32 0
-}
-
-define void @foo(i32 %x) {
- call void @llvm.foo(metadata !{i8*** @G, i32 %x})
-; CHECK: call void @llvm.foo(metadata !{null, i32 %x})
- ret void
-}
-
-declare void @llvm.foo(metadata) nounwind readnone
-
-!named = !{!0}
-
-!0 = metadata !{i8*** @G}
-; CHECK: !0 = metadata !{null}