summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: dddc1cf)
raw | patch | inline | side by side (parent: dddc1cf)
author | Dmitri Gribenko <gribozavr@gmail.com> | |
Sat, 9 Jun 2012 00:01:45 +0000 (00:01 +0000) | ||
committer | Dmitri Gribenko <gribozavr@gmail.com> | |
Sat, 9 Jun 2012 00:01:45 +0000 (00:01 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@158248 91177308-0d34-0410-b5e6-96231b3b80d8
index 45469ed7de8048a2715b27ed7890fde9aa5e39a4..2b6c35b82f998d9860c1d6f330357498b85f6135 100644 (file)
/// PointKind - The type of a collector-safe point.
///
enum PointKind {
- Loop, //< Instr is a loop (backwards branch).
- Return, //< Instr is a return instruction.
- PreCall, //< Instr is a call instruction.
- PostCall //< Instr is the return address of a call.
+ Loop, ///< Instr is a loop (backwards branch).
+ Return, ///< Instr is a return instruction.
+ PreCall, ///< Instr is a call instruction.
+ PostCall ///< Instr is the return address of a call.
};
}
/// GCPoint - Metadata for a collector-safe point in machine code.
///
struct GCPoint {
- GC::PointKind Kind; //< The kind of the safe point.
- MCSymbol *Label; //< A label.
+ GC::PointKind Kind; ///< The kind of the safe point.
+ MCSymbol *Label; ///< A label.
DebugLoc Loc;
GCPoint(GC::PointKind K, MCSymbol *L, DebugLoc DL)
/// GCRoot - Metadata for a pointer to an object managed by the garbage
/// collector.
struct GCRoot {
- int Num; //< Usually a frame index.
- int StackOffset; //< Offset from the stack pointer.
+ int Num; ///< Usually a frame index.
+ int StackOffset; ///< Offset from the stack pointer.
const Constant *Metadata;//< Metadata straight from the call to llvm.gcroot.
GCRoot(int N, const Constant *MD) : Num(N), StackOffset(-1), Metadata(MD) {}
index 1cbd36abfbf82ed360df3e015354f7007cd65ebd..dfc26d72dc9f6a0a762e9c70f18c5b2acdc65f4c 100644 (file)
list_type Functions;
protected:
- unsigned NeededSafePoints; //< Bitmask of required safe points.
- bool CustomReadBarriers; //< Default is to insert loads.
- bool CustomWriteBarriers; //< Default is to insert stores.
- bool CustomRoots; //< Default is to pass through to backend.
- bool CustomSafePoints; //< Default is to use NeededSafePoints
- // to find safe points.
- bool InitRoots; //< If set, roots are nulled during lowering.
- bool UsesMetadata; //< If set, backend must emit metadata tables.
+ unsigned NeededSafePoints; ///< Bitmask of required safe points.
+ bool CustomReadBarriers; ///< Default is to insert loads.
+ bool CustomWriteBarriers; ///< Default is to insert stores.
+ bool CustomRoots; ///< Default is to pass through to backend.
+ bool CustomSafePoints; ///< Default is to use NeededSafePoints
+ ///< to find safe points.
+ bool InitRoots; ///< If set, roots are nulled during lowering.
+ bool UsesMetadata; ///< If set, backend must emit metadata tables.
public:
GCStrategy();
index 6d38c95715589b9656240e358e89b7e49aaaa7e2..8d797097a840c9dc834dc6e0fce33e61558d27af 100644 (file)
/// C:\foo\bar => C:,/,foo,bar
///
class const_iterator {
- StringRef Path; //< The entire path.
- StringRef Component; //< The current component. Not necessarily in Path.
- size_t Position; //< The iterators current position within Path.
+ StringRef Path; ///< The entire path.
+ StringRef Component; ///< The current component. Not necessarily in Path.
+ size_t Position; ///< The iterators current position within Path.
// An end iterator has Position = Path.size() + 1.
friend const_iterator begin(StringRef path);
index 10239958f33140656a01d17427969e97f407c1f1..98910eb7578f9d558d63fff6bbdb899d3384b7ae 100644 (file)
enum MappingType {
MT_Block,
MT_Flow,
- MT_Inline //< An inline mapping node is used for "[key: value]".
+ MT_Inline ///< An inline mapping node is used for "[key: value]".
};
MappingNode(OwningPtr<Document> &D, StringRef Anchor, MappingType MT)
index a6251e7d3345d39f72f9547394827d4c2a98ba89..f8cebefb0eae6d79056490bf4596b50010917aa2 100644 (file)
static const uint64_t ByValOffs = 4;
static const uint64_t Nest = 1ULL<<5; ///< Nested fn static chain
static const uint64_t NestOffs = 5;
- static const uint64_t ByValAlign = 0xFULL << 6; //< Struct alignment
+ static const uint64_t ByValAlign = 0xFULL << 6; ///< Struct alignment
static const uint64_t ByValAlignOffs = 6;
static const uint64_t Split = 1ULL << 10;
static const uint64_t SplitOffs = 10;
static const uint64_t OrigAlign = 0x1FULL<<27;
static const uint64_t OrigAlignOffs = 27;
- static const uint64_t ByValSize = 0xffffffffULL << 32; //< Struct size
+ static const uint64_t ByValSize = 0xffffffffULL << 32; ///< Struct size
static const uint64_t ByValSizeOffs = 32;
- static const uint64_t One = 1ULL; //< 1 of this type, for shifts
+ static const uint64_t One = 1ULL; ///< 1 of this type, for shifts
uint64_t Flags;
public:
index d116f392fb314bb57afed98bb444b289a2a32efd..4f94ab751cb681875588a95a9b3f643abbd3753f 100644 (file)
/// @note The unusual order of elements in the structure attempts to reduce
/// padding and make the structure slightly more cache friendly.
struct TargetAlignElem {
- AlignTypeEnum AlignType : 8; //< Alignment type (AlignTypeEnum)
- unsigned ABIAlign; //< ABI alignment for this type/bitw
- unsigned PrefAlign; //< Pref. alignment for this type/bitw
- uint32_t TypeBitWidth; //< Type bit width
+ AlignTypeEnum AlignType : 8; ///< Alignment type (AlignTypeEnum)
+ unsigned ABIAlign; ///< ABI alignment for this type/bitw
+ unsigned PrefAlign; ///< Pref. alignment for this type/bitw
+ uint32_t TypeBitWidth; ///< Type bit width
/// Initializer
static TargetAlignElem get(AlignTypeEnum align_type, unsigned abi_align,
diff --git a/lib/Object/Archive.cpp b/lib/Object/Archive.cpp
index 71d5a64c152b8e5e1e5eb7f8c50207ee601a0448..2a5951ada506e1a028905aa39a5cb75c08a8f9a3 100644 (file)
--- a/lib/Object/Archive.cpp
+++ b/lib/Object/Archive.cpp
char UID[6];
char GID[6];
char AccessMode[8];
- char Size[10]; //< Size of data, not including header or padding.
+ char Size[10]; ///< Size of data, not including header or padding.
char Terminator[2];
///! Get the name without looking up long names.
index 29d938b3874bfcb2613db91ba1a448708b7bbce8..8b7658fd9ca9b308b5149be1eaaf799bdbe86c80 100644 (file)
using namespace yaml;
enum UnicodeEncodingForm {
- UEF_UTF32_LE, //< UTF-32 Little Endian
- UEF_UTF32_BE, //< UTF-32 Big Endian
- UEF_UTF16_LE, //< UTF-16 Little Endian
- UEF_UTF16_BE, //< UTF-16 Big Endian
- UEF_UTF8, //< UTF-8 or ascii.
- UEF_Unknown //< Not a valid Unicode encoding.
+ UEF_UTF32_LE, ///< UTF-32 Little Endian
+ UEF_UTF32_BE, ///< UTF-32 Big Endian
+ UEF_UTF16_LE, ///< UTF-16 Little Endian
+ UEF_UTF16_BE, ///< UTF-16 Big Endian
+ UEF_UTF8, ///< UTF-8 or ascii.
+ UEF_Unknown ///< Not a valid Unicode encoding.
};
/// EncodingInfo - Holds the encoding type and length of the byte order mark if
index d2b167acb0e7c4c33ca87809edde2ae510f812c9..9f8043d6fa8330e36c0f1bf2812099f532d3836d 100644 (file)
namespace {
/// A class for recording information about inlining through an invoke.
class InvokeInliningInfo {
- BasicBlock *OuterResumeDest; //< Destination of the invoke's unwind.
- BasicBlock *InnerResumeDest; //< Destination for the callee's resume.
- LandingPadInst *CallerLPad; //< LandingPadInst associated with the invoke.
- PHINode *InnerEHValuesPHI; //< PHI for EH values from landingpad insts.
+ BasicBlock *OuterResumeDest; ///< Destination of the invoke's unwind.
+ BasicBlock *InnerResumeDest; ///< Destination for the callee's resume.
+ LandingPadInst *CallerLPad; ///< LandingPadInst associated with the invoke.
+ PHINode *InnerEHValuesPHI; ///< PHI for EH values from landingpad insts.
SmallVector<Value*, 8> UnwindDestPHIValues;
public: