summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: beab873)
raw | patch | inline | side by side (parent: beab873)
author | Rafael Espindola <rafael.espindola@gmail.com> | |
Tue, 9 Sep 2014 15:21:00 +0000 (15:21 +0000) | ||
committer | Rafael Espindola <rafael.espindola@gmail.com> | |
Tue, 9 Sep 2014 15:21:00 +0000 (15:21 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@217449 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Linker/LinkModules.cpp | patch | blob | history |
index 6e425992393f5dea5f6963a1276c819b6d5a2da2..87d075fb03ee2658dfe40449ad252615c1771827 100644 (file)
bool run();
private:
+ bool shouldLinkFromSource(const GlobalValue &Dest, const GlobalValue &Src);
+
/// emitError - Helper method for setting a message and returning an error
/// code.
bool emitError(const Twine &Message) {
return V.isDeclaration();
}
+bool ModuleLinker::shouldLinkFromSource(const GlobalValue &Dest,
+ const GlobalValue &Src) {
+ bool SrcIsDeclaration = isDeclaration(Src);
+ bool DestIsDeclaration = isDeclaration(Dest);
+
+ if (SrcIsDeclaration) {
+ // If Src is external or if both Src & Dest are external.. Just link the
+ // external globals, we aren't adding anything.
+ if (Src.hasDLLImportStorageClass())
+ // If one of GVs is marked as DLLImport, result should be dllimport'ed.
+ return DestIsDeclaration;
+ // If the Dest is weak, use the source linkage.
+ return Dest.hasExternalWeakLinkage();
+ }
+
+ if (DestIsDeclaration)
+ // If Dest is external but Src is not:
+ return true;
+
+ if (Src.isWeakForLinker()) {
+ assert(!Dest.hasExternalWeakLinkage());
+ assert(!Dest.hasAvailableExternallyLinkage());
+ if (Dest.hasLinkOnceLinkage() && Src.hasWeakLinkage())
+ return true;
+
+ return (Dest.hasLinkOnceLinkage() || Dest.hasWeakLinkage()) &&
+ Src.hasCommonLinkage();
+ }
+
+ if (Dest.isWeakForLinker()) {
+ assert(Src.hasExternalLinkage());
+ return true;
+ }
+
+ assert(!Src.hasExternalWeakLinkage());
+ assert(!Dest.hasExternalWeakLinkage());
+ assert(Dest.hasExternalLinkage() && Src.hasExternalLinkage() &&
+ "Unexpected linkage type!");
+ return emitError("Linking globals named '" + Src.getName() +
+ "': symbol multiply defined!");
+}
+
/// This analyzes the two global values and determines what the result will look
/// like in the destination module. In particular, it computes the resultant
/// linkage type and visibility, computes whether the global in the source
@@ -694,57 +738,15 @@ bool ModuleLinker::getLinkageResult(GlobalValue *Dest, const GlobalValue *Src,
assert(!Src->hasLocalLinkage() &&
"If Src has internal linkage, Dest shouldn't be set!");
- bool SrcIsDeclaration = isDeclaration(*Src);
- bool DestIsDeclaration = isDeclaration(*Dest);
+ assert(ErrorMsg.empty());
+ LinkFromSrc = shouldLinkFromSource(*Dest, *Src);
+ if (!ErrorMsg.empty())
+ return true;
- if (SrcIsDeclaration) {
- // If Src is external or if both Src & Dest are external.. Just link the
- // external globals, we aren't adding anything.
- if (Src->hasDLLImportStorageClass()) {
- // If one of GVs is marked as DLLImport, result should be dllimport'ed.
- if (DestIsDeclaration) {
- LinkFromSrc = true;
- LT = Src->getLinkage();
- } else {
- LinkFromSrc = false;
- LT = Dest->getLinkage();
- }
- } else if (Dest->hasExternalWeakLinkage()) {
- // If the Dest is weak, use the source linkage.
- LinkFromSrc = true;
- LT = Src->getLinkage();
- } else {
- LinkFromSrc = false;
- LT = Dest->getLinkage();
- }
- } else if (DestIsDeclaration) {
- // If Dest is external but Src is not:
- LinkFromSrc = true;
+ if (LinkFromSrc)
LT = Src->getLinkage();
- } else if (Src->isWeakForLinker()) {
- assert(!Dest->hasExternalWeakLinkage());
- assert(!Dest->hasAvailableExternallyLinkage());
- if ((Dest->hasLinkOnceLinkage() && Src->hasWeakLinkage()) ||
- ((Dest->hasLinkOnceLinkage() || Dest->hasWeakLinkage()) &&
- Src->hasCommonLinkage())) {
- LinkFromSrc = true;
- LT = Src->getLinkage();
- } else {
- LinkFromSrc = false;
- LT = Dest->getLinkage();
- }
- } else if (Dest->isWeakForLinker()) {
- assert(!Src->hasExternalWeakLinkage());
- LinkFromSrc = true;
- LT = GlobalValue::ExternalLinkage;
- } else {
- assert(!Src->hasExternalWeakLinkage());
- assert(!Dest->hasExternalWeakLinkage());
- assert(Dest->hasExternalLinkage() && Src->hasExternalLinkage() &&
- "Unexpected linkage type!");
- return emitError("Linking globals named '" + Src->getName() +
- "': symbol multiply defined!");
- }
+ else
+ LT = Dest->getLinkage();
// Compute the visibility. We follow the rules in the System V Application
// Binary Interface.