summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 98e0b9c)
raw | patch | inline | side by side (parent: 98e0b9c)
author | Daniel Dunbar <daniel@zuster.org> | |
Thu, 3 Nov 2011 17:30:16 +0000 (17:30 +0000) | ||
committer | Daniel Dunbar <daniel@zuster.org> | |
Thu, 3 Nov 2011 17:30:16 +0000 (17:30 +0000) |
for now).
- Mostly complete except for the data that needs to come from the build system
or the dependencies.
- Has some small improvements from current llvm-config:
o Uses TargetRegistry directly to get some information.
o Designed to work correctly when used from a CMake build tree (relatively
untested currently) (although pcc fixed this recently for old llvm-config).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@143616 91177308-0d34-0410-b5e6-96231b3b80d8
- Mostly complete except for the data that needs to come from the build system
or the dependencies.
- Has some small improvements from current llvm-config:
o Uses TargetRegistry directly to get some information.
o Designed to work correctly when used from a CMake build tree (relatively
untested currently) (although pcc fixed this recently for old llvm-config).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@143616 91177308-0d34-0410-b5e6-96231b3b80d8
tools/CMakeLists.txt | patch | blob | history | |
tools/Makefile | patch | blob | history | |
tools/llvm-config-2/CMakeLists.txt | [new file with mode: 0644] | patch | blob |
tools/llvm-config-2/Makefile | [new file with mode: 0644] | patch | blob |
tools/llvm-config-2/llvm-config.cpp | [new file with mode: 0644] | patch | blob |
diff --git a/tools/CMakeLists.txt b/tools/CMakeLists.txt
index 49c73b718fcc548509e7be1409d06b8173fbe220..4269ae842be8e279eff98e003c11c324d6c8c9b5 100644 (file)
--- a/tools/CMakeLists.txt
+++ b/tools/CMakeLists.txt
add_subdirectory(llvm-config)
endif()
+add_subdirectory(llvm-config-2)
add_subdirectory(opt)
add_subdirectory(llvm-as)
add_subdirectory(llvm-dis)
diff --git a/tools/Makefile b/tools/Makefile
index 2da39177815235f8257a85395cc6109eaf7654e1..278546bc1625b7e02c7d6bcf44a1d2da0712422f 100644 (file)
--- a/tools/Makefile
+++ b/tools/Makefile
bugpoint llvm-bcanalyzer llvm-stub \
llvm-diff macho-dump llvm-objdump \
llvm-rtdyld llvm-dwarfdump llvm-cov \
- llvm-size
+ llvm-size llvm-config-2
# Let users override the set of tools to build from the command line.
ifdef ONLY_TOOLS
diff --git a/tools/llvm-config-2/CMakeLists.txt b/tools/llvm-config-2/CMakeLists.txt
--- /dev/null
@@ -0,0 +1,5 @@
+set(LLVM_LINK_COMPONENTS support)
+
+add_llvm_tool(llvm-config-2
+ llvm-config.cpp
+ )
diff --git a/tools/llvm-config-2/Makefile b/tools/llvm-config-2/Makefile
--- /dev/null
@@ -0,0 +1,17 @@
+##===- tools/llvm-config/Makefile---------------------------*- Makefile -*-===##
+#
+# The LLVM Compiler Infrastructure
+#
+# This file is distributed under the University of Illinois Open Source
+# License. See LICENSE.TXT for details.
+#
+##===----------------------------------------------------------------------===##
+
+LEVEL := ../..
+TOOLNAME := llvm-config-2
+LINK_COMPONENTS := support
+
+# This tool has no plugins, optimize startup time.
+TOOL_NO_EXPORTS := 1
+
+include $(LEVEL)/Makefile.common
diff --git a/tools/llvm-config-2/llvm-config.cpp b/tools/llvm-config-2/llvm-config.cpp
--- /dev/null
@@ -0,0 +1,259 @@
+//===-- llvm-config.cpp - LLVM project configuration utility --------------===//
+//
+// The LLVM Compiler Infrastructure
+//
+// This file is distributed under the University of Illinois Open Source
+// License. See LICENSE.TXT for details.
+//
+//===----------------------------------------------------------------------===//
+//
+// This tool encapsulates information about an LLVM project configuration for
+// use by other project's build environments (to determine installed path,
+// available features, required libraries, etc.).
+//
+// Note that although this tool *may* be used by some parts of LLVM's build
+// itself (i.e., the Makefiles use it to compute required libraries when linking
+// tools), this tool is primarily designed to support external projects.
+//
+//===----------------------------------------------------------------------===//
+
+#include "llvm/ADT/StringRef.h"
+#include "llvm/ADT/Twine.h"
+#include "llvm/Config/config.h"
+#include "llvm/Config/llvm-config.h"
+#include "llvm/Support/FileSystem.h"
+#include "llvm/Support/Path.h"
+#include "llvm/Support/TargetRegistry.h"
+#include "llvm/Support/raw_ostream.h"
+#include <cstdlib>
+#include <vector>
+
+using namespace llvm;
+
+// FIXME: Need to get various bits of build time information.
+const char LLVM_SRC_ROOT[] = "FIXME";
+const char LLVM_OBJ_ROOT[] = "FIXME";
+const char LLVM_CPPFLAGS[] = "FIXME";
+const char LLVM_CFLAGS[] = "FIXME";
+const char LLVM_LDFLAGS[] = "FIXME";
+const char LLVM_CXXFLAGS[] = "FIXME";
+const char LLVM_BUILDMODE[] = "FIXME";
+const char LLVM_SYSTEM_LIBS[] = "FIXME";
+
+// FIXME: Include component table.
+struct AvailableComponent {
+ const char *Name;
+} AvailableComponents[1] = {};
+unsigned NumAvailableComponents = 0;
+
+void ComputeLibsForComponents(const std::vector<StringRef> &Components,
+ std::vector<StringRef> &RequiredLibs) {
+ // FIXME: Implement.
+ RequiredLibs = Components;
+}
+
+/* *** */
+
+void usage() {
+ errs() << "\
+usage: llvm-config <OPTION>... [<COMPONENT>...]\n\
+\n\
+Get various configuration information needed to compile programs which use\n\
+LLVM. Typically called from 'configure' scripts. Examples:\n\
+ llvm-config --cxxflags\n\
+ llvm-config --ldflags\n\
+ llvm-config --libs engine bcreader scalaropts\n\
+\n\
+Options:\n\
+ --version Print LLVM version.\n\
+ --prefix Print the installation prefix.\n\
+ --src-root Print the source root LLVM was built from.\n\
+ --obj-root Print the object root used to build LLVM.\n\
+ --bindir Directory containing LLVM executables.\n\
+ --includedir Directory containing LLVM headers.\n\
+ --libdir Directory containing LLVM libraries.\n\
+ --cppflags C preprocessor flags for files that include LLVM headers.\n\
+ --cflags C compiler flags for files that include LLVM headers.\n\
+ --cxxflags C++ compiler flags for files that include LLVM headers.\n\
+ --ldflags Print Linker flags.\n\
+ --libs Libraries needed to link against LLVM components.\n\
+ --libnames Bare library names for in-tree builds.\n\
+ --libfiles Fully qualified library filenames for makefile depends.\n\
+ --components List of all possible components.\n\
+ --targets-built List of all targets currently built.\n\
+ --host-target Target triple used to configure LLVM.\n\
+ --build-mode Print build mode of LLVM tree (e.g. Debug or Release).\n\
+Typical components:\n\
+ all All LLVM libraries (default).\n\
+ backend Either a native backend or the C backend.\n\
+ engine Either a native JIT or a bitcode interpreter.\n";
+ exit(1);
+}
+
+llvm::sys::Path GetExecutablePath(const char *Argv0) {
+ // This just needs to be some symbol in the binary; C++ doesn't
+ // allow taking the address of ::main however.
+ void *P = (void*) (intptr_t) GetExecutablePath;
+ return llvm::sys::Path::GetMainExecutable(Argv0, P);
+}
+
+int main(int argc, char **argv) {
+ std::vector<StringRef> Components;
+ bool PrintLibs = false, PrintLibNames = false, PrintLibFiles = false;
+ bool HasAnyOption = false;
+
+ // llvm-config is designed to support being run both from a development tree
+ // and from an installed path. We try and auto-detect which case we are in so
+ // that we can report the correct information when run from a development
+ // tree.
+ bool IsInDevelopmentTree, DevelopmentTreeLayoutIsCMakeStyle;
+ llvm::SmallString<256> CurrentPath(GetExecutablePath(argv[0]).str());
+ std::string CurrentExecPrefix;
+
+ // Create an absolute path, and pop up one directory (we expect to be inside a
+ // bin dir).
+ sys::fs::make_absolute(CurrentPath);
+ CurrentExecPrefix = sys::path::parent_path(
+ sys::path::parent_path(CurrentPath)).str();
+
+ // Check to see if we are inside a development tree by comparing to possible
+ // locations (prefix style or CMake style). This could be wrong in the face of
+ // symbolic links, but is good enough.
+ if (CurrentExecPrefix == std::string(LLVM_OBJ_ROOT) + "/" + LLVM_BUILDMODE) {
+ IsInDevelopmentTree = true;
+ DevelopmentTreeLayoutIsCMakeStyle = false;
+ } else if (CurrentExecPrefix == std::string(LLVM_OBJ_ROOT) + "/bin") {
+ IsInDevelopmentTree = true;
+ DevelopmentTreeLayoutIsCMakeStyle = true;
+ } else {
+ IsInDevelopmentTree = false;
+ }
+
+ // Compute various directory locations based on the derived location
+ // information.
+ std::string ActivePrefix, ActiveBinDir, ActiveIncludeDir, ActiveLibDir;
+ std::string ActiveIncludeOption;
+ if (IsInDevelopmentTree) {
+ ActivePrefix = CurrentExecPrefix;
+
+ // CMake organizes the products differently than a normal prefix style
+ // layout.
+ if (DevelopmentTreeLayoutIsCMakeStyle) {
+ ActiveIncludeDir = std::string(LLVM_OBJ_ROOT) + "/include";
+ ActiveBinDir = std::string(LLVM_OBJ_ROOT) + "/bin/" + LLVM_BUILDMODE;
+ ActiveLibDir = std::string(LLVM_OBJ_ROOT) + "/lib/" + LLVM_BUILDMODE;
+ } else {
+ ActiveIncludeDir = std::string(LLVM_OBJ_ROOT) + "/include";
+ ActiveBinDir = std::string(LLVM_OBJ_ROOT) + "/" + LLVM_BUILDMODE + "/bin";
+ ActiveLibDir = std::string(LLVM_OBJ_ROOT) + "/" + LLVM_BUILDMODE + "/lib";
+ }
+
+ // We need to include files from both the source and object trees.
+ ActiveIncludeOption = ("-I" + ActiveIncludeDir + " " +
+ "-I" + LLVM_OBJ_ROOT + "/include");
+ } else {
+ ActivePrefix = CurrentExecPrefix;
+ ActiveIncludeDir = ActivePrefix + "/include";
+ ActiveBinDir = ActivePrefix + "/bin";
+ ActiveLibDir = ActivePrefix + "/lib";
+ ActiveIncludeOption = "-I" + ActiveIncludeDir;
+ }
+
+ raw_ostream &OS = outs();
+ for (int i = 1; i != argc; ++i) {
+ StringRef Arg = argv[i];
+
+ if (Arg.startswith("-")) {
+ HasAnyOption = true;
+ if (Arg == "--version") {
+ OS << PACKAGE_VERSION << '\n';
+ } else if (Arg == "--prefix") {
+ OS << ActivePrefix << '\n';
+ } else if (Arg == "--bindir") {
+ OS << ActiveBinDir << '\n';
+ } else if (Arg == "--includedir") {
+ OS << ActiveIncludeDir << '\n';
+ } else if (Arg == "--libdir") {
+ OS << ActiveLibDir << '\n';
+ } else if (Arg == "--cppflags") {
+ OS << ActiveIncludeOption << ' ' << LLVM_CPPFLAGS << '\n';
+ } else if (Arg == "--cflags") {
+ OS << ActiveIncludeOption << ' ' << LLVM_CFLAGS << '\n';
+ } else if (Arg == "--cxxflags") {
+ OS << ActiveIncludeOption << ' ' << LLVM_CXXFLAGS << '\n';
+ } else if (Arg == "--ldflags") {
+ OS << "-L" << ActiveLibDir << ' ' << LLVM_LDFLAGS
+ << ' ' << LLVM_SYSTEM_LIBS << '\n';
+ } else if (Arg == "--libs") {
+ PrintLibs = true;
+ } else if (Arg == "--libnames") {
+ PrintLibNames = true;
+ } else if (Arg == "--libfiles") {
+ PrintLibFiles = true;
+ } else if (Arg == "--components") {
+ for (unsigned j = 0; j != NumAvailableComponents; ++j) {
+ if (j)
+ OS << ' ';
+ OS << AvailableComponents[j].Name;
+ }
+ OS << '\n';
+ } else if (Arg == "--targets-built") {
+ bool First = true;
+ for (TargetRegistry::iterator I = TargetRegistry::begin(),
+ E = TargetRegistry::end(); I != E; First = false, ++I) {
+ if (!First)
+ OS << ' ';
+ OS << I->getName();
+ }
+ OS << '\n';
+ } else if (Arg == "--host-target") {
+ OS << LLVM_DEFAULT_TARGET_TRIPLE << '\n';
+ } else if (Arg == "--build-mode") {
+ OS << LLVM_BUILDMODE << '\n';
+ } else if (Arg == "--obj-root") {
+ OS << LLVM_OBJ_ROOT << '\n';
+ } else if (Arg == "--src-root") {
+ OS << LLVM_SRC_ROOT << '\n';
+ } else {
+ usage();
+ }
+ } else {
+ Components.push_back(Arg);
+ }
+ }
+
+ if (!HasAnyOption)
+ usage();
+
+ if (PrintLibs || PrintLibNames || PrintLibFiles) {
+ // Construct the list of all the required libraries.
+ std::vector<StringRef> RequiredLibs;
+ ComputeLibsForComponents(Components, RequiredLibs);
+
+ for (unsigned i = 0, e = RequiredLibs.size(); i != e; ++i) {
+ StringRef Lib = RequiredLibs[i];
+ if (i)
+ OS << ' ';
+
+ if (PrintLibs) {
+ OS << Lib;
+ } else if (PrintLibFiles) {
+ OS << ActiveLibDir << Lib;
+ } else if (PrintLibNames) {
+ // If this is a typical library name, include it using -l.
+ if (Lib.startswith("lib") && Lib.endswith(".a")) {
+ OS << "-l" << Lib.slice(3, Lib.size()-2);
+ continue;
+ }
+
+ // Otherwise, print the full path.
+ OS << ActiveLibDir << Lib;
+ }
+ }
+ } else if (!Components.empty()) {
+ errs() << "llvm-config: error: components given, but unused\n\n";
+ usage();
+ }
+
+ return 0;
+}