summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: f963cd3)
raw | patch | inline | side by side (parent: f963cd3)
author | Eric Christopher <echristo@apple.com> | |
Thu, 15 Mar 2012 08:19:33 +0000 (08:19 +0000) | ||
committer | Eric Christopher <echristo@apple.com> | |
Thu, 15 Mar 2012 08:19:33 +0000 (08:19 +0000) |
out the DW_AT_name. Older gdbs unfortunately still use it to
disambiguate member functions in templated classes (gdb.cp/templates.exp).
rdar://11043421 (which is now deferred for a bit)
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@152782 91177308-0d34-0410-b5e6-96231b3b80d8
disambiguate member functions in templated classes (gdb.cp/templates.exp).
rdar://11043421 (which is now deferred for a bit)
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@152782 91177308-0d34-0410-b5e6-96231b3b80d8
diff --git a/lib/CodeGen/AsmPrinter/DwarfCompileUnit.cpp b/lib/CodeGen/AsmPrinter/DwarfCompileUnit.cpp
index 63194948f4d7ec12a83c43c19054f087231be2d3..389ae46b646eb3e3a4922de39e32a7a96b5c6e94 100644 (file)
// Add function template parameters.
addTemplateParams(*SPDie, SP.getTemplateParams());
+ // Unfortunately this code needs to stay here to work around
+ // a bug in older gdbs that requires the linkage name to resolve
+ // multiple template functions.
+ StringRef LinkageName = SP.getLinkageName();
+ if (!LinkageName.empty())
+ addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
+ getRealLinkageName(LinkageName));
+
// If this DIE is going to refer declaration info using AT_specification
// then there is no need to add other attributes.
if (DeclDie) {
return SPDie;
}
- StringRef LinkageName = SP.getLinkageName();
- if (!LinkageName.empty())
- addString(SPDie, dwarf::DW_AT_MIPS_linkage_name,
- getRealLinkageName(LinkageName));
-
// Constructors and operators for anonymous aggregates do not have names.
if (!SP.getName().empty())
addString(SPDie, dwarf::DW_AT_name, SP.getName());
index c4951da127cf0752d080032279979d639c6ece83..e4c5c807bfdbc22a597cec53585d60abb6905b00 100644 (file)
; test that the DW_AT_specification is a back edge in the file.
; CHECK: 0x00000038: DW_TAG_subprogram [5] *
-; CHECK: 0x0000005a: DW_AT_specification [DW_FORM_ref4] (cu + 0x0038 => {0x00000038})
+; CHECK: 0x0000005e: DW_AT_specification [DW_FORM_ref4] (cu + 0x0038 => {0x00000038})
@_ZZN3foo3barEvE1x = constant i32 0, align 4
diff --git a/test/DebugInfo/X86/concrete_out_of_line.ll b/test/DebugInfo/X86/concrete_out_of_line.ll
index 8e486651fc6a0b5401bde8c1bc16512746e5158c..055a9bf034f60918da57fbacc3d020f32e9c8c11 100644 (file)
; first check that we have a TAG_subprogram at a given offset and it has
; AT_inline.
-; CHECK: 0x0000012c: DW_TAG_subprogram [18]
+; CHECK: 0x00000130: DW_TAG_subprogram [18]
+; CHECK-NEXT: DW_AT_MIPS_linkage_name
; CHECK-NEXT: DW_AT_specification
; CHECK-NEXT: DW_AT_inline
; and then that a TAG_subprogram refers to it with AT_abstract_origin.
-; CHECK: 0x00000170: DW_TAG_subprogram [20]
-; CHECK-NEXT: DW_AT_abstract_origin [DW_FORM_ref4] (cu + 0x012c => {0x0000012c})
+; CHECK: 0x00000180: DW_TAG_subprogram [20]
+; CHECK-NEXT: DW_AT_abstract_origin [DW_FORM_ref4] (cu + 0x0130 => {0x00000130})
define i32 @_ZN17nsAutoRefCnt7ReleaseEv() {
entry:
index cdffca84ec596d766dfd99097ce3db8181bf8185..84884348e2aa73a04418e6dee0ad8e2fcfd08fb5 100644 (file)
; test that the DW_AT_specification is a back edge in the file.
; CHECK: 0x0000005a: DW_TAG_subprogram [5]
-; CHECK: 0x00000076: DW_AT_specification [DW_FORM_ref4] (cu + 0x005a => {0x0000005a})
+; CHECK: 0x0000007a: DW_AT_specification [DW_FORM_ref4] (cu + 0x005a => {0x0000005a})
%struct.foo = type { i8 }
diff --git a/test/DebugInfo/linkage-name.ll b/test/DebugInfo/linkage-name.ll
+++ /dev/null
@@ -1,56 +0,0 @@
-; RUN: llc -mtriple=x86_64-macosx %s -o %t -filetype=obj
-; RUN: llvm-dwarfdump %t | FileCheck %s
-
-; CHECK: DW_TAG_subprogram [9] *
-; CHECK-NOT: DW_AT_MIPS_linkage_name
-; CHECK: DW_AT_specification
-
-%class.A = type { i8 }
-
-@a = global %class.A zeroinitializer, align 1
-
-define i32 @_ZN1A1aEi(%class.A* %this, i32 %b) nounwind uwtable ssp align 2 {
-entry:
- %this.addr = alloca %class.A*, align 8
- %b.addr = alloca i32, align 4
- store %class.A* %this, %class.A** %this.addr, align 8
- call void @llvm.dbg.declare(metadata !{%class.A** %this.addr}, metadata !21), !dbg !23
- store i32 %b, i32* %b.addr, align 4
- call void @llvm.dbg.declare(metadata !{i32* %b.addr}, metadata !24), !dbg !25
- %this1 = load %class.A** %this.addr
- %0 = load i32* %b.addr, align 4, !dbg !26
- ret i32 %0, !dbg !26
-}
-
-declare void @llvm.dbg.declare(metadata, metadata) nounwind readnone
-
-!llvm.dbg.cu = !{!0}
-
-!0 = metadata !{i32 786449, i32 0, i32 4, metadata !"foo.cpp", metadata !"/Users/echristo", metadata !"clang version 3.1 (trunk 152691) (llvm/trunk 152692)", i1 true, i1 false, metadata !"", i32 0, metadata !1, metadata !1, metadata !3, metadata !18} ; [ DW_TAG_compile_unit ]
-!1 = metadata !{metadata !2}
-!2 = metadata !{i32 0}
-!3 = metadata !{metadata !4}
-!4 = metadata !{metadata !5}
-!5 = metadata !{i32 786478, i32 0, null, metadata !"a", metadata !"a", metadata !"_ZN1A1aEi", metadata !6, i32 5, metadata !7, i1 false, i1 true, i32 0, i32 0, null, i32 256, i1 false, i32 (%class.A*, i32)* @_ZN1A1aEi, null, metadata !13, metadata !16} ; [ DW_TAG_subprogram ]
-!6 = metadata !{i32 786473, metadata !"foo.cpp", metadata !"/Users/echristo", null} ; [ DW_TAG_file_type ]
-!7 = metadata !{i32 786453, i32 0, metadata !"", i32 0, i32 0, i64 0, i64 0, i64 0, i32 0, null, metadata !8, i32 0, i32 0} ; [ DW_TAG_subroutine_type ]
-!8 = metadata !{metadata !9, metadata !10, metadata !9}
-!9 = metadata !{i32 786468, null, metadata !"int", null, i32 0, i64 32, i64 32, i64 0, i32 0, i32 5} ; [ DW_TAG_base_type ]
-!10 = metadata !{i32 786447, i32 0, metadata !"", i32 0, i32 0, i64 64, i64 64, i64 0, i32 64, metadata !11} ; [ DW_TAG_pointer_type ]
-!11 = metadata !{i32 786434, null, metadata !"A", metadata !6, i32 1, i64 8, i64 8, i32 0, i32 0, null, metadata !12, i32 0, null, null} ; [ DW_TAG_class_type ]
-!12 = metadata !{metadata !13}
-!13 = metadata !{i32 786478, i32 0, metadata !11, metadata !"a", metadata !"a", metadata !"_ZN1A1aEi", metadata !6, i32 2, metadata !7, i1 false, i1 false, i32 0, i32 0, null, i32 257, i1 false, null, null, i32 0, metadata !14} ; [ DW_TAG_subprogram ]
-!14 = metadata !{metadata !15}
-!15 = metadata !{i32 786468} ; [ DW_TAG_base_type ]
-!16 = metadata !{metadata !17}
-!17 = metadata !{i32 786468} ; [ DW_TAG_base_type ]
-!18 = metadata !{metadata !19}
-!19 = metadata !{metadata !20}
-!20 = metadata !{i32 786484, i32 0, null, metadata !"a", metadata !"a", metadata !"", metadata !6, i32 9, metadata !11, i32 0, i32 1, %class.A* @a} ; [ DW_TAG_variable ]
-!21 = metadata !{i32 786689, metadata !5, metadata !"this", metadata !6, i32 16777221, metadata !22, i32 64, i32 0} ; [ DW_TAG_arg_variable ]
-!22 = metadata !{i32 786447, null, metadata !"", null, i32 0, i64 64, i64 64, i64 0, i32 0, metadata !11} ; [ DW_TAG_pointer_type ]
-!23 = metadata !{i32 5, i32 8, metadata !5, null}
-!24 = metadata !{i32 786689, metadata !5, metadata !"b", metadata !6, i32 33554437, metadata !9, i32 0, i32 0} ; [ DW_TAG_arg_variable ]
-!25 = metadata !{i32 5, i32 14, metadata !5, null}
-!26 = metadata !{i32 6, i32 4, metadata !27, null}
-!27 = metadata !{i32 786443, metadata !5, i32 5, i32 17, metadata !6, i32 0} ; [ DW_TAG_lexical_block ]