summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: f9b5976)
raw | patch | inline | side by side (parent: f9b5976)
author | Manman Ren <manman.ren@gmail.com> | |
Mon, 28 Jul 2014 19:14:13 +0000 (19:14 +0000) | ||
committer | Manman Ren <manman.ren@gmail.com> | |
Mon, 28 Jul 2014 19:14:13 +0000 (19:14 +0000) |
This is the second of a series of patches to handle type uniqueing of the
type array for a subroutine type.
For vector and array types, getElements returns the array of subranges, so it
is a better name than getTypeArray. Even for class, struct and enum types,
getElements returns the members, which can be subprograms.
setArrays can set up to two arrays, the second is the templates.
This commit should have no functionality change.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214112 91177308-0d34-0410-b5e6-96231b3b80d8
type array for a subroutine type.
For vector and array types, getElements returns the array of subranges, so it
is a better name than getTypeArray. Even for class, struct and enum types,
getElements returns the members, which can be subprograms.
setArrays can set up to two arrays, the second is the templates.
This commit should have no functionality change.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214112 91177308-0d34-0410-b5e6-96231b3b80d8
index 19108ae625047d4db73c94b75cd14aebb6985721..1cc4b53ade52d3ce7e30b4c0cd5ef801919dc13c 100644 (file)
public:
explicit DICompositeType(const MDNode *N = nullptr) : DIDerivedType(N) {}
- DIArray getTypeArray() const { return getFieldAs<DIArray>(10); }
- void setTypeArray(DIArray Elements, DIArray TParams = DIArray());
+ DIArray getElements() const { return getFieldAs<DIArray>(10); }
+ void setArrays(DIArray Elements, DIArray TParams = DIArray());
unsigned getRunTimeLang() const { return getUnsignedField(11); }
DITypeRef getContainingType() const { return getFieldAs<DITypeRef>(12); }
void setContainingType(DICompositeType ContainingType);
index b45d5917615eb60ddebcda023b8e653f53218e2e..89e9547bdb7706a35c791f3f3f1eebc00317f53d 100644 (file)
if (tag == dwarf::DW_TAG_pointer_type)
subType = resolve(DIDerivedType(Ty).getTypeDerivedFrom());
- DIArray Elements = DICompositeType(subType).getTypeArray();
+ DIArray Elements = DICompositeType(subType).getElements();
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
DIDerivedType DT(Elements.getElement(i));
if (getName() == DT.getName())
// If this is a variadic function, add an unspecified parameter.
DISubprogram SP(Scope->getScopeNode());
- DIArray FnArgs = SP.getType().getTypeArray();
+ DIArray FnArgs = SP.getType().getElements();
if (FnArgs.getElement(FnArgs.getNumElements() - 1)
.isUnspecifiedParameter()) {
Children.push_back(
index 9538bee7bca8fd7a4b6eb858aa2c170ca9fc0517..e20a3fbfc32771124c979da9299851f87d666070 100644 (file)
// Find the __forwarding field and the variable field in the __Block_byref
// struct.
- DIArray Fields = blockStruct.getTypeArray();
+ DIArray Fields = blockStruct.getElements();
DIDerivedType varField;
DIDerivedType forwardingField;
break;
case dwarf::DW_TAG_subroutine_type: {
// Add return type. A void return won't have a type.
- DIArray Elements = CTy.getTypeArray();
+ DIArray Elements = CTy.getElements();
DIType RTy(Elements.getElement(0));
if (RTy)
addType(Buffer, RTy);
case dwarf::DW_TAG_union_type:
case dwarf::DW_TAG_class_type: {
// Add elements to structure type.
- DIArray Elements = CTy.getTypeArray();
+ DIArray Elements = CTy.getElements();
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
DIDescriptor Element = Elements.getElement(i);
if (Element.isSubprogram())
assert(SPTy.getTag() == dwarf::DW_TAG_subroutine_type &&
"the type of a subprogram should be a subroutine");
- DIArray Args = SPTy.getTypeArray();
+ DIArray Args = SPTy.getElements();
// Add a return type. If this is a type like a C/C++ void type we don't add a
// return type.
if (Args.getElement(0))
}
// Add subranges to array type.
- DIArray Elements = CTy.getTypeArray();
+ DIArray Elements = CTy.getElements();
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
DIDescriptor Element = Elements.getElement(i);
if (Element.getTag() == dwarf::DW_TAG_subrange_type)
/// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
- DIArray Elements = CTy.getTypeArray();
+ DIArray Elements = CTy.getElements();
// Add enumerators to enumeration type.
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
diff --git a/lib/IR/DebugInfo.cpp b/lib/IR/DebugInfo.cpp
index 8e05435cb3319b17037ce6713290d489dc16fde3..6c06bf18de6c740b9cfaaad26b0841ed1ca7c976 100644 (file)
--- a/lib/IR/DebugInfo.cpp
+++ b/lib/IR/DebugInfo.cpp
#endif
/// \brief Set the array of member DITypes.
-void DICompositeType::setTypeArray(DIArray Elements, DIArray TParams) {
+void DICompositeType::setArrays(DIArray Elements, DIArray TParams) {
assert((!TParams || DbgNode->getNumOperands() == 15) &&
"If you're setting the template parameters this should include a slot "
"for that!");
if (DT.isCompositeType()) {
DICompositeType DCT(DT);
processType(DCT.getTypeDerivedFrom().resolve(TypeIdentifierMap));
- DIArray DA = DCT.getTypeArray();
+ DIArray DA = DCT.getElements();
for (unsigned i = 0, e = DA.getNumElements(); i != e; ++i) {
DIDescriptor D = DA.getElement(i);
if (D.isType())
void DICompositeType::printInternal(raw_ostream &OS) const {
DIType::printInternal(OS);
- DIArray A = getTypeArray();
+ DIArray A = getElements();
OS << " [" << A.getNumElements() << " elements]";
}
diff --git a/lib/Transforms/Instrumentation/DebugIR.cpp b/lib/Transforms/Instrumentation/DebugIR.cpp
index f2f1738808be89e5174c4fc2e092b937d51b9241..2c78c9e0bba53f28e764f33d2ed7a5f1d08a1ce2 100644 (file)
Elements.push_back(getOrCreateType(T->getStructElementType(i)));
// set struct elements
- StructDescriptor.setTypeArray(Builder.getOrCreateArray(Elements));
+ StructDescriptor.setArrays(Builder.getOrCreateArray(Elements));
} else if (T->isPointerTy()) {
Type *PointeeTy = T->getPointerElementType();
if (!(N = getType(PointeeTy)))