summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: efbd8e5)
raw | patch | inline | side by side (parent: efbd8e5)
author | Quentin Colombet <qcolombet@apple.com> | |
Tue, 11 Feb 2014 01:59:02 +0000 (01:59 +0000) | ||
committer | Quentin Colombet <qcolombet@apple.com> | |
Tue, 11 Feb 2014 01:59:02 +0000 (01:59 +0000) |
The addressing mode matcher checks at some point the profitability of folding an
instruction into the addressing mode. When the instruction to be folded has
several uses, it checks that the instruction can be folded in each use.
To do so, it creates a new matcher for each use and check if the instruction is
in the list of the matched instructions of this new matcher.
The new matchers may promote some instructions and this has to be undone to keep
the state of the original matcher consistent.
A test case will follow.
<rdar://problem/16020230>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@201121 91177308-0d34-0410-b5e6-96231b3b80d8
instruction into the addressing mode. When the instruction to be folded has
several uses, it checks that the instruction can be folded in each use.
To do so, it creates a new matcher for each use and check if the instruction is
in the list of the matched instructions of this new matcher.
The new matchers may promote some instructions and this has to be undone to keep
the state of the original matcher consistent.
A test case will follow.
<rdar://problem/16020230>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@201121 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Scalar/CodeGenPrepare.cpp | patch | blob | history |
index 6fce0f320bfd3bbb22f17076bb26286bba3dfac8..0efeba4af1cb55094f63d72d82cd082a2ce64468 100644 (file)
// will tell us if the addressing mode for the memory operation will
// *actually* cover the shared instruction.
ExtAddrMode Result;
+ TypePromotionTransaction::ConstRestorationPt LastKnownGood =
+ TPT.getRestorationPoint();
AddressingModeMatcher Matcher(MatchedAddrModeInsts, TLI, AddressAccessTy,
MemoryInst, Result, InsertedTruncs,
PromotedInsts, TPT);
bool Success = Matcher.MatchAddr(Address, 0);
(void)Success; assert(Success && "Couldn't select *anything*?");
+ // The match was to check the profitability, the changes made are not
+ // part of the original matcher. Therefore, they should be dropped
+ // otherwise the original matcher will not present the right state.
+ TPT.rollback(LastKnownGood);
+
// If the match didn't cover I, then it won't be shared by it.
if (std::find(MatchedAddrModeInsts.begin(), MatchedAddrModeInsts.end(),
I) == MatchedAddrModeInsts.end())