summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 279b550)
raw | patch | inline | side by side (parent: 279b550)
author | Hal Finkel <hfinkel@anl.gov> | |
Wed, 15 Oct 2014 17:34:48 +0000 (17:34 +0000) | ||
committer | Hal Finkel <hfinkel@anl.gov> | |
Wed, 15 Oct 2014 17:34:48 +0000 (17:34 +0000) |
We need to make sure that we visit all operands of an instruction before moving
deeper in the operand graph. We had been pushing operands onto the back of the work
set, and popping them off the back as well, meaning that we might visit an
instruction before visiting all of its uses that sit in between it and the call
to @llvm.assume.
To provide an explicit example, given the following:
%q0 = extractelement <4 x float> %rd, i32 0
%q1 = extractelement <4 x float> %rd, i32 1
%q2 = extractelement <4 x float> %rd, i32 2
%q3 = extractelement <4 x float> %rd, i32 3
%q4 = fadd float %q0, %q1
%q5 = fadd float %q2, %q3
%q6 = fadd float %q4, %q5
%qi = fcmp olt float %q6, %q5
call void @llvm.assume(i1 %qi)
%q5 is used by both %qi and %q6. When we visit %qi, it will be marked as
ephemeral, and we'll queue %q6 and %q5. %q6 will be marked as ephemeral and
we'll queue %q4 and %q5. Under the old system, we'd then visit %q4, which
would become ephemeral, %q1 and then %q0, which would become ephemeral as
well, and now we have a problem. We'd visit %rd, but it would not be marked as
ephemeral because we've not yet visited %q2 and %q3 (because we've not yet
visited %q5).
This will be covered by a test case in a follow-up commit that enables
ephemeral-value awareness in the SLP vectorizer.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@219815 91177308-0d34-0410-b5e6-96231b3b80d8
deeper in the operand graph. We had been pushing operands onto the back of the work
set, and popping them off the back as well, meaning that we might visit an
instruction before visiting all of its uses that sit in between it and the call
to @llvm.assume.
To provide an explicit example, given the following:
%q0 = extractelement <4 x float> %rd, i32 0
%q1 = extractelement <4 x float> %rd, i32 1
%q2 = extractelement <4 x float> %rd, i32 2
%q3 = extractelement <4 x float> %rd, i32 3
%q4 = fadd float %q0, %q1
%q5 = fadd float %q2, %q3
%q6 = fadd float %q4, %q5
%qi = fcmp olt float %q6, %q5
call void @llvm.assume(i1 %qi)
%q5 is used by both %qi and %q6. When we visit %qi, it will be marked as
ephemeral, and we'll queue %q6 and %q5. %q6 will be marked as ephemeral and
we'll queue %q4 and %q5. Under the old system, we'd then visit %q4, which
would become ephemeral, %q1 and then %q0, which would become ephemeral as
well, and now we have a problem. We'd visit %rd, but it would not be marked as
ephemeral because we've not yet visited %q2 and %q3 (because we've not yet
visited %q5).
This will be covered by a test case in a follow-up commit that enables
ephemeral-value awareness in the SLP vectorizer.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@219815 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Analysis/CodeMetrics.cpp | patch | blob | history |
index 97d04636fc59013253a6902534530f7b2566b031..f3b34bfe089b64d942d74cc14ebc741d1c02d25e 100644 (file)
// alive only by ephemeral values.
while (!WorkSet.empty()) {
- const Value *V = WorkSet.pop_back_val();
+ const Value *V = WorkSet.front();
+ WorkSet.erase(WorkSet.begin());
+
if (!Visited.insert(V))
continue;