summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1552e50)
raw | patch | inline | side by side (parent: 1552e50)
author | Chandler Carruth <chandlerc@gmail.com> | |
Thu, 22 Jan 2015 21:53:09 +0000 (21:53 +0000) | ||
committer | Chandler Carruth <chandlerc@gmail.com> | |
Thu, 22 Jan 2015 21:53:09 +0000 (21:53 +0000) |
I had already factored this analysis specifically to enable doing this,
but hadn't actually committed the necessary wiring to get at this from
the new pass manager. This also nicely shows how the separate cache
object can be directly managed by the new pass manager.
This analysis didn't have any direct tests and so I've added a printer
pass and a boring test case. I chose to print the i1 value which is
being assumed rather than the call to llvm.assume as that seems much
more useful for testing... but suggestions on an even better printing
strategy welcome. My main goal was to make sure things actually work. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226868 91177308-0d34-0410-b5e6-96231b3b80d8
but hadn't actually committed the necessary wiring to get at this from
the new pass manager. This also nicely shows how the separate cache
object can be directly managed by the new pass manager.
This analysis didn't have any direct tests and so I've added a printer
pass and a boring test case. I chose to print the i1 value which is
being assumed rather than the call to llvm.assume as that seems much
more useful for testing... but suggestions on an even better printing
strategy welcome. My main goal was to make sure things actually work. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226868 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Analysis/AssumptionCache.h | patch | blob | history | |
lib/Analysis/AssumptionCache.cpp | patch | blob | history | |
test/Analysis/AssumptionCache/basic.ll | [new file with mode: 0644] | patch | blob |
tools/opt/PassRegistry.def | patch | blob | history | |
tools/opt/Passes.cpp | patch | blob | history |
index b129e67963283acb784797aa7b50040c51ebe8f6..fc1393fc47a2b1efdc1a063591d27c5203a13460 100644 (file)
namespace llvm {
+// FIXME: Replace this brittle forward declaration with the include of the new
+// PassManager.h when doing so doesn't break the PassManagerBuilder.
+template <typename IRUnitT> class AnalysisManager;
+class PreservedAnalyses;
+
/// \brief A cache of @llvm.assume calls within a function.
///
/// This cache provides fast lookup of assumptions within a function by caching
}
};
+/// \brief A function analysis which provides an \c AssumptionCache.
+///
+/// This analysis is intended for use with the new pass manager and will vend
+/// assumption caches for a given function.
+class AssumptionAnalysis {
+ static char PassID;
+
+public:
+ typedef AssumptionCache Result;
+
+ /// \brief Opaque, unique identifier for this analysis pass.
+ static void *ID() { return (void *)&PassID; }
+
+ /// \brief Provide a name for the analysis for debugging and logging.
+ static StringRef name() { return "AssumptionAnalysis"; }
+
+ AssumptionAnalysis() {}
+ AssumptionAnalysis(const AssumptionAnalysis &Arg) {}
+ AssumptionAnalysis(AssumptionAnalysis &&Arg) {}
+ AssumptionAnalysis &operator=(const AssumptionAnalysis &RHS) { return *this; }
+ AssumptionAnalysis &operator=(AssumptionAnalysis &&RHS) { return *this; }
+
+ AssumptionCache run(Function &F) { return AssumptionCache(F); }
+};
+
+/// \brief Printer pass for the \c AssumptionAnalysis results.
+class AssumptionPrinterPass {
+ raw_ostream &OS;
+
+public:
+ explicit AssumptionPrinterPass(raw_ostream &OS) : OS(OS) {}
+ PreservedAnalyses run(Function &F, AnalysisManager<Function> *AM);
+
+ static StringRef name() { return "AssumptionPrinterPass"; }
+};
+
/// \brief An immutable pass that tracks lazily created \c AssumptionCache
/// objects.
///
index da5ba18fc43bb5ba87612a0282f05877cc55b326..f468a43ef0b8c7b765cf2af9b8f10de5b65e2c95 100644 (file)
#include "llvm/IR/Function.h"
#include "llvm/IR/Instructions.h"
#include "llvm/IR/IntrinsicInst.h"
+#include "llvm/IR/PassManager.h"
#include "llvm/IR/PatternMatch.h"
#include "llvm/Support/Debug.h"
using namespace llvm;
#endif
}
+char AssumptionAnalysis::PassID;
+
+PreservedAnalyses AssumptionPrinterPass::run(Function &F,
+ AnalysisManager<Function> *AM) {
+ AssumptionCache &AC = AM->getResult<AssumptionAnalysis>(F);
+
+ OS << "Cached assumptions for function: " << F.getName() << "\n";
+ for (auto &VH : AC.assumptions())
+ if (VH)
+ OS << " " << *cast<CallInst>(VH)->getArgOperand(0) << "\n";
+
+ return PreservedAnalyses::all();
+}
+
void AssumptionCacheTracker::FunctionCallbackVH::deleted() {
auto I = ACT->AssumptionCaches.find_as(cast<Function>(getValPtr()));
if (I != ACT->AssumptionCaches.end())
diff --git a/test/Analysis/AssumptionCache/basic.ll b/test/Analysis/AssumptionCache/basic.ll
--- /dev/null
@@ -0,0 +1,22 @@
+; RUN: opt < %s -disable-output -passes='print<assumptions>' 2>&1 | FileCheck %s
+
+target datalayout = "e-i64:64-f80:128-n8:16:32:64-S128"
+
+declare void @llvm.assume(i1)
+
+define void @test1(i32 %a) {
+; CHECK-LABEL: Cached assumptions for function: test1
+; CHECK-NEXT: icmp ne i32 %{{.*}}, 0
+; CHECK-NEXT: icmp slt i32 %{{.*}}, 0
+; CHECK-NEXT: icmp sgt i32 %{{.*}}, 0
+
+entry:
+ %cond1 = icmp ne i32 %a, 0
+ call void @llvm.assume(i1 %cond1)
+ %cond2 = icmp slt i32 %a, 0
+ call void @llvm.assume(i1 %cond2)
+ %cond3 = icmp sgt i32 %a, 0
+ call void @llvm.assume(i1 %cond3)
+
+ ret void
+}
index 66ee5e56272096b57a671e712385b7409af120a8..b3296aa5ec00f438de43c679270ed2d85c3cdbf7 100644 (file)
#ifndef FUNCTION_ANALYSIS
#define FUNCTION_ANALYSIS(NAME, CREATE_PASS)
#endif
+FUNCTION_ANALYSIS("assumptions", AssumptionAnalysis())
FUNCTION_ANALYSIS("domtree", DominatorTreeAnalysis())
FUNCTION_ANALYSIS("loops", LoopAnalysis())
FUNCTION_ANALYSIS("no-op-function", NoOpFunctionAnalysis())
FUNCTION_PASS("invalidate<all>", InvalidateAllAnalysesPass())
FUNCTION_PASS("no-op-function", NoOpFunctionPass())
FUNCTION_PASS("print", PrintFunctionPass(dbgs()))
+FUNCTION_PASS("print<assumptions>", AssumptionPrinterPass(dbgs()))
FUNCTION_PASS("print<domtree>", DominatorTreePrinterPass(dbgs()))
FUNCTION_PASS("print<loops>", LoopPrinterPass(dbgs()))
FUNCTION_PASS("verify", VerifierPass())
diff --git a/tools/opt/Passes.cpp b/tools/opt/Passes.cpp
index ee51543055474411d514810b0b766cf9bb582f95..5488059905e51282ab2823e3ed6d0b492e390251 100644 (file)
--- a/tools/opt/Passes.cpp
+++ b/tools/opt/Passes.cpp
//===----------------------------------------------------------------------===//
#include "Passes.h"
+#include "llvm/Analysis/AssumptionCache.h"
#include "llvm/Analysis/CGSCCPassManager.h"
#include "llvm/Analysis/LazyCallGraph.h"
#include "llvm/Analysis/LoopInfo.h"