summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c664d76)
raw | patch | inline | side by side (parent: c664d76)
author | Andrew Kaylor <andrew.kaylor@intel.com> | |
Sat, 5 Oct 2013 01:52:09 +0000 (01:52 +0000) | ||
committer | Andrew Kaylor <andrew.kaylor@intel.com> | |
Sat, 5 Oct 2013 01:52:09 +0000 (01:52 +0000) |
Patch by Ashok Thirumurthi
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@192020 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@192020 91177308-0d34-0410-b5e6-96231b3b80d8
lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.cpp | patch | blob | history | |
lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.h | patch | blob | history |
diff --git a/lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.cpp b/lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.cpp
index eb2a1a771d7490a4d8411810534e0d4c7fdb033e..a438dcd87991159f11341374cd2adf833b273521 100644 (file)
}
void RuntimeDyldELF::updateGOTEntries(StringRef Name, uint64_t Addr) {
- for (int i = 0, e = GOTEntries.size(); i != e; ++i) {
- if (GOTEntries[i].SymbolName != 0 && GOTEntries[i].SymbolName == Name) {
- GOTEntries[i].Offset = Addr;
+
+ SmallVectorImpl<std::pair<SID, GOTRelocations> >::iterator it;
+ SmallVectorImpl<std::pair<SID, GOTRelocations> >::iterator end = GOTs.end();
+
+ for (it = GOTs.begin(); it != end; ++it) {
+ GOTRelocations &GOTEntries = it->second;
+ for (int i = 0, e = GOTEntries.size(); i != e; ++i) {
+ if (GOTEntries[i].SymbolName != 0 && GOTEntries[i].SymbolName == Name) {
+ GOTEntries[i].Offset = Addr;
+ }
}
}
}
uint64_t RuntimeDyldELF::findGOTEntry(uint64_t LoadAddress,
uint64_t Offset) {
- assert(GOTSectionID != 0
- && "Attempting to lookup GOT entry but the GOT was never allocated.");
- if (GOTSectionID == 0) {
- return 0;
- }
- size_t GOTEntrySize = getGOTEntrySize();
+ const size_t GOTEntrySize = getGOTEntrySize();
+
+ SmallVectorImpl<std::pair<SID, GOTRelocations> >::const_iterator it;
+ SmallVectorImpl<std::pair<SID, GOTRelocations> >::const_iterator end = GOTs.end();
- // Find the matching entry in our vector.
int GOTIndex = -1;
- uint64_t SymbolOffset = 0;
- for (int i = 0, e = GOTEntries.size(); i != e; ++i) {
- if (GOTEntries[i].SymbolName == 0) {
- if (getSectionLoadAddress(GOTEntries[i].SectionID) == LoadAddress &&
- GOTEntries[i].Offset == Offset) {
- GOTIndex = i;
- SymbolOffset = GOTEntries[i].Offset;
- break;
- }
- } else {
- // GOT entries for external symbols use the addend as the address when
- // the external symbol has been resolved.
- if (GOTEntries[i].Offset == LoadAddress) {
- GOTIndex = i;
- // Don't use the Addend here. The relocation handler will use it.
- break;
+ for (it = GOTs.begin(); it != end; ++it) {
+ SID GOTSectionID = it->first;
+ const GOTRelocations &GOTEntries = it->second;
+
+ // Find the matching entry in our vector.
+ uint64_t SymbolOffset = 0;
+ for (int i = 0, e = GOTEntries.size(); i != e; ++i) {
+ if (GOTEntries[i].SymbolName == 0) {
+ if (getSectionLoadAddress(GOTEntries[i].SectionID) == LoadAddress &&
+ GOTEntries[i].Offset == Offset) {
+ GOTIndex = i;
+ SymbolOffset = GOTEntries[i].Offset;
+ break;
+ }
+ } else {
+ // GOT entries for external symbols use the addend as the address when
+ // the external symbol has been resolved.
+ if (GOTEntries[i].Offset == LoadAddress) {
+ GOTIndex = i;
+ // Don't use the Addend here. The relocation handler will use it.
+ break;
+ }
}
}
- }
- assert(GOTIndex != -1 && "Unable to find requested GOT entry.");
- if (GOTIndex == -1)
- return 0;
- if (GOTEntrySize == sizeof(uint64_t)) {
- uint64_t *LocalGOTAddr = (uint64_t*)getSectionAddress(GOTSectionID);
- // Fill in this entry with the address of the symbol being referenced.
- LocalGOTAddr[GOTIndex] = LoadAddress + SymbolOffset;
- } else {
- uint32_t *LocalGOTAddr = (uint32_t*)getSectionAddress(GOTSectionID);
- // Fill in this entry with the address of the symbol being referenced.
- LocalGOTAddr[GOTIndex] = (uint32_t)(LoadAddress + SymbolOffset);
+ if (GOTIndex != -1) {
+ if (GOTEntrySize == sizeof(uint64_t)) {
+ uint64_t *LocalGOTAddr = (uint64_t*)getSectionAddress(GOTSectionID);
+ // Fill in this entry with the address of the symbol being referenced.
+ LocalGOTAddr[GOTIndex] = LoadAddress + SymbolOffset;
+ } else {
+ uint32_t *LocalGOTAddr = (uint32_t*)getSectionAddress(GOTSectionID);
+ // Fill in this entry with the address of the symbol being referenced.
+ LocalGOTAddr[GOTIndex] = (uint32_t)(LoadAddress + SymbolOffset);
+ }
+
+ // Calculate the load address of this entry
+ return getSectionLoadAddress(GOTSectionID) + (GOTIndex * GOTEntrySize);
+ }
}
- // Calculate the load address of this entry
- return getSectionLoadAddress(GOTSectionID) + (GOTIndex * GOTEntrySize);
+ assert(GOTIndex != -1 && "Unable to find requested GOT entry.");
+ return 0;
}
void RuntimeDyldELF::finalizeLoad() {
- // Allocate the GOT if necessary
- size_t numGOTEntries = GOTEntries.size();
- if (numGOTEntries != 0) {
- // Allocate memory for the section
- unsigned SectionID = Sections.size();
- size_t TotalSize = numGOTEntries * getGOTEntrySize();
- uint8_t *Addr = MemMgr->allocateDataSection(
- TotalSize, getGOTEntrySize(), SectionID, ".got", false);
- if (!Addr)
- report_fatal_error("Unable to allocate memory for GOT!");
- Sections.push_back(SectionEntry(".got", Addr, TotalSize, 0));
- // For now, initialize all GOT entries to zero. We'll fill them in as
- // needed when GOT-based relocations are applied.
- memset(Addr, 0, TotalSize);
- GOTSectionID = SectionID;
+ if (MemMgr) {
+ // Allocate the GOT if necessary
+ size_t numGOTEntries = GOTEntries.size();
+ if (numGOTEntries != 0) {
+ // Allocate memory for the section
+ unsigned SectionID = Sections.size();
+ size_t TotalSize = numGOTEntries * getGOTEntrySize();
+ uint8_t *Addr = MemMgr->allocateDataSection(TotalSize, getGOTEntrySize(),
+ SectionID, ".got", false);
+ if (!Addr)
+ report_fatal_error("Unable to allocate memory for GOT!");
+
+ GOTs.push_back(std::make_pair(SectionID, GOTEntries));
+ Sections.push_back(SectionEntry(".got", Addr, TotalSize, 0));
+ // For now, initialize all GOT entries to zero. We'll fill them in as
+ // needed when GOT-based relocations are applied.
+ memset(Addr, 0, TotalSize);
+ }
+ }
+ else {
+ report_fatal_error("Unable to allocate memory for GOT!");
}
}
diff --git a/lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.h b/lib/ExecutionEngine/RuntimeDyld/RuntimeDyldELF.h
index 14fb5740e5f3c061364a1adae9d5d1db9e83c748..67dc693b1b6840d2ef214dc9d29331804d47533f 100644 (file)
#define LLVM_RUNTIME_DYLD_ELF_H
#include "RuntimeDyldImpl.h"
+#include "llvm/ADT/DenseMap.h"
using namespace llvm;
virtual void updateGOTEntries(StringRef Name, uint64_t Addr);
- SmallVector<RelocationValueRef, 2> GOTEntries;
- unsigned GOTSectionID;
+ // Relocation entries for symbols whose position-independant offset is
+ // updated in a global offset table.
+ typedef unsigned SID; // Type for SectionIDs
+ typedef SmallVector<RelocationValueRef, 2> GOTRelocations;
+ GOTRelocations GOTEntries; // List of entries requiring finalization.
+ SmallVector<std::pair<SID, GOTRelocations>, 8> GOTs; // Allocated tables.
public:
- RuntimeDyldELF(RTDyldMemoryManager *mm) : RuntimeDyldImpl(mm),
- GOTSectionID(0)
+ RuntimeDyldELF(RTDyldMemoryManager *mm) : RuntimeDyldImpl(mm)
{}
virtual void resolveRelocation(const RelocationEntry &RE, uint64_t Value);