summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: 67d5257)
raw | patch | inline | side by side (from parent 1: 67d5257)
author | Chandler Carruth <chandlerc@gmail.com> | |
Wed, 21 Jan 2015 11:38:17 +0000 (11:38 +0000) | ||
committer | Chandler Carruth <chandlerc@gmail.com> | |
Wed, 21 Jan 2015 11:38:17 +0000 (11:38 +0000) |
Because in its primary function pass the combiner is run repeatedly over
the same function until doing so produces no changes, it is essentially
to not re-allocate the worklist. However, as a utility, the more common
pattern would be to put a limited set of instructions in the worklist
rather than the entire function body. That is also the more likely
pattern when used by the new pass manager.
The result is a very light weight combiner that does the visiting with
a separable worklist. This can then be wrapped up in a helper function
for users that want a combiner utility, or as I have here it can be
wrapped up in a pass which manages the iterations used when combining an
entire function's instructions.
Hopefully this removes some of the worst of the interface warts that
became apparant with the last patch here. However, there is clearly more
work. I've again left some FIXMEs for the most egregious. The ones that
stick out to me are the exposure of the worklist and IR builder as
public members, and the use of pointers rather than references. However,
fixing these is likely to be much more mechanical and less interesting
so I didn't want to touch them in this patch.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226655 91177308-0d34-0410-b5e6-96231b3b80d8
the same function until doing so produces no changes, it is essentially
to not re-allocate the worklist. However, as a utility, the more common
pattern would be to put a limited set of instructions in the worklist
rather than the entire function body. That is also the more likely
pattern when used by the new pass manager.
The result is a very light weight combiner that does the visiting with
a separable worklist. This can then be wrapped up in a helper function
for users that want a combiner utility, or as I have here it can be
wrapped up in a pass which manages the iterations used when combining an
entire function's instructions.
Hopefully this removes some of the worst of the interface warts that
became apparant with the last patch here. However, there is clearly more
work. I've again left some FIXMEs for the most egregious. The ones that
stick out to me are the exposure of the worklist and IR builder as
public members, and the use of pointers rather than references. However,
fixing these is likely to be much more mechanical and less interesting
so I didn't want to touch them in this patch.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226655 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/InstCombine/InstCombine.h | patch | blob | history | |
lib/Transforms/InstCombine/InstructionCombining.cpp | patch | blob | history |
index 5aaba2c17e2ed0b1f24c2e9cfdcd93d2d3080799..346dcaa705dc28fa92e59fde57b221a7d98c40f5 100644 (file)
/// of the LLVM pass pipeline.
class LLVM_LIBRARY_VISIBILITY InstCombiner
: public InstVisitor<InstCombiner, Instruction *> {
- AssumptionCache *AC;
- const DataLayout *DL;
- TargetLibraryInfo *TLI;
- DominatorTree *DT;
- LoopInfo *LI;
- bool MadeIRChange;
- bool MinimizeSize;
-
+ // FIXME: These members shouldn't be public.
public:
/// \brief A worklist of the instructions that need to be simplified.
- InstCombineWorklist Worklist;
+ InstCombineWorklist &Worklist;
/// \brief An IRBuilder that automatically inserts new instructions into the
/// worklist.
typedef IRBuilder<true, TargetFolder, InstCombineIRInserter> BuilderTy;
BuilderTy *Builder;
- InstCombiner() : DL(nullptr), DT(nullptr), LI(nullptr), Builder(nullptr) {
- MinimizeSize = false;
- }
+private:
+ // Mode in which we are running the combiner.
+ const bool MinimizeSize;
+
+ // Required analyses.
+ // FIXME: These can never be null and should be references.
+ AssumptionCache *AC;
+ TargetLibraryInfo *TLI;
+ DominatorTree *DT;
+
+ // Optional analyses. When non-null, these can both be used to do better
+ // combining and will be updated to reflect any changes.
+ const DataLayout *DL;
+ LoopInfo *LI;
+
+ bool MadeIRChange;
public:
- bool run(Function &F, AssumptionCache *AC, const DataLayout *DL,
- TargetLibraryInfo *TLI, DominatorTree *DT, LoopInfo *LI);
+ InstCombiner(InstCombineWorklist &Worklist, BuilderTy *Builder,
+ bool MinimizeSize, AssumptionCache *AC, TargetLibraryInfo *TLI,
+ DominatorTree *DT, const DataLayout *DL, LoopInfo *LI)
+ : Worklist(Worklist), Builder(Builder), MinimizeSize(MinimizeSize),
+ AC(AC), TLI(TLI), DT(DT), DL(DL), LI(LI), MadeIRChange(false) {}
- bool DoOneIteration(Function &F, unsigned ItNum);
+ /// \brief Run the combiner over the entire worklist until it is empty.
+ ///
+ /// \returns true if the IR is changed.
+ bool run();
AssumptionCache *getAssumptionCache() const { return AC; }
diff --git a/lib/Transforms/InstCombine/InstructionCombining.cpp b/lib/Transforms/InstCombine/InstructionCombining.cpp
index 9436f23345b6e7328d1849edc4a4df5590ea9964..1e7adfa9aca9b29f2a1ce91341007178bde0e184 100644 (file)
return nullptr;
}
-
-
-
/// TryToSinkInstruction - Try to move the specified instruction from its
/// current block into the beginning of DestBlock, which can only happen if it's
/// safe to move the instruction past all of the instructions between it and the
return true;
}
-
-/// AddReachableCodeToWorklist - Walk the function in depth-first order, adding
-/// all reachable code to the worklist.
-///
-/// This has a couple of tricks to make the code faster and more powerful. In
-/// particular, we constant fold and DCE instructions as we go, to avoid adding
-/// them to the worklist (this significantly speeds up instcombine on code where
-/// many instructions are dead or constant). Additionally, if we find a branch
-/// whose condition is a known constant, we only visit the reachable successors.
-///
-static bool AddReachableCodeToWorklist(BasicBlock *BB,
- SmallPtrSetImpl<BasicBlock*> &Visited,
- InstCombiner &IC,
- const DataLayout *DL,
- const TargetLibraryInfo *TLI) {
- bool MadeIRChange = false;
- SmallVector<BasicBlock*, 256> Worklist;
- Worklist.push_back(BB);
-
- SmallVector<Instruction*, 128> InstrsForInstCombineWorklist;
- DenseMap<ConstantExpr*, Constant*> FoldedConstants;
-
- do {
- BB = Worklist.pop_back_val();
-
- // We have now visited this block! If we've already been here, ignore it.
- if (!Visited.insert(BB).second)
- continue;
-
- for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
- Instruction *Inst = BBI++;
-
- // DCE instruction if trivially dead.
- if (isInstructionTriviallyDead(Inst, TLI)) {
- ++NumDeadInst;
- DEBUG(dbgs() << "IC: DCE: " << *Inst << '\n');
- Inst->eraseFromParent();
- continue;
- }
-
- // ConstantProp instruction if trivially constant.
- if (!Inst->use_empty() && isa<Constant>(Inst->getOperand(0)))
- if (Constant *C = ConstantFoldInstruction(Inst, DL, TLI)) {
- DEBUG(dbgs() << "IC: ConstFold to: " << *C << " from: "
- << *Inst << '\n');
- Inst->replaceAllUsesWith(C);
- ++NumConstProp;
- Inst->eraseFromParent();
- continue;
- }
-
- if (DL) {
- // See if we can constant fold its operands.
- for (User::op_iterator i = Inst->op_begin(), e = Inst->op_end();
- i != e; ++i) {
- ConstantExpr *CE = dyn_cast<ConstantExpr>(i);
- if (CE == nullptr) continue;
-
- Constant*& FoldRes = FoldedConstants[CE];
- if (!FoldRes)
- FoldRes = ConstantFoldConstantExpression(CE, DL, TLI);
- if (!FoldRes)
- FoldRes = CE;
-
- if (FoldRes != CE) {
- *i = FoldRes;
- MadeIRChange = true;
- }
- }
- }
-
- InstrsForInstCombineWorklist.push_back(Inst);
- }
-
- // Recursively visit successors. If this is a branch or switch on a
- // constant, only visit the reachable successor.
- TerminatorInst *TI = BB->getTerminator();
- if (BranchInst *BI = dyn_cast<BranchInst>(TI)) {
- if (BI->isConditional() && isa<ConstantInt>(BI->getCondition())) {
- bool CondVal = cast<ConstantInt>(BI->getCondition())->getZExtValue();
- BasicBlock *ReachableBB = BI->getSuccessor(!CondVal);
- Worklist.push_back(ReachableBB);
- continue;
- }
- } else if (SwitchInst *SI = dyn_cast<SwitchInst>(TI)) {
- if (ConstantInt *Cond = dyn_cast<ConstantInt>(SI->getCondition())) {
- // See if this is an explicit destination.
- for (SwitchInst::CaseIt i = SI->case_begin(), e = SI->case_end();
- i != e; ++i)
- if (i.getCaseValue() == Cond) {
- BasicBlock *ReachableBB = i.getCaseSuccessor();
- Worklist.push_back(ReachableBB);
- continue;
- }
-
- // Otherwise it is the default destination.
- Worklist.push_back(SI->getDefaultDest());
- continue;
- }
- }
-
- for (unsigned i = 0, e = TI->getNumSuccessors(); i != e; ++i)
- Worklist.push_back(TI->getSuccessor(i));
- } while (!Worklist.empty());
-
- // Once we've found all of the instructions to add to instcombine's worklist,
- // add them in reverse order. This way instcombine will visit from the top
- // of the function down. This jives well with the way that it adds all uses
- // of instructions to the worklist after doing a transformation, thus avoiding
- // some N^2 behavior in pathological cases.
- IC.Worklist.AddInitialGroup(&InstrsForInstCombineWorklist[0],
- InstrsForInstCombineWorklist.size());
-
- return MadeIRChange;
-}
-
-bool InstCombiner::DoOneIteration(Function &F, unsigned Iteration) {
- MadeIRChange = false;
-
- DEBUG(dbgs() << "\n\nINSTCOMBINE ITERATION #" << Iteration << " on "
- << F.getName() << "\n");
-
- {
- // Do a depth-first traversal of the function, populate the worklist with
- // the reachable instructions. Ignore blocks that are not reachable. Keep
- // track of which blocks we visit.
- SmallPtrSet<BasicBlock*, 64> Visited;
- MadeIRChange |= AddReachableCodeToWorklist(F.begin(), Visited, *this, DL,
- TLI);
-
- // Do a quick scan over the function. If we find any blocks that are
- // unreachable, remove any instructions inside of them. This prevents
- // the instcombine code from having to deal with some bad special cases.
- for (Function::iterator BB = F.begin(), E = F.end(); BB != E; ++BB) {
- if (Visited.count(BB)) continue;
-
- // Delete the instructions backwards, as it has a reduced likelihood of
- // having to update as many def-use and use-def chains.
- Instruction *EndInst = BB->getTerminator(); // Last not to be deleted.
- while (EndInst != BB->begin()) {
- // Delete the next to last instruction.
- BasicBlock::iterator I = EndInst;
- Instruction *Inst = --I;
- if (!Inst->use_empty())
- Inst->replaceAllUsesWith(UndefValue::get(Inst->getType()));
- if (isa<LandingPadInst>(Inst)) {
- EndInst = Inst;
- continue;
- }
- if (!isa<DbgInfoIntrinsic>(Inst)) {
- ++NumDeadInst;
- MadeIRChange = true;
- }
- Inst->eraseFromParent();
- }
- }
- }
-
+bool InstCombiner::run() {
while (!Worklist.isEmpty()) {
Instruction *I = Worklist.RemoveOne();
if (I == nullptr) continue; // skip null values.
return MadeIRChange;
}
-// FIXME: Passing all of the analyses here in the run method is ugly. We should
-// separate out the worklist from the combiner so that we can construct
-// a combiner once per function while re-using the storage of an external
-// worklist.
-bool InstCombiner::run(Function &F, AssumptionCache *AC, const DataLayout *DL,
- TargetLibraryInfo *TLI, DominatorTree *DT,
- LoopInfo *LI) {
- // Set up our analysis pointers.
- this->AC = AC;
- this->DL = DL;
- this->TLI = TLI;
- this->DT = DT;
- this->LI = LI;
+/// AddReachableCodeToWorklist - Walk the function in depth-first order, adding
+/// all reachable code to the worklist.
+///
+/// This has a couple of tricks to make the code faster and more powerful. In
+/// particular, we constant fold and DCE instructions as we go, to avoid adding
+/// them to the worklist (this significantly speeds up instcombine on code where
+/// many instructions are dead or constant). Additionally, if we find a branch
+/// whose condition is a known constant, we only visit the reachable successors.
+///
+static bool AddReachableCodeToWorklist(BasicBlock *BB,
+ SmallPtrSetImpl<BasicBlock*> &Visited,
+ InstCombineWorklist &ICWorklist,
+ const DataLayout *DL,
+ const TargetLibraryInfo *TLI) {
+ bool MadeIRChange = false;
+ SmallVector<BasicBlock*, 256> Worklist;
+ Worklist.push_back(BB);
+
+ SmallVector<Instruction*, 128> InstrsForInstCombineWorklist;
+ DenseMap<ConstantExpr*, Constant*> FoldedConstants;
- // Minimizing size?
- MinimizeSize = F.getAttributes().hasAttribute(AttributeSet::FunctionIndex,
- Attribute::MinSize);
+ do {
+ BB = Worklist.pop_back_val();
- /// Builder - This is an IRBuilder that automatically inserts new
- /// instructions into the worklist when they are created.
- IRBuilder<true, TargetFolder, InstCombineIRInserter> TheBuilder(
- F.getContext(), TargetFolder(DL), InstCombineIRInserter(Worklist, AC));
- Builder = &TheBuilder;
+ // We have now visited this block! If we've already been here, ignore it.
+ if (!Visited.insert(BB).second)
+ continue;
- bool EverMadeChange = false;
+ for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
+ Instruction *Inst = BBI++;
- // Lower dbg.declare intrinsics otherwise their value may be clobbered
- // by instcombiner.
- EverMadeChange = LowerDbgDeclare(F);
+ // DCE instruction if trivially dead.
+ if (isInstructionTriviallyDead(Inst, TLI)) {
+ ++NumDeadInst;
+ DEBUG(dbgs() << "IC: DCE: " << *Inst << '\n');
+ Inst->eraseFromParent();
+ continue;
+ }
- // Iterate while there is work to do.
- unsigned Iteration = 0;
- while (DoOneIteration(F, Iteration++))
- EverMadeChange = true;
+ // ConstantProp instruction if trivially constant.
+ if (!Inst->use_empty() && isa<Constant>(Inst->getOperand(0)))
+ if (Constant *C = ConstantFoldInstruction(Inst, DL, TLI)) {
+ DEBUG(dbgs() << "IC: ConstFold to: " << *C << " from: "
+ << *Inst << '\n');
+ Inst->replaceAllUsesWith(C);
+ ++NumConstProp;
+ Inst->eraseFromParent();
+ continue;
+ }
+
+ if (DL) {
+ // See if we can constant fold its operands.
+ for (User::op_iterator i = Inst->op_begin(), e = Inst->op_end();
+ i != e; ++i) {
+ ConstantExpr *CE = dyn_cast<ConstantExpr>(i);
+ if (CE == nullptr) continue;
+
+ Constant*& FoldRes = FoldedConstants[CE];
+ if (!FoldRes)
+ FoldRes = ConstantFoldConstantExpression(CE, DL, TLI);
+ if (!FoldRes)
+ FoldRes = CE;
- Builder = nullptr;
- return EverMadeChange;
+ if (FoldRes != CE) {
+ *i = FoldRes;
+ MadeIRChange = true;
+ }
+ }
+ }
+
+ InstrsForInstCombineWorklist.push_back(Inst);
+ }
+
+ // Recursively visit successors. If this is a branch or switch on a
+ // constant, only visit the reachable successor.
+ TerminatorInst *TI = BB->getTerminator();
+ if (BranchInst *BI = dyn_cast<BranchInst>(TI)) {
+ if (BI->isConditional() && isa<ConstantInt>(BI->getCondition())) {
+ bool CondVal = cast<ConstantInt>(BI->getCondition())->getZExtValue();
+ BasicBlock *ReachableBB = BI->getSuccessor(!CondVal);
+ Worklist.push_back(ReachableBB);
+ continue;
+ }
+ } else if (SwitchInst *SI = dyn_cast<SwitchInst>(TI)) {
+ if (ConstantInt *Cond = dyn_cast<ConstantInt>(SI->getCondition())) {
+ // See if this is an explicit destination.
+ for (SwitchInst::CaseIt i = SI->case_begin(), e = SI->case_end();
+ i != e; ++i)
+ if (i.getCaseValue() == Cond) {
+ BasicBlock *ReachableBB = i.getCaseSuccessor();
+ Worklist.push_back(ReachableBB);
+ continue;
+ }
+
+ // Otherwise it is the default destination.
+ Worklist.push_back(SI->getDefaultDest());
+ continue;
+ }
+ }
+
+ for (unsigned i = 0, e = TI->getNumSuccessors(); i != e; ++i)
+ Worklist.push_back(TI->getSuccessor(i));
+ } while (!Worklist.empty());
+
+ // Once we've found all of the instructions to add to instcombine's worklist,
+ // add them in reverse order. This way instcombine will visit from the top
+ // of the function down. This jives well with the way that it adds all uses
+ // of instructions to the worklist after doing a transformation, thus avoiding
+ // some N^2 behavior in pathological cases.
+ ICWorklist.AddInitialGroup(&InstrsForInstCombineWorklist[0],
+ InstrsForInstCombineWorklist.size());
+
+ return MadeIRChange;
+}
+
+/// \brief Populate the IC worklist from a function, and prune any dead basic
+/// blocks discovered in the process.
+///
+/// This also does basic constant propagation and other forward fixing to make
+/// the combiner itself run much faster.
+static bool prepareICWorklistFromFunction(Function &F, const DataLayout *DL,
+ TargetLibraryInfo *TLI,
+ InstCombineWorklist &ICWorklist) {
+ bool MadeIRChange = false;
+
+ // Do a depth-first traversal of the function, populate the worklist with
+ // the reachable instructions. Ignore blocks that are not reachable. Keep
+ // track of which blocks we visit.
+ SmallPtrSet<BasicBlock *, 64> Visited;
+ MadeIRChange |=
+ AddReachableCodeToWorklist(F.begin(), Visited, ICWorklist, DL, TLI);
+
+ // Do a quick scan over the function. If we find any blocks that are
+ // unreachable, remove any instructions inside of them. This prevents
+ // the instcombine code from having to deal with some bad special cases.
+ for (Function::iterator BB = F.begin(), E = F.end(); BB != E; ++BB) {
+ if (Visited.count(BB))
+ continue;
+
+ // Delete the instructions backwards, as it has a reduced likelihood of
+ // having to update as many def-use and use-def chains.
+ Instruction *EndInst = BB->getTerminator(); // Last not to be deleted.
+ while (EndInst != BB->begin()) {
+ // Delete the next to last instruction.
+ BasicBlock::iterator I = EndInst;
+ Instruction *Inst = --I;
+ if (!Inst->use_empty())
+ Inst->replaceAllUsesWith(UndefValue::get(Inst->getType()));
+ if (isa<LandingPadInst>(Inst)) {
+ EndInst = Inst;
+ continue;
+ }
+ if (!isa<DbgInfoIntrinsic>(Inst)) {
+ ++NumDeadInst;
+ MadeIRChange = true;
+ }
+ Inst->eraseFromParent();
+ }
+ }
+
+ return MadeIRChange;
}
namespace {
/// This is a basic whole-function wrapper around the instcombine utility. It
/// will try to combine all instructions in the function.
class InstructionCombiningPass : public FunctionPass {
- InstCombiner IC;
+ InstCombineWorklist Worklist;
public:
static char ID; // Pass identification, replacement for typeid
if (skipOptnoneFunction(F))
return false;
+ // Lower dbg.declare intrinsics otherwise their value may be clobbered
+ // by instcombiner.
+ bool DbgDeclaresChanged = LowerDbgDeclare(F);
+
+ // Required analyses.
auto &AC = getAnalysis<AssumptionCacheTracker>().getAssumptionCache(F);
- auto *DLP = getAnalysisIfAvailable<DataLayoutPass>();
- auto *DL = DLP ? &DLP->getDataLayout() : nullptr;
auto &TLI = getAnalysis<TargetLibraryInfoWrapperPass>().getTLI();
auto &DT = getAnalysis<DominatorTreeWrapperPass>().getDomTree();
+
+ // Optional analyses.
+ auto *DLP = getAnalysisIfAvailable<DataLayoutPass>();
+ auto *DL = DLP ? &DLP->getDataLayout() : nullptr;
auto *LIWP = getAnalysisIfAvailable<LoopInfoWrapperPass>();
auto *LI = LIWP ? &LIWP->getLoopInfo() : nullptr;
- return IC.run(F, &AC, DL, &TLI, &DT, LI);
+ // Minimizing size?
+ bool MinimizeSize = F.getAttributes().hasAttribute(
+ AttributeSet::FunctionIndex, Attribute::MinSize);
+
+ /// Builder - This is an IRBuilder that automatically inserts new
+ /// instructions into the worklist when they are created.
+ IRBuilder<true, TargetFolder, InstCombineIRInserter> Builder(
+ F.getContext(), TargetFolder(DL), InstCombineIRInserter(Worklist, &AC));
+
+ // Iterate while there is work to do.
+ int Iteration = 0;
+ for (;;) {
+ ++Iteration;
+ DEBUG(dbgs() << "\n\nINSTCOMBINE ITERATION #" << Iteration << " on "
+ << F.getName() << "\n");
+
+ bool Changed = false;
+ if (prepareICWorklistFromFunction(F, DL, &TLI, Worklist))
+ Changed = true;
+
+ InstCombiner IC(Worklist, &Builder, MinimizeSize, &AC, &TLI, &DT, DL, LI);
+ if (IC.run())
+ Changed = true;
+
+ if (!Changed)
+ break;
+ }
+
+ return DbgDeclaresChanged || Iteration > 1;
}
char InstructionCombiningPass::ID = 0;