summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2d74092)
raw | patch | inline | side by side (parent: 2d74092)
author | Stepan Dyatkovskiy <stpworld@narod.ru> | |
Thu, 13 Mar 2014 11:54:50 +0000 (11:54 +0000) | ||
committer | Stepan Dyatkovskiy <stpworld@narod.ru> | |
Thu, 13 Mar 2014 11:54:50 +0000 (11:54 +0000) |
O(N*log(N)). The idea is to introduce total ordering among functions set.
That allows to build binary tree and perform function look-up procedure in O(log(N)) time.
This patch description:
Introduced total ordering among Type instances. Actually it is improvement for existing
isEquivalentType.
0. Coerce pointer of 0 address space to integer.
1. If left and right types are equal (the same Type* value), return 0 (means equal).
2. If types are of different kind (different type IDs). Return result of type IDs
comparison, treating them as numbers.
3. If types are vectors or integers, return result of its
pointers comparison (casted to numbers).
4. Check whether type ID belongs to the next group:
* Void
* Float
* Double
* X86_FP80
* FP128
* PPC_FP128
* Label
* Metadata
If so, return 0.
5. If left and right are pointers, return result of address space
comparison (numbers comparison).
6. If types are complex.
Then both LEFT and RIGHT will be expanded and their element types will be checked with
the same way. If we get Res != 0 on some stage, return it. Otherwise return 0.
7. For all other cases put llvm_unreachable.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@203788 91177308-0d34-0410-b5e6-96231b3b80d8
That allows to build binary tree and perform function look-up procedure in O(log(N)) time.
This patch description:
Introduced total ordering among Type instances. Actually it is improvement for existing
isEquivalentType.
0. Coerce pointer of 0 address space to integer.
1. If left and right types are equal (the same Type* value), return 0 (means equal).
2. If types are of different kind (different type IDs). Return result of type IDs
comparison, treating them as numbers.
3. If types are vectors or integers, return result of its
pointers comparison (casted to numbers).
4. Check whether type ID belongs to the next group:
* Void
* Float
* Double
* X86_FP80
* FP128
* PPC_FP128
* Label
* Metadata
If so, return 0.
5. If left and right are pointers, return result of address space
comparison (numbers comparison).
6. If types are complex.
Then both LEFT and RIGHT will be expanded and their element types will be checked with
the same way. If we get Res != 0 on some stage, return it. Otherwise return 0.
7. For all other cases put llvm_unreachable.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@203788 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/IPO/MergeFunctions.cpp | patch | blob | history |
index ff16b1ecdf8c97dfd47e0378c6f004943c818e28..54e423d36a27531178a7f38ec631a95dfae651c6 100644 (file)
return isEquivalentGEP(cast<GEPOperator>(GEP1), cast<GEPOperator>(GEP2));
}
- /// Compare two Types, treating all pointer types as equal.
- bool isEquivalentType(Type *Ty1, Type *Ty2) const;
+ /// cmpType - compares two types,
+ /// defines total ordering among the types set.
+ ///
+ /// Return values:
+ /// 0 if types are equal,
+ /// -1 if Left is less than Right,
+ /// +1 if Left is greater than Right.
+ ///
+ /// Description:
+ /// Comparison is broken onto stages. Like in lexicographical comparison
+ /// stage coming first has higher priority.
+ /// On each explanation stage keep in mind total ordering properties.
+ ///
+ /// 0. Before comparison we coerce pointer types of 0 address space to integer.
+ /// We also don't bother with same type at left and right, so
+ /// just return 0 in this case.
+ ///
+ /// 1. If types are of different kind (different type IDs).
+ /// Return result of type IDs comparison, treating them as numbers.
+ /// 2. If types are vectors or integers, compare Type* values as numbers.
+ /// 3. Types has same ID, so check whether they belongs to the next group:
+ /// * Void
+ /// * Float
+ /// * Double
+ /// * X86_FP80
+ /// * FP128
+ /// * PPC_FP128
+ /// * Label
+ /// * Metadata
+ /// If so - return 0, yes - we can treat these types as equal only because
+ /// their IDs are same.
+ /// 4. If Left and Right are pointers, return result of address space
+ /// comparison (numbers comparison). We can treat pointer types of same
+ /// address space as equal.
+ /// 5. If types are complex.
+ /// Then both Left and Right are to be expanded and their element types will
+ /// be checked with the same way. If we get Res != 0 on some stage, return it.
+ /// Otherwise return 0.
+ /// 6. For all other cases put llvm_unreachable.
+ int cmpType(Type *TyL, Type *TyR) const;
+
+ bool isEquivalentType(Type *Ty1, Type *Ty2) const {
+ return cmpType(Ty1, Ty2) == 0;
+ }
+
+ int cmpNumbers(uint64_t L, uint64_t R) const;
// The two functions undergoing comparison.
const Function *F1, *F2;
}
-// Any two pointers in the same address space are equivalent, intptr_t and
-// pointers are equivalent. Otherwise, standard type equivalence rules apply.
-bool FunctionComparator::isEquivalentType(Type *Ty1, Type *Ty2) const {
+int FunctionComparator::cmpNumbers(uint64_t L, uint64_t R) const {
+ if (L < R) return -1;
+ if (L > R) return 1;
+ return 0;
+}
- PointerType *PTy1 = dyn_cast<PointerType>(Ty1);
- PointerType *PTy2 = dyn_cast<PointerType>(Ty2);
+/// cmpType - compares two types,
+/// defines total ordering among the types set.
+/// See method declaration comments for more details.
+int FunctionComparator::cmpType(Type *TyL, Type *TyR) const {
+
+ PointerType *PTy1 = dyn_cast<PointerType>(TyL);
+ PointerType *PTy2 = dyn_cast<PointerType>(TyR);
if (DL) {
- if (PTy1 && PTy1->getAddressSpace() == 0) Ty1 = DL->getIntPtrType(Ty1);
- if (PTy2 && PTy2->getAddressSpace() == 0) Ty2 = DL->getIntPtrType(Ty2);
+ if (PTy1 && PTy1->getAddressSpace() == 0) TyL = DL->getIntPtrType(TyL);
+ if (PTy2 && PTy2->getAddressSpace() == 0) TyR = DL->getIntPtrType(TyR);
}
- if (Ty1 == Ty2)
- return true;
+ if (TyL == TyR)
+ return 0;
- if (Ty1->getTypeID() != Ty2->getTypeID())
- return false;
+ if (int Res = cmpNumbers(TyL->getTypeID(), TyR->getTypeID()))
+ return Res;
- switch (Ty1->getTypeID()) {
+ switch (TyL->getTypeID()) {
default:
llvm_unreachable("Unknown type!");
// Fall through in Release mode.
case Type::IntegerTyID:
case Type::VectorTyID:
- // Ty1 == Ty2 would have returned true earlier.
- return false;
+ // TyL == TyR would have returned true earlier.
+ return cmpNumbers((uint64_t)TyL, (uint64_t)TyR);
case Type::VoidTyID:
case Type::FloatTyID:
case Type::PPC_FP128TyID:
case Type::LabelTyID:
case Type::MetadataTyID:
- return true;
+ return 0;
case Type::PointerTyID: {
assert(PTy1 && PTy2 && "Both types must be pointers here.");
- return PTy1->getAddressSpace() == PTy2->getAddressSpace();
+ return cmpNumbers(PTy1->getAddressSpace(), PTy2->getAddressSpace());
}
case Type::StructTyID: {
- StructType *STy1 = cast<StructType>(Ty1);
- StructType *STy2 = cast<StructType>(Ty2);
+ StructType *STy1 = cast<StructType>(TyL);
+ StructType *STy2 = cast<StructType>(TyR);
if (STy1->getNumElements() != STy2->getNumElements())
- return false;
+ return cmpNumbers(STy1->getNumElements(), STy2->getNumElements());
if (STy1->isPacked() != STy2->isPacked())
- return false;
+ return cmpNumbers(STy1->isPacked(), STy2->isPacked());
for (unsigned i = 0, e = STy1->getNumElements(); i != e; ++i) {
- if (!isEquivalentType(STy1->getElementType(i), STy2->getElementType(i)))
- return false;
+ if (int Res = cmpType(STy1->getElementType(i),
+ STy2->getElementType(i)))
+ return Res;
}
- return true;
+ return 0;
}
case Type::FunctionTyID: {
- FunctionType *FTy1 = cast<FunctionType>(Ty1);
- FunctionType *FTy2 = cast<FunctionType>(Ty2);
- if (FTy1->getNumParams() != FTy2->getNumParams() ||
- FTy1->isVarArg() != FTy2->isVarArg())
- return false;
+ FunctionType *FTy1 = cast<FunctionType>(TyL);
+ FunctionType *FTy2 = cast<FunctionType>(TyR);
+ if (FTy1->getNumParams() != FTy2->getNumParams())
+ return cmpNumbers(FTy1->getNumParams(), FTy2->getNumParams());
- if (!isEquivalentType(FTy1->getReturnType(), FTy2->getReturnType()))
- return false;
+ if (FTy1->isVarArg() != FTy2->isVarArg())
+ return cmpNumbers(FTy1->isVarArg(), FTy2->isVarArg());
+
+ if (int Res = cmpType(FTy1->getReturnType(), FTy2->getReturnType()))
+ return Res;
for (unsigned i = 0, e = FTy1->getNumParams(); i != e; ++i) {
- if (!isEquivalentType(FTy1->getParamType(i), FTy2->getParamType(i)))
- return false;
+ if (int Res = cmpType(FTy1->getParamType(i), FTy2->getParamType(i)))
+ return Res;
}
- return true;
+ return 0;
}
case Type::ArrayTyID: {
- ArrayType *ATy1 = cast<ArrayType>(Ty1);
- ArrayType *ATy2 = cast<ArrayType>(Ty2);
- return ATy1->getNumElements() == ATy2->getNumElements() &&
- isEquivalentType(ATy1->getElementType(), ATy2->getElementType());
+ ArrayType *ATy1 = cast<ArrayType>(TyL);
+ ArrayType *ATy2 = cast<ArrayType>(TyR);
+ if (ATy1->getNumElements() != ATy2->getNumElements())
+ return cmpNumbers(ATy1->getNumElements(), ATy2->getNumElements());
+ return cmpType(ATy1->getElementType(), ATy2->getElementType());
}
}
}