summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 57683b8)
raw | patch | inline | side by side (parent: 57683b8)
author | Chandler Carruth <chandlerc@gmail.com> | |
Wed, 23 Apr 2014 10:31:17 +0000 (10:31 +0000) | ||
committer | Chandler Carruth <chandlerc@gmail.com> | |
Wed, 23 Apr 2014 10:31:17 +0000 (10:31 +0000) |
up the stack finishing the exploration of each entries children before
we're finished in addition to accounting for their low-links. Added
a unittest that really hammers home the need for this with interlocking
cycles that would each appear distinct otherwise and crash or compute
the wrong result. As part of this, nuke a stale fixme and bring the rest
of the implementation still more closely in line with the original
algorithm.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@206966 91177308-0d34-0410-b5e6-96231b3b80d8
we're finished in addition to accounting for their low-links. Added
a unittest that really hammers home the need for this with interlocking
cycles that would each appear distinct otherwise and crash or compute
the wrong result. As part of this, nuke a stale fixme and bring the rest
of the implementation still more closely in line with the original
algorithm.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@206966 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Analysis/LazyCallGraph.h | patch | blob | history | |
lib/Analysis/LazyCallGraph.cpp | patch | blob | history | |
unittests/Analysis/LazyCallGraphTest.cpp | patch | blob | history |
index cf74101c6e9d69251cf400353a5f293bd6bf439c..aefad6f913a5b48f2e75309d9279462a52d19c4e 100644 (file)
/// \brief Helper to form a new SCC out of the top of a DFSStack-like
/// structure.
SCC *formSCCFromDFSStack(
- SmallVectorImpl<std::pair<Node *, Node::iterator>> &DFSStack);
+ SmallVectorImpl<std::pair<Node *, Node::iterator>> &DFSStack,
+ SmallVectorImpl<std::pair<Node *, Node::iterator>>::iterator SCCBegin);
/// \brief Retrieve the next node in the post-order SCC walk of the call graph.
SCC *getNextSCCInPostOrder();
index 0a71b9d275860f73780b68cbe1dec4495cdfdae9..a86c96971689737a888bb79a93e4648893114925 100644 (file)
}
LazyCallGraph::SCC *LazyCallGraph::formSCCFromDFSStack(
- SmallVectorImpl<std::pair<Node *, Node::iterator>> &DFSStack) {
+ SmallVectorImpl<std::pair<Node *, Node::iterator>> &DFSStack,
+ SmallVectorImpl<std::pair<Node *, Node::iterator>>::iterator SCCBegin) {
// The tail of the stack is the new SCC. Allocate the SCC and pop the stack
// into it.
SCC *NewSCC = new (SCCBPA.Allocate()) SCC();
- // Because we don't follow the strict Tarjan recursive formulation, walk
- // from the top of the stack down, propagating the lowest link and stopping
- // when the DFS number is the lowest link.
- int LowestLink = DFSStack.back().first->LowLink;
- do {
- Node *SCCN = DFSStack.pop_back_val().first;
+ for (auto I = SCCBegin, E = DFSStack.end(); I != E; ++I) {
+ Node *SCCN = I->first;
+ assert(SCCN->LowLink >= SCCBegin->first->LowLink &&
+ "We cannot have a low link in an SCC lower than its root on the "
+ "stack!");
+
SCCMap[&SCCN->getFunction()] = NewSCC;
NewSCC->Nodes.push_back(SCCN);
- LowestLink = std::min(LowestLink, SCCN->LowLink);
bool Inserted =
NewSCC->NodeSet.insert(&SCCN->getFunction());
(void)Inserted;
assert(Inserted && "Cannot have duplicates in the DFSStack!");
- } while (!DFSStack.empty() && LowestLink <= DFSStack.back().first->DFSNumber);
- assert(LowestLink == NewSCC->Nodes.back()->DFSNumber &&
- "Cannot stop with a DFS number greater than the lowest link!");
+ }
+ DFSStack.erase(SCCBegin, DFSStack.end());
// A final pass over all edges in the SCC (this remains linear as we only
// do this once when we build the SCC) to connect it to the parent sets of
DFSStack.push_back(std::make_pair(N, N->begin()));
}
- Node *N = DFSStack.back().first;
- if (N->DFSNumber == 0) {
+ auto SI = DFSStack.rbegin();
+ if (SI->first->DFSNumber == 0) {
// This node hasn't been visited before, assign it a DFS number and remove
// it from the entry set.
- N->LowLink = N->DFSNumber = NextDFSNumber++;
- SCCEntryNodes.remove(&N->getFunction());
+ SI->first->LowLink = SI->first->DFSNumber = NextDFSNumber++;
+ SCCEntryNodes.remove(&SI->first->getFunction());
}
- for (auto I = DFSStack.back().second, E = N->end(); I != E; ++I) {
- Node *ChildN = *I;
- if (ChildN->DFSNumber == 0) {
- // Mark that we should start at this child when next this node is the
- // top of the stack. We don't start at the next child to ensure this
- // child's lowlink is reflected.
- // FIXME: I don't actually think this is required, and we could start
- // at the next child.
- DFSStack.back().second = I;
-
- // Recurse onto this node via a tail call.
- DFSStack.push_back(std::make_pair(ChildN, ChildN->begin()));
- return LazyCallGraph::getNextSCCInPostOrder();
+ do {
+ Node *N = SI->first;
+ for (auto I = SI->second, E = N->end(); I != E; ++I) {
+ Node *ChildN = *I;
+ if (ChildN->DFSNumber == 0) {
+ // Mark that we should start at this child when next this node is the
+ // top of the stack. We don't start at the next child to ensure this
+ // child's lowlink is reflected.
+ SI->second = I;
+
+ // Recurse onto this node via a tail call.
+ DFSStack.push_back(std::make_pair(ChildN, ChildN->begin()));
+ return LazyCallGraph::getNextSCCInPostOrder();
+ }
+
+ // Track the lowest link of the childen, if any are still in the stack.
+ if (ChildN->LowLink < N->LowLink && !SCCMap.count(&ChildN->getFunction()))
+ N->LowLink = ChildN->LowLink;
}
+ // No more children to process for this stack entry.
+ SI->second = N->end();
- // Track the lowest link of the childen, if any are still in the stack.
- if (ChildN->LowLink < N->LowLink && !SCCMap.count(&ChildN->getFunction()))
- N->LowLink = ChildN->LowLink;
- }
+ if (N->LowLink == N->DFSNumber)
+ // Form the new SCC out of the top of the DFS stack.
+ return formSCCFromDFSStack(DFSStack, std::prev(SI.base()));
+
+ ++SI;
+ } while (SI != DFSStack.rend());
- // Form the new SCC out of the top of the DFS stack.
- return formSCCFromDFSStack(DFSStack);
+ llvm_unreachable(
+ "We cannot reach the bottom of the stack without popping an SCC.");
}
char LazyCallGraphAnalysis::PassID;
index c224afbbb859a031c43feaadd3c12243fe50de42..bdb9d151674de41446c66a145684957c9358ec73 100644 (file)
EXPECT_EQ(CG.postorder_scc_end(), SCCI);
}
+static Function &lookupFunction(Module &M, StringRef Name) {
+ for (Function &F : M)
+ if (F.getName() == Name)
+ return F;
+ report_fatal_error("Couldn't find function!");
+}
+
+TEST(LazyCallGraphTest, MultiArmSCC) {
+ // Two interlocking cycles. The really useful thing about this SCC is that it
+ // will require Tarjan's DFS to backtrack and finish processing all of the
+ // children of each node in the SCC.
+ std::unique_ptr<Module> M = parseAssembly(
+ "define void @a() {\n"
+ "entry:\n"
+ " call void @b()\n"
+ " call void @d()\n"
+ " ret void\n"
+ "}\n"
+ "define void @b() {\n"
+ "entry:\n"
+ " call void @c()\n"
+ " ret void\n"
+ "}\n"
+ "define void @c() {\n"
+ "entry:\n"
+ " call void @a()\n"
+ " ret void\n"
+ "}\n"
+ "define void @d() {\n"
+ "entry:\n"
+ " call void @e()\n"
+ " ret void\n"
+ "}\n"
+ "define void @e() {\n"
+ "entry:\n"
+ " call void @a()\n"
+ " ret void\n"
+ "}\n");
+ LazyCallGraph CG(*M);
+
+ // Force the graph to be fully expanded.
+ auto SCCI = CG.postorder_scc_begin();
+ LazyCallGraph::SCC *SCC = *SCCI++;
+ EXPECT_EQ(CG.postorder_scc_end(), SCCI);
+
+ LazyCallGraph::Node *A = CG.lookup(lookupFunction(*M, "a"));
+ LazyCallGraph::Node *B = CG.lookup(lookupFunction(*M, "b"));
+ LazyCallGraph::Node *C = CG.lookup(lookupFunction(*M, "c"));
+ LazyCallGraph::Node *D = CG.lookup(lookupFunction(*M, "d"));
+ LazyCallGraph::Node *E = CG.lookup(lookupFunction(*M, "e"));
+ EXPECT_EQ(SCC, CG.lookupSCC(A->getFunction()));
+ EXPECT_EQ(SCC, CG.lookupSCC(B->getFunction()));
+ EXPECT_EQ(SCC, CG.lookupSCC(C->getFunction()));
+ EXPECT_EQ(SCC, CG.lookupSCC(D->getFunction()));
+ EXPECT_EQ(SCC, CG.lookupSCC(E->getFunction()));
+}
+
}