summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 0c25726)
raw | patch | inline | side by side (parent: 0c25726)
author | Kostya Serebryany <kcc@google.com> | |
Fri, 17 Jan 2014 11:00:30 +0000 (11:00 +0000) | ||
committer | Kostya Serebryany <kcc@google.com> | |
Fri, 17 Jan 2014 11:00:30 +0000 (11:00 +0000) |
- add a mode for collecting per-block coverage (-asan-coverage=2).
So far the implementation is naive (all blocks are instrumented),
the performance overhead on top of asan could be as high as 30%.
- Make sure the one-time calls to __sanitizer_cov are moved to function buttom,
which in turn required to copy the original debug info into the call insn.
Here is the performance data on SPEC 2006
(train data, comparing asan with asan-coverage={0,1,2}):
asan+cov0 asan+cov1 diff 0-1 asan+cov2 diff 0-2 diff 1-2
400.perlbench, 65.60, 65.80, 1.00, 76.20, 1.16, 1.16
401.bzip2, 65.10, 65.50, 1.01, 75.90, 1.17, 1.16
403.gcc, 1.64, 1.69, 1.03, 2.04, 1.24, 1.21
429.mcf, 21.90, 22.60, 1.03, 23.20, 1.06, 1.03
445.gobmk, 166.00, 169.00, 1.02, 205.00, 1.23, 1.21
456.hmmer, 88.30, 87.90, 1.00, 91.00, 1.03, 1.04
458.sjeng, 210.00, 222.00, 1.06, 258.00, 1.23, 1.16
462.libquantum, 1.73, 1.75, 1.01, 2.11, 1.22, 1.21
464.h264ref, 147.00, 152.00, 1.03, 160.00, 1.09, 1.05
471.omnetpp, 115.00, 116.00, 1.01, 140.00, 1.22, 1.21
473.astar, 133.00, 131.00, 0.98, 142.00, 1.07, 1.08
483.xalancbmk, 118.00, 120.00, 1.02, 154.00, 1.31, 1.28
433.milc, 19.80, 20.00, 1.01, 20.10, 1.02, 1.01
444.namd, 16.20, 16.20, 1.00, 17.60, 1.09, 1.09
447.dealII, 41.80, 42.20, 1.01, 43.50, 1.04, 1.03
450.soplex, 7.51, 7.82, 1.04, 8.25, 1.10, 1.05
453.povray, 14.00, 14.40, 1.03, 15.80, 1.13, 1.10
470.lbm, 33.30, 34.10, 1.02, 34.10, 1.02, 1.00
482.sphinx3, 12.40, 12.30, 0.99, 13.00, 1.05, 1.06
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@199488 91177308-0d34-0410-b5e6-96231b3b80d8
So far the implementation is naive (all blocks are instrumented),
the performance overhead on top of asan could be as high as 30%.
- Make sure the one-time calls to __sanitizer_cov are moved to function buttom,
which in turn required to copy the original debug info into the call insn.
Here is the performance data on SPEC 2006
(train data, comparing asan with asan-coverage={0,1,2}):
asan+cov0 asan+cov1 diff 0-1 asan+cov2 diff 0-2 diff 1-2
400.perlbench, 65.60, 65.80, 1.00, 76.20, 1.16, 1.16
401.bzip2, 65.10, 65.50, 1.01, 75.90, 1.17, 1.16
403.gcc, 1.64, 1.69, 1.03, 2.04, 1.24, 1.21
429.mcf, 21.90, 22.60, 1.03, 23.20, 1.06, 1.03
445.gobmk, 166.00, 169.00, 1.02, 205.00, 1.23, 1.21
456.hmmer, 88.30, 87.90, 1.00, 91.00, 1.03, 1.04
458.sjeng, 210.00, 222.00, 1.06, 258.00, 1.23, 1.16
462.libquantum, 1.73, 1.75, 1.01, 2.11, 1.22, 1.21
464.h264ref, 147.00, 152.00, 1.03, 160.00, 1.09, 1.05
471.omnetpp, 115.00, 116.00, 1.01, 140.00, 1.22, 1.21
473.astar, 133.00, 131.00, 0.98, 142.00, 1.07, 1.08
483.xalancbmk, 118.00, 120.00, 1.02, 154.00, 1.31, 1.28
433.milc, 19.80, 20.00, 1.01, 20.10, 1.02, 1.01
444.namd, 16.20, 16.20, 1.00, 17.60, 1.09, 1.09
447.dealII, 41.80, 42.20, 1.01, 43.50, 1.04, 1.03
450.soplex, 7.51, 7.82, 1.04, 8.25, 1.10, 1.05
453.povray, 14.00, 14.40, 1.03, 15.80, 1.13, 1.10
470.lbm, 33.30, 34.10, 1.02, 34.10, 1.02, 1.00
482.sphinx3, 12.40, 12.30, 0.99, 13.00, 1.05, 1.06
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@199488 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Instrumentation/AddressSanitizer.cpp | patch | blob | history | |
test/Instrumentation/AddressSanitizer/coverage.ll | patch | blob | history |
diff --git a/lib/Transforms/Instrumentation/AddressSanitizer.cpp b/lib/Transforms/Instrumentation/AddressSanitizer.cpp
index c03075c9ea06baf4101a53e9c0b53f25d767df28..fe875192f581852995083972cbf8842a54b0be02 100644 (file)
#include "llvm/IR/InlineAsm.h"
#include "llvm/IR/IntrinsicInst.h"
#include "llvm/IR/LLVMContext.h"
+#include "llvm/IR/MDBuilder.h"
#include "llvm/IR/Module.h"
#include "llvm/IR/Type.h"
#include "llvm/InstVisitor.h"
// This flag may need to be replaced with -f[no]asan-globals.
static cl::opt<bool> ClGlobals("asan-globals",
cl::desc("Handle global objects"), cl::Hidden, cl::init(true));
-static cl::opt<bool> ClCoverage("asan-coverage",
- cl::desc("ASan coverage"), cl::Hidden, cl::init(false));
+static cl::opt<int> ClCoverage("asan-coverage",
+ cl::desc("ASan coverage. 0: none, 1: entry block, 2: all blocks"),
+ cl::Hidden, cl::init(false));
static cl::opt<bool> ClInitializers("asan-initialization-order",
cl::desc("Handle C++ initializer order"), cl::Hidden, cl::init(false));
static cl::opt<bool> ClMemIntrin("asan-memintrin",
bool LooksLikeCodeInBug11395(Instruction *I);
void FindDynamicInitializers(Module &M);
bool GlobalIsLinkerInitialized(GlobalVariable *G);
- bool InjectCoverage(Function &F);
+ bool InjectCoverage(Function &F, const ArrayRef<BasicBlock*> AllBlocks);
+ void InjectCoverageAtBlock(Function &F, BasicBlock &BB);
bool CheckInitOrder;
bool CheckUseAfterReturn;
AsanHandleNoReturnFunc = checkInterfaceFunction(M.getOrInsertFunction(
kAsanHandleNoReturnName, IRB.getVoidTy(), NULL));
AsanCovFunction = checkInterfaceFunction(M.getOrInsertFunction(
- kAsanCovName, IRB.getVoidTy(), IntptrTy, NULL));
+ kAsanCovName, IRB.getVoidTy(), NULL));
// We insert an empty inline asm after __asan_report* to avoid callback merge.
EmptyAsm = InlineAsm::get(FunctionType::get(IRB.getVoidTy(), false),
StringRef(""), StringRef(""),
return false;
}
-// Poor man's coverage that works with ASan.
-// We create a Guard boolean variable with the same linkage
-// as the function and inject this code into the entry block:
-// if (*Guard) {
-// __sanitizer_cov(&F);
-// *Guard = 1;
-// }
-// The accesses to Guard are atomic. The rest of the logic is
-// in __sanitizer_cov (it's fine to call it more than once).
-//
-// This coverage implementation provides very limited data:
-// it only tells if a given function was ever executed.
-// No counters, no per-basic-block or per-edge data.
-// But for many use cases this is what we need and the added slowdown
-// is negligible. This simple implementation will probably be obsoleted
-// by the upcoming Clang-based coverage implementation.
-// By having it here and now we hope to
-// a) get the functionality to users earlier and
-// b) collect usage statistics to help improve Clang coverage design.
-bool AddressSanitizer::InjectCoverage(Function &F) {
- if (!ClCoverage) return false;
-
+void AddressSanitizer::InjectCoverageAtBlock(Function &F, BasicBlock &BB) {
+ BasicBlock::iterator IP = BB.getFirstInsertionPt(), BE = BB.end();
// Skip static allocas at the top of the entry block so they don't become
// dynamic when we split the block. If we used our optimized stack layout,
// then there will only be one alloca and it will come first.
- BasicBlock &Entry = F.getEntryBlock();
- BasicBlock::iterator IP = Entry.getFirstInsertionPt(), BE = Entry.end();
for (; IP != BE; ++IP) {
AllocaInst *AI = dyn_cast<AllocaInst>(IP);
if (!AI || !AI->isStaticAlloca())
Load->setAtomic(Monotonic);
Load->setAlignment(1);
Value *Cmp = IRB.CreateICmpEQ(Constant::getNullValue(Int8Ty), Load);
- Instruction *Ins = SplitBlockAndInsertIfThen(Cmp, IP, false);
+ Instruction *Ins = SplitBlockAndInsertIfThen(
+ Cmp, IP, false, MDBuilder(*C).createBranchWeights(1, 100000));
IRB.SetInsertPoint(Ins);
// We pass &F to __sanitizer_cov. We could avoid this and rely on
// GET_CALLER_PC, but having the PC of the first instruction is just nice.
- IRB.CreateCall(AsanCovFunction, IRB.CreatePointerCast(&F, IntptrTy));
+ Instruction *Call = IRB.CreateCall(AsanCovFunction);
+ Call->setDebugLoc(IP->getDebugLoc());
StoreInst *Store = IRB.CreateStore(ConstantInt::get(Int8Ty, 1), Guard);
Store->setAtomic(Monotonic);
Store->setAlignment(1);
+}
+
+// Poor man's coverage that works with ASan.
+// We create a Guard boolean variable with the same linkage
+// as the function and inject this code into the entry block (-asan-coverage=1)
+// or all blocks (-asan-coverage=2):
+// if (*Guard) {
+// __sanitizer_cov(&F);
+// *Guard = 1;
+// }
+// The accesses to Guard are atomic. The rest of the logic is
+// in __sanitizer_cov (it's fine to call it more than once).
+//
+// This coverage implementation provides very limited data:
+// it only tells if a given function (block) was ever executed.
+// No counters, no per-edge data.
+// But for many use cases this is what we need and the added slowdown
+// is negligible. This simple implementation will probably be obsoleted
+// by the upcoming Clang-based coverage implementation.
+// By having it here and now we hope to
+// a) get the functionality to users earlier and
+// b) collect usage statistics to help improve Clang coverage design.
+bool AddressSanitizer::InjectCoverage(Function &F,
+ const ArrayRef<BasicBlock *> AllBlocks) {
+ if (!ClCoverage) return false;
+
+ if (ClCoverage == 1) {
+ InjectCoverageAtBlock(F, F.getEntryBlock());
+ } else {
+ for (size_t i = 0, n = AllBlocks.size(); i < n; i++)
+ InjectCoverageAtBlock(F, *AllBlocks[i]);
+ }
return true;
}
SmallSet<Value*, 16> TempsToInstrument;
SmallVector<Instruction*, 16> ToInstrument;
SmallVector<Instruction*, 8> NoReturnCalls;
+ SmallVector<BasicBlock*, 16> AllBlocks;
int NumAllocas = 0;
bool IsWrite;
// Fill the set of memory operations to instrument.
for (Function::iterator FI = F.begin(), FE = F.end();
FI != FE; ++FI) {
+ AllBlocks.push_back(FI);
TempsToInstrument.clear();
int NumInsnsPerBB = 0;
for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
bool res = NumInstrumented > 0 || ChangedStack || !NoReturnCalls.empty();
- if (InjectCoverage(F))
+ if (InjectCoverage(F, AllBlocks))
res = true;
DEBUG(dbgs() << "ASAN done instrumenting: " << res << " " << F << "\n");
diff --git a/test/Instrumentation/AddressSanitizer/coverage.ll b/test/Instrumentation/AddressSanitizer/coverage.ll
index 47a54c0ef85e7cb29c115f0d872ad8ffcf41eab3..6697f4b0f24aa93c7bfadbdc5897abf3704af068 100644 (file)
-; RUN: opt < %s -asan -asan-coverage=1 -S | FileCheck %s
+; RUN: opt < %s -asan -asan-coverage=1 -S | FileCheck %s --check-prefix=CHECK1
+; RUN: opt < %s -asan -asan-coverage=2 -S | FileCheck %s --check-prefix=CHECK2
target datalayout = "e-p:64:64:64-i1:8:8-i8:8:8-i16:16:16-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v64:64:64-v128:128:128-a0:0:64-s0:64:64-f80:128:128-n8:16:32:64"
target triple = "x86_64-unknown-linux-gnu"
-define i32 @foo(i32* %a) sanitize_address {
+define void @foo(i32* %a) sanitize_address {
entry:
- ret i32 0
+ %tobool = icmp eq i32* %a, null
+ br i1 %tobool, label %if.end, label %if.then
+
+ if.then: ; preds = %entry
+ store i32 0, i32* %a, align 4
+ br label %if.end
+
+ if.end: ; preds = %entry, %if.then
+ ret void
}
-; CHECK: define i32 @foo(i32* %a) #0 {
-; CHECK: %0 = load atomic i8* @__asan_gen_cov_foo monotonic, align 1
-; CHECK: %1 = icmp eq i8 0, %0
-; CHECK: br i1 %1, label %2, label %3
-; CHECK: call void @__sanitizer_cov(i64 ptrtoint (i32 (i32*)* @foo to i64))
-; CHECK: store atomic i8 1, i8* @__asan_gen_cov_foo monotonic, align 1
+; CHECK1-LABEL: define void @foo
+; CHECK1: %0 = load atomic i8* @__asan_gen_cov_foo monotonic, align 1
+; CHECK1: %1 = icmp eq i8 0, %0
+; CHECK1: br i1 %1, label %2, label %3
+; CHECK1: call void @__sanitizer_cov
+; CHECK1-NOT: call void @__sanitizer_cov
+; CHECK1: store atomic i8 1, i8* @__asan_gen_cov_foo monotonic, align 1
+
+; CHECK2-LABEL: define void @foo
+; CHECK2: call void @__sanitizer_cov
+; CHECK2: call void @__sanitizer_cov
+; CHECK2: call void @__sanitizer_cov
+; CHECK2-NOT: call void @__sanitizer_cov
+; CHECK2: ret void