summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 09a6371)
raw | patch | inline | side by side (parent: 09a6371)
author | Alexander Potapenko <glider@google.com> | |
Wed, 25 Dec 2013 14:22:15 +0000 (14:22 +0000) | ||
committer | Alexander Potapenko <glider@google.com> | |
Wed, 25 Dec 2013 14:22:15 +0000 (14:22 +0000) |
This should fix http://llvm.org/bugs/show_bug.cgi?id=17976
Another test checking for the global variables' locations and prefixes on Darwin will be committed separately.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@198017 91177308-0d34-0410-b5e6-96231b3b80d8
Another test checking for the global variables' locations and prefixes on Darwin will be committed separately.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@198017 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/Instrumentation/AddressSanitizer.cpp | patch | blob | history |
diff --git a/lib/Transforms/Instrumentation/AddressSanitizer.cpp b/lib/Transforms/Instrumentation/AddressSanitizer.cpp
index 17c3c58e9d60406e97b9822aa3fe144600cef820..72825f5f6f4260a31d8fde018e3d095cf9552e80 100644 (file)
}
// \brief Create a constant for Str so that we can pass it to the run-time lib.
-static GlobalVariable *createPrivateGlobalForString(Module &M, StringRef Str) {
+static GlobalVariable *createPrivateGlobalForString(
+ Module &M, StringRef Str, bool AllowMerging) {
Constant *StrConst = ConstantDataArray::getString(M.getContext(), Str);
- GlobalVariable *GV = new GlobalVariable(M, StrConst->getType(), true,
- GlobalValue::InternalLinkage, StrConst,
- kAsanGenPrefix);
- GV->setUnnamedAddr(true); // Ok to merge these.
+ // For module-local strings that can be merged with another one we set the
+ // internal linkage and the unnamed_addr attribute.
+ // Non-mergeable strings are made linker_private to remove them from the
+ // symbol table. "private" linkage doesn't work for Darwin, where the
+ // "L"-prefixed globals end up in __TEXT,__const section
+ // (see http://llvm.org/bugs/show_bug.cgi?id=17976 for more info).
+ GlobalValue::LinkageTypes linkage =
+ AllowMerging ? GlobalValue::InternalLinkage
+ : GlobalValue::LinkerPrivateLinkage;
+ GlobalVariable *GV =
+ new GlobalVariable(M, StrConst->getType(), true,
+ linkage, StrConst, kAsanGenPrefix);
+ if (AllowMerging) GV->setUnnamedAddr(true);
GV->setAlignment(1); // Strings may not be merged w/o setting align 1.
return GV;
}
bool HasDynamicallyInitializedGlobals = false;
- GlobalVariable *ModuleName = createPrivateGlobalForString(
- M, M.getModuleIdentifier());
// We shouldn't merge same module names, as this string serves as unique
// module ID in runtime.
- ModuleName->setUnnamedAddr(false);
+ GlobalVariable *ModuleName = createPrivateGlobalForString(
+ M, M.getModuleIdentifier(), /*AllowMerging*/false);
for (size_t i = 0; i < n; i++) {
static const uint64_t kMaxGlobalRedzone = 1 << 18;
NewTy, G->getInitializer(),
Constant::getNullValue(RightRedZoneTy), NULL);
- GlobalVariable *Name = createPrivateGlobalForString(M, G->getName());
+ GlobalVariable *Name =
+ createPrivateGlobalForString(M, G->getName(), /*AllowMerging*/true);
// Create a new global variable with enough space for a redzone.
GlobalValue::LinkageTypes Linkage = G->getLinkage();
IRB.CreateAdd(LocalStackBase, ConstantInt::get(IntptrTy, ASan.LongSize/8)),
IntptrPtrTy);
GlobalVariable *StackDescriptionGlobal =
- createPrivateGlobalForString(*F.getParent(), L.DescriptionString);
+ createPrivateGlobalForString(*F.getParent(), L.DescriptionString,
+ /*AllowMerging*/true);
Value *Description = IRB.CreatePointerCast(StackDescriptionGlobal,
IntptrTy);
IRB.CreateStore(Description, BasePlus1);