summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2131eb4)
raw | patch | inline | side by side (parent: 2131eb4)
author | Jakob Stoklund Olesen <stoklund@2pi.dk> | |
Sun, 16 Sep 2012 02:15:36 +0000 (02:15 +0000) | ||
committer | Jakob Stoklund Olesen <stoklund@2pi.dk> | |
Sun, 16 Sep 2012 02:15:36 +0000 (02:15 +0000) |
The live range of an SSA value forms a sub-tree of the dominator tree.
That means the live ranges of two values overlap if and only if the def
of one value lies within the live range of the other.
This can be used to simplify the interference checking a bit: Visit each
def in the two registers about to be joined. Check for interference
against the value that is live in the other register at the def point
only. It is not necessary to scan the set of overlapping live ranges,
this interference check can be done while computing the value mapping
required for the final live range join.
The new algorithm is prepared to handle more complicated conflict
resolution - We can allow overlapping live ranges with different values
as long as the differing lanes are undef or unused in the other
register.
The implementation in this patch doesn't do that yet, it creates code
that is nearly identical to the old algorithm's, except:
- The new stripCopies() function sees through multiple copies while
the old RegistersDefinedFromSameValue() only can handle one.
- There are a few rare cases where the new algorithm can erase an
IMPLICIT_DEF instuction that RegistersDefinedFromSameValue() couldn't
handle.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@163991 91177308-0d34-0410-b5e6-96231b3b80d8
That means the live ranges of two values overlap if and only if the def
of one value lies within the live range of the other.
This can be used to simplify the interference checking a bit: Visit each
def in the two registers about to be joined. Check for interference
against the value that is live in the other register at the def point
only. It is not necessary to scan the set of overlapping live ranges,
this interference check can be done while computing the value mapping
required for the final live range join.
The new algorithm is prepared to handle more complicated conflict
resolution - We can allow overlapping live ranges with different values
as long as the differing lanes are undef or unused in the other
register.
The implementation in this patch doesn't do that yet, it creates code
that is nearly identical to the old algorithm's, except:
- The new stripCopies() function sees through multiple copies while
the old RegistersDefinedFromSameValue() only can handle one.
- There are a few rare cases where the new algorithm can erase an
IMPLICIT_DEF instuction that RegistersDefinedFromSameValue() couldn't
handle.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@163991 91177308-0d34-0410-b5e6-96231b3b80d8
lib/CodeGen/RegisterCoalescer.cpp | patch | blob | history |
index f8165d3fe08611a6a2581373b08dd989c385c4df..85a62b26458945815d8027fcab0699b6e0c3a49a 100644 (file)
cl::desc("Verify machine instrs before and after register coalescing"),
cl::Hidden);
+// Temporary option for testing new coalescer algo.
+static cl::opt<bool>
+NewCoalescer("new-coalescer", cl::Hidden,
+ cl::desc("Use new coalescer algorithm"));
+
namespace {
class RegisterCoalescer : public MachineFunctionPass,
private LiveRangeEdit::Delegate {
/// can use this information below to update aliases.
bool joinIntervals(CoalescerPair &CP);
+ /// Attempt joining two virtual registers. Return true on success.
+ bool joinVirtRegs(CoalescerPair &CP);
+
/// Attempt joining with a reserved physreg.
bool joinReservedPhysReg(CoalescerPair &CP);
return true;
}
+//===----------------------------------------------------------------------===//
+// Interference checking and interval joining
+//===----------------------------------------------------------------------===//
+//
+// In the easiest case, the two live ranges being joined are disjoint, and
+// there is no interference to consider. It is quite common, though, to have
+// overlapping live ranges, and we need to check if the interference can be
+// resolved.
+//
+// The live range of a single SSA value forms a sub-tree of the dominator tree.
+// This means that two SSA values overlap if and only if the def of one value
+// is contained in the live range of the other value. As a special case, the
+// overlapping values can be defined at the same index.
+//
+// The interference from an overlapping def can be resolved in these cases:
+//
+// 1. Coalescable copies. The value is defined by a copy that would become an
+// identity copy after joining SrcReg and DstReg. The copy instruction will
+// be removed, and the value will be merged with the source value.
+//
+// There can be several copies back and forth, causing many values to be
+// merged into one. We compute a list of ultimate values in the joined live
+// range as well as a mappings from the old value numbers.
+//
+// 2. IMPLICIT_DEF. This instruction is only inserted to ensure all PHI
+// predecessors have a live out value. It doesn't cause real interference,
+// and can be merged into the value it overlaps. Like a coalescable copy, it
+// can be erased after joining.
+//
+// 3. Copy of external value. The overlapping def may be a copy of a value that
+// is already in the other register. This is like a coalescable copy, but
+// the live range of the source register must be trimmed after erasing the
+// copy instruction:
+//
+// %src = COPY %ext
+// %dst = COPY %ext <-- Remove this COPY, trim the live range of %ext.
+//
+// 4. Clobbering undefined lanes. Vector registers are sometimes built by
+// defining one lane at a time:
+//
+// %dst:ssub0<def,read-undef> = FOO
+// %src = BAR
+// %dst:ssub1<def> = COPY %src
+//
+// The live range of %src overlaps the %dst value defined by FOO, but
+// merging %src into %dst:ssub1 is only going to clobber the ssub1 lane
+// which was undef anyway.
+//
+// The value mapping is more complicated in this case. The final live range
+// will have different value numbers for both FOO and BAR, but there is no
+// simple mapping from old to new values. It may even be necessary to add
+// new PHI values.
+//
+// 5. Clobbering dead lanes. A def may clobber a lane of a vector register that
+// is live, but never read. This can happen because we don't compute
+// individual live ranges per lane.
+//
+// %dst<def> = FOO
+// %src = BAR
+// %dst:ssub1<def> = COPY %src
+//
+// This kind of interference is only resolved locally. If the clobbered
+// lane value escapes the block, the join is aborted.
+
+namespace {
+/// Track information about values in a single virtual register about to be
+/// joined. Objects of this class are always created in pairs - one for each
+/// side of the CoalescerPair.
+class JoinVals {
+ LiveInterval &LI;
+
+ // Location of this register in the final joined register.
+ // Either CP.DstIdx or CP.SrcIdx.
+ unsigned SubIdx;
+
+ // Values that will be present in the final live range.
+ SmallVectorImpl<VNInfo*> &NewVNInfo;
+
+ const CoalescerPair &CP;
+ LiveIntervals *LIS;
+ SlotIndexes *Indexes;
+ const TargetRegisterInfo *TRI;
+
+ // Value number assignments. Maps value numbers in LI to entries in NewVNInfo.
+ // This is suitable for passing to LiveInterval::join().
+ SmallVector<int, 8> Assignments;
+
+ // Conflict resolution for overlapping values.
+ enum ConflictResolution {
+ // No overlap, simply keep this value.
+ CR_Keep,
+
+ // Merge this value into OtherVNI and erase the defining instruction.
+ // Used for IMPLICIT_DEF, coalescable copies, and copies from external
+ // values.
+ CR_Erase,
+
+ // Merge this value into OtherVNI but keep the defining instruction.
+ // This is for the special case where OtherVNI is defined by the same
+ // instruction.
+ CR_Merge,
+
+ // Keep this value, and have it replace OtherVNI where possible. This
+ // complicates value mapping since OtherVNI maps to two different values
+ // before and after this def.
+ // Used when clobbering undefined or dead lanes.
+ CR_Replace,
+
+ // Unresolved conflict. Visit later when all values have been mapped.
+ CR_Unresolved,
+
+ // Unresolvable conflict. Abort the join.
+ CR_Impossible
+ };
+
+ // Per-value info for LI. The lane bit masks are all relative to the final
+ // joined register, so they can be compared directly between SrcReg and
+ // DstReg.
+ struct Val {
+ ConflictResolution Resolution;
+
+ // Lanes written by this def, 0 for unanalyzed values.
+ unsigned WriteLanes;
+
+ // Lanes with defined values in this register. Other lanes are undef and
+ // safe to clobber.
+ unsigned ValidLanes;
+
+ // Value in LI being redefined by this def.
+ VNInfo *RedefVNI;
+
+ // Value in the other live range that overlaps this def, if any.
+ VNInfo *OtherVNI;
+
+ Val() : Resolution(CR_Keep), WriteLanes(0), ValidLanes(0),
+ RedefVNI(0), OtherVNI(0) {}
+
+ bool isAnalyzed() const { return WriteLanes != 0; }
+ };
+
+ // One entry per value number in LI.
+ SmallVector<Val, 8> Vals;
+
+ unsigned computeWriteLanes(const MachineInstr *DefMI, bool &Redef);
+ VNInfo *stripCopies(VNInfo *VNI);
+ ConflictResolution analyzeValue(unsigned ValNo, JoinVals &Other);
+ void computeAssignment(unsigned ValNo, JoinVals &Other);
+
+public:
+ JoinVals(LiveInterval &li, unsigned subIdx,
+ SmallVectorImpl<VNInfo*> &newVNInfo,
+ const CoalescerPair &cp,
+ LiveIntervals *lis,
+ const TargetRegisterInfo *tri)
+ : LI(li), SubIdx(subIdx), NewVNInfo(newVNInfo), CP(cp), LIS(lis),
+ Indexes(LIS->getSlotIndexes()), TRI(tri),
+ Assignments(LI.getNumValNums(), -1), Vals(LI.getNumValNums())
+ {}
+
+ /// Analyze defs in LI and compute a value mapping in NewVNInfo.
+ /// Returns false if any conflicts were impossible to resolve.
+ bool mapValues(JoinVals &Other);
+
+ /// Try to resolve conflicts that require all values to be mapped.
+ /// Returns false if any conflicts were impossible to resolve.
+ bool resolveConflicts(JoinVals &Other);
+
+ /// Erase any machine instructions that have been coalesced away.
+ /// Add erased instructions to ErasedInstrs.
+ /// Add foreign virtual registers to ShrinkRegs if their live range ended at
+ /// the erased instrs.
+ void eraseInstrs(SmallPtrSet<MachineInstr*, 8> &ErasedInstrs,
+ SmallVectorImpl<unsigned> &ShrinkRegs);
+
+ /// Get the value assignments suitable for passing to LiveInterval::join.
+ const int *getAssignments() const { return &Assignments[0]; }
+};
+} // end anonymous namespace
+
+/// Compute the bitmask of lanes actually written by DefMI.
+/// Set Redef if there are any partial register definitions that depend on the
+/// previous value of the register.
+unsigned JoinVals::computeWriteLanes(const MachineInstr *DefMI, bool &Redef) {
+ unsigned L = 0;
+ for (ConstMIOperands MO(DefMI); MO.isValid(); ++MO) {
+ if (!MO->isReg() || MO->getReg() != LI.reg || !MO->isDef())
+ continue;
+ L |= TRI->getSubRegIndexLaneMask(compose(*TRI, SubIdx, MO->getSubReg()));
+ if (MO->readsReg())
+ Redef = true;
+ }
+ return L;
+}
+
+/// Find the ultimate value that VNI was copied from.
+VNInfo *JoinVals::stripCopies(VNInfo *VNI) {
+ while (!VNI->isPHIDef()) {
+ MachineInstr *MI = Indexes->getInstructionFromIndex(VNI->def);
+ assert(MI && "No defining instruction");
+ if (!MI->isFullCopy())
+ break;
+ unsigned Reg = MI->getOperand(1).getReg();
+ if (!TargetRegisterInfo::isVirtualRegister(Reg))
+ break;
+ LiveRangeQuery LRQ(LIS->getInterval(Reg), VNI->def);
+ if (!LRQ.valueIn())
+ break;
+ VNI = LRQ.valueIn();
+ }
+ return VNI;
+}
+
+/// Analyze ValNo in this live range, and set all fields of Vals[ValNo].
+/// Return a conflict resolution when possible, but leave the hard cases as
+/// CR_Unresolved.
+/// Recursively calls computeAssignment() on this and Other, guaranteeing that
+/// both OtherVNI and RedefVNI have been analyzed and mapped before returning.
+/// The recursion always goes upwards in the dominator tree, making loops
+/// impossible.
+JoinVals::ConflictResolution
+JoinVals::analyzeValue(unsigned ValNo, JoinVals &Other) {
+ Val &V = Vals[ValNo];
+ assert(!V.isAnalyzed() && "Value has already been analyzed!");
+ VNInfo *VNI = LI.getValNumInfo(ValNo);
+ if (VNI->isUnused()) {
+ V.WriteLanes = ~0u;
+ return CR_Keep;
+ }
+
+ // Get the instruction defining this value, compute the lanes written.
+ const MachineInstr *DefMI = 0;
+ if (VNI->isPHIDef()) {
+ // Conservatively assume that all lanes in a PHI are valid.
+ V.ValidLanes = V.WriteLanes = TRI->getSubRegIndexLaneMask(SubIdx);
+ } else {
+ DefMI = Indexes->getInstructionFromIndex(VNI->def);
+ bool Redef = false;
+ V.ValidLanes = V.WriteLanes = computeWriteLanes(DefMI, Redef);
+
+ // If this is a read-modify-write instruction, there may be more valid
+ // lanes than the ones written by this instruction.
+ // This only covers partial redef operands. DefMI may have normal use
+ // operands reading the register. They don't contribute valid lanes.
+ //
+ // This adds ssub1 to the set of valid lanes in %src:
+ //
+ // %src:ssub1<def> = FOO
+ //
+ // This leaves only ssub1 valid, making any other lanes undef:
+ //
+ // %src:ssub1<def,read-undef> = FOO %src:ssub2
+ //
+ // The <read-undef> flag on the def operand means that old lane values are
+ // not important.
+ if (Redef) {
+ V.RedefVNI = LiveRangeQuery(LI, VNI->def).valueIn();
+ assert(V.RedefVNI && "Instruction is reading nonexistent value");
+ computeAssignment(V.RedefVNI->id, Other);
+ V.ValidLanes |= Vals[V.RedefVNI->id].ValidLanes;
+ }
+
+ // An IMPLICIT_DEF writes undef values.
+ if (DefMI->isImplicitDef())
+ V.ValidLanes &= ~V.WriteLanes;
+ }
+
+ // Find the value in Other that overlaps VNI->def, if any.
+ LiveRangeQuery OtherLRQ(Other.LI, VNI->def);
+
+ // It is possible that both values are defined by the same instruction, or
+ // the values are PHIs defined in the same block. When that happens, the two
+ // values should be merged into one, but not into any preceding value.
+ // The first value defined or visited gets CR_Keep, the other gets CR_Merge.
+ if (VNInfo *OtherVNI = OtherLRQ.valueDefined()) {
+ DEBUG(dbgs() << "\t\tDouble def: " << VNI->def << '\n');
+ assert(SlotIndex::isSameInstr(VNI->def, OtherVNI->def) && "Broken LRQ");
+
+ // One value stays, the other is merged. Keep the earlier one, or the first
+ // one we see.
+ if (OtherVNI->def < VNI->def)
+ Other.computeAssignment(OtherVNI->id, *this);
+ else if (VNI->def < OtherVNI->def && OtherLRQ.valueIn()) {
+ // This is an early-clobber def overlapping a live-in value in the other
+ // register. Not mergeable.
+ V.OtherVNI = OtherLRQ.valueIn();
+ return CR_Impossible;
+ }
+ V.OtherVNI = OtherVNI;
+ Val &OtherV = Other.Vals[OtherVNI->id];
+ // Keep this value, check for conflicts when analyzing OtherVNI.
+ if (!OtherV.isAnalyzed())
+ return CR_Keep;
+ // Both sides have been analyzed now. Do they conflict?
+ if (V.ValidLanes & OtherV.ValidLanes)
+ // Overlapping lanes can't be resolved now, maybe later.
+ return CR_Unresolved;
+ else
+ return CR_Merge;
+ }
+
+ // No simultaneous def. Is Other live at the def?
+ V.OtherVNI = OtherLRQ.valueIn();
+ if (!V.OtherVNI)
+ // No overlap, no conflict.
+ return CR_Keep;
+
+ assert(!SlotIndex::isSameInstr(VNI->def, V.OtherVNI->def) && "Broken LRQ");
+
+ // We have overlapping values, or possibly a kill of Other.
+ // Recursively compute assignments up the dominator tree.
+ Other.computeAssignment(V.OtherVNI->id, *this);
+
+ // Don't attempt resolving PHI values for now.
+ if (VNI->isPHIDef())
+ return CR_Impossible;
+
+ // Check for simple erasable conflicts.
+ if (DefMI->isImplicitDef())
+ return CR_Erase;
+
+ // Include the non-conflict where DefMI is a coalescable copy that kills
+ // OtherVNI. We still want the copy erased and value numbers merged.
+ if (CP.isCoalescable(DefMI)) {
+ // Some of the lanes copied from OtherVNI may be undef, making them undef
+ // here too.
+ V.ValidLanes &= ~V.WriteLanes | Other.Vals[V.OtherVNI->id].ValidLanes;
+ return CR_Erase;
+ }
+
+ // This may not be a real conflict if DefMI simply kills Other and defines
+ // VNI.
+ if (OtherLRQ.isKill() && OtherLRQ.endPoint() <= VNI->def)
+ return CR_Keep;
+
+ // Handle the case where VNI and OtherVNI can be proven to be identical:
+ //
+ // %other = COPY %ext
+ // %this = COPY %ext <-- Erase this copy
+ //
+ if (DefMI->isFullCopy() && !CP.isPartial() &&
+ stripCopies(VNI) == stripCopies(V.OtherVNI))
+ return CR_Erase;
+
+ // FIXME: Identify CR_Replace opportunities.
+ return CR_Impossible;
+}
+
+/// Compute the value assignment for ValNo in LI.
+/// This may be called recursively by analyzeValue(), but never for a ValNo on
+/// the stack.
+void JoinVals::computeAssignment(unsigned ValNo, JoinVals &Other) {
+ Val &V = Vals[ValNo];
+ if (V.isAnalyzed()) {
+ // Recursion should always move up the dominator tree, so ValNo is not
+ // supposed to reappear before it has been assigned.
+ assert(Assignments[ValNo] != -1 && "Bad recursion?");
+ return;
+ }
+ switch ((V.Resolution = analyzeValue(ValNo, Other))) {
+ case CR_Erase:
+ case CR_Merge:
+ // Merge this ValNo into OtherVNI.
+ assert(V.OtherVNI && "OtherVNI not assigned, can't merge.");
+ assert(Other.Vals[V.OtherVNI->id].isAnalyzed() && "Missing recursion");
+ Assignments[ValNo] = Other.Assignments[V.OtherVNI->id];
+ DEBUG(dbgs() << "\t\tmerge " << PrintReg(LI.reg) << ':' << ValNo << '@'
+ << LI.getValNumInfo(ValNo)->def << " into "
+ << PrintReg(Other.LI.reg) << ':' << V.OtherVNI->id << '@'
+ << V.OtherVNI->def << " --> @"
+ << NewVNInfo[Assignments[ValNo]]->def << '\n');
+ break;
+ default:
+ // This value number needs to go in the final joined live range.
+ Assignments[ValNo] = NewVNInfo.size();
+ NewVNInfo.push_back(LI.getValNumInfo(ValNo));
+ break;
+ }
+}
+
+bool JoinVals::mapValues(JoinVals &Other) {
+ for (unsigned i = 0, e = LI.getNumValNums(); i != e; ++i) {
+ computeAssignment(i, Other);
+ if (Vals[i].Resolution == CR_Impossible) {
+ DEBUG(dbgs() << "\t\tinterference at " << PrintReg(LI.reg) << ':' << i
+ << '@' << LI.getValNumInfo(i)->def << '\n');
+ return false;
+ }
+ }
+ return true;
+}
+
+bool JoinVals::resolveConflicts(JoinVals &Other) {
+ for (unsigned i = 0, e = LI.getNumValNums(); i != e; ++i) {
+ assert (Vals[i].Resolution != CR_Impossible && "Unresolvable conflict");
+ if (Vals[i].Resolution != CR_Unresolved)
+ continue;
+ // FIXME: Actually resolve dead lane conflicts.
+ DEBUG(dbgs() << "\t\tconflict at " << PrintReg(LI.reg) << ':' << i
+ << '@' << LI.getValNumInfo(i)->def << '\n');
+ return false;
+ }
+ return true;
+}
+
+void JoinVals::eraseInstrs(SmallPtrSet<MachineInstr*, 8> &ErasedInstrs,
+ SmallVectorImpl<unsigned> &ShrinkRegs) {
+ for (unsigned i = 0, e = LI.getNumValNums(); i != e; ++i) {
+ if (Vals[i].Resolution != CR_Erase)
+ continue;
+ SlotIndex Def = LI.getValNumInfo(i)->def;
+ MachineInstr *MI = Indexes->getInstructionFromIndex(Def);
+ assert(MI && "No instruction to erase");
+ if (MI->isCopy()) {
+ unsigned Reg = MI->getOperand(1).getReg();
+ if (TargetRegisterInfo::isVirtualRegister(Reg) &&
+ Reg != CP.getSrcReg() && Reg != CP.getDstReg())
+ ShrinkRegs.push_back(Reg);
+ }
+ ErasedInstrs.insert(MI);
+ DEBUG(dbgs() << "\t\terased:\t" << Def << '\t' << *MI);
+ LIS->RemoveMachineInstrFromMaps(MI);
+ MI->eraseFromParent();
+ }
+}
+
+bool RegisterCoalescer::joinVirtRegs(CoalescerPair &CP) {
+ SmallVector<VNInfo*, 16> NewVNInfo;
+ LiveInterval &RHS = LIS->getInterval(CP.getSrcReg());
+ LiveInterval &LHS = LIS->getInterval(CP.getDstReg());
+ JoinVals RHSVals(RHS, CP.getSrcIdx(), NewVNInfo, CP, LIS, TRI);
+ JoinVals LHSVals(LHS, CP.getDstIdx(), NewVNInfo, CP, LIS, TRI);
+
+ DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
+ << "\n\t\tLHS = " << PrintReg(CP.getDstReg()) << ' ' << LHS
+ << '\n');
+
+ // First compute NewVNInfo and the simple value mappings.
+ // Detect impossible conflicts early.
+ if (!LHSVals.mapValues(RHSVals) || !RHSVals.mapValues(LHSVals))
+ return false;
+
+ // Some conflicts can only be resolved after all values have been mapped.
+ if (!LHSVals.resolveConflicts(RHSVals) || !RHSVals.resolveConflicts(LHSVals))
+ return false;
+
+ // All clear, the live ranges can be merged.
+
+ // Erase COPY and IMPLICIT_DEF instructions. This may cause some external
+ // registers to require trimming.
+ SmallVector<unsigned, 8> ShrinkRegs;
+ LHSVals.eraseInstrs(ErasedInstrs, ShrinkRegs);
+ RHSVals.eraseInstrs(ErasedInstrs, ShrinkRegs);
+ while (!ShrinkRegs.empty())
+ LIS->shrinkToUses(&LIS->getInterval(ShrinkRegs.pop_back_val()));
+
+ // Join RHS into LHS.
+ LHS.join(RHS, LHSVals.getAssignments(), RHSVals.getAssignments(), NewVNInfo,
+ MRI);
+
+ // Kill flags are going to be wrong if the live ranges were overlapping.
+ // Eventually, we should simply clear all kill flags when computing live
+ // ranges. They are reinserted after register allocation.
+ MRI->clearKillFlags(LHS.reg);
+ MRI->clearKillFlags(RHS.reg);
+ return true;
+}
+
/// ComputeUltimateVN - Assuming we are going to join two live intervals,
/// compute what the resultant value numbers for each value in the input two
/// ranges will be. This is complicated by copies between the two which can
if (CP.isPhys())
return joinReservedPhysReg(CP);
+ if (NewCoalescer)
+ return joinVirtRegs(CP);
+
LiveInterval &RHS = LIS->getInterval(CP.getSrcReg());
DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
<< '\n');