summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2e46e78)
raw | patch | inline | side by side (parent: 2e46e78)
author | Owen Anderson <resistor@mac.com> | |
Tue, 31 Aug 2010 04:41:06 +0000 (04:41 +0000) | ||
committer | Owen Anderson <resistor@mac.com> | |
Tue, 31 Aug 2010 04:41:06 +0000 (04:41 +0000) |
fixable at the optimizer level. I'll investigate reimplementing it in DAGCombine.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@112575 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@112575 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Transforms/InstCombine/InstCombineLoadStoreAlloca.cpp | patch | blob | history | |
test/Transforms/InstCombine/2010-08-19-StoreNarrowing.ll | [deleted file] | patch | blob | history |
diff --git a/lib/Transforms/InstCombine/InstCombineLoadStoreAlloca.cpp b/lib/Transforms/InstCombine/InstCombineLoadStoreAlloca.cpp
index 87533d3fe2e9c1295d44a88b1708572c654f8b74..b68fbc2db5c9a6c92f5b8f641cfbc3059ebbe713 100644 (file)
#include "InstCombine.h"
#include "llvm/IntrinsicInst.h"
#include "llvm/Analysis/Loads.h"
-#include "llvm/Support/PatternMatch.h"
#include "llvm/Target/TargetData.h"
#include "llvm/Transforms/Utils/BasicBlockUtils.h"
#include "llvm/Transforms/Utils/Local.h"
#include "llvm/ADT/Statistic.h"
using namespace llvm;
-using namespace PatternMatch;
STATISTIC(NumDeadStore, "Number of dead stores eliminated");
if (SI.isVolatile()) return 0; // Don't hack volatile stores.
- // Attempt to narrow sequences where we load a wide value, perform bitmasks
- // that only affect the low bits of it, and then store it back. This
- // typically arises from bitfield initializers in C++.
- ConstantInt *CI1 =0, *CI2 = 0;
- Value *Ld = 0;
- if (getTargetData() &&
- match(SI.getValueOperand(),
- m_And(m_Or(m_Value(Ld), m_ConstantInt(CI1)), m_ConstantInt(CI2))) &&
- isa<LoadInst>(Ld) &&
- equivalentAddressValues(cast<LoadInst>(Ld)->getPointerOperand(), Ptr)) {
- APInt OrMask = CI1->getValue();
- APInt AndMask = CI2->getValue();
-
- // Compute the prefix of the value that is unmodified by the bitmasking.
- unsigned LeadingAndOnes = AndMask.countLeadingOnes();
- unsigned LeadingOrZeros = OrMask.countLeadingZeros();
- unsigned Prefix = std::min(LeadingAndOnes, LeadingOrZeros);
- uint64_t NewWidth = AndMask.getBitWidth() - Prefix;
- while (NewWidth < AndMask.getBitWidth() &&
- getTargetData()->isIllegalInteger(NewWidth))
- NewWidth = NextPowerOf2(NewWidth);
-
- // If we can find a power-of-2 prefix (and if the values we're working with
- // are themselves POT widths), then we can narrow the store. We rely on
- // later iterations of instcombine to propagate the demanded bits to narrow
- // the other computations in the chain.
- if (NewWidth < AndMask.getBitWidth() &&
- getTargetData()->isLegalInteger(NewWidth)) {
- const Type *NewType = IntegerType::get(Ptr->getContext(), NewWidth);
- const Type *NewPtrType = PointerType::getUnqual(NewType);
-
- Value *NewVal = Builder->CreateTrunc(SI.getValueOperand(), NewType);
- Value *NewPtr = Builder->CreateBitCast(Ptr, NewPtrType);
-
- // On big endian targets, we need to offset from the original pointer
- // in order to store to the low-bit suffix.
- if (getTargetData()->isBigEndian()) {
- uint64_t GEPOffset = (AndMask.getBitWidth() - NewWidth) / 8;
- NewPtr = Builder->CreateConstGEP1_64(NewPtr, GEPOffset);
- }
-
- return new StoreInst(NewVal, NewPtr);
- }
- }
-
// store X, null -> turns into 'unreachable' in SimplifyCFG
if (isa<ConstantPointerNull>(Ptr) && SI.getPointerAddressSpace() == 0) {
if (!isa<UndefValue>(Val)) {
diff --git a/test/Transforms/InstCombine/2010-08-19-StoreNarrowing.ll b/test/Transforms/InstCombine/2010-08-19-StoreNarrowing.ll
+++ /dev/null
@@ -1,21 +0,0 @@
-; RUN: opt -S -instcombine %s | not grep and
-target datalayout = "e-p:64:64:64-i1:8:8-i8:8:8-i16:16:16-i32:32:32-i64:64:64-f32:32:32-f64:64:64-v64:64:64-v128:128:128-a0:0:64-s0:64:64-f80:128:128-n8:16:32:64"
-target triple = "x86_64-apple-darwin10.0.0"
-
-%class.A = type { i8, [3 x i8] }
-
-define void @_ZN1AC2Ev(%class.A* %this) nounwind ssp align 2 {
-entry:
- %0 = bitcast %class.A* %this to i32* ; <i32*> [#uses=5]
- %1 = load i32* %0, align 4 ; <i32> [#uses=1]
- %2 = and i32 %1, -8 ; <i32> [#uses=2]
- store i32 %2, i32* %0, align 4
- %3 = and i32 %2, -57 ; <i32> [#uses=1]
- %4 = or i32 %3, 8 ; <i32> [#uses=2]
- store i32 %4, i32* %0, align 4
- %5 = and i32 %4, -65 ; <i32> [#uses=2]
- store i32 %5, i32* %0, align 4
- %6 = and i32 %5, -129 ; <i32> [#uses=1]
- store i32 %6, i32* %0, align 4
- ret void
-}