summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 861e2ef)
raw | patch | inline | side by side (parent: 861e2ef)
author | Filipe Cabecinhas <me@filcab.net> | |
Mon, 19 May 2014 19:45:57 +0000 (19:45 +0000) | ||
committer | Filipe Cabecinhas <me@filcab.net> | |
Mon, 19 May 2014 19:45:57 +0000 (19:45 +0000) |
Summary:
When inserting an element that's coming from a vector load or a broadcast
of a vector (or scalar) load, combine the load into the insertps
instruction.
Added PerformINSERTPSCombine for the case where we need to fix the load
(load of a vector + insertps with a non-zero CountS).
Added patterns for the broadcasts.
Also added tests for SSE4.1, AVX, and AVX2.
Reviewers: delena, nadav, craig.topper
Subscribers: llvm-commits
Differential Revision: http://reviews.llvm.org/D3581
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209156 91177308-0d34-0410-b5e6-96231b3b80d8
When inserting an element that's coming from a vector load or a broadcast
of a vector (or scalar) load, combine the load into the insertps
instruction.
Added PerformINSERTPSCombine for the case where we need to fix the load
(load of a vector + insertps with a non-zero CountS).
Added patterns for the broadcasts.
Also added tests for SSE4.1, AVX, and AVX2.
Reviewers: delena, nadav, craig.topper
Subscribers: llvm-commits
Differential Revision: http://reviews.llvm.org/D3581
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209156 91177308-0d34-0410-b5e6-96231b3b80d8
index e1db618baf18b97f2390df141fe192f0c3d8f7ca..cfdaf0f8e3abe6fa3ff6d288fe87ef4413da9e85 100644 (file)
getShuffleSHUFImmediate(SVOp), DAG);
}
+static SDValue NarrowVectorLoadToElement(LoadSDNode *Load, unsigned Index,
+ SelectionDAG &DAG) {
+ SDLoc dl(Load);
+ MVT VT = Load->getSimpleValueType(0);
+ MVT EVT = VT.getVectorElementType();
+ SDValue Addr = Load->getOperand(1);
+ SDValue NewAddr = DAG.getNode(
+ ISD::ADD, dl, Addr.getSimpleValueType(), Addr,
+ DAG.getConstant(Index * EVT.getStoreSize(), Addr.getSimpleValueType()));
+
+ SDValue NewLoad =
+ DAG.getLoad(EVT, dl, Load->getChain(), NewAddr,
+ DAG.getMachineFunction().getMachineMemOperand(
+ Load->getMemOperand(), 0, EVT.getStoreSize()));
+ return NewLoad;
+}
+
// It is only safe to call this function if isINSERTPSMask is true for
// this shufflevector mask.
static SDValue getINSERTPS(ShuffleVectorSDNode *SVOp, SDLoc &dl,
// If we're transferring an i32 from memory to a specific element in a
// register, we output a generic DAG that will match the PINSRD
// instruction.
- // TODO: Optimize for AVX cases too (VINSERTPS)
MVT VT = SVOp->getSimpleValueType(0);
MVT EVT = VT.getVectorElementType();
SDValue V1 = SVOp->getOperand(0);
// Trivial case, when From comes from a load and is only used by the
// shuffle. Make it use insertps from the vector that we need from that
// load.
- SDValue Addr = From.getOperand(1);
- SDValue NewAddr =
- DAG.getNode(ISD::ADD, dl, Addr.getSimpleValueType(), Addr,
- DAG.getConstant(DestIndex * EVT.getStoreSize(),
- Addr.getSimpleValueType()));
-
- LoadSDNode *Load = cast<LoadSDNode>(From);
SDValue NewLoad =
- DAG.getLoad(EVT, dl, Load->getChain(), NewAddr,
- DAG.getMachineFunction().getMachineMemOperand(
- Load->getMemOperand(), 0, EVT.getStoreSize()));
+ NarrowVectorLoadToElement(cast<LoadSDNode>(From), DestIndex, DAG);
+ if (!NewLoad.getNode())
+ return SDValue();
if (EVT == MVT::f32) {
// Create this as a scalar to vector to match the instruction pattern.
return SDValue();
}
+static SDValue PerformINSERTPSCombine(SDNode *N, SelectionDAG &DAG,
+ const X86Subtarget *Subtarget) {
+ SDLoc dl(N);
+ MVT VT = N->getOperand(1)->getSimpleValueType(0);
+ assert(VT == MVT::v4f32 ||
+ VT == MVT::v4i32 && "X86insertps is only defined for v4x32");
+
+ SDValue Ld = N->getOperand(1);
+ if (MayFoldLoad(Ld)) {
+ // Extract the countS bits from the immediate so we can get the proper
+ // address when narrowing the vector load to a specific element.
+ // When the second source op is a memory address, interps doesn't use
+ // countS and just gets an f32 from that address.
+ unsigned DestIndex =
+ cast<ConstantSDNode>(N->getOperand(2))->getZExtValue() >> 6;
+ Ld = NarrowVectorLoadToElement(cast<LoadSDNode>(Ld), DestIndex, DAG);
+ } else
+ return SDValue();
+
+ // Create this as a scalar to vector to match the instruction pattern.
+ SDValue LoadScalarToVector = DAG.getNode(ISD::SCALAR_TO_VECTOR, dl, VT, Ld);
+ // countS bits are ignored when loading from memory on insertps, which
+ // means we don't need to explicitly set them to 0.
+ return DAG.getNode(X86ISD::INSERTPS, dl, VT, N->getOperand(0),
+ LoadScalarToVector, N->getOperand(2));
+}
+
// Helper function of PerformSETCCCombine. It is to materialize "setb reg"
// as "sbb reg,reg", since it can be extended without zext and produces
// an all-ones bit which is more useful than 0/1 in some cases.
case ISD::FMA: return PerformFMACombine(N, DAG, Subtarget);
case ISD::INTRINSIC_WO_CHAIN:
return PerformINTRINSIC_WO_CHAINCombine(N, DAG, Subtarget);
+ case X86ISD::INSERTPS:
+ return PerformINSERTPSCombine(N, DAG, Subtarget);
}
return SDValue();
index ac28d07cc683abd764c7bce66655c7249bc8f6a7..1eb04851b721719623e0b89c170bd708e8ec7d6a 100644 (file)
defm INSERTPS : SS41I_insertf32<0x21, "insertps", 1, SSE_INSERT_ITINS>;
}
+let Predicates = [UseSSE41] in {
+ // If we're inserting an element from a load or a null pshuf of a load,
+ // fold the load into the insertps instruction.
+ def : Pat<(v4f32 (X86insertps (v4f32 VR128:$src1), (X86PShufd (v4f32
+ (scalar_to_vector (loadf32 addr:$src2))), (i8 0)),
+ imm:$src3)),
+ (INSERTPSrm VR128:$src1, addr:$src2, imm:$src3)>;
+ def : Pat<(v4f32 (X86insertps (v4f32 VR128:$src1), (X86PShufd
+ (loadv4f32 addr:$src2), (i8 0)), imm:$src3)),
+ (INSERTPSrm VR128:$src1, addr:$src2, imm:$src3)>;
+}
+
+let Predicates = [UseAVX] in {
+ // If we're inserting an element from a vbroadcast of a load, fold the
+ // load into the X86insertps instruction.
+ def : Pat<(v4f32 (X86insertps (v4f32 VR128:$src1),
+ (X86VBroadcast (loadf32 addr:$src2)), imm:$src3)),
+ (VINSERTPSrm VR128:$src1, addr:$src2, imm:$src3)>;
+ def : Pat<(v4f32 (X86insertps (v4f32 VR128:$src1),
+ (X86VBroadcast (loadv4f32 addr:$src2)), imm:$src3)),
+ (VINSERTPSrm VR128:$src1, addr:$src2, imm:$src3)>;
+}
+
//===----------------------------------------------------------------------===//
// SSE4.1 - Round Instructions
//===----------------------------------------------------------------------===//
index 208e3844f11e05b541713a3807154dd09a360aee..6069c14f0d800f9d5d3a604222a459956e33074c 100644 (file)
--- a/test/CodeGen/X86/avx.ll
+++ b/test/CodeGen/X86/avx.ll
-; RUN: llc < %s -mtriple=x86_64-apple-darwin -mcpu=corei7-avx | FileCheck %s
+; RUN: llc < %s -mtriple=i686-apple-darwin -mcpu=corei7-avx | FileCheck %s -check-prefix=X32 --check-prefix=CHECK
+; RUN: llc < %s -mtriple=x86_64-apple-darwin -mcpu=corei7-avx | FileCheck %s -check-prefix=X64 --check-prefix=CHECK
define <4 x i32> @blendvb_fallback_v4i32(<4 x i1> %mask, <4 x i32> %x, <4 x i32> %y) {
; CHECK-LABEL: @blendvb_fallback_v4i32
%ret = select <8 x i1> %mask, <8 x float> %x, <8 x float> %y
ret <8 x float> %ret
}
+
+declare <4 x float> @llvm.x86.sse41.insertps(<4 x float>, <4 x float>, i32) nounwind readnone
+
+define <4 x float> @insertps_from_vector_load(<4 x float> %a, <4 x float>* nocapture readonly %pb) {
+; CHECK-LABEL: insertps_from_vector_load:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %pb, align 16
+ %2 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %1, i32 48)
+ ret <4 x float> %2
+}
+
+;; Use a non-zero CountS for insertps
+define <4 x float> @insertps_from_vector_load_offset(<4 x float> %a, <4 x float>* nocapture readonly %pb) {
+; CHECK-LABEL: insertps_from_vector_load_offset:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; CHECK-NOT: mov
+;; Try to match a bit more of the instr, since we need the load's offset.
+; CHECK: insertps $96, 4(%{{...}}), %
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %pb, align 16
+ %2 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %1, i32 96)
+ ret <4 x float> %2
+}
+
+define <4 x float> @insertps_from_vector_load_offset_2(<4 x float> %a, <4 x float>* nocapture readonly %pb, i64 %index) {
+; CHECK-LABEL: insertps_from_vector_load_offset_2:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; X32: movl 8(%esp), %ecx
+; CHECK-NOT: mov
+;; Try to match a bit more of the instr, since we need the load's offset.
+; CHECK: vinsertps $192, 12(%{{...}},%{{...}}), %
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds <4 x float>* %pb, i64 %index
+ %2 = load <4 x float>* %1, align 16
+ %3 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %2, i32 192)
+ ret <4 x float> %3
+}
+
+define <4 x float> @insertps_from_broadcast_loadf32(<4 x float> %a, float* nocapture readonly %fb, i64 %index) {
+; CHECK-LABEL: insertps_from_broadcast_loadf32:
+; On X32, account for the arguments' move to registers
+; X32: movl 8(%esp), %eax
+; X32: movl 4(%esp), %ecx
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds float* %fb, i64 %index
+ %2 = load float* %1, align 4
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ ret <4 x float> %7
+}
+
+define <4 x float> @insertps_from_broadcast_loadv4f32(<4 x float> %a, <4 x float>* nocapture readonly %b) {
+; CHECK-LABEL: insertps_from_broadcast_loadv4f32:
+; On X32, account for the arguments' move to registers
+; X32: movl 4(%esp), %{{...}}
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %b, align 4
+ %2 = extractelement <4 x float> %1, i32 0
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ ret <4 x float> %7
+}
+
+;; FIXME: We're emitting an extraneous pshufd/vbroadcast.
+define <4 x float> @insertps_from_broadcast_multiple_use(<4 x float> %a, <4 x float> %b, <4 x float> %c, <4 x float> %d, float* nocapture readonly %fb, i64 %index) {
+; CHECK-LABEL: insertps_from_broadcast_multiple_use:
+; On X32, account for the arguments' move to registers
+; X32: movl 8(%esp), %eax
+; X32: movl 4(%esp), %ecx
+; CHECK: vbroadcastss
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: vaddps
+; CHECK: vaddps
+; CHECK: vaddps
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds float* %fb, i64 %index
+ %2 = load float* %1, align 4
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ %8 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %b, <4 x float> %6, i32 48)
+ %9 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %c, <4 x float> %6, i32 48)
+ %10 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %d, <4 x float> %6, i32 48)
+ %11 = fadd <4 x float> %7, %8
+ %12 = fadd <4 x float> %9, %10
+ %13 = fadd <4 x float> %11, %12
+ ret <4 x float> %13
+}
index e85d8f78c0525fdcde3146584d5c1c134cd0f74f..96c5be4f752f72847cb949b3fdf3366d8718a410 100644 (file)
; loads from m32.
define void @sample_test(<4 x float>* %source, <2 x float>* %dest) nounwind {
; CHECK: sample_test
-; CHECK: movaps
+; CHECK-NOT: movaps
; CHECK: insertps
entry:
%source.addr = alloca <4 x float>*, align 8
index 3652d8c0d02292224d53d67b1b3c70c2ff83c162..a3c62016c436c89333b6d121392bfebb43f7a4a7 100644 (file)
@@ -584,3 +584,111 @@ define <8 x i16> @blendvb_fallback(<8 x i1> %mask, <8 x i16> %x, <8 x i16> %y) {
%ret = select <8 x i1> %mask, <8 x i16> %x, <8 x i16> %y
ret <8 x i16> %ret
}
+
+define <4 x float> @insertps_from_vector_load(<4 x float> %a, <4 x float>* nocapture readonly %pb) {
+; CHECK-LABEL: insertps_from_vector_load:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %pb, align 16
+ %2 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %1, i32 48)
+ ret <4 x float> %2
+}
+
+;; Use a non-zero CountS for insertps
+define <4 x float> @insertps_from_vector_load_offset(<4 x float> %a, <4 x float>* nocapture readonly %pb) {
+; CHECK-LABEL: insertps_from_vector_load_offset:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; CHECK-NOT: mov
+;; Try to match a bit more of the instr, since we need the load's offset.
+; CHECK: insertps $96, 4(%{{...}}), %
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %pb, align 16
+ %2 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %1, i32 96)
+ ret <4 x float> %2
+}
+
+define <4 x float> @insertps_from_vector_load_offset_2(<4 x float> %a, <4 x float>* nocapture readonly %pb, i64 %index) {
+; CHECK-LABEL: insertps_from_vector_load_offset_2:
+; On X32, account for the argument's move to registers
+; X32: movl 4(%esp), %eax
+; X32: movl 8(%esp), %ecx
+; CHECK-NOT: mov
+;; Try to match a bit more of the instr, since we need the load's offset.
+; CHECK: insertps $192, 12(%{{...}},%{{...}}), %
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds <4 x float>* %pb, i64 %index
+ %2 = load <4 x float>* %1, align 16
+ %3 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %2, i32 192)
+ ret <4 x float> %3
+}
+
+define <4 x float> @insertps_from_broadcast_loadf32(<4 x float> %a, float* nocapture readonly %fb, i64 %index) {
+; CHECK-LABEL: insertps_from_broadcast_loadf32:
+; On X32, account for the arguments' move to registers
+; X32: movl 8(%esp), %eax
+; X32: movl 4(%esp), %ecx
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds float* %fb, i64 %index
+ %2 = load float* %1, align 4
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ ret <4 x float> %7
+}
+
+define <4 x float> @insertps_from_broadcast_loadv4f32(<4 x float> %a, <4 x float>* nocapture readonly %b) {
+; CHECK-LABEL: insertps_from_broadcast_loadv4f32:
+; On X32, account for the arguments' move to registers
+; X32: movl 4(%esp), %{{...}}
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK-NEXT: ret
+ %1 = load <4 x float>* %b, align 4
+ %2 = extractelement <4 x float> %1, i32 0
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ ret <4 x float> %7
+}
+
+;; FIXME: We're emitting an extraneous pshufd/vbroadcast.
+define <4 x float> @insertps_from_broadcast_multiple_use(<4 x float> %a, <4 x float> %b, <4 x float> %c, <4 x float> %d, float* nocapture readonly %fb, i64 %index) {
+; CHECK-LABEL: insertps_from_broadcast_multiple_use:
+; On X32, account for the arguments' move to registers
+; X32: movl 8(%esp), %eax
+; X32: movl 4(%esp), %ecx
+; CHECK: movss
+; CHECK-NOT: mov
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: insertps $48
+; CHECK: addps
+; CHECK: addps
+; CHECK: addps
+; CHECK-NEXT: ret
+ %1 = getelementptr inbounds float* %fb, i64 %index
+ %2 = load float* %1, align 4
+ %3 = insertelement <4 x float> undef, float %2, i32 0
+ %4 = insertelement <4 x float> %3, float %2, i32 1
+ %5 = insertelement <4 x float> %4, float %2, i32 2
+ %6 = insertelement <4 x float> %5, float %2, i32 3
+ %7 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %a, <4 x float> %6, i32 48)
+ %8 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %b, <4 x float> %6, i32 48)
+ %9 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %c, <4 x float> %6, i32 48)
+ %10 = tail call <4 x float> @llvm.x86.sse41.insertps(<4 x float> %d, <4 x float> %6, i32 48)
+ %11 = fadd <4 x float> %7, %8
+ %12 = fadd <4 x float> %9, %10
+ %13 = fadd <4 x float> %11, %12
+ ret <4 x float> %13
+}