summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 42090c6)
raw | patch | inline | side by side (parent: 42090c6)
author | Hal Finkel <hfinkel@anl.gov> | |
Mon, 3 Nov 2014 23:19:16 +0000 (23:19 +0000) | ||
committer | Hal Finkel <hfinkel@anl.gov> | |
Mon, 3 Nov 2014 23:19:16 +0000 (23:19 +0000) |
LoadCombine can be smarter about aborting when a writing instruction is
encountered, instead of aborting upon encountering any writing instruction, use
an AliasSetTracker, and only abort when encountering some write that might
alias with the loads that could potentially be combined.
This was originally motivated by comments made (and a test case provided) by
David Majnemer in response to PR21448. It turned out that LoadCombine was not
responsible for that PR, but LoadCombine should also be improved so that
unrelated stores (and @llvm.assume) don't interrupt load combining.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@221203 91177308-0d34-0410-b5e6-96231b3b80d8
encountered, instead of aborting upon encountering any writing instruction, use
an AliasSetTracker, and only abort when encountering some write that might
alias with the loads that could potentially be combined.
This was originally motivated by comments made (and a test case provided) by
David Majnemer in response to PR21448. It turned out that LoadCombine was not
responsible for that PR, but LoadCombine should also be improved so that
unrelated stores (and @llvm.assume) don't interrupt load combining.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@221203 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Analysis/AliasSetTracker.h | patch | blob | history | |
lib/Analysis/AliasSetTracker.cpp | patch | blob | history | |
lib/Transforms/Scalar/LoadCombine.cpp | patch | blob | history | |
test/Transforms/LoadCombine/load-combine-aa.ll | [new file with mode: 0644] | patch | blob |
test/Transforms/LoadCombine/load-combine-assume.ll | [new file with mode: 0644] | patch | blob |
index 6dcd4a0441f1f17c42b6922d165ee282cdd1894d..403a2b586f689f4219d82ee315d8bd0ec1bb414b 100644 (file)
/// alias sets.
bool containsPointer(Value *P, uint64_t Size, const AAMDNodes &AAInfo) const;
+ /// Return true if the specified instruction "may" (or must) alias one of the
+ /// members in any of the sets.
+ bool containsUnknown(Instruction *I) const;
+
/// getAliasAnalysis - Return the underlying alias analysis object used by
/// this tracker.
AliasAnalysis &getAliasAnalysis() const { return AA; }
index 843a54132095f68c14ba24e2c825811b2de9078f..9d941e557978c6183e4b7f5e14496c102ad99976 100644 (file)
return false;
}
-
+bool AliasSetTracker::containsUnknown(Instruction *Inst) const {
+ for (const_iterator I = begin(), E = end(); I != E; ++I)
+ if (!I->Forward && I->aliasesUnknownInst(Inst, AA))
+ return true;
+ return false;
+}
AliasSet *AliasSetTracker::findAliasSetForUnknownInst(Instruction *Inst) {
AliasSet *FoundSet = nullptr;
index 648626a7c125870becc873770a463a24207cc5d5..11e4d7606d96de6c04dca6ba05498d0db05cb32e 100644 (file)
#include "llvm/ADT/DenseMap.h"
#include "llvm/ADT/Statistic.h"
+#include "llvm/Analysis/AliasAnalysis.h"
+#include "llvm/Analysis/AliasSetTracker.h"
#include "llvm/Analysis/TargetFolder.h"
#include "llvm/Pass.h"
#include "llvm/IR/DataLayout.h"
class LoadCombine : public BasicBlockPass {
LLVMContext *C;
const DataLayout *DL;
+ AliasAnalysis *AA;
public:
LoadCombine()
: BasicBlockPass(ID),
- C(nullptr), DL(nullptr) {
+ C(nullptr), DL(nullptr), AA(nullptr) {
initializeSROAPass(*PassRegistry::getPassRegistry());
}
if (skipOptnoneFunction(BB) || !DL)
return false;
+ AA = &getAnalysis<AliasAnalysis>();
+
IRBuilder<true, TargetFolder>
TheBuilder(BB.getContext(), TargetFolder(DL));
Builder = &TheBuilder;
DenseMap<const Value *, SmallVector<LoadPOPPair, 8>> LoadMap;
+ AliasSetTracker AST(*AA);
bool Combined = false;
unsigned Index = 0;
for (auto &I : BB) {
- if (I.mayWriteToMemory() || I.mayThrow()) {
+ if (I.mayThrow() || (I.mayWriteToMemory() && AST.containsUnknown(&I))) {
if (combineLoads(LoadMap))
Combined = true;
LoadMap.clear();
+ AST.clear();
continue;
}
LoadInst *LI = dyn_cast<LoadInst>(&I);
if (!POP.Pointer)
continue;
LoadMap[POP.Pointer].push_back(LoadPOPPair(LI, POP, Index++));
+ AST.add(LI);
}
if (combineLoads(LoadMap))
Combined = true;
void LoadCombine::getAnalysisUsage(AnalysisUsage &AU) const {
AU.setPreservesCFG();
+
+ AU.addRequired<AliasAnalysis>();
+ AU.addPreserved<AliasAnalysis>();
}
char LoadCombine::ID = 0;
return new LoadCombine();
}
-INITIALIZE_PASS(LoadCombine, "load-combine", "Combine Adjacent Loads", false,
- false)
+INITIALIZE_PASS_BEGIN(LoadCombine, "load-combine", "Combine Adjacent Loads",
+ false, false)
+INITIALIZE_AG_DEPENDENCY(AliasAnalysis)
+INITIALIZE_PASS_END(LoadCombine, "load-combine", "Combine Adjacent Loads",
+ false, false)
+
diff --git a/test/Transforms/LoadCombine/load-combine-aa.ll b/test/Transforms/LoadCombine/load-combine-aa.ll
--- /dev/null
@@ -0,0 +1,39 @@
+; RUN: opt -basicaa -load-combine -instcombine -S < %s | FileCheck %s
+target datalayout = "e-m:e-i64:64-f80:128-n8:16:32:64-S128"
+target triple = "x86_64-unknown-linux-gnu"
+
+define i64 @test1(i32* nocapture readonly noalias %a, i32* nocapture readonly noalias %b) {
+; CHECK-LABEL: @test1
+
+; CHECK: load i64*
+; CHECK: ret i64
+
+ %load1 = load i32* %a, align 4
+ %conv = zext i32 %load1 to i64
+ %arrayidx1 = getelementptr inbounds i32* %a, i64 1
+ store i32 %load1, i32* %b, align 4
+ %load2 = load i32* %arrayidx1, align 4
+ %conv2 = zext i32 %load2 to i64
+ %shl = shl nuw i64 %conv2, 32
+ %add = or i64 %shl, %conv
+ ret i64 %add
+}
+
+define i64 @test2(i32* nocapture readonly %a, i32* nocapture readonly %b) {
+; CHECK-LABEL: @test2
+
+; CHECK: load i32*
+; CHECK: load i32*
+; CHECK: ret i64
+
+ %load1 = load i32* %a, align 4
+ %conv = zext i32 %load1 to i64
+ %arrayidx1 = getelementptr inbounds i32* %a, i64 1
+ store i32 %load1, i32* %b, align 4
+ %load2 = load i32* %arrayidx1, align 4
+ %conv2 = zext i32 %load2 to i64
+ %shl = shl nuw i64 %conv2, 32
+ %add = or i64 %shl, %conv
+ ret i64 %add
+}
+
diff --git a/test/Transforms/LoadCombine/load-combine-assume.ll b/test/Transforms/LoadCombine/load-combine-assume.ll
--- /dev/null
@@ -0,0 +1,44 @@
+; RUN: opt -basicaa -load-combine -instcombine -S < %s | FileCheck %s
+target datalayout = "e-m:e-i64:64-f80:128-n8:16:32:64-S128"
+target triple = "x86_64-unknown-linux-gnu"
+
+declare void @llvm.assume(i1) nounwind
+
+; 'load' before the 'call' gets optimized:
+define i64 @test1(i32* nocapture readonly %a, i1 %b) {
+; CHECK-LABEL: @test1
+
+; CHECK-DAG: load i64* %1, align 4
+; CHECK-DAG: tail call void @llvm.assume(i1 %b)
+; CHECK: ret i64
+
+ %load1 = load i32* %a, align 4
+ %conv = zext i32 %load1 to i64
+ %arrayidx1 = getelementptr inbounds i32* %a, i64 1
+ %load2 = load i32* %arrayidx1, align 4
+ tail call void @llvm.assume(i1 %b)
+ %conv2 = zext i32 %load2 to i64
+ %shl = shl nuw i64 %conv2, 32
+ %add = or i64 %shl, %conv
+ ret i64 %add
+}
+
+; 'call' before the 'load' doesn't get optimized:
+define i64 @test2(i32* nocapture readonly %a, i1 %b) {
+; CHECK-LABEL: @test2
+
+; CHECK-DAG: load i64* %1, align 4
+; CHECK-DAG: tail call void @llvm.assume(i1 %b)
+; CHECK: ret i64
+
+ %load1 = load i32* %a, align 4
+ %conv = zext i32 %load1 to i64
+ %arrayidx1 = getelementptr inbounds i32* %a, i64 1
+ tail call void @llvm.assume(i1 %b)
+ %load2 = load i32* %arrayidx1, align 4
+ %conv2 = zext i32 %load2 to i64
+ %shl = shl nuw i64 %conv2, 32
+ %add = or i64 %shl, %conv
+ ret i64 %add
+}
+