summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3d37204)
raw | patch | inline | side by side (parent: 3d37204)
author | Eli Bendersky <eliben@google.com> | |
Wed, 12 Mar 2014 16:12:36 +0000 (16:12 +0000) | ||
committer | Eli Bendersky <eliben@google.com> | |
Wed, 12 Mar 2014 16:12:36 +0000 (16:12 +0000) |
There's a bit of duplicated "magic" code in opt.cpp and Clang's CodeGen that
computes the inliner threshold from opt level and size opt level.
This patch moves the code to a function that lives alongside the inliner itself,
providing a convenient overload to the inliner creation.
A separate patch can be committed to Clang to use this once it's committed to
LLVM. Standalone tools that use the inlining pass can also avoid duplicating
this code and fearing it will go out of sync.
Note: this patch also restructures the conditinal logic of the computation to
be cleaner.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@203669 91177308-0d34-0410-b5e6-96231b3b80d8
computes the inliner threshold from opt level and size opt level.
This patch moves the code to a function that lives alongside the inliner itself,
providing a convenient overload to the inliner creation.
A separate patch can be committed to Clang to use this once it's committed to
LLVM. Standalone tools that use the inlining pass can also avoid duplicating
this code and fearing it will go out of sync.
Note: this patch also restructures the conditinal logic of the computation to
be cleaner.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@203669 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Transforms/IPO.h | patch | blob | history | |
lib/Transforms/IPO/InlineSimple.cpp | patch | blob | history | |
tools/opt/opt.cpp | patch | blob | history |
index b4f65b25d5f1d87916e293d0c575f1f3638ce6d0..ae9d5c1d09b6962df2e987d3cd9fd4979a9ed3e1 100644 (file)
//===----------------------------------------------------------------------===//
//
-// These functions strips symbols from functions and modules.
+// These functions strips symbols from functions and modules.
// Only debugging information is not stripped.
//
ModulePass *createStripNonDebugSymbolsPass();
/// the specified global values. Otherwise, it deletes as much of the module as
/// possible, except for the global values specified.
///
-ModulePass *createGVExtractionPass(std::vector<GlobalValue*>& GVs, bool
+ModulePass *createGVExtractionPass(std::vector<GlobalValue*>& GVs, bool
deleteFn = false);
//===----------------------------------------------------------------------===//
/// createFunctionInliningPass - Return a new pass object that uses a heuristic
/// to inline direct function calls to small functions.
///
+/// The Threshold can be passed directly, or asked to be computed from the
+/// given optimization and size optimization arguments.
+///
/// The -inline-threshold command line option takes precedence over the
/// threshold given here.
Pass *createFunctionInliningPass();
Pass *createFunctionInliningPass(int Threshold);
+Pass *createFunctionInliningPass(unsigned OptLevel, unsigned SizeOptLevel);
//===----------------------------------------------------------------------===//
-/// createAlwaysInlinerPass - Return a new pass object that inlines only
+/// createAlwaysInlinerPass - Return a new pass object that inlines only
/// functions that are marked as "always_inline".
Pass *createAlwaysInlinerPass();
Pass *createAlwaysInlinerPass(bool InsertLifetime);
/// createPartialInliningPass - This pass inlines parts of functions.
///
ModulePass *createPartialInliningPass();
-
+
//===----------------------------------------------------------------------===//
// createMetaRenamerPass - Rename everything with metasyntatic names.
//
index eecd9b103086dd96c652b7d8a08470e7807da00b..e5f46d7a7837dc142d57c0bb7617b79eeaa639d2 100644 (file)
void getAnalysisUsage(AnalysisUsage &AU) const override;
};
+static int computeThresholdFromOptLevels(unsigned OptLevel,
+ unsigned SizeOptLevel) {
+ if (OptLevel > 2)
+ return 275;
+ if (SizeOptLevel == 1)
+ return 75;
+ if (SizeOptLevel == 2)
+ return 25;
+ return 225;
+}
+
} // end anonymous namespace
char SimpleInliner::ID = 0;
return new SimpleInliner(Threshold);
}
+Pass *llvm::createFunctionInliningPass(unsigned OptLevel,
+ unsigned SizeOptLevel) {
+ return new SimpleInliner(
+ computeThresholdFromOptLevels(OptLevel, SizeOptLevel));
+}
+
bool SimpleInliner::runOnSCC(CallGraphSCC &SCC) {
ICA = &getAnalysis<InlineCostAnalysis>();
return Inliner::runOnSCC(SCC);
diff --git a/tools/opt/opt.cpp b/tools/opt/opt.cpp
index 14a40a4af764134b1def7e430d42d1205871a71e..4dd9544fc32b923a1461044069d41470c0563dd3 100644 (file)
--- a/tools/opt/opt.cpp
+++ b/tools/opt/opt.cpp
@@ -210,14 +210,7 @@ static void AddOptimizationPasses(PassManagerBase &MPM,FunctionPassManager &FPM,
if (DisableInline) {
// No inlining pass
} else if (OptLevel > 1) {
- unsigned Threshold = 225;
- if (SizeLevel == 1) // -Os
- Threshold = 75;
- else if (SizeLevel == 2) // -Oz
- Threshold = 25;
- if (OptLevel > 2)
- Threshold = 275;
- Builder.Inliner = createFunctionInliningPass(Threshold);
+ Builder.Inliner = createFunctionInliningPass(OptLevel, SizeLevel);
} else {
Builder.Inliner = createAlwaysInlinerPass();
}