summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: a630cb0)
raw | patch | inline | side by side (from parent 1: a630cb0)
author | Aaron Ballman <aaron@aaronballman.com> | |
Thu, 15 Aug 2013 23:17:53 +0000 (23:17 +0000) | ||
committer | Aaron Ballman <aaron@aaronballman.com> | |
Thu, 15 Aug 2013 23:17:53 +0000 (23:17 +0000) |
Patch with help from Nick Kledzik.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188508 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188508 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/Support/YAMLTraits.h | patch | blob | history | |
lib/Support/YAMLTraits.cpp | patch | blob | history | |
unittests/Support/YAMLIOTest.cpp | patch | blob | history |
index 0f57f44340c23acd2d0a19cdf24160441f6ff37f..98964fc00200527d19230b6ab106339496490e68 100644 (file)
virtual bool preflightElement(unsigned, void *&) = 0;
virtual void postflightElement(void*) = 0;
virtual void endSequence() = 0;
+ virtual bool canElideEmptySequence() = 0;
virtual unsigned beginFlowSequence() = 0;
virtual bool preflightFlowElement(unsigned, void *&) = 0;
typename llvm::enable_if_c<has_SequenceTraits<T>::value,void>::type
mapOptional(const char* Key, T& Val) {
// omit key/value instead of outputting empty sequence
- if ( this->outputting() && !(Val.begin() != Val.end()) )
+ if ( this->canElideEmptySequence() && !(Val.begin() != Val.end()) )
return;
this->processKey(Key, Val, false);
}
virtual void endBitSetScalar();
virtual void scalarString(StringRef &);
virtual void setError(const Twine &message);
+ virtual bool canElideEmptySequence();
class HNode {
public:
virtual void endBitSetScalar();
virtual void scalarString(StringRef &);
virtual void setError(const Twine &message);
-
+ virtual bool canElideEmptySequence();
public:
// These are only used by operator<<. They could be private
// if that templated operator could be made a friend.
index b0cd415186379840c27b6aad25ee4dce171d1d57..ae7f7dcb0d0555d0aee934c1f10617464e8e077b 100644 (file)
this->setError(CurrentNode, Message);
}
+bool Input::canElideEmptySequence() {
+ return false;
+}
+
Input::MapHNode::~MapHNode() {
for (MapHNode::NameToNode::iterator i = Mapping.begin(), End = Mapping.end();
i != End; ++i) {
void Output::setError(const Twine &message) {
}
+bool Output::canElideEmptySequence() {
+ // Normally, with an optional key/value where the value is an empty sequence,
+ // the whole key/value can be not written. But, that produces wrong yaml
+ // if the key/value is the only thing in the map and the map is used in
+ // a sequence. This detects if the this sequence is the first key/value
+ // in map that itself is embedded in a sequnce.
+ if (StateStack.size() < 2)
+ return true;
+ if (StateStack.back() != inMapFirstKey)
+ return true;
+ return (StateStack[StateStack.size()-2] != inSeq);
+}
+
void Output::output(StringRef s) {
Column += s.size();
Out << s;
index 0993d8c0b555e53c47ceaae5619aacade2caa5a7..eedc5842b633247476ea07e827f50d6cb37081c8 100644 (file)
EXPECT_TRUE(yin.error());
}
+struct OptionalTest {
+ std::vector<int> Numbers;
+};
+
+struct OptionalTestSeq {
+ std::vector<OptionalTest> Tests;
+};
+
+LLVM_YAML_IS_SEQUENCE_VECTOR(OptionalTest);
+namespace llvm {
+namespace yaml {
+ template <>
+ struct MappingTraits<OptionalTest> {
+ static void mapping(IO& IO, OptionalTest &OT) {
+ IO.mapOptional("Numbers", OT.Numbers);
+ }
+ };
+
+ template <>
+ struct MappingTraits<OptionalTestSeq> {
+ static void mapping(IO &IO, OptionalTestSeq &OTS) {
+ IO.mapOptional("Tests", OTS.Tests);
+ }
+ };
+}
+}
+
+TEST(YAMLIO, SequenceElideTest) {
+ // Test that writing out a purely optional structure with its fields set to
+ // default followed by other data is properly read back in.
+ OptionalTestSeq Seq;
+ OptionalTest One, Two, Three, Four;
+ int N[] = {1, 2, 3};
+ Three.Numbers.assign(N, N + 3);
+ Seq.Tests.push_back(One);
+ Seq.Tests.push_back(Two);
+ Seq.Tests.push_back(Three);
+ Seq.Tests.push_back(Four);
+
+ std::string intermediate;
+ {
+ llvm::raw_string_ostream ostr(intermediate);
+ Output yout(ostr);
+ yout << Seq;
+ }
+
+ Input yin(intermediate);
+ OptionalTestSeq Seq2;
+ yin >> Seq2;
+
+ EXPECT_FALSE(yin.error());
+
+ EXPECT_EQ(4UL, Seq2.Tests.size());
+
+ EXPECT_TRUE(Seq2.Tests[0].Numbers.empty());
+ EXPECT_TRUE(Seq2.Tests[1].Numbers.empty());
+
+ EXPECT_EQ(1, Seq2.Tests[2].Numbers[0]);
+ EXPECT_EQ(2, Seq2.Tests[2].Numbers[1]);
+ EXPECT_EQ(3, Seq2.Tests[2].Numbers[2]);
+
+ EXPECT_TRUE(Seq2.Tests[3].Numbers.empty());
+}