summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b49fb7b)
raw | patch | inline | side by side (parent: b49fb7b)
author | Tom Stellard <thomas.stellard@amd.com> | |
Wed, 14 Aug 2013 23:24:17 +0000 (23:24 +0000) | ||
committer | Tom Stellard <thomas.stellard@amd.com> | |
Wed, 14 Aug 2013 23:24:17 +0000 (23:24 +0000) |
The previous code declared the operand as unknown:$vaddr, which made
it possible for scalar registers to be used instead of vector registers.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188425 91177308-0d34-0410-b5e6-96231b3b80d8
it possible for scalar registers to be used instead of vector registers.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@188425 91177308-0d34-0410-b5e6-96231b3b80d8
index 147578ce8d2b95fc5ec86065783cbb5f6a7592f3..572ed6ae16aac4ec92220ce12aa77ec072bf3f5f 100644 (file)
#ifndef SIDEFINES_H_
#define SIDEFINES_H_
+namespace SIInstrFlags {
+enum {
+ MIMG = 1 << 3
+};
+}
+
#define R_00B028_SPI_SHADER_PGM_RSRC1_PS 0x00B028
#define R_00B02C_SPI_SHADER_PGM_RSRC2_PS 0x00B02C
#define S_00B02C_EXTRA_LDS_SIZE(x) (((x) & 0xFF) << 8)
index a76e6ee3145ca7265e26ded8188ff936ac0ff3e7..4631f8a3a8b4fb3c00153d14827426fcec5f4d39 100644 (file)
/// \brief Fold the instructions after slecting them
SDNode *SITargetLowering::PostISelFolding(MachineSDNode *Node,
SelectionDAG &DAG) const {
+ const SIInstrInfo *TII =
+ static_cast<const SIInstrInfo*>(getTargetMachine().getInstrInfo());
Node = AdjustRegClass(Node, DAG);
- if (AMDGPU::isMIMG(Node->getMachineOpcode()) != -1)
+ if (TII->isMIMG(Node->getMachineOpcode()))
adjustWritemask(Node, DAG);
return foldOperands(Node, DAG);
/// bits set in the writemask
void SITargetLowering::AdjustInstrPostInstrSelection(MachineInstr *MI,
SDNode *Node) const {
- if (AMDGPU::isMIMG(MI->getOpcode()) == -1)
+ const SIInstrInfo *TII =
+ static_cast<const SIInstrInfo*>(getTargetMachine().getInstrInfo());
+ if (!TII->isMIMG(MI->getOpcode()))
return;
unsigned VReg = MI->getOperand(0).getReg();
index 434aa7e0bf0b88bb040f02417da42df6fc950251..cd1bbcd670ef38950e505fe28ab9441eef44b0d5 100644 (file)
field bits<1> VM_CNT = 0;
field bits<1> EXP_CNT = 0;
field bits<1> LGKM_CNT = 0;
+ field bits<1> MIMG = 0;
let TSFlags{0} = VM_CNT;
let TSFlags{1} = EXP_CNT;
let TSFlags{2} = LGKM_CNT;
+ let TSFlags{3} = MIMG;
}
class Enc32 <dag outs, dag ins, string asm, list<dag> pattern> :
let VM_CNT = 1;
let EXP_CNT = 1;
+ let MIMG = 1;
}
def EXP : Enc64<
index 551ae8683ed477eca16f2d9ffecc507bc155c216..9bb4ad9abc5e2c71fafadd97325feaf87fe3ec48 100644 (file)
#include "SIInstrInfo.h"
#include "AMDGPUTargetMachine.h"
+#include "SIDefines.h"
#include "llvm/CodeGen/MachineInstrBuilder.h"
#include "llvm/CodeGen/MachineRegisterInfo.h"
#include "llvm/MC/MCInstrDesc.h"
return RC != &AMDGPU::EXECRegRegClass;
}
+int SIInstrInfo::isMIMG(uint16_t Opcode) const {
+ return get(Opcode).TSFlags & SIInstrFlags::MIMG;
+}
+
//===----------------------------------------------------------------------===//
// Indirect addressing callbacks
//===----------------------------------------------------------------------===//
index 87eff4d6c95c9d9f9867e2b2903ba6ac449001d7..8d24ab4bf14dab0eb9b9b08307e96a7149671040 100644 (file)
virtual bool isMov(unsigned Opcode) const;
virtual bool isSafeToMoveRegClassDefs(const TargetRegisterClass *RC) const;
+ int isMIMG(uint16_t Opcode) const;
virtual int getIndirectIndexBegin(const MachineFunction &MF) const;
int getVOPe64(uint16_t Opcode);
int getCommuteRev(uint16_t Opcode);
int getCommuteOrig(uint16_t Opcode);
- int isMIMG(uint16_t Opcode);
} // End namespace AMDGPU
index 302fa2475cfea0b93d35f6a054856247a775c43c..71d20eaa0fb6a5a9eb0910ca65f9e2fa0eff1bd2 100644 (file)
@@ -397,11 +397,12 @@ class MTBUF_Load_Helper <bits<3> op, string asm, RegisterClass regClass> : MTBUF
let mayStore = 0;
}
-class MIMG_NoSampler_Helper <bits<7> op, string asm> : MIMG <
+class MIMG_NoSampler_Helper <bits<7> op, string asm,
+ RegisterClass src_rc> : MIMG <
op,
(outs VReg_128:$vdata),
(ins i32imm:$dmask, i1imm:$unorm, i1imm:$glc, i1imm:$da, i1imm:$r128,
- i1imm:$tfe, i1imm:$lwe, i1imm:$slc, unknown:$vaddr,
+ i1imm:$tfe, i1imm:$lwe, i1imm:$slc, src_rc:$vaddr,
SReg_256:$srsrc),
asm#" $vdata, $dmask, $unorm, $glc, $da, $r128,"
#" $tfe, $lwe, $slc, $vaddr, $srsrc",
let hasPostISelHook = 1;
}
-class MIMG_Sampler_Helper <bits<7> op, string asm> : MIMG <
+multiclass MIMG_NoSampler <bits<7> op, string asm> {
+ def _V1 : MIMG_NoSampler_Helper <op, asm, VReg_32>;
+ def _V2 : MIMG_NoSampler_Helper <op, asm, VReg_64>;
+ def _V4 : MIMG_NoSampler_Helper <op, asm, VReg_128>;
+}
+
+class MIMG_Sampler_Helper <bits<7> op, string asm,
+ RegisterClass src_rc> : MIMG <
op,
(outs VReg_128:$vdata),
(ins i32imm:$dmask, i1imm:$unorm, i1imm:$glc, i1imm:$da, i1imm:$r128,
- i1imm:$tfe, i1imm:$lwe, i1imm:$slc, unknown:$vaddr,
+ i1imm:$tfe, i1imm:$lwe, i1imm:$slc, src_rc:$vaddr,
SReg_256:$srsrc, SReg_128:$ssamp),
asm#" $vdata, $dmask, $unorm, $glc, $da, $r128,"
#" $tfe, $lwe, $slc, $vaddr, $srsrc, $ssamp",
let hasPostISelHook = 1;
}
+multiclass MIMG_Sampler <bits<7> op, string asm> {
+ def _V1 : MIMG_Sampler_Helper <op, asm, VReg_32>;
+ def _V2 : MIMG_Sampler_Helper <op, asm, VReg_64>;
+ def _V4 : MIMG_Sampler_Helper <op, asm, VReg_128>;
+ def _V8 : MIMG_Sampler_Helper <op, asm, VReg_256>;
+ def _V16 : MIMG_Sampler_Helper <op, asm, VReg_512>;
+}
+
//===----------------------------------------------------------------------===//
// Vector instruction mappings
//===----------------------------------------------------------------------===//
let ValueCols = [["1"]];
}
-// Test if the supplied opcode is an MIMG instruction
-def isMIMG : InstrMapping {
- let FilterClass = "MIMG";
- let RowFields = ["Inst"];
- let ColFields = ["Size"];
- let KeyCol = ["8"];
- let ValueCols = [["8"]];
-}
-
include "SIInstructions.td"
index 909c9762369bbe6f00ffb4c4ff0080438ca6502f..5fbd68f3e7c7cd296ee611baba974a0fd732d737 100644 (file)
//def S_MEMTIME : SMRD_ <0x0000001e, "S_MEMTIME", []>;
//def S_DCACHE_INV : SMRD_ <0x0000001f, "S_DCACHE_INV", []>;
-def IMAGE_LOAD : MIMG_NoSampler_Helper <0x00000000, "IMAGE_LOAD">;
-def IMAGE_LOAD_MIP : MIMG_NoSampler_Helper <0x00000001, "IMAGE_LOAD_MIP">;
+defm IMAGE_LOAD : MIMG_NoSampler <0x00000000, "IMAGE_LOAD">;
+defm IMAGE_LOAD_MIP : MIMG_NoSampler <0x00000001, "IMAGE_LOAD_MIP">;
//def IMAGE_LOAD_PCK : MIMG_NoPattern_ <"IMAGE_LOAD_PCK", 0x00000002>;
//def IMAGE_LOAD_PCK_SGN : MIMG_NoPattern_ <"IMAGE_LOAD_PCK_SGN", 0x00000003>;
//def IMAGE_LOAD_MIP_PCK : MIMG_NoPattern_ <"IMAGE_LOAD_MIP_PCK", 0x00000004>;
//def IMAGE_STORE_MIP : MIMG_NoPattern_ <"IMAGE_STORE_MIP", 0x00000009>;
//def IMAGE_STORE_PCK : MIMG_NoPattern_ <"IMAGE_STORE_PCK", 0x0000000a>;
//def IMAGE_STORE_MIP_PCK : MIMG_NoPattern_ <"IMAGE_STORE_MIP_PCK", 0x0000000b>;
-def IMAGE_GET_RESINFO : MIMG_NoSampler_Helper <0x0000000e, "IMAGE_GET_RESINFO">;
+def IMAGE_GET_RESINFO : MIMG_NoSampler_Helper <0x0000000e, "IMAGE_GET_RESINFO", VReg_32>;
//def IMAGE_ATOMIC_SWAP : MIMG_NoPattern_ <"IMAGE_ATOMIC_SWAP", 0x0000000f>;
//def IMAGE_ATOMIC_CMPSWAP : MIMG_NoPattern_ <"IMAGE_ATOMIC_CMPSWAP", 0x00000010>;
//def IMAGE_ATOMIC_ADD : MIMG_NoPattern_ <"IMAGE_ATOMIC_ADD", 0x00000011>;
@@ -528,20 +528,20 @@ def IMAGE_GET_RESINFO : MIMG_NoSampler_Helper <0x0000000e, "IMAGE_GET_RESINFO">;
//def IMAGE_ATOMIC_FCMPSWAP : MIMG_NoPattern_ <"IMAGE_ATOMIC_FCMPSWAP", 0x0000001d>;
//def IMAGE_ATOMIC_FMIN : MIMG_NoPattern_ <"IMAGE_ATOMIC_FMIN", 0x0000001e>;
//def IMAGE_ATOMIC_FMAX : MIMG_NoPattern_ <"IMAGE_ATOMIC_FMAX", 0x0000001f>;
-def IMAGE_SAMPLE : MIMG_Sampler_Helper <0x00000020, "IMAGE_SAMPLE">;
+defm IMAGE_SAMPLE : MIMG_Sampler <0x00000020, "IMAGE_SAMPLE">;
//def IMAGE_SAMPLE_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_CL", 0x00000021>;
-def IMAGE_SAMPLE_D : MIMG_Sampler_Helper <0x00000022, "IMAGE_SAMPLE_D">;
+defm IMAGE_SAMPLE_D : MIMG_Sampler <0x00000022, "IMAGE_SAMPLE_D">;
//def IMAGE_SAMPLE_D_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_D_CL", 0x00000023>;
-def IMAGE_SAMPLE_L : MIMG_Sampler_Helper <0x00000024, "IMAGE_SAMPLE_L">;
-def IMAGE_SAMPLE_B : MIMG_Sampler_Helper <0x00000025, "IMAGE_SAMPLE_B">;
+defm IMAGE_SAMPLE_L : MIMG_Sampler <0x00000024, "IMAGE_SAMPLE_L">;
+defm IMAGE_SAMPLE_B : MIMG_Sampler <0x00000025, "IMAGE_SAMPLE_B">;
//def IMAGE_SAMPLE_B_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_B_CL", 0x00000026>;
//def IMAGE_SAMPLE_LZ : MIMG_NoPattern_ <"IMAGE_SAMPLE_LZ", 0x00000027>;
-def IMAGE_SAMPLE_C : MIMG_Sampler_Helper <0x00000028, "IMAGE_SAMPLE_C">;
+defm IMAGE_SAMPLE_C : MIMG_Sampler <0x00000028, "IMAGE_SAMPLE_C">;
//def IMAGE_SAMPLE_C_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_C_CL", 0x00000029>;
-def IMAGE_SAMPLE_C_D : MIMG_Sampler_Helper <0x0000002a, "IMAGE_SAMPLE_C_D">;
+defm IMAGE_SAMPLE_C_D : MIMG_Sampler <0x0000002a, "IMAGE_SAMPLE_C_D">;
//def IMAGE_SAMPLE_C_D_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_C_D_CL", 0x0000002b>;
-def IMAGE_SAMPLE_C_L : MIMG_Sampler_Helper <0x0000002c, "IMAGE_SAMPLE_C_L">;
-def IMAGE_SAMPLE_C_B : MIMG_Sampler_Helper <0x0000002d, "IMAGE_SAMPLE_C_B">;
+defm IMAGE_SAMPLE_C_L : MIMG_Sampler <0x0000002c, "IMAGE_SAMPLE_C_L">;
+defm IMAGE_SAMPLE_C_B : MIMG_Sampler <0x0000002d, "IMAGE_SAMPLE_C_B">;
//def IMAGE_SAMPLE_C_B_CL : MIMG_NoPattern_ <"IMAGE_SAMPLE_C_B_CL", 0x0000002e>;
//def IMAGE_SAMPLE_C_LZ : MIMG_NoPattern_ <"IMAGE_SAMPLE_C_LZ", 0x0000002f>;
//def IMAGE_SAMPLE_O : MIMG_NoPattern_ <"IMAGE_SAMPLE_O", 0x00000030>;
/* int_SI_sample for simple 1D texture lookup */
def : Pat <
(int_SI_sample v1i32:$addr, v32i8:$rsrc, v16i8:$sampler, imm),
- (IMAGE_SAMPLE 0xf, 0, 0, 0, 0, 0, 0, 0, $addr, $rsrc, $sampler)
+ (IMAGE_SAMPLE_V1 0xf, 0, 0, 0, 0, 0, 0, 0, $addr, $rsrc, $sampler)
>;
class SamplePattern<Intrinsic name, MIMG opcode, ValueType vt> : Pat <
>;
/* int_SI_sample* for texture lookups consuming more address parameters */
-multiclass SamplePatterns<ValueType addr_type> {
- def : SamplePattern <int_SI_sample, IMAGE_SAMPLE, addr_type>;
- def : SampleRectPattern <int_SI_sample, IMAGE_SAMPLE, addr_type>;
- def : SampleArrayPattern <int_SI_sample, IMAGE_SAMPLE, addr_type>;
- def : SampleShadowPattern <int_SI_sample, IMAGE_SAMPLE_C, addr_type>;
- def : SampleShadowArrayPattern <int_SI_sample, IMAGE_SAMPLE_C, addr_type>;
-
- def : SamplePattern <int_SI_samplel, IMAGE_SAMPLE_L, addr_type>;
- def : SampleArrayPattern <int_SI_samplel, IMAGE_SAMPLE_L, addr_type>;
- def : SampleShadowPattern <int_SI_samplel, IMAGE_SAMPLE_C_L, addr_type>;
- def : SampleShadowArrayPattern <int_SI_samplel, IMAGE_SAMPLE_C_L, addr_type>;
-
- def : SamplePattern <int_SI_sampleb, IMAGE_SAMPLE_B, addr_type>;
- def : SampleArrayPattern <int_SI_sampleb, IMAGE_SAMPLE_B, addr_type>;
- def : SampleShadowPattern <int_SI_sampleb, IMAGE_SAMPLE_C_B, addr_type>;
- def : SampleShadowArrayPattern <int_SI_sampleb, IMAGE_SAMPLE_C_B, addr_type>;
-
- def : SamplePattern <int_SI_sampled, IMAGE_SAMPLE_D, addr_type>;
- def : SampleArrayPattern <int_SI_sampled, IMAGE_SAMPLE_D, addr_type>;
- def : SampleShadowPattern <int_SI_sampled, IMAGE_SAMPLE_C_D, addr_type>;
- def : SampleShadowArrayPattern <int_SI_sampled, IMAGE_SAMPLE_C_D, addr_type>;
+multiclass SamplePatterns<MIMG sample, MIMG sample_c, MIMG sample_l,
+ MIMG sample_c_l, MIMG sample_b, MIMG sample_c_b,
+MIMG sample_d, MIMG sample_c_d, ValueType addr_type> {
+ def : SamplePattern <int_SI_sample, sample, addr_type>;
+ def : SampleRectPattern <int_SI_sample, sample, addr_type>;
+ def : SampleArrayPattern <int_SI_sample, sample, addr_type>;
+ def : SampleShadowPattern <int_SI_sample, sample_c, addr_type>;
+ def : SampleShadowArrayPattern <int_SI_sample, sample_c, addr_type>;
+
+ def : SamplePattern <int_SI_samplel, sample_l, addr_type>;
+ def : SampleArrayPattern <int_SI_samplel, sample_l, addr_type>;
+ def : SampleShadowPattern <int_SI_samplel, sample_c_l, addr_type>;
+ def : SampleShadowArrayPattern <int_SI_samplel, sample_c_l, addr_type>;
+
+ def : SamplePattern <int_SI_sampleb, sample_b, addr_type>;
+ def : SampleArrayPattern <int_SI_sampleb, sample_b, addr_type>;
+ def : SampleShadowPattern <int_SI_sampleb, sample_c_b, addr_type>;
+ def : SampleShadowArrayPattern <int_SI_sampleb, sample_c_b, addr_type>;
+
+ def : SamplePattern <int_SI_sampled, sample_d, addr_type>;
+ def : SampleArrayPattern <int_SI_sampled, sample_d, addr_type>;
+ def : SampleShadowPattern <int_SI_sampled, sample_c_d, addr_type>;
+ def : SampleShadowArrayPattern <int_SI_sampled, sample_c_d, addr_type>;
}
-defm : SamplePatterns<v2i32>;
-defm : SamplePatterns<v4i32>;
-defm : SamplePatterns<v8i32>;
-defm : SamplePatterns<v16i32>;
+defm : SamplePatterns<IMAGE_SAMPLE_V2, IMAGE_SAMPLE_C_V2,
+ IMAGE_SAMPLE_L_V2, IMAGE_SAMPLE_C_L_V2,
+ IMAGE_SAMPLE_B_V2, IMAGE_SAMPLE_C_B_V2,
+ IMAGE_SAMPLE_D_V2, IMAGE_SAMPLE_C_D_V2,
+ v2i32>;
+defm : SamplePatterns<IMAGE_SAMPLE_V4, IMAGE_SAMPLE_C_V4,
+ IMAGE_SAMPLE_L_V4, IMAGE_SAMPLE_C_L_V4,
+ IMAGE_SAMPLE_B_V4, IMAGE_SAMPLE_C_B_V4,
+ IMAGE_SAMPLE_D_V4, IMAGE_SAMPLE_C_D_V4,
+ v4i32>;
+defm : SamplePatterns<IMAGE_SAMPLE_V8, IMAGE_SAMPLE_C_V8,
+ IMAGE_SAMPLE_L_V8, IMAGE_SAMPLE_C_L_V8,
+ IMAGE_SAMPLE_B_V8, IMAGE_SAMPLE_C_B_V8,
+ IMAGE_SAMPLE_D_V8, IMAGE_SAMPLE_C_D_V8,
+ v8i32>;
+defm : SamplePatterns<IMAGE_SAMPLE_V16, IMAGE_SAMPLE_C_V16,
+ IMAGE_SAMPLE_L_V16, IMAGE_SAMPLE_C_L_V16,
+ IMAGE_SAMPLE_B_V16, IMAGE_SAMPLE_C_B_V16,
+ IMAGE_SAMPLE_D_V16, IMAGE_SAMPLE_C_D_V16,
+ v16i32>;
/* int_SI_imageload for texture fetches consuming varying address parameters */
class ImageLoadPattern<Intrinsic name, MIMG opcode, ValueType addr_type> : Pat <
@@ -1407,15 +1425,21 @@ class ImageLoadArrayMSAAPattern<Intrinsic name, MIMG opcode, ValueType addr_type
(opcode 0xf, 0, 0, 1, 0, 0, 0, 0, $addr, $rsrc)
>;
-multiclass ImageLoadPatterns<ValueType addr_type> {
- def : ImageLoadPattern <int_SI_imageload, IMAGE_LOAD_MIP, addr_type>;
- def : ImageLoadArrayPattern <int_SI_imageload, IMAGE_LOAD_MIP, addr_type>;
- def : ImageLoadMSAAPattern <int_SI_imageload, IMAGE_LOAD, addr_type>;
- def : ImageLoadArrayMSAAPattern <int_SI_imageload, IMAGE_LOAD, addr_type>;
+multiclass ImageLoadPatterns<MIMG opcode, ValueType addr_type> {
+ def : ImageLoadPattern <int_SI_imageload, opcode, addr_type>;
+ def : ImageLoadArrayPattern <int_SI_imageload, opcode, addr_type>;
}
-defm : ImageLoadPatterns<v2i32>;
-defm : ImageLoadPatterns<v4i32>;
+multiclass ImageLoadMSAAPatterns<MIMG opcode, ValueType addr_type> {
+ def : ImageLoadMSAAPattern <int_SI_imageload, opcode, addr_type>;
+ def : ImageLoadArrayMSAAPattern <int_SI_imageload, opcode, addr_type>;
+}
+
+defm : ImageLoadPatterns<IMAGE_LOAD_MIP_V2, v2i32>;
+defm : ImageLoadPatterns<IMAGE_LOAD_MIP_V4, v4i32>;
+
+defm : ImageLoadMSAAPatterns<IMAGE_LOAD_V2, v2i32>;
+defm : ImageLoadMSAAPatterns<IMAGE_LOAD_V4, v4i32>;
/* Image resource information */
def : Pat <
index 1ed4dd42ae6304abade27f88c0935ed6b0254688..3817034aa42341c587dbe0fc0f5d62425ef3c380 100644 (file)
ret void
}
+; Test that ccordinates are stored in vgprs and not sgprs
+; CHECK: vgpr_coords
+; CHECK: IMAGE_LOAD_MIP VGPR{{[0-9]}}_VGPR{{[0-9]}}_VGPR{{[0-9]}}_VGPR{{[0-9]}}, 15, 0, 0, 0, 0, 0, 0, 0, VGPR{{[0-9]}}_VGPR{{[0-9]}}_VGPR{{[0-9]}}_VGPR{{[0-9]}}
+define void @vgpr_coords(float addrspace(2)* addrspace(2)* inreg, <16 x i8> addrspace(2)* inreg, <32 x i8> addrspace(2)* inreg, i32 inreg, <2 x i32>, <2 x i32>, <2 x i32>, <3 x i32>, <2 x i32>, <2 x i32>, <2 x i32>, float, float, float, float, float, float, float, float, float) #0 {
+main_body:
+ %20 = getelementptr float addrspace(2)* addrspace(2)* %0, i32 0
+ %21 = load float addrspace(2)* addrspace(2)* %20, !tbaa !0
+ %22 = getelementptr float addrspace(2)* %21, i32 0
+ %23 = load float addrspace(2)* %22, !tbaa !0, !invariant.load !1
+ %24 = getelementptr float addrspace(2)* %21, i32 1
+ %25 = load float addrspace(2)* %24, !tbaa !0, !invariant.load !1
+ %26 = getelementptr float addrspace(2)* %21, i32 4
+ %27 = load float addrspace(2)* %26, !tbaa !0, !invariant.load !1
+ %28 = getelementptr <32 x i8> addrspace(2)* %2, i32 0
+ %29 = load <32 x i8> addrspace(2)* %28, !tbaa !0
+ %30 = bitcast float %27 to i32
+ %31 = bitcast float %23 to i32
+ %32 = bitcast float %25 to i32
+ %33 = insertelement <4 x i32> undef, i32 %31, i32 0
+ %34 = insertelement <4 x i32> %33, i32 %32, i32 1
+ %35 = insertelement <4 x i32> %34, i32 %30, i32 2
+ %36 = insertelement <4 x i32> %35, i32 undef, i32 3
+ %37 = call <4 x i32> @llvm.SI.imageload.v4i32(<4 x i32> %36, <32 x i8> %29, i32 2)
+ %38 = extractelement <4 x i32> %37, i32 0
+ %39 = extractelement <4 x i32> %37, i32 1
+ %40 = extractelement <4 x i32> %37, i32 2
+ %41 = extractelement <4 x i32> %37, i32 3
+ %42 = bitcast i32 %38 to float
+ %43 = bitcast i32 %39 to float
+ %44 = bitcast i32 %40 to float
+ %45 = bitcast i32 %41 to float
+ call void @llvm.SI.export(i32 15, i32 1, i32 1, i32 0, i32 0, float %42, float %43, float %44, float %45)
+ ret void
+}
+
declare <4 x i32> @llvm.SI.imageload.(<4 x i32>, <8 x i32>, i32) readnone
+; Function Attrs: nounwind readnone
+declare <4 x i32> @llvm.SI.imageload.v4i32(<4 x i32>, <32 x i8>, i32) #1
declare void @llvm.SI.export(i32, i32, i32, i32, i32, float, float, float, float)
+
+attributes #0 = { "ShaderType"="0" }
+attributes #1 = { nounwind readnone }
+
+!0 = metadata !{metadata !"const", null, i32 1}
+!1 = metadata !{}
+