]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commitdiff
Revert "InstCombine: Improvement to check if signed addition overflows."
authorRafael Espindola <rafael.espindola@gmail.com>
Wed, 28 May 2014 18:48:10 +0000 (18:48 +0000)
committerRafael Espindola <rafael.espindola@gmail.com>
Wed, 28 May 2014 18:48:10 +0000 (18:48 +0000)
This reverts commit r209746.

It looks it is causing a crash while building libcxx. I am trying to get a
reduced testcase.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209762 91177308-0d34-0410-b5e6-96231b3b80d8

lib/Transforms/InstCombine/InstCombineAddSub.cpp
test/Transforms/InstCombine/AddOverflow.ll [deleted file]

index eca4e4a7870262fae2c9a765ac2a14b1abfe9815..c37a9cf2ef9fb98f5b05826bfed2ffd625ea54c0 100644 (file)
@@ -889,34 +889,11 @@ static inline Value *dyn_castFoldableMul(Value *V, Constant *&CST) {
   return nullptr;
 }
 
-// If one of the operands only has one non-zero bit, and if the other
-// operand has a known-zero bit in a more significant place than it (not
-// including the sign bit) the ripple may go up to and fill the zero, but
-// won't change the sign. For example, (X & ~4) + 1.
-// FIXME: Handle case where LHS has a zero before the 1 in the RHS, but also
-// has one after.
-static bool CheckRippleForAdd(APInt Op0KnownZero, APInt Op0KnownOne,
-                              APInt Op1KnownZero, APInt Op1KnownOne) {
-  // Make sure that one of the operand has only one bit set to 1 and all other
-  // bit set to 0.
-  if ((~Op1KnownZero).countPopulation() == 1) {
-    int BitWidth = Op0KnownZero.getBitWidth();
-    // Ignore Sign Bit.
-    Op0KnownZero.clearBit(BitWidth - 1);
-    int Op1OnePosition = BitWidth - Op1KnownOne.countLeadingZeros() - 1;
-    int Op0ZeroPosition = BitWidth - Op0KnownZero.countLeadingZeros() - 1;
-    if ((Op0ZeroPosition != (BitWidth - 1)) &&
-        (Op0ZeroPosition >= Op1OnePosition))
-      return true;
-  }
-  return false;
-}
 
 /// WillNotOverflowSignedAdd - Return true if we can prove that:
 ///    (sext (add LHS, RHS))  === (add (sext LHS), (sext RHS))
 /// This basically requires proving that the add in the original type would not
 /// overflow to change the sign bit or have a carry out.
-/// TODO: Handle this for Vectors.
 bool InstCombiner::WillNotOverflowSignedAdd(Value *LHS, Value *RHS) {
   // There are different heuristics we can use for this.  Here are some simple
   // ones.
@@ -928,29 +905,14 @@ bool InstCombiner::WillNotOverflowSignedAdd(Value *LHS, Value *RHS) {
   if (ComputeNumSignBits(LHS) > 1 && ComputeNumSignBits(RHS) > 1)
     return true;
 
-  if (IntegerType *IT = dyn_cast<IntegerType>(LHS->getType())) {
 
-    int BitWidth = IT->getBitWidth();
-    APInt LHSKnownZero(BitWidth, 0, /*isSigned*/ true);
-    APInt LHSKnownOne(BitWidth, 0, /*isSigned*/ true);
-    computeKnownBits(LHS, LHSKnownZero, LHSKnownOne);
+  // If one of the operands only has one non-zero bit, and if the other operand
+  // has a known-zero bit in a more significant place than it (not including the
+  // sign bit) the ripple may go up to and fill the zero, but won't change the
+  // sign.  For example, (X & ~4) + 1.
+
+  // TODO: Implement.
 
-    APInt RHSKnownZero(BitWidth, 0, /*isSigned*/ true);
-    APInt RHSKnownOne(BitWidth, 0, /*isSigned*/ true);
-    computeKnownBits(RHS, RHSKnownZero, RHSKnownOne);
-
-    // Addition of two 2's compliment numbers having opposite signs will never
-    // overflow.
-    if ((LHSKnownOne[BitWidth - 1] && RHSKnownZero[BitWidth - 1]) ||
-        (LHSKnownZero[BitWidth - 1] && RHSKnownOne[BitWidth - 1]))
-      return true;
-
-    // Check if carry bit of addition will not cause overflow.
-    if (CheckRippleForAdd(LHSKnownZero, LHSKnownOne, RHSKnownZero, RHSKnownOne))
-      return true;
-    if (CheckRippleForAdd(RHSKnownZero, RHSKnownOne, LHSKnownZero, LHSKnownOne))
-      return true;
-  }
   return false;
 }
 
diff --git a/test/Transforms/InstCombine/AddOverflow.ll b/test/Transforms/InstCombine/AddOverflow.ll
deleted file mode 100644 (file)
index 1bbd1fc..0000000
+++ /dev/null
@@ -1,56 +0,0 @@
-; RUN: opt < %s -instcombine -S | FileCheck %s
-
-target datalayout = "e-m:e-i64:64-f80:128-n8:16:32:64-S128"
-target triple = "x86_64-unknown-linux-gnu"
-
-; CHECK-LABEL: @ripple(
-; CHECK: add nsw i16 %tmp1, 1
-define i32 @ripple(i16 signext %x) {
-bb:
-  %tmp = sext i16 %x to i32
-  %tmp1 = and i32 %tmp, -5
-  %tmp2 = trunc i32 %tmp1 to i16
-  %tmp3 = sext i16 %tmp2 to i32
-  %tmp4 = add i32 %tmp3, 1
-  ret i32 %tmp4
-}
-
-; CHECK-LABEL: @ripplenot(
-; CHECK: add i32 %tmp3, 4
-define i32 @ripplenot(i16 signext %x) {
-bb:
-  %tmp = sext i16 %x to i32
-  %tmp1 = and i32 %tmp, -3
-  %tmp2 = trunc i32 %tmp1 to i16
-  %tmp3 = sext i16 %tmp2 to i32
-  %tmp4 = add i32 %tmp3, 4
-  ret i32 %tmp4
-}
-
-; CHECK-LABEL: @oppositesign(
-; CHECK: add nsw i16 %tmp1, 4
-define i32 @oppositesign(i16 signext %x) {
-bb:
-  %tmp = sext i16 %x to i32
-  %tmp1 = or i32 %tmp, 32768
-  %tmp2 = trunc i32 %tmp1 to i16
-  %tmp3 = sext i16 %tmp2 to i32
-  %tmp4 = add i32 %tmp3, 4
-  ret i32 %tmp4
-}
-
-; CHECK-LABEL: @ripplenot_var(
-; CHECK: add i32 %tmp6, %tmp7
-define i32 @ripplenot_var(i16 signext %x, i16 signext %y) {
-bb:
-  %tmp = sext i16 %x to i32
-  %tmp1 = and i32 %tmp, -5
-  %tmp2 = trunc i32 %tmp1 to i16
-  %tmp3 = sext i16 %y to i32
-  %tmp4 = or i32 %tmp3, 2
-  %tmp5 = trunc i32 %tmp4 to i16
-  %tmp6 = sext i16 %tmp5 to i32
-  %tmp7 = sext i16 %tmp2 to i32
-  %tmp8 = add i32 %tmp6, %tmp7
-  ret i32 %tmp8
-}