]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/commitdiff
[ValueTracking] Extend range metadata to call/invoke
authorJingyue Wu <jingyue@google.com>
Thu, 19 Jun 2014 16:50:16 +0000 (16:50 +0000)
committerJingyue Wu <jingyue@google.com>
Thu, 19 Jun 2014 16:50:16 +0000 (16:50 +0000)
Summary:
With this patch, range metadata can be added to call/invoke including
IntrinsicInst. Previously, it could only be added to load.

Rename computeKnownBitsLoad to computeKnownBitsFromRangeMetadata because
range metadata is not only used by load.

Update the language reference to reflect this change.

Test Plan:
Add several tests in range-2.ll to confirm the verifier is happy with
having range metadata on call/invoke.

Add two tests in AddOverFlow.ll to confirm annotating range metadata to
call/invoke can benefit InstCombine.

Reviewers: meheff, nlewycky, reames, hfinkel, eliben

Reviewed By: eliben

Subscribers: llvm-commits

Differential Revision: http://reviews.llvm.org/D4187

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211281 91177308-0d34-0410-b5e6-96231b3b80d8

docs/LangRef.rst
include/llvm/Analysis/ValueTracking.h
lib/Analysis/ValueTracking.cpp
lib/CodeGen/SelectionDAG/SelectionDAG.cpp
lib/IR/Verifier.cpp
test/Transforms/InstCombine/AddOverFlow.ll
test/Transforms/InstCombine/add2.ll
test/Verifier/range-1.ll
test/Verifier/range-2.ll

index cb94d3967b13813b84ec154f62c075cc6a2909a8..b75058fa9a5f50136180fe8f066ee69118a0abf8 100644 (file)
@@ -2749,11 +2749,12 @@ number representing the maximum relative error, for example:
 '``range``' Metadata
 ^^^^^^^^^^^^^^^^^^^^
 
-``range`` metadata may be attached only to loads of integer types. It
-expresses the possible ranges the loaded value is in. The ranges are
-represented with a flattened list of integers. The loaded value is known
-to be in the union of the ranges defined by each consecutive pair. Each
-pair has the following properties:
+``range`` metadata may be attached only to ``load``, ``call`` and ``invoke`` of
+integer types. It expresses the possible ranges the loaded value or the value
+returned by the called function at this call site is in. The ranges are
+represented with a flattened list of integers. The loaded value or the value
+returned is known to be in the union of the ranges defined by each consecutive
+pair. Each pair has the following properties:
 
 -  The type must match the type loaded by the instruction.
 -  The pair ``a,b`` represents the range ``[a,b)``.
@@ -2771,8 +2772,9 @@ Examples:
 
       %a = load i8* %x, align 1, !range !0 ; Can only be 0 or 1
       %b = load i8* %y, align 1, !range !1 ; Can only be 255 (-1), 0 or 1
-      %c = load i8* %z, align 1, !range !2 ; Can only be 0, 1, 3, 4 or 5
-      %d = load i8* %z, align 1, !range !3 ; Can only be -2, -1, 3, 4 or 5
+      %c = call i8 @foo(),       !range !2 ; Can only be 0, 1, 3, 4 or 5
+      %d = invoke i8 @bar() to label %cont
+             unwind label %lpad, !range !3 ; Can only be -2, -1, 3, 4 or 5
     ...
     !0 = metadata !{ i8 0, i8 2 }
     !1 = metadata !{ i8 255, i8 2 }
index ce7896738d8cb9a4c703f7f8e5dc4f63acaa8888..83b5408fb1c2aff3e2a8911b37a328d941081434 100644 (file)
@@ -37,7 +37,10 @@ namespace llvm {
   /// for all of the elements in the vector.
   void computeKnownBits(Value *V,  APInt &KnownZero, APInt &KnownOne,
                         const DataLayout *TD = nullptr, unsigned Depth = 0);
-  void computeKnownBitsLoad(const MDNode &Ranges, APInt &KnownZero);
+  /// Compute known bits from the range metadata.
+  /// \p KnownZero the set of bits that are known to be zero
+  void computeKnownBitsFromRangeMetadata(const MDNode &Ranges,
+                                         APInt &KnownZero);
 
   /// ComputeSignBit - Determine whether the sign bit is known to be zero or
   /// one.  Convenience wrapper around computeKnownBits.
index 4f48753578289057d39c0e0b5257182cceb2355f..9de945ed701648b71ca32a3d3fcd31bc86f02d57 100644 (file)
@@ -188,7 +188,8 @@ static void computeKnownBitsMul(Value *Op0, Value *Op1, bool NSW,
     KnownOne.setBit(BitWidth - 1);
 }
 
-void llvm::computeKnownBitsLoad(const MDNode &Ranges, APInt &KnownZero) {
+void llvm::computeKnownBitsFromRangeMetadata(const MDNode &Ranges,
+                                             APInt &KnownZero) {
   unsigned BitWidth = KnownZero.getBitWidth();
   unsigned NumRanges = Ranges.getNumOperands() / 2;
   assert(NumRanges >= 1);
@@ -338,7 +339,7 @@ void llvm::computeKnownBits(Value *V, APInt &KnownZero, APInt &KnownOne,
   default: break;
   case Instruction::Load:
     if (MDNode *MD = cast<LoadInst>(I)->getMetadata(LLVMContext::MD_range))
-      computeKnownBitsLoad(*MD, KnownZero);
+      computeKnownBitsFromRangeMetadata(*MD, KnownZero);
     break;
   case Instruction::And: {
     // If either the LHS or the RHS are Zero, the result is zero.
@@ -733,6 +734,12 @@ void llvm::computeKnownBits(Value *V, APInt &KnownZero, APInt &KnownOne,
     break;
   }
   case Instruction::Call:
+  case Instruction::Invoke:
+    if (MDNode *MD = cast<Instruction>(I)->getMetadata(LLVMContext::MD_range))
+      computeKnownBitsFromRangeMetadata(*MD, KnownZero);
+    // If a range metadata is attached to this IntrinsicInst, intersect the
+    // explicit range specified by the metadata and the implicit range of
+    // the intrinsic.
     if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(I)) {
       switch (II->getIntrinsicID()) {
       default: break;
@@ -742,16 +749,16 @@ void llvm::computeKnownBits(Value *V, APInt &KnownZero, APInt &KnownOne,
         // If this call is undefined for 0, the result will be less than 2^n.
         if (II->getArgOperand(1) == ConstantInt::getTrue(II->getContext()))
           LowBits -= 1;
-        KnownZero = APInt::getHighBitsSet(BitWidth, BitWidth - LowBits);
+        KnownZero |= APInt::getHighBitsSet(BitWidth, BitWidth - LowBits);
         break;
       }
       case Intrinsic::ctpop: {
         unsigned LowBits = Log2_32(BitWidth)+1;
-        KnownZero = APInt::getHighBitsSet(BitWidth, BitWidth - LowBits);
+        KnownZero |= APInt::getHighBitsSet(BitWidth, BitWidth - LowBits);
         break;
       }
       case Intrinsic::x86_sse42_crc32_64_64:
-        KnownZero = APInt::getHighBitsSet(64, 32);
+        KnownZero |= APInt::getHighBitsSet(64, 32);
         break;
       }
     }
index 639eb462e7ff9ed66de9e9d34e13979bca620c7a..5923f0e208e1036701526d09b8949b2cf5026d11 100644 (file)
@@ -2084,7 +2084,7 @@ void SelectionDAG::computeKnownBits(SDValue Op, APInt &KnownZero,
       unsigned MemBits = VT.getScalarType().getSizeInBits();
       KnownZero |= APInt::getHighBitsSet(BitWidth, BitWidth - MemBits);
     } else if (const MDNode *Ranges = LD->getRanges()) {
-      computeKnownBitsLoad(*Ranges, KnownZero);
+      computeKnownBitsFromRangeMetadata(*Ranges, KnownZero);
     }
     break;
   }
index d1c7f7d25c3955d0059f58bc787065e4d56ee1d3..ad3c29c564e77d9df33fb95925de0e479667b7bb 100644 (file)
@@ -2233,7 +2233,8 @@ void Verifier::visitInstruction(Instruction &I) {
   }
 
   MDNode *MD = I.getMetadata(LLVMContext::MD_range);
-  Assert1(!MD || isa<LoadInst>(I), "Ranges are only for loads!", &I);
+  Assert1(!MD || isa<LoadInst>(I) || isa<CallInst>(I) || isa<InvokeInst>(I),
+          "Ranges are only for loads, calls and invokes!", &I);
 
   InstsInThisBlock.insert(&I);
 }
index 70178ec83b6ea5e1b80feb4da3df976cd8a7997a..8f3d429c8d6046e4749c801df0db5fa37ce86979 100644 (file)
@@ -34,6 +34,44 @@ define i16 @zero_sign_bit2(i16 %a, i16 %b) {
   ret i16 %3
 }
 
+declare i16 @bounded(i16 %input);
+declare i32 @__gxx_personality_v0(...);
+!0 = metadata !{i16 0, i16 32768} ; [0, 32767]
+!1 = metadata !{i16 0, i16 32769} ; [0, 32768]
+
+define i16 @add_bounded_values(i16 %a, i16 %b) {
+; CHECK-LABEL: @add_bounded_values(
+entry:
+  %c = call i16 @bounded(i16 %a), !range !0
+  %d = invoke i16 @bounded(i16 %b) to label %cont unwind label %lpad, !range !0
+cont:
+; %c and %d are in [0, 32767]. Therefore, %c + %d doesn't unsigned overflow.
+  %e = add i16 %c, %d
+; CHECK: add nuw i16 %c, %d
+  ret i16 %e
+lpad:
+  %0 = landingpad { i8*, i32 } personality i8* bitcast (i32 (...)* @__gxx_personality_v0 to i8*)
+          filter [0 x i8*] zeroinitializer
+  ret i16 42
+}
+
+define i16 @add_bounded_values_2(i16 %a, i16 %b) {
+; CHECK-LABEL: @add_bounded_values_2(
+entry:
+  %c = call i16 @bounded(i16 %a), !range !1
+  %d = invoke i16 @bounded(i16 %b) to label %cont unwind label %lpad, !range !1
+cont:
+; Similar to add_bounded_values, but %c and %d are in [0, 32768]. Therefore,
+; %c + %d may unsigned overflow and we cannot add NUW.
+  %e = add i16 %c, %d
+; CHECK: add i16 %c, %d
+  ret i16 %e
+lpad:
+  %0 = landingpad { i8*, i32 } personality i8* bitcast (i32 (...)* @__gxx_personality_v0 to i8*)
+          filter [0 x i8*] zeroinitializer
+  ret i16 42
+}
+
 ; CHECK-LABEL: @ripple_nsw1
 ; CHECK: add nsw i16 %a, %b
 define i16 @ripple_nsw1(i16 %x, i16 %y) {
index 0328c4ff6e3fca4f7570df45768a1465c6ea204a..821fce0dabcc89802f97f9df148aaa7ed7a5581d 100644 (file)
@@ -217,3 +217,44 @@ define i32 @mul_add_to_mul_6(i32 %x, i32 %y) {
 ; CHECK-NEXT: %add = mul nsw i32 %mul1, 6
 ; CHECK-NEXT: ret i32 %add
 }
+
+; This test and the next test verify that when a range metadata is attached to
+; llvm.cttz, ValueTracking correctly intersects the range specified by the
+; metadata and the range implied by the intrinsic.
+;
+; In this test, the range specified by the metadata is more strict. Therefore,
+; ValueTracking uses that range.
+define i16 @add_cttz(i16 %a) {
+; CHECK-LABEL: @add_cttz(
+  ; llvm.cttz.i16(..., /*is_zero_undefined=*/true) implies the value returned
+  ; is in [0, 16). The range metadata indicates the value returned is in [0, 8).
+  ; Intersecting these ranges, we know the value returned is in [0, 8).
+  ; Therefore, InstCombine will transform
+  ;     add %cttz, 1111 1111 1111 1000 ; decimal -8
+  ; to
+  ;     or  %cttz, 1111 1111 1111 1000
+  %cttz = call i16 @llvm.cttz.i16(i16 %a, i1 true), !range !0
+  %b = add i16 %cttz, -8
+; CHECK: or i16 %cttz, -8
+  ret i16 %b
+}
+declare i16 @llvm.cttz.i16(i16, i1)
+!0 = metadata !{i16 0, i16 8}
+
+; Similar to @add_cttz, but in this test, the range implied by the
+; intrinsic is more strict. Therefore, ValueTracking uses that range.
+define i16 @add_cttz_2(i16 %a) {
+; CHECK-LABEL: @add_cttz_2(
+  ; llvm.cttz.i16(..., /*is_zero_undefined=*/true) implies the value returned
+  ; is in [0, 16). The range metadata indicates the value returned is in
+  ; [0, 32). Intersecting these ranges, we know the value returned is in
+  ; [0, 16). Therefore, InstCombine will transform
+  ;     add %cttz, 1111 1111 1111 0000 ; decimal -16
+  ; to
+  ;     or  %cttz, 1111 1111 1111 0000
+  %cttz = call i16 @llvm.cttz.i16(i16 %a, i1 true), !range !1
+  %b = add i16 %cttz, -16
+; CHECK: or i16 %cttz, -16
+  ret i16 %b
+}
+!1 = metadata !{i16 0, i16 32}
index b6a75d13bba0963f18068607f7add705c0ea5e65..f15ca3f740656f697b558f9d95647f70fa05aefc 100644 (file)
@@ -6,7 +6,7 @@ entry:
   ret void
 }
 !0 = metadata !{i8 0, i8 1}
-; CHECK: Ranges are only for loads!
+; CHECK: Ranges are only for loads, calls and invokes!
 ; CHECK-NEXT: store i8 0, i8* %x, align 1, !range !0
 
 define i8 @f2(i8* %x) {
index 8d85d19151950260a2771b5c3d29c45601688c36..1d2e0575d76a64c05a3fdb3881526a166c0ac436 100644 (file)
@@ -34,3 +34,33 @@ entry:
   ret i8 %y
 }
 !4 = metadata !{i8 -1, i8 0, i8 1, i8 -2}
+
+; We can annotate the range of the return value of a CALL.
+define void @call_all(i8* %x) {
+entry:
+  %v1 = call i8 @f1(i8* %x), !range !0
+  %v2 = call i8 @f2(i8* %x), !range !1
+  %v3 = call i8 @f3(i8* %x), !range !2
+  %v4 = call i8 @f4(i8* %x), !range !3
+  %v5 = call i8 @f5(i8* %x), !range !4
+  ret void
+}
+
+; We can annotate the range of the return value of an INVOKE.
+define void @invoke_all(i8* %x) {
+entry:
+  %v1 = invoke i8 @f1(i8* %x) to label %cont unwind label %lpad, !range !0
+  %v2 = invoke i8 @f2(i8* %x) to label %cont unwind label %lpad, !range !1
+  %v3 = invoke i8 @f3(i8* %x) to label %cont unwind label %lpad, !range !2
+  %v4 = invoke i8 @f4(i8* %x) to label %cont unwind label %lpad, !range !3
+  %v5 = invoke i8 @f5(i8* %x) to label %cont unwind label %lpad, !range !4
+
+cont:
+  ret void
+
+lpad:
+  %4 = landingpad { i8*, i32 } personality i8* bitcast (i32 (...)* @__gxx_personality_v0 to i8*)
+          filter [0 x i8*] zeroinitializer
+  ret void
+}
+declare i32 @__gxx_personality_v0(...)