summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 5385df6)
raw | patch | inline | side by side (parent: 5385df6)
author | David Blaikie <dblaikie@gmail.com> | |
Thu, 23 Oct 2014 00:06:27 +0000 (00:06 +0000) | ||
committer | David Blaikie <dblaikie@gmail.com> | |
Thu, 23 Oct 2014 00:06:27 +0000 (00:06 +0000) |
Now that we're sure the only root (non-abstract) scope is the current
function scope, there's no need for isCurrentFunctionScope, the property
can be tested directly instead.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@220451 91177308-0d34-0410-b5e6-96231b3b80d8
function scope, there's no need for isCurrentFunctionScope, the property
can be tested directly instead.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@220451 91177308-0d34-0410-b5e6-96231b3b80d8
include/llvm/CodeGen/LexicalScopes.h | patch | blob | history | |
lib/CodeGen/AsmPrinter/DwarfDebug.cpp | patch | blob | history | |
lib/CodeGen/AsmPrinter/DwarfDebug.h | patch | blob | history |
index 1eb7299f48861b28adcf6b4e3e8ba2456dbb4479..021fd98750a0fde165e4507732e6b30520aebe33 100644 (file)
/// empty - Return true if there is any lexical scope information available.
bool empty() { return CurrentFnLexicalScope == nullptr; }
- /// isCurrentFunctionScope - Return true if given lexical scope represents
- /// current function.
- bool isCurrentFunctionScope(const LexicalScope *LS) {
- return LS == CurrentFnLexicalScope;
- }
-
/// getCurrentFunctionScope - Return lexical scope for the current function.
LexicalScope *getCurrentFunctionScope() const {
return CurrentFnLexicalScope;
index f13ca2281a28b954c8234146926db50df84c54bb..9fb9d43b89b3da09a2ba81fb5dc1ffaa1ae26947 100644 (file)
void DwarfDebug::createAbstractVariable(const DIVariable &Var,
LexicalScope *Scope) {
auto AbsDbgVariable = make_unique<DbgVariable>(Var, DIExpression(), this);
- addScopeVariable(Scope, AbsDbgVariable.get());
+ addNonArgumentScopeVariable(Scope, AbsDbgVariable.get());
AbstractVariables[Var] = std::move(AbsDbgVariable);
}
// If Var is a current function argument then add it to CurrentFnArguments list.
bool DwarfDebug::addCurrentFnArgument(DbgVariable *Var, LexicalScope *Scope) {
- if (!LScopes.isCurrentFunctionScope(Scope))
+ if (Scope->getParent())
return false;
DIVariable DV = Var->getVariable();
if (DV.getTag() != dwarf::DW_TAG_arg_variable)
// Find variables for each lexical scope.
void
-DwarfDebug::collectVariableInfo(SmallPtrSetImpl<const MDNode *> &Processed) {
- LexicalScope *FnScope = LScopes.getCurrentFunctionScope();
- DwarfCompileUnit *TheCU = SPMap.lookup(FnScope->getScopeNode());
-
+DwarfDebug::collectVariableInfo(DwarfCompileUnit &TheCU, DISubprogram SP,
+ SmallPtrSetImpl<const MDNode *> &Processed) {
// Grab the variable info that was squirreled away in the MMI side-table.
collectVariableInfoFromMMITable(Processed);
DotDebugLocEntries.resize(DotDebugLocEntries.size() + 1);
DebugLocList &LocList = DotDebugLocEntries.back();
- LocList.CU = TheCU;
+ LocList.CU = &TheCU;
LocList.Label =
Asm->GetTempSymbol("debug_loc", DotDebugLocEntries.size() - 1);
}
// Collect info for variables that were optimized out.
- DIArray Variables = DISubprogram(FnScope->getScopeNode()).getVariables();
+ DIArray Variables = SP.getVariables();
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
assert(DV.isVariable());
void DwarfDebug::addScopeVariable(LexicalScope *LS, DbgVariable *Var) {
if (addCurrentFnArgument(Var, LS))
return;
+ addNonArgumentScopeVariable(LS, Var);
+}
+
+void DwarfDebug::addNonArgumentScopeVariable(LexicalScope *LS,
+ DbgVariable *Var) {
SmallVectorImpl<DbgVariable *> &Vars = ScopeVariables[LS];
DIVariable DV = Var->getVariable();
// Variables with positive arg numbers are parameters.
// Set DwarfDwarfCompileUnitID in MCContext to default value.
Asm->OutStreamer.getContext().setDwarfCompileUnitID(0);
- SmallPtrSet<const MDNode *, 16> ProcessedVars;
- collectVariableInfo(ProcessedVars);
-
LexicalScope *FnScope = LScopes.getCurrentFunctionScope();
- DwarfCompileUnit &TheCU = *SPMap.lookup(FnScope->getScopeNode());
+ DISubprogram SP(FnScope->getScopeNode());
+ DwarfCompileUnit &TheCU = *SPMap.lookup(SP);
+
+ SmallPtrSet<const MDNode *, 16> ProcessedVars;
+ collectVariableInfo(TheCU, SP, ProcessedVars);
// Add the range of this function to the list of ranges for the CU.
TheCU.addRange(RangeSpan(FunctionBeginSym, FunctionEndSym));
index 069787a7015c24f526ca98cad0762b57bd0999d8..169e9421699c0c808aaf8fb123f24fb1be208906 100644 (file)
MCDwarfDwoLineTable *getDwoLineTable(const DwarfCompileUnit &);
void addScopeVariable(LexicalScope *LS, DbgVariable *Var);
+ void addNonArgumentScopeVariable(LexicalScope *LS, DbgVariable *Var);
const SmallVectorImpl<std::unique_ptr<DwarfUnit>> &getUnits() {
return InfoHolder.getUnits();
bool addCurrentFnArgument(DbgVariable *Var, LexicalScope *Scope);
/// \brief Populate LexicalScope entries with variables' info.
- void collectVariableInfo(SmallPtrSetImpl<const MDNode *> &ProcessedVars);
+ void collectVariableInfo(DwarfCompileUnit &TheCU, DISubprogram SP,
+ SmallPtrSetImpl<const MDNode *> &ProcessedVars);
/// \brief Build the location list for all DBG_VALUEs in the
/// function that describe the same variable.