summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: e94349f)
raw | patch | inline | side by side (parent: e94349f)
author | Timur Iskhodzhanov <timurrrr@google.com> | |
Wed, 3 Apr 2013 11:27:54 +0000 (11:27 +0000) | ||
committer | Timur Iskhodzhanov <timurrrr@google.com> | |
Wed, 3 Apr 2013 11:27:54 +0000 (11:27 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@178634 91177308-0d34-0410-b5e6-96231b3b80d8
lib/Target/X86/X86CallingConv.td | patch | blob | history | |
test/CodeGen/X86/thiscall-struct-return.ll | [deleted file] | patch | blob | history |
test/CodeGen/X86/win32_sret.ll | patch | blob | history |
index b516be069699681fee9f5551b7e35fc3caf70908..9eafbd55a5ae5231de099b6e4a546a400769e962 100644 (file)
// Promote i8/i16 arguments to i32.
CCIfType<[i8, i16], CCPromoteToType<i32>>,
- // Pass sret arguments indirectly through EAX
- CCIfSRet<CCAssignToReg<[EAX]>>,
+ // Pass sret arguments indirectly through stack.
+ CCIfSRet<CCAssignToStack<4, 4>>,
// The first integer argument is passed in ECX
CCIfType<[i32], CCAssignToReg<[ECX]>>,
diff --git a/test/CodeGen/X86/thiscall-struct-return.ll b/test/CodeGen/X86/thiscall-struct-return.ll
+++ /dev/null
@@ -1,47 +0,0 @@
-; RUN: llc < %s -mtriple=i386-PC-Win32 | FileCheck %s
-
-%class.C = type { i8 }
-%struct.S = type { i32 }
-%struct.M = type { i32, i32 }
-
-declare void @_ZN1CC1Ev(%class.C* %this) unnamed_addr nounwind align 2
-declare x86_thiscallcc void @_ZNK1C5SmallEv(%struct.S* noalias sret %agg.result, %class.C* %this) nounwind align 2
-declare x86_thiscallcc void @_ZNK1C6MediumEv(%struct.M* noalias sret %agg.result, %class.C* %this) nounwind align 2
-
-define void @testv() nounwind {
-; CHECK: testv:
-; CHECK: leal 16(%esp), %esi
-; CHECK-NEXT: movl %esi, (%esp)
-; CHECK-NEXT: calll _ZN1CC1Ev
-; CHECK: leal 8(%esp), %eax
-; CHECK-NEXT: movl %esi, %ecx
-; CHECK-NEXT: calll _ZNK1C5SmallEv
-entry:
- %c = alloca %class.C, align 1
- %tmp = alloca %struct.S, align 4
- call void @_ZN1CC1Ev(%class.C* %c)
- ; This call should put the return structure as a pointer
- ; into EAX instead of returning directly in EAX. The this
- ; pointer should go into ECX
- call x86_thiscallcc void @_ZNK1C5SmallEv(%struct.S* sret %tmp, %class.C* %c)
- ret void
-}
-
-define void @test2v() nounwind {
-; CHECK: test2v:
-; CHECK: leal 16(%esp), %esi
-; CHECK-NEXT: movl %esi, (%esp)
-; CHECK-NEXT: calll _ZN1CC1Ev
-; CHECK: leal 8(%esp), %eax
-; CHECK-NEXT: movl %esi, %ecx
-; CHECK-NEXT: calll _ZNK1C6MediumEv
-entry:
- %c = alloca %class.C, align 1
- %tmp = alloca %struct.M, align 4
- call void @_ZN1CC1Ev(%class.C* %c)
- ; This call should put the return structure as a pointer
- ; into EAX instead of returning directly in EAX/EDX. The this
- ; pointer should go into ECX
- call x86_thiscallcc void @_ZNK1C6MediumEv(%struct.M* sret %tmp, %class.C* %c)
- ret void
-}
index 19cbfd45edaf72188342697355b7b9a4bd0765e5..f1dd99543bdc948b49aa6f0c3c17e6b665ce22b4 100644 (file)
store i32 42, i32* %x, align 4
ret void
}
+
+%struct.S5 = type { i32 }
+%class.C5 = type { i8 }
+
+define x86_thiscallcc void @"\01?foo@C5@@QAE?AUS5@@XZ"(%struct.S5* noalias sret %agg.result, %class.C5* %this) {
+entry:
+ %this.addr = alloca %class.C5*, align 4
+ store %class.C5* %this, %class.C5** %this.addr, align 4
+ %this1 = load %class.C5** %this.addr
+ %x = getelementptr inbounds %struct.S5* %agg.result, i32 0, i32 0
+ store i32 42, i32* %x, align 4
+ ret void
+; WIN32: {{^}}"?foo@C5@@QAE?AUS5@@XZ":
+
+; The address of the return structure is passed as an implicit parameter.
+; In the -O0 build, %eax is spilled at the beginning of the function, hence we
+; should match both 4(%esp) and 8(%esp).
+; WIN32: {{[48]}}(%esp), %eax
+; WIN32: movl $42, (%eax)
+; WIN32: ret $4
+}
+
+define void @call_foo5() {
+entry:
+ %c = alloca %class.C5, align 1
+ %s = alloca %struct.S5, align 4
+ call x86_thiscallcc void @"\01?foo@C5@@QAE?AUS5@@XZ"(%struct.S5* sret %s, %class.C5* %c)
+; WIN32: {{^}}_call_foo5:
+
+; Load the address of the result and put it onto stack
+; (through %ecx in the -O0 build).
+; WIN32: leal {{[0-9]+}}(%esp), %eax
+; WIN32: movl %eax, (%e{{[sc][px]}})
+
+; The this pointer goes to ECX.
+; WIN32-NEXT: leal {{[0-9]+}}(%esp), %ecx
+; WIN32-NEXT: calll "?foo@C5@@QAE?AUS5@@XZ"
+; WIN32: ret
+ ret void
+}