summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2259a26)
raw | patch | inline | side by side (parent: 2259a26)
author | Jim Grosbach <grosbach@apple.com> | |
Tue, 29 Apr 2014 22:41:50 +0000 (22:41 +0000) | ||
committer | Jim Grosbach <grosbach@apple.com> | |
Tue, 29 Apr 2014 22:41:50 +0000 (22:41 +0000) |
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@207583 91177308-0d34-0410-b5e6-96231b3b80d8
lib/CodeGen/SelectionDAG/DAGCombiner.cpp | patch | blob | history |
index 7f156537cb8a510aeebc02eba1b54c0c7d46614c..014e97d7b2a9d85d1b9809cefdb958d7c85c4023 100644 (file)
assert(N0.getOperand(0).getValueType() == N1.getOperand(0).getValueType() &&
"Inputs to shuffles are not the same type");
-
+
// Check that both shuffles use the same mask. The masks are known to be of
// the same length because the result vector type is the same.
// Check also that shuffles have only one use to avoid introducing extra
// two ways to fold this node into a shuffle.
SmallVector<int,4> Mask1;
SmallVector<int,4> Mask2;
-
+
for (unsigned i = 0; i != NumElts && CanFold; ++i) {
int M0 = SV0->getMaskElt(i);
int M1 = SV1->getMaskElt(i);
-
+
// Both shuffle indexes are undef. Propagate Undef.
if (M0 < 0 && M1 < 0) {
Mask1.push_back(M0);
CanFold = false;
break;
}
-
+
Mask1.push_back(M0 < (int)NumElts ? M0 : M1 + NumElts);
Mask2.push_back(M1 < (int)NumElts ? M1 : M0 + NumElts);
}
// tryToFoldExtendOfConstant - Try to fold a sext/zext/aext
// dag node into a ConstantSDNode or a build_vector of constants.
// This function is called by the DAGCombiner when visiting sext/zext/aext
-// dag nodes (see for example method DAGCombiner::visitSIGN_EXTEND).
+// dag nodes (see for example method DAGCombiner::visitSIGN_EXTEND).
// Vector extends are not folded if operations are legal; this is to
// avoid introducing illegal build_vector dag nodes.
static SDNode *tryToFoldExtendOfConstant(SDNode *N, const TargetLowering &TLI,
@@ -4730,7 +4730,7 @@ static SDNode *tryToFoldExtendOfConstant(SDNode *N, const TargetLowering &TLI,
(!LegalTypes || (!LegalOperations && TLI.isTypeLegal(SVT))) &&
ISD::isBuildVectorOfConstantSDNodes(N0.getNode())))
return nullptr;
-
+
// We can fold this node into a build_vector.
unsigned VTBits = SVT.getSizeInBits();
unsigned EVTBits = N0->getValueType(0).getScalarType().getSizeInBits();
}
}
- // If everything is good, we can make a shuffle operation.
+ // If everything is good, we can make a shuffle operation.
if (VecIn1.getNode()) {
SmallVector<int, 8> Mask;
for (unsigned i = 0; i != NumInScalars; ++i) {