From: Adrian Prantl Date: Wed, 21 Jan 2015 00:59:20 +0000 (+0000) Subject: Make DIExpression::Verify() stricter by checking that the number of X-Git-Url: https://git.ti.com/gitweb?p=opencl%2Fllvm.git;a=commitdiff_plain;h=4d569edd37897df7a614c689ed4f978fd8cb2d78 Make DIExpression::Verify() stricter by checking that the number of elements and the ordering is sane and cleanup the accessors. git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@226627 91177308-0d34-0410-b5e6-96231b3b80d8 --- diff --git a/include/llvm/IR/DebugInfo.h b/include/llvm/IR/DebugInfo.h index 75209225a5..3e7764c85d 100644 --- a/include/llvm/IR/DebugInfo.h +++ b/include/llvm/IR/DebugInfo.h @@ -1036,6 +1036,9 @@ public: /// \brief Process DILocation. void processLocation(const Module &M, DILocation Loc); + /// \brief Process DIExpression. + void processExpression(DIExpression Expr); + /// \brief Clear all lists. void reset(); diff --git a/lib/IR/DebugInfo.cpp b/lib/IR/DebugInfo.cpp index 9003fff707..5dff50d362 100644 --- a/lib/IR/DebugInfo.cpp +++ b/lib/IR/DebugInfo.cpp @@ -148,17 +148,18 @@ uint64_t DIExpression::getElement(unsigned Idx) const { } bool DIExpression::isVariablePiece() const { - return getNumElements() && getElement(0) == dwarf::DW_OP_piece; + unsigned N = getNumElements(); + return N >=3 && getElement(N-3) == dwarf::DW_OP_piece; } uint64_t DIExpression::getPieceOffset() const { - assert(isVariablePiece()); - return getElement(1); + assert(isVariablePiece() && "not a piece"); + return getElement(getNumElements()-2); } uint64_t DIExpression::getPieceSize() const { - assert(isVariablePiece()); - return getElement(2); + assert(isVariablePiece() && "not a piece"); + return getElement(getNumElements()-1); } //===----------------------------------------------------------------------===// @@ -593,6 +594,24 @@ bool DIExpression::Verify() const { if (!DbgNode) return true; + unsigned N = getNumElements(); + for (unsigned I = 0; I < N; ++I) + switch (getElement(I)) { + case DW_OP_piece: + // DW_OP_piece has to be the last element in the expression and take two + // arguments. + if (getElement(I) == DW_OP_piece && !isVariablePiece()) + return false; + I += 2; + break; + case DW_OP_plus: + // Takes one argument. + if (I+1 == N) + return false; + I += 1; + break; + default: break; + } return isExpression() && DbgNode->getNumOperands() == 1; } diff --git a/lib/IR/Verifier.cpp b/lib/IR/Verifier.cpp index c95018d177..8a523c2801 100644 --- a/lib/IR/Verifier.cpp +++ b/lib/IR/Verifier.cpp @@ -2841,12 +2841,20 @@ void DebugInfoVerifier::processCallInst(DebugInfoFinder &Finder, if (Function *F = CI.getCalledFunction()) if (Intrinsic::ID ID = (Intrinsic::ID)F->getIntrinsicID()) switch (ID) { - case Intrinsic::dbg_declare: - Finder.processDeclare(*M, cast(&CI)); + case Intrinsic::dbg_declare: { + auto *DDI = cast(&CI); + Finder.processDeclare(*M, DDI); + if (auto E = DDI->getExpression()) + Assert1(DIExpression(E).Verify(), "DIExpression does not Verify!", E); break; - case Intrinsic::dbg_value: - Finder.processValue(*M, cast(&CI)); + } + case Intrinsic::dbg_value: { + auto *DVI = cast(&CI); + Finder.processValue(*M, DVI); + if (auto E = DVI->getExpression()) + Assert1(DIExpression(E).Verify(), "DIExpression does not Verify!", E); break; + } default: break; } diff --git a/test/DebugInfo/piece-verifier.ll b/test/DebugInfo/piece-verifier.ll new file mode 100644 index 0000000000..462bf277d9 --- /dev/null +++ b/test/DebugInfo/piece-verifier.ll @@ -0,0 +1,54 @@ +; RUN: not llvm-as -disable-output -verify-debug-info < %s 2>&1 | FileCheck %s +target datalayout = "e-m:o-i64:64-f80:128-n8:16:32:64-S128" +target triple = "x86_64-apple-macosx10.9.0" + +; Function Attrs: nounwind ssp uwtable +define i32 @foo(i64 %s.coerce0, i32 %s.coerce1) #0 { +entry: + call void @llvm.dbg.value(metadata i64 %s.coerce0, i64 0, metadata !20, metadata !24), !dbg !21 + call void @llvm.dbg.value(metadata i32 %s.coerce1, i64 0, metadata !22, metadata !27), !dbg !21 + ret i32 %s.coerce1, !dbg !23 +} + +; Function Attrs: nounwind readnone +declare void @llvm.dbg.declare(metadata, metadata, metadata) #1 + +; Function Attrs: nounwind readnone +declare void @llvm.dbg.value(metadata, i64, metadata, metadata) #1 + +attributes #0 = { nounwind ssp uwtable "no-frame-pointer-elim"="true" "no-frame-pointer-elim-non-leaf" } +attributes #1 = { nounwind readnone } + +!llvm.dbg.cu = !{!0} +!llvm.module.flags = !{!17, !18} +!llvm.ident = !{!19} + +!0 = !{!"0x11\0012\00clang version 3.5 \001\00\000\00\001", !1, !2, !2, !3, !2, !2} ; [ DW_TAG_compile_unit ] +!1 = !{!"pieces.c", !""} +!2 = !{} +!3 = !{!4} +!4 = !{!"0x2e\00foo\00foo\00\003\000\001\000\006\00256\001\003", !1, !5, !6, null, i32 (i64, i32)* @foo, null, null, !15} ; [ DW_TAG_subprogram ] [line 3] [def] [foo] +!5 = !{!"0x29", !1} ; [ DW_TAG_file_type ] [/pieces.c] +!6 = !{!"0x15\00\000\000\000\000\000\000", i32 0, null, null, !7, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ] +!7 = !{!8, !9} +!8 = !{!"0x24\00int\000\0032\0032\000\000\005", null, null} ; [ DW_TAG_base_type ] [int] [line 0, size 32, align 32, offset 0, enc DW_ATE_signed] +!9 = !{!"0x16\00S\001\000\000\000\000", !1, null, !10} ; [ DW_TAG_typedef ] [S] [line 1, size 0, align 0, offset 0] [from ] +!10 = !{!"0x13\00\001\00128\0064\000\000\000", !1, null, null, !11, null, null, null} ; [ DW_TAG_structure_type ] [line 1, size 128, align 64, offset 0] [def] [from ] +!11 = !{!12, !14} +!12 = !{!"0xd\00a\001\0064\0064\000\000", !1, !10, !13} ; [ DW_TAG_member ] [a] [line 1, size 64, align 64, offset 0] [from long int] +!13 = !{!"0x24\00long int\000\0064\0064\000\000\005", null, null} ; [ DW_TAG_base_type ] [long int] [line 0, size 64, align 64, offset 0, enc DW_ATE_signed] +!14 = !{!"0xd\00b\001\0032\0032\0064\000", !1, !10, !8} ; [ DW_TAG_member ] [b] [line 1, size 32, align 32, offset 64] [from int] +!15 = !{!16} +!16 = !{!"0x101\00s\0016777219\000", !4, !5, !9} ; [ DW_TAG_arg_variable ] [s] [line 3] +!17 = !{i32 2, !"Dwarf Version", i32 4} +!18 = !{i32 1, !"Debug Info Version", i32 2} +!19 = !{!"clang version 3.5 "} +!20 = !{!"0x101\00s\0016777219\000", !4, !5, !9} ; [ DW_TAG_arg_variable ] [s] [line 3] +!21 = !MDLocation(line: 3, scope: !4) +!22 = !{!"0x101\00s\0016777219\000", !4, !5, !9} ; [ DW_TAG_arg_variable ] [s] [line 3] +!23 = !MDLocation(line: 4, scope: !4) +!24 = !{!"0x102\006\00147\000\008"} ; [ DW_TAG_expression ] [DW_OP_piece 0 8] [piece, size 8, offset 0] +!25 = !{} +; This expression has elements after DW_OP_piece. +; CHECK: DIExpression does not Verify +!27 = !{!"0x102\00147\008\004\006"} ; [ DW_TAG_expression ] [DW_OP_piece 8 4] [piece, size 4, offset 8]