]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - cmake
Remove FIXMEs. The scope of a Variable is always a lexical scope; there is
[opencl/llvm.git] / cmake /
2014-03-29 Tim NorthoverARM64: initial backend import
2014-03-27 Hans WennborgWin installer: provide a pretty icon
2014-03-25 Yaron KerenRemove cmake module support for Visual C++ 2010 (MSVC10)
2014-03-25 Yaron KerenDisable Visual C++ warning 4722 about aborting a destru...
2014-03-16 NAKAMURA Takumi[CMake][cygming] Disable --out-implib from executables.
2014-03-13 Alexey Samsonov[CMake] Put -Werror to CMAKE_CXX_FLAGS instead of using...
2014-03-13 Ted Kremenek[CMake] Enable a bunch of Xcode build settings that...
2014-03-12 Rafael EspindolaUse -std=gnu++11 on cygwin and mingw.
2014-03-04 NAKAMURA Takumi[CMake] add_llvm_target(): No need to include TABLEGEN_...
2014-03-01 Chandler Carruth[C++11] Switch the CMake option from LLVM_ENABLE_CXX11...
2014-02-28 Rafael EspindolaWith rpaths being set correctly, SHLIBPATH_VAR is not...
2014-02-28 NAKAMURA Takumi[CMake] llvm_add_library(SHARED|STATIC): Fix broken...
2014-02-26 NAKAMURA Takumi[CMake] Work around to use target_link_libraries(PUBLIC...
2014-02-26 NAKAMURA Takumi[CMake] Move LLVMBUILD_LIB_DEPS stuff from add_llvm_lib...
2014-02-26 NAKAMURA Takumi[CMake] Use target_link_libraries(INTERFACE|PRIVATE...
2014-02-23 NAKAMURA TakumiTableGen.cmake: Functionalize and reformat.
2014-02-23 NAKAMURA TakumiSimplify linking to system libraries
2014-02-22 NAKAMURA TakumiPrune debug message in AddLLVM.cmake.
2014-02-21 NAKAMURA Takumi[CMake] llvm_add_library: Add dependencies also to...
2014-02-21 NAKAMURA Takumi[CMake] Introduce "llvm_add_library(SHARED STATIC)...
2014-02-21 NAKAMURA TakumiTeach LLVM-Config to use logical target names (2/2)
2014-02-21 NAKAMURA TakumiTeach LLVM-Config to use logical target names (1/2)
2014-02-20 NAKAMURA Takumi[CMake] Move intrinsics_gen to lib/Target out of add_pu...
2014-02-20 Evgeniy StepanovUnconditionally include msan_interface.h when building...
2014-02-19 Evgeniy StepanovBuild PIE binaries when cross-compiling to Android.
2014-02-16 NAKAMURA TakumiLLVMExports.cmake: Add System libs $(LIBS) to LLVMSuppo...
2014-02-16 NAKAMURA TakumiLLVMExports.cmake: Exclude gtest since they are not...
2014-02-13 NAKAMURA Takumi[CMake] Let llvm_add_library(MODULE) check capability...
2014-02-13 NAKAMURA Takumi[CMake] Move the target property PREFIX from add_llvm_l...
2014-02-13 NAKAMURA Takumi[CMake] llvm_add_library(MODULE) may use CMAKE_MODULE_L...
2014-02-13 NAKAMURA Takumi[CMake] LLVM_PLUGIN_EXT: Use CMAKE_SHARED_LIBRARY_SUFFI...
2014-02-13 NAKAMURA Takumi[CMake] llvm_add_library: Add handling of the parameter...
2014-02-12 NAKAMURA TakumiTeach tablegen() macro to check needed variables
2014-02-10 Reid Klecknercmake: Do not export targets when installing toolchain...
2014-02-10 NAKAMURA Takumi[CMake] LLVMSupport should be responsible to provide...
2014-02-10 NAKAMURA Takumi[CMake] Introduce llvm_add_library().
2014-02-10 NAKAMURA Takumi[CMake] LLVMProcessSources.cmake: Prune add_file_depend...
2014-02-10 NAKAMURA Takumi[CMake] Re-apply r200765, "Get rid of llvm_config(...
2014-02-09 Bob WilsonRemove shell comment in the middle of a single-line...
2014-02-09 NAKAMURA TakumiWhitespace.
2014-02-09 NAKAMURA TakumiProvide CMake package modules in install tree
2014-02-09 NAKAMURA TakumiLoad exported lib and exe targets from LLVMConfig
2014-02-09 NAKAMURA TakumiExport lib and exe build target names from build tree
2014-02-09 NAKAMURA TakumiExport lib and exe build target names from install...
2014-02-09 NAKAMURA TakumiProvide LLVMConfig in both build and install tree
2014-02-09 NAKAMURA TakumiTeach LLVMConfig to avoid modifying CMAKE_MODULE_PATH
2014-02-09 NAKAMURA TakumiDe-duplicate references to share/llvm/cmake path
2014-02-05 Todd FialaFix configure to find arc4random via header files.
2014-02-05 Jordan Rose[CMake] Deliberately get all LLVM library dependencies...
2014-02-05 Jordan Rose[CMake] Move -stdlib=libc++ handling into its own file.
2014-02-04 NAKAMURA Takumi[CMake] Get rid of llvm_config() to expand dependencies.
2014-02-04 NAKAMURA Takumi[CMake] LLVM-Config.cmake: Split explicit_map_component...
2014-02-04 NAKAMURA Takumi[CMake] add_llvm_loadable_module: Fixup r200762, I...
2014-02-04 NAKAMURA TakumiRevert r122395, "Fixes file extension for loadable...
2014-02-04 Alexey Samsonov[CMake] Revert r200695 and fix the problem with missing...
2014-02-04 Alexey Samsonov[CMake] Add -stdlib=libc++ to host Clang build flags...
2014-02-04 NAKAMURA TakumiRevert r200150, "[CMake] tablegen(): Use -I <dir> accor...
2014-02-03 Evgeniy StepanovDon't use -ffunction-sections if -fno-function-sections...
2014-02-02 NAKAMURA Takumi[CMake] Untabify.
2014-01-31 Peter CollingbourneIntroduce line editor library.
2014-01-31 NAKAMURA TakumiAddLLVM.cmake: Untabify.
2014-01-31 NAKAMURA TakumiHandleLLVMOptions.cmake: Typo, s/proerty/property/
2014-01-30 NAKAMURA Takumi[CMake] llvm_update_compile_flags: Honor LLVM_COMPILE_F...
2014-01-30 NAKAMURA TakumiHandleLLVMOptions.cmake: Typo in comment.
2014-01-29 Evgeniy StepanovRemove -arm-enable-ehabi from Android build rules....
2014-01-28 NAKAMURA Takumi[CMake] llvm_update_compile_flags(name) doesn't require...
2014-01-28 NAKAMURA Takumi[CMake] Prune CMAKE_CXX_FLAGS stuff in llvm_process_sou...
2014-01-28 NAKAMURA Takumi[CMake] Enhance llvm_update_compile_flags(name sources...
2014-01-28 NAKAMURA Takumi[CMake] Apply -ffunction-data-sectinos not only to...
2014-01-28 NAKAMURA Takumi[CMake] Move -ffunction-data-sections stuff to HandleLL...
2014-01-28 NAKAMURA Takumi[CMake] Let llvm_process_sources check not only *.cpp...
2014-01-27 NAKAMURA Takumi[CMake] Put *_exports into "Misc" folder.
2014-01-26 NAKAMURA Takumi[CMake] tablegen(): Use -I <dir> according to the list...
2014-01-26 NAKAMURA Takumi[CMake] Functionalize tblgen().
2014-01-26 NAKAMURA Takumi[CMake] configure_lit_site_cfg: ${SHLIBDIR} should...
2014-01-21 Chandler CarruthDon't clobber CMAKE_REQUIRED_FLAGS, it ends up being...
2014-01-21 Amara EmersonFix VS2012 ID/version check.
2014-01-21 Evgeniy StepanovFix libstdc++4.7 test on Android.
2014-01-20 NAKAMURA Takumi[CMake] LLVMProcessSources.cmake: Add include(CMakePars...
2014-01-20 NAKAMURA Takumi[CMake] llvm_process_sources: Introduce a parameter...
2014-01-19 NAKAMURA Takumi[CMake] Introduce new scheme of LLVM_TOOLS_BINARY_DIR...
2014-01-19 NAKAMURA Takumi[CMake] Prune deprecate usage of CMAKE_RUNTIME_OUTPUT_D...
2014-01-17 Chandler CarruthAdd the test for libstdc++ versions newer than 4.6...
2014-01-16 Quentin Colombet[cmake] Attempt to fix sanitizer buildbot.
2014-01-13 Chandler CarruthFactor the option and checking of compiler version...
2014-01-13 Chandler CarruthAdd a check that the host compiler is modern to CMake...
2014-01-12 NAKAMURA Takumi[CMake] Add a comment to tablegen's copy_if_different...
2014-01-08 Alp TokerCMake: Provide LLVM_PLUGIN_EXT definition
2014-01-07 NAKAMURA Takumi[CMake] Introduce llvm_update_compile_flags(target_name...
2014-01-06 Jean-Daniel DupasIntroduce a cmake LLVM_ENABLE_LIBCXX build parameter...
2014-01-05 Nico WeberAdd a FIXME.
2014-01-02 Jordan Rose[CMake] Add missing set_output_directory after Takumi...
2014-01-02 Douglas GregorCMake separate projects: use correct name for LIBRARY_O...
2014-01-02 Douglas GregorRemove CMake-Xcode hack that symlinked llvm-config...
2013-12-30 NAKAMURA Takumi[CMake][VS][XCode] Restruct the output directory layout...
2013-12-30 Yaron Keren Visual C++ does not support -ffunction-sections -fdata...
2013-12-30 Nico WeberPort r198087 and r198089 (strip dead code by default...
2013-12-29 Nico Weber[cmake] In add_llvm_loadable_module, don't clobber...
2013-12-29 NAKAMURA TakumiFix mis-merging in AddLLVM.cmake, take #2. LINK.EXE...
2013-12-29 NAKAMURA TakumiFix mis-merging in AddLLVM.cmake. Sorry.
next