Linker: Don't use MDNode::replaceOperandWith()
[opencl/llvm.git] / include / llvm / IR / Metadata.h
2015-01-07 Duncan P. N. Exon... Linker: Don't use MDNode::replaceOperandWith()
2015-01-07 Duncan P. N. Exon... IR: Remove MDNode::getWhenValsUnresolved()
2015-01-07 Duncan P. N. Exon... Remove invalid TODO
2015-01-05 Duncan P. N. Exon... IR: Prune arguments to ValueAsMetadata::ValueAsMetadata()
2014-12-11 Duncan P. N. Exon... Bitcode: Use unsigned char to record MDStrings
2014-12-10 Duncan P. N. Exon... IR: Move call to dropAllReferences() to MDNode subclasses
2014-12-09 Duncan P. N. Exon... IR: Metadata: Detect an RAUW recursion
2014-12-09 Duncan P. N. Exon... IR: Metadata/Value split: RAUW in a deterministic order
2014-12-09 Hans WennborgTry fixing MSVC build after r223802
2014-12-09 Duncan P. N. Exon... IR: Split Metadata from Value
2014-12-05 Duncan P. N. Exon... IR: Stop relying on GetStringMapEntryFromValue()
2014-11-18 Duncan P. N. Exon... IR: Sink MDNode::Hash down to GenericMDNode::Hash
2014-11-18 Duncan P. N. Exon... IR: Move MDNode operands from the back to the front
2014-11-18 Duncan P. N. Exon... IR: Split MDNode into GenericMDNode and MDNodeFwdDecl
2014-11-17 Duncan P. N. Exon... IR: Simplify uniquing for MDNode
2014-11-14 Duncan P. N. Exon... IR: Make MDString inherit from Metadata
2014-11-14 Duncan P. N. Exon... IR: Take an LLVMContext in Metadata::Metadata()
2014-11-14 Duncan P. N. Exon... IR: Rewrite uniquing and creation of MDString
2014-11-13 Duncan P. N. Exon... IR: Make MDString::getName() private
2014-11-13 Duncan P. N. Exon... IR: Create the Metadata class
2014-11-11 Duncan P. N. Exon... Revert "IR: MDNode => Value"
2014-11-05 Duncan P. N. Exon... IR: MDNode => Value: NamedMDNode::getOperator()
2014-11-05 Duncan P. N. Exon... IR: MDNode => Value: NamedMDNode::addOperand()
2014-10-15 Duncan P. N. Exon... IR: Move NumOperands from User to Value, NFC
2014-10-15 Duncan P. N. Exon... IR: Cleanup comments for Value, User, and MDNode
2014-10-04 Benjamin KramerMake AAMDNodes ctor and operator bool (!!!) explicit...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-07-24 Hal FinkelAdd scoped-noalias metadata
2014-07-24 Hal FinkelAA metadata refactoring (introduce AAMDNodes)
2014-04-23 Rafael EspindolaRemove AssemblyAnnotationWriter from NamedMDNode::print.
2014-04-09 Craig Topper[C++11] More 'nullptr' conversion or in some cases...
2014-03-11 Benjamin KramerRemove copy ctors that did the same thing as the defaul...
2014-03-06 Owen AndersonChange the tag on this iterator to bidir and implement...
2014-03-06 Owen AndersonFix issues in the NamedMDNode operand iterator, includi...
2014-03-06 Owen AndersonAdd a iterator and interator_range interface to the...
2014-03-02 Alp Toker[C++11] Expand and eliminate the LLVM_ENUM_INT_TYPE...
2013-12-02 Manman RenDebug Info: Move the constant for Debug Info Version...
2013-09-06 Manman RenTBAA: add isTBAAVtableAccess to MDNode so clients can...
2013-07-13 Craig TopperRemove unneeded forward declarations.
2013-07-12 Benjamin KramerMark MDNode::getOperand as readonly.
2013-01-10 Jakub StaszakRemove trailing spaces.
2013-01-10 Jakub StaszakFix include guards so they exactly match file names.
2013-01-02 Chandler CarruthMove all of the header files which are involved in...