]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - include
Spelling. Thanks, Eric.
[opencl/llvm.git] / include /
2013-04-30 Rafael EspindolaChange getSlotIndex to return unsigned.
2013-04-30 Rafael EspindolaFix Addend computation for non external relocations...
2013-04-29 Bill WendlingEmit the TLS initialization function pointers into...
2013-04-29 Rafael EspindolaAdd getSymbolAlignment to the ObjectFile interface.
2013-04-29 Rafael EspindolaRemove unused method.
2013-04-29 Reid KlecknerRevert "revert r179735, it has no testcases, and doesn...
2013-04-29 Andrew KaylorExposing MCJIT through C API
2013-04-27 Eric ChristopherRegen.
2013-04-27 Joerg SonnenbergerOnly use cxxabi.h's demangler, if it is actually available.
2013-04-27 Andrew TrickGeneralize the MachineTraceMetrics public API.
2013-04-27 Andrew TrickAdd target flags to MachineMemOperands.
2013-04-27 Andrew Trickwhitespace
2013-04-27 Eric ChristopherUse the target triple from the target machine rather...
2013-04-27 Manman RenStruct-path aware TBAA: change the format of TBAAStruct...
2013-04-26 Adrian PrantlCleanup and document MachineLocation.
2013-04-26 Rafael EspindolaUse llvm/Object/MachO.h in macho-dumper. Drop the old...
2013-04-26 Adrian Prantlfix a typo that due to cu&paste quadrupled itself
2013-04-26 Adrian PrantlBugfix for the debug intrinsic handling in InstCombiner:
2013-04-25 Andrew KaylorRe-enabling MCJIT object caching with memory leak fixed
2013-04-25 Chris Lattnerrevert r179735, it has no testcases, and doesn't really...
2013-04-25 Reid Kleckner[mc-coff] Forward Linker Option flags into the .drectve...
2013-04-25 Rafael EspindolaClarify getRelocationAddress x getRelocationOffset...
2013-04-25 Rafael EspindolaRevert "Adding object caching support to MCJIT"
2013-04-25 Rafael EspindolaRevert "Exposing MCJIT through C API"
2013-04-24 Andrew KaylorExposing MCJIT through C API
2013-04-24 Andrew KaylorMaking invalidateInstructionCache automatic in SectionM...
2013-04-24 Andrew TrickMI Sched: eliminate local vreg copies.
2013-04-24 Eric ChristopherAdd include guards.
2013-04-23 Andrew TrickComment a strange field in ScheduleDAG.
2013-04-23 Eric ChristopherFix dependency layering issues caused by r180112.
2013-04-23 Andrew KaylorFixing typo in comment.
2013-04-23 Andrew KaylorAdding object caching support to MCJIT
2013-04-23 Tom StellardWrap.h: Define wrap / unwrap function for ExecutionEngine
2013-04-23 Carlo Kokc vs c++ mistake in header file typedef for AtomicRMW...
2013-04-23 Carlo KokExpose IRBuilder::CreateAtomicRMW as LLVMBuildAtomicRMW...
2013-04-23 Alexey SamsonovAdd more guards around zlib-dependent code
2013-04-23 Alexey SamsonovAdd basic zlib support to LLVM. This would allow to...
2013-04-22 Matt ArsenaultRemove unused DwarfSectionOffsetDirective string
2013-04-22 Eric ChristopherMove C++ code out of the C headers and into either...
2013-04-22 Chad Rosier[ms-inline asm] Add the OpDecl to the InlineAsmIdentifi...
2013-04-22 Eli BenderskyOptimize MachineBasicBlock::getSymbol by caching the...
2013-04-22 Eli BenderskyFix comment that didn't match the method it was above
2013-04-22 Chad Rosier[ms-inline asm] Remove the identifier parsing logic...
2013-04-22 Chad Rosier[ms-inline asm] Refactor/clean up the SemaLookup interf...
2013-04-22 Jia Liutypo
2013-04-22 Benjamin KramerMake doxygen comment match declaration.
2013-04-22 Rafael EspindolaClarify that llvm.used can contain aliases.
2013-04-22 Eric ChristopherAdd the same todo about a command iterator interface...
2013-04-22 Eric ChristopherAdd a TODO about wanting an iterator interface.
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-21 Stephen LinRemove unused, undefined ArgFlagsTy::getArgFlagsString...
2013-04-20 Tim NorthoverRemove unused ShouldFoldAtomicFences flag.
2013-04-20 Tim NorthoverRemove unused MEMBARRIER DAG node; it's been replaced...
2013-04-20 Stephen LinAdd CodeGen support for functions that always return...
2013-04-19 Eli BenderskySimplify the code in FastISel::tryToFoldLoad, add an...
2013-04-19 Eli BenderskyMove TryToFoldFastISelLoad to FastISel, where it belong...
2013-04-19 Michael LiaoArrayRefize getMachineNode(). No functionality change.
2013-04-19 Jakob Stoklund OlesenAdd an MRI::verifyUseLists() function.
2013-04-19 Eric ChristopherReformat and nuke trailing whitespace.
2013-04-19 Adrian PrantlRename ClassType to the more accurate UnderlyingType...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-04-19 Lang HamesAdd support for index resources (for a SlotIndex) to...
2013-04-18 Chad Rosier[asm parser] Add support for predicating MnemonicAlias...
2013-04-18 Bill WendlingMake the TargetIndependent flag have the right boolean...
2013-04-18 Eli BenderskyFix typo
2013-04-18 Bill WendlingCleanup patch:
2013-04-18 Bill WendlingThis patch addresses two cleanup issues:
2013-04-18 Tom StellardC API: Fix coding style
2013-04-18 Rafael EspindolaAt Jim Grosbach's request detemplate Object/MachO.h.
2013-04-18 Chad RosierFix comment spacing.
2013-04-17 Bill WendlingAdd an option `-enable-old-style-attr-syntax' to print...
2013-04-17 Rafael EspindolaTwo small cleanups for ELF's templates.
2013-04-17 Peter CollingbourneAdd support for subsections to the ELF assembler. Fixes...
2013-04-17 Alexey SamsonovCreate a stub for DWARF parser unittests
2013-04-16 Tom StellardC API: Add LLVMTargetMachineEmitToMemoryBuffer()
2013-04-16 Tom StellardC API: Add LLVMGetBufferSize()
2013-04-16 Tom StellardC API: Add LLVMGetBufferStart()
2013-04-16 Tom StellardC API: Add LLVMAddTargetDependentFunctionAttr()
2013-04-16 Eli BenderskyCleanup naming: DataLayout s/TD/DL/
2013-04-16 Hans WennborgAdd four new functions and one new enum to the C API:
2013-04-15 Rafael EspindolaFix silly typo that broke big endian hosts.
2013-04-15 Rafael EspindolaFix endianness on some MSVC versions.
2013-04-15 Jim GrosbachSimplify the MCInst operator iterator declaration.
2013-04-15 Rafael EspindolaTry to fix the mingw builds.
2013-04-15 Arnold SchwaighoferFix bit size of v64i8 and v32i16 vector types.
2013-04-15 Rafael EspindolaRemove getters now that we can specialize structs on...
2013-04-15 Rafael EspindolaRemove unused function.
2013-04-15 Rafael EspindolaMake the host endianness check an integer constant...
2013-04-15 Andy GibbsReplace uses of the deprecated std::auto_ptr with Ownin...
2013-04-15 Nadav RotemAdd an option -vectorize-slp-aggressive for running...
2013-04-15 Nadav RotemRename the slp-vectorizer clang/llvm flags. No function...
2013-04-13 Andrew TrickMI-Sched: schedule physreg copies.
2013-04-13 Rafael EspindolaAdd typenames to see if bot goes green.
2013-04-13 Rafael EspindolaSome versions of gcc don't like typenames in these...
2013-04-13 Rafael EspindolaFinish templating MachObjectFile over endianness.
2013-04-12 Benjamin KramerRevert broken pieces of r179373.
2013-04-12 Andy GibbsReplace uses of the deprecated std::auto_ptr with Ownin...
2013-04-12 Nico RieckAdd missing relocation names
2013-04-12 Nico RieckSupport MIPS64EL relocation type names
next