]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - include
Revert "Move copying of global initializers below the cloning of functions."
[opencl/llvm.git] / include /
2013-11-09 Lang HamesRewrite the PBQP graph data structure.
2013-11-08 Juergen Ributzka[Stackmap] Add AnyReg calling convention support for...
2013-11-08 Lang HamesAdd a method to get the object-file appropriate stack...
2013-11-08 Arnaud A. de Grand... Revert "CalculateSpillWeights does not need to be a...
2013-11-08 Arnaud A. de Grand... CalculateSpillWeights does not need to be a pass
2013-11-08 Jordan RoseAdd ImmutableSet profiling info for 'bool'.
2013-11-08 Artyom SkrobovExport MCDisassembler's SubtargetInfo, to allow archite...
2013-11-07 NAKAMURA Takumillvm-c/Support.h: Add a newline at eof.
2013-11-06 Simon AtanasyanAdd DT_VERSYM dynamic table entry tag definition.
2013-11-06 Peter Zotov[llvm-c] Add parameter names in Target.h for C99 compliance
2013-11-06 Peter Zotov[llvm-c] Improve TargetMachine bindings
2013-11-06 Peter Zotov[llvm-c] Correctly check for existence of native AsmPar...
2013-11-06 Peter Zotov[llvm-c] Add functions for initializing native AsmPrint...
2013-11-06 Peter Zotov[llvm-c] Expose LLVMLoadLibraryPermanently
2013-11-06 Peter Zotov[llvm-c] Expose IRReader interface
2013-11-06 Peter Zotov[llvm-c] Implement LLVMPrintValueToString
2013-11-06 Andrew TrickRewrite SCEV's backedge taken count computation.
2013-11-05 Rafael EspindolaRemove another unused, and IMHO, not very desirable...
2013-11-05 Dmitri GribenkoConvert comments to documentation comments (// -> ///)
2013-11-05 Rafael EspindolaUse error_code in GVMaterializer.
2013-11-05 Jiangning LiuImplement AArch64 Neon Crypto instruction classes AES...
2013-11-05 Peter Zotov[llvm-c] (PR16190) Add LLVMIsA* functions for ConstantD...
2013-11-05 Alp TokerFix symbol defines in config.h.cmake
2013-11-05 Yuchen WuSupport for reading run counts in llvm-cov.
2013-11-05 Rafael EspindolaFix MSVC build by not putting an error_code directly...
2013-11-05 Rafael EspindolaSimplify ErrorOr.
2013-11-05 Hal FinkelAdd a runtime unrolling parameter to the LoopUnroll...
2013-11-04 Cameron McInallyAdd support for AVX512 masked vector blend intrinsics.
2013-11-04 Zoran JovanovicSupport for microMIPS branch instructions.
2013-11-04 Elena DemikhovskyAVX-512: fixed a typo in builtin name
2013-11-04 Filip PizloMake the pretty stack trace be an opt-in, rather than...
2013-11-03 Elena DemikhovskyAVX-512: added VPCONFLICT instruction and intrinsics,
2013-11-03 Bob WilsonConvert calls to __sinpi and __cospi into __sincospi_stret
2013-11-03 Filip PizloAdd a comment to note that LLVMDisablePrettyStackTrace...
2013-11-03 Filip PizloWhen LLVM is embedded in a larger application, it's...
2013-11-02 Rafael Espindolamove getSymbolNMTypeChar to the one program that needs...
2013-11-02 Yuchen WuAdded command-line option to output llvm-cov to file.
2013-11-01 Rafael EspindolaRemove linkonce_odr_auto_hide.
2013-11-01 Kevin EnderbyAdd to the disassembler C API output reference types for
2013-10-31 Chad Rosier[AArch64] Add support for NEON scalar fixed-point conve...
2013-10-31 Andrew TrickAdd new calling convention for WebKit Java Script.
2013-10-31 Andrew TrickAdd support for stack map generation in the X86 backend.
2013-10-31 Rafael EspindolaUse LTO_SYMBOL_SCOPE_DEFAULT_CAN_BE_HIDDEN instead...
2013-10-31 Chad Rosier[AArch64] Add support for NEON scalar shift immediate...
2013-10-31 Manman RenCleanup: update comments.
2013-10-31 Andrew TrickLower stackmap intrinsics directly to their target...
2013-10-31 Andrew TrickAdd experimental stackmap intrinsics to definition...
2013-10-31 Andrew TrickEnable variable arguments support for intrinsics.
2013-10-31 Rafael EspindolaRemove another unused flag.
2013-10-31 Rafael EspindolaRemove unused flag.
2013-10-31 Cameron McInallyAdd AVX512 unmasked integer broadcast intrinsics and...
2013-10-31 Rafael EspindolaMerge CallGraph and BasicCallGraph.
2013-10-30 Rafael EspindolaProduce .weak_def_can_be_hidden for some linkonce_odr...
2013-10-30 Simon Atanasyan[Mips] Add more SHF_MIPS_xxx ELF section flags.
2013-10-30 Rui UeyamaAdd {start,end}with_lower methods to StringRef.
2013-10-30 Daniel Sanders[mips][msa] Correct definition of bins[lr] and CHECK...
2013-10-30 Daniel Sanders[mips][msa] Added support for matching bmnz, bmnzi...
2013-10-30 Chad Rosier[AArch64] Add support for NEON scalar floating-point...
2013-10-30 Cameron McInallyRefactor the AVX512 intrinsics. Cluster the intrinsics...
2013-10-30 Howard HinnantRehash but don't grow when full of tombstones.
2013-10-30 Daniel Sanders[mips][msa] Added support for matching bins[lr]i.[bhwd...
2013-10-30 Josh MageeReformat code with clang-format.
2013-10-30 NAKAMURA TakumiStackProtector.h: Fix trailing comments for doxygen...
2013-10-30 NAKAMURA TakumiTrailing whitespace in a comment line.
2013-10-29 Josh Magee[stackprotector] Update the StackProtector pass to...
2013-10-29 Matt ArsenaultUpdate comment
2013-10-29 Matt ArsenaultWorkaround MSVC 32-bit miscompile of getCondCodeAction.
2013-10-29 Rafael EspindolaRemove declared but not implemented function.
2013-10-29 Rafael EspindolaMove getSymbol to TargetLoweringObjectFile.
2013-10-29 Rafael EspindolaAdd a helper getSymbol to AsmPrinter.
2013-10-29 Zoran JovanovicSupport for microMIPS jump instructions
2013-10-29 Rafael EspindolaClarify that GlobalVariables definitions must have...
2013-10-29 Anders Waldenborgllvm-c: Make LLVM{Get,Set}Alignment work on {Load,Store...
2013-10-29 Alp TokerFix "existant" typos
2013-10-29 Joerg SonnenbergerMove the STT_FILE symbols out of the normal symbol...
2013-10-28 Alexey SamsonovDWARF parser: Use ArrayRef to represent form sizes...
2013-10-28 Alexey SamsonovDebugInfo: Introduce the notion of "form classes"
2013-10-28 Logan Chien[arm] Implement eabi_attribute, cpu, and fpu directives.
2013-10-28 Richard SandifordKeep TBAA info when rewriting SelectionDAG loads and...
2013-10-27 Elena DemikhovskyAVX-512: PMIN/PMAX intrinsics and patterns
2013-10-27 Shuxin YangRevert r193251 : Use address-taken to disambiguate...
2013-10-26 Wan XiaofeiQuick look-up for block in loop.
2013-10-25 Andrew TrickFix SCEVExpander: don't try to expand quadratic recurre...
2013-10-25 Rafael EspindolaChange MemoryBuffer::getFile to take a Twine.
2013-10-25 David BlaikieDIEHash: Summary hashing of nested types
2013-10-25 Rafael EspindolaCall destroy from ~BasicCallGraph.
2013-10-25 Rafael EspindolaUse c comments.
2013-10-25 Tim NorthoverARM: allow .thumb_func to be separated from symbol...
2013-10-25 Tim NorthoverLegalizeDAG: allow libcalls for max/min atomic operations
2013-10-25 Richard SmithFix ODR violation.
2013-10-25 Yuchen WuSupport for reading program counts in llvm-cov.
2013-10-24 David BlaikieMCStreamer: Reimplement the virtual EmitRawText as...
2013-10-24 Reid Klecknerlto.h: Use lto_bool_t instead of int to restore the ABI
2013-10-24 Eric ChristopherFormatting and whitespace.
2013-10-24 John ThompsonReverting my r193344 checkin due to build breakage.
2013-10-24 John ThompsonAdded std::string as a built-in type for mapping.
2013-10-24 Nuno Lopesfix PR17635: false positive with packed structures
2013-10-24 Zonr ChangInclude missing Compiler.h for using LLVM_ENUM_INT_TYPE.
2013-10-24 Elena DemikhovskyAVX-512: added VCVTPH2PS, VCVTPS2PH with intrinsics
2013-10-24 Yuchen WuFixed llvm-cov to count edges instead of blocks.
next