]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - include
DAGCombine: fold (or (and X, M), (and X, N)) -> (and X, (or M, N))
[opencl/llvm.git] / include /
2015-01-21 Matthias BraunLiveIntervalAnalysis: Mark subregister defs as undef...
2015-01-21 Chris BienemanAdding a new cl::HideUnrelatedOptions API to allow...
2015-01-21 Matthias BraunLiveIntervalAnalysis: Factor out code to update livenes...
2015-01-21 Matthias BraunLiveIntervalAnalysis: document removePhysRegDefAt(...
2015-01-21 Matthias BraunLiveIntervalAnalysis: Factor out code to update livenes...
2015-01-21 Matthias BraunLiveIntervalAnalysis: Remove unused pruneValue() variant.
2015-01-21 Chandler Carruth[PM] Replace an abuse of inheritance to override a...
2015-01-21 Adrian PrantlMake DIExpression::Verify() stricter by checking that...
2015-01-20 Chandler Carruth[PM] Separate the InstCombiner from its pass.
2015-01-20 Manman Ren[llvm link] Destroy ConstantArrays in LLVMContext if...
2015-01-20 Chandler Carruth[PM] Don't spend time making self moves no-ops. They...
2015-01-20 Duncan P. N. Exon... Revert "IR: Specify underlying type instead of r226570...
2015-01-20 Duncan P. N. Exon... IR: Specify underlying type instead of r226570, NFC
2015-01-20 Duncan P. N. Exon... IR: Store StorageType as an unsigned bitfield
2015-01-20 Chandler Carruth[PM] Port LoopInfo to the new pass manager, adding...
2015-01-20 Chandler Carruth[PM] Make the LoopInfoBase and LoopInfo objects movable...
2015-01-20 Chandler Carruth[PM] Fix a moderately scary typo in the deleted copy...
2015-01-20 Chandler Carruth[PM] Use range-based for and auto to clean up some...
2015-01-20 Duncan P. N. Exon... IR: Move MDNode clone() methods from ValueMapper to...
2015-01-20 Chandler Carruth[PM] Replace the Pass argument in MergeBasicBlockIntoOn...
2015-01-20 Duncan P. N. Exon... IR: Detect whether to call recalculateHash() via SFINAE...
2015-01-20 Duncan P. N. Exon... IR: Introduce GenericDwarfNode
2015-01-19 Duncan P. N. Exon... IR: Cleanup MDNode field use, NFC
2015-01-19 Duncan P. N. Exon... IR: Move replaceWithUniqued(), etc., to source file...
2015-01-19 Duncan P. N. Exon... IR: Merge UniquableMDNode back into MDNode, NFC
2015-01-19 Duncan P. N. Exon... IR: Simplify uniquifyImpl(), NFC
2015-01-19 Duncan P. N. Exon... IR: Simplify erasing from uniquing store, NFC
2015-01-19 Duncan P. N. Exon... Remove dead code, NFC
2015-01-19 Duncan P. N. Exon... Utils: Simplify MapMetadata(), NFC
2015-01-19 Duncan P. N. Exon... IR: Allow temporary nodes to become uniqued or distinct
2015-01-19 Duncan P. N. Exon... IR: Remove templates from TempMDNodeDeleter, NFC
2015-01-19 Duncan P. N. Exon... IR: Split out countUnresolvedOperands(), NFC
2015-01-19 Duncan P. N. Exon... IR: Return unique_ptr from MDNode::getTemporary()
2015-01-19 Rafael EspindolaAdd r224985 back with fixes.
2015-01-19 Duncan P. N. Exon... IR: Add MDLocation::getTemporary()
2015-01-19 Duncan P. N. Exon... IR: Remove MDNodeFwdDecl
2015-01-19 Duncan P. N. Exon... IR: Extract out and reuse `storeImpl()`, NFC
2015-01-19 Duncan P. N. Exon... IR: Reuse `getImpl()` for `getDistinct()`, NFC
2015-01-19 Duncan P. N. Exon... IR: Move replaceAllUsesWith() back up to MDNode
2015-01-19 Duncan P. N. Exon... IR: Be specific about what MDNode::get() returns, NFC
2015-01-19 Duncan P. N. Exon... Remove dead code, NFC
2015-01-19 Duncan P. N. Exon... IR: Unify code for MDNode::isResolved(), NFC
2015-01-19 Duncan P. N. Exon... IR: Store RAUW support and Context in the same pointer...
2015-01-19 Duncan P. N. Exon... IR: Add isUniqued() and isTemporary()
2015-01-19 Duncan P. N. Exon... IR: Use an enum to describe Metadata storage, NFC
2015-01-19 Adrian PrantlRemove support for DIVariable's FlagIndirectVariable...
2015-01-19 Chandler Carruth[PM] Replace the Pass argument to SplitEdge with specif...
2015-01-19 Chandler Carruth[PM] Cleanup a dead option to critical edge splitting...
2015-01-19 Chandler Carruth[PM] Remove the Pass argument from all of the critical...
2015-01-19 Sergey Dmitrouk[NFC] Update createMachineScheduler() comment
2015-01-19 Craig Topper[x86] Change AVX512 intrinsics to take a 8-bit immediat...
2015-01-19 Michael Gottesman[tinyptrvector] Add in a MutableArrayRef implicit conve...
2015-01-19 Chandler Carruth[PM] Lift the analyses into the interface for
2015-01-19 Michael GottesmanChange using => typedef to please the MSVC bots.
2015-01-19 Michael GottesmanHide the state of TinyPtrVector and remove the single...
2015-01-18 David Blaikieunique_ptrify the RelInfo parameter to TargetRegistry...
2015-01-18 David BlaikieAttempt to fix the MSVC build by working around a layer...
2015-01-18 David Blaikiestd::unique_ptrify the MCStreamer argument to createAsm...
2015-01-18 Chandler Carruth[PM] Pull the analyses used for another utility routine...
2015-01-18 Chandler Carruth[PM] Sink the specific analyses preserved by SplitBlock...
2015-01-18 Chandler Carruth[PM] Replace another Pass argument with specific analys...
2015-01-18 Chandler Carruth[PM] Lift the actual analyses used into the inferface...
2015-01-18 Chandler Carruth[PM] Now that LoopInfo isn't in the Pass type hierarchy...
2015-01-17 Chandler Carruth[PM] Split the LoopInfo object apart from the legacy...
2015-01-16 Philip Reamesclang-format all the GC related files (NFC)
2015-01-16 Lang Hames[RuntimeDyld] Track symbol visibility in RuntimeDyld.
2015-01-16 Kevin EnderbyFix the Archive::Child::getRawSize() method used by...
2015-01-16 Lang Hames[RuntimeDyld] Add 'stub_addr' to comment describing...
2015-01-16 Philip ReamesMove ownership of GCStrategy objects to LLVMContext
2015-01-16 Philip ReamesRemove gc.root's findCustomSafePoints mechanism
2015-01-16 Adam Nemet[AVX512] Add intrinsics for masked aligned FP loads...
2015-01-16 Filipe CabecinhasUse report_fatal_error instead of llvm_unreachable...
2015-01-16 Sanjoy DasAdd a new pass "inductive range check elimination"
2015-01-15 Kevin EnderbyAdd the option, -archive-headers, used with -macho...
2015-01-15 Lang Hames[Object] Add SF_Exported flag. This flag will be set...
2015-01-15 Sanjoy DasRevert r226201 (Add a new pass "inductive range check...
2015-01-15 Sanjoy DasAdd a new pass "inductive range check elimination"
2015-01-15 Chandler Carruth[PM] Port TargetLibraryInfo to the new pass manager...
2015-01-15 Chandler Carruth[PM] Separate the TargetLibraryInfo object from the...
2015-01-15 Chandler Carruth[PM] Clean up the TLI doxygen comments prior to refacto...
2015-01-15 Chandler Carruth[PM] Move TargetLibraryInfo into the Analysis library.
2015-01-15 Adrian PrantlAdd missing include directive for llvm::make_unique().
2015-01-14 Ramkumar Ramachandra[GC] CodeGenPrep transform: simplify offsetable relocate
2015-01-14 Duncan P. N. Exon... IR: Fix comment spelling, NFC
2015-01-14 Duncan P. N. Exon... IR: Move MDLocation into place
2015-01-14 Duncan P. N. Exon... IR: Drop metadata references more aggressively during...
2015-01-14 David BlaikieAdd comment about a gotcha I ran across while touching...
2015-01-14 David Blaikieunique_ptrify the value in DominatorTreeBase::DomTreeNodes
2015-01-14 Rafael EspindolaRevert "Add r224985 back with two fixes."
2015-01-14 Reid KlecknerRemove dead code for llvm.eh.selector in the old EH...
2015-01-14 Chandler Carruth[cleanup] Re-sort all the #include lines in LLVM using
2015-01-14 Chandler Carruth[dom] Make the DominatorTreeBase not a dynamic class!
2015-01-14 Chandler Carruth[PM] Port domtree to the new pass manager (at last).
2015-01-14 Chandler Carruth[PM] Make DominatorTrees (corectly) movable so that...
2015-01-14 Mehdi AminiFold a loop for array processing in ComputeLinearIndex
2015-01-14 JF BastienRevert "Insert random noops to increase security agains...
2015-01-14 Chandler Carruth[dom] Remove extraneous inline keywords. Template funct...
2015-01-14 Chandler Carruth[dom] The formatting of the generic domtree has bitrott...
2015-01-14 Chandler Carruth[dom] Clean up some comments in this header that were...
2015-01-14 NAKAMURA TakumiTargetInstrInfo.h: Fix \param in r225772. [-Wdocumentation]
next