]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/Bitcode/Reader/BitcodeReader.cpp
[cleanup] Re-sort all the #include lines in LLVM using
[opencl/llvm.git] / lib / Bitcode / Reader / BitcodeReader.cpp
2015-01-14 Chandler Carruth[cleanup] Re-sort all the #include lines in LLVM using
2015-01-13 Duncan P. N. Exon... AsmParser/Bitcode: Add support for MDLocation
2015-01-12 Duncan P. N. Exon... IR: Split GenericMDNode into MDTuple and UniquableMDNode
2015-01-10 Rafael EspindolaUse the DiagnosticHandler to print diagnostics when...
2015-01-09 Duncan P. N. Exon... Revert "Bitcode: Move the DEBUG_LOC record to DEBUG_LOC...
2015-01-09 Duncan P. N. Exon... Bitcode: Share logic for last instruction, NFC
2015-01-09 Duncan P. N. Exon... Bitcode: Move the DEBUG_LOC record to DEBUG_LOC_OLD
2015-01-08 Duncan P. N. Exon... IR: Add 'distinct' MDNodes to bitcode and assembly
2015-01-08 Rafael EspindolaExplicitly handle LinkOnceODRAutoHideLinkage. NFC....
2015-01-08 Rafael EspindolaUpdate naming style and clang-format. NFC.
2014-12-18 Yaron KerenFix Visual C++ error "'llvm::make_unique' : ambiguous...
2014-12-18 Rafael EspindolaModernize the getStreamedBitcodeModule interface a...
2014-12-12 Duncan P. N. Exon... Bitcode: Add missing "Remove in 4.0" comments
2014-12-11 Duncan P. N. Exon... Bitcode: Add METADATA_NODE and METADATA_VALUE
2014-12-11 Duncan P. N. Exon... Bitcode: Add `OLD_` prefix to metadata node records
2014-12-09 Duncan P. N. Exon... IR: Split Metadata from Value
2014-12-06 Duncan P. N. Exon... IR: Disallow function-local metadata attachments
2014-12-06 Duncan P. N. Exon... IR: Disallow complicated function-local metadata
2014-12-03 Rafael EspindolaAsk the module for its the identified types.
2014-12-03 Peter CollingbournePrologue support
2014-11-21 Richard TrieuAdd accessor marcos to ConstantPlaceHolder, similar...
2014-11-12 Rafael EspindolaReturn the number of read bytes in MemoryObject::readBytes.
2014-11-12 Rafael EspindolaReduce code duplication a bit. NFC.
2014-11-01 Rafael EspindolaRemove redundant calls to isMaterializable.
2014-10-29 NAKAMURA TakumiUntabify.
2014-10-24 Rafael EspindolaModernize the error handling of the Materialize function.
2014-10-24 Rafael EspindolaDon't ever call materializeAllPermanently during LTO.
2014-10-23 Rafael Espindolaclang-format two code snippets to make the next patch...
2014-09-23 Petar JovanovicDo not destroy external linkage when deleting function...
2014-09-19 Chris BienemanEliminating static destructor for the BitCodeErrorCateg...
2014-09-03 Rafael EspindolaPass a && to getLazyBitcodeModule.
2014-08-27 Rafael EspindolaFix a double free in llvm::getBitcodeTargetTriple.
2014-08-26 Rafael EspindolaPass a std::unique_ptr<MemoryBuffer>& to getLazyBitcode...
2014-08-26 Rafael EspindolaPass a MemoryBufferRef when we can avoid taking ownership.
2014-08-16 Duncan P. N. Exon... BitcodeReader: Only create one basic block for each...
2014-08-16 Duncan P. N. Exon... UseListOrder: Correctly count the number of uses
2014-08-05 Duncan P. N. Exon... BitcodeReader: Fix non-determinism in use-list order
2014-08-01 Duncan P. N. Exon... UseListOrder: Fix blockaddress use-list order
2014-08-01 Duncan P. N. Exon... BitcodeReader: Change mechanics of BlockAddress forward...
2014-08-01 Duncan P. N. Exon... BitcodeReader: Fix some BlockAddress forward reference...
2014-07-29 Rafael EspindolaHave a single enum for "not a bitcode" error.
2014-07-29 Rafael EspindolaMove the bitcode error enum to the include directory.
2014-07-28 Duncan P. N. Exon... Bitcode: Serialize (and recover) use-list order
2014-07-18 Hal FinkelAdd a dereferenceable attribute
2014-07-18 Hal FinkelRename AlignAttribute to IntAttribute
2014-07-16 Reid KlecknerRoundtrip the inalloca bit on allocas through bitcode
2014-07-04 Rafael EspindolaFix a bug in the conversion to ErrorOr.
2014-07-04 Rafael EspindolaRevert "Convert a few std::strings to StringRef."
2014-07-04 Rafael EspindolaConvert a few std::strings to StringRef.
2014-07-04 Rafael EspindolaConvert these functions to use ErrorOr.
2014-07-04 Rafael EspindolaRemove unused old-style error handling.
2014-06-27 David MajnemerIR: Add COMDATs to the IR
2014-06-27 Alp TokerIRReader: don't mark MemoryBuffers const
2014-06-27 Alp TokerPropagate const-correctness into parseBitcodeFile()
2014-06-25 Eli BenderskyRename loop unrolling and loop vectorizer metadata...
2014-06-23 Rafael EspindolaMake ObjectFile and BitcodeReader always own the Memory...
2014-06-18 Rafael EspindolaRevert a C API difference that I incorrectly introduced.
2014-06-18 Rafael EspindolaRemove BitcodeReader::setBufferOwned.
2014-06-13 Tim NorthoverIR: add "cmpxchg weak" variant to support permitted...
2014-06-13 Rafael EspindolaRemove 'using std::errro_code' from lib.
2014-06-13 Rafael EspindolaRemove all uses of 'using std::error_code' from headers.
2014-06-12 Rafael EspindolaDon't import error_category into the llvm namespace.
2014-06-10 Rafael EspindolaMark a few functions noexcept.
2014-06-06 Rafael EspindolaAllow aliases to be unnamed_addr.
2014-06-05 Tom RoederAdd a new attribute called 'jumptable' that creates...
2014-06-04 Rafael EspindolaClauses in a landingpad are always Constant. Use a...
2014-06-03 Rafael EspindolaAllow alias to point to an arbitrary ConstantExpr.
2014-05-31 Rafael EspindolaUse error_code() instead of error_code::succes()
2014-05-28 Rafael Espindola[pr19844] Add thread local mode to aliases.
2014-05-20 Nick LewyckyAdd 'nonnull', a new parameter and return attribute...
2014-05-17 Rafael EspindolaUse create methods since msvc doesn't handle delegating...
2014-05-17 Rafael EspindolaReduce abuse of default values in the GlobalAlias const...
2014-05-16 Reid KlecknerAdd comdat key field to llvm.global_ctors and llvm...
2014-05-16 Rafael EspindolaFix most of PR10367.
2014-05-16 Rafael EspindolaSmall dyn_cast and auto cleanup.
2014-05-16 Rafael EspindolaChange the GlobalAlias constructor to look a bit more...
2014-05-07 Duncan P. N. Exon... IR: Don't allow non-default visibility on local linkage
2014-05-01 Michael J. Spencer[IR] Make {extract,insert}element accept an index of...
2014-04-24 Reid KlecknerAdd 'musttail' marker to call instructions
2014-04-15 Craig Topper[C++11] More 'nullptr' conversion. In some cases just...
2014-03-27 Karthik BhatAll new elements except the last one initialized to...
2014-03-15 Justin BognerSupport: Make error_category's constructor public
2014-03-13 Rafael EspindolaRemove the linker_private and linker_private_weak linkages.
2014-03-11 Tim NorthoverIR: add a second ordering operand to cmpxhg for failure
2014-03-09 Chandler Carruth[C++11] Add range based accessors for the Use-Def chain...
2014-03-05 Chandler Carruth[Layering] Move AutoUpgrade.h into the IR library where its
2014-03-02 Craig TopperSwitch all uses of LLVM_OVERRIDE to just use 'override...
2014-01-15 Rafael EspindolaMake parseBitcodeFile return an ErrorOr<Module *>.
2014-01-14 Rafael EspindolaReturn an error_code from materializeAllPermanently.
2014-01-14 Nico RieckDecouple dllexport/dllimport from linkage
2014-01-14 Nico RieckRevert "Decouple dllexport/dllimport from linkage"
2014-01-14 Nico RieckDecouple dllexport/dllimport from linkage
2014-01-13 Rafael EspindolaUpdate getLazyBitcodeModule to use ErrorOr for error...
2013-12-19 Reid KlecknerBegin adding docs and IR-level support for the inalloca...
2013-12-02 Manman RenDebug Info: drop debug info via upgrading path if versi...
2013-11-18 Matt ArsenaultFix spacing, forward declare order.
2013-11-15 Matt ArsenaultAdd addrspacecast instruction.
2013-11-12 Reid KlecknerExtract a bc attr parsing helper that returns Attribute...
2013-11-05 Rafael EspindolaUse error_code in GVMaterializer.
2013-11-05 Rafael EspindolaConvert FindFunctionInStream to return an error_code.
next