]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/CodeGen/AsmPrinter/DwarfDebug.cpp
Updates to sync with changes in upstream.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.cpp
2015-01-19 Adrian PrantlRemove support for DIVariable's FlagIndirectVariable...
2015-01-14 Chandler Carruth[cleanup] Re-sort all the #include lines in LLVM using
2015-01-13 Adrian PrantlDebug Info: Move the complex expression handling (...
2015-01-13 Adrian Prantlcleanup.
2015-01-13 Adrian PrantlDebug Info: Move support for constants into DwarfExpres...
2015-01-05 Frederic RissMake DIE.h a public CodeGen header.
2014-12-30 David BlaikieDebugInfo: Omit is_stmt from line table entries on...
2014-12-16 Adrian PrantlARM/AArch64: Attach the FrameSetup MIFlag to CFI instru...
2014-12-12 Ekaterina RomanovaA fix for PR21176.
2014-12-11 Ekaterina RomanovaReverting commit 223981, because the test that I added...
2014-12-10 Ekaterina RomanovaA fix for PR21176.
2014-11-19 David BlaikieUpdate SetVector to rely on the underlying set's insert...
2014-11-12 Frederic RissFix emission of Dwarf accelerator table when there...
2014-11-11 Duncan P. N. Exon... Revert "IR: MDNode => Value"
2014-11-05 Duncan P. N. Exon... IR: MDNode => Value: NamedMDNode::getOperator()
2014-11-04 David BlaikieProvide gmlt-like inline scope information in the skele...
2014-11-03 David BlaikieUse common range handling for the CU's ranges
2014-11-03 David BlaikiePush the CURangeList down into the skeleton CU (where...
2014-11-03 David BlaikieAdd DwarfCompileUnit::BaseAddress to track the base...
2014-11-03 David BlaikieSink DwarfUnit::CURanges into DwarfCompileUnit
2014-11-02 David BlaikieFormatting
2014-11-02 David BlaikieAdd DwarfUnit::isDwoUnit and use it to generalize strin...
2014-11-02 David BlaikieDebugInfo: Sink accelerator table lists down (GlobalNam...
2014-11-02 David BlaikieDrop DwarfCompileUnit::getLocalLabel* in favor of just...
2014-11-01 David BlaikieRemove DwarfUnit::LabelEnd in favor of computing the...
2014-11-01 David BlaikieSink DwarfUnit::SectionSym into DwarfCompileUnit as...
2014-11-01 David BlaikieAnd... fix the build some more.
2014-11-01 David BlaikieJust iterate the DwarfCompileUnits rather than trying...
2014-11-01 David BlaikieAdd '*' to auto variable that is a pointer, as per...
2014-11-01 David BlaikieAdd DwarfCompileUnit::getSkeleton that returns DwarfCom...
2014-10-31 David BlaikieSink some of DwarfDebug::collectDeadVariables down...
2014-10-31 David BlaikieSink most of DwarfDebug::constructAbstractSubprogramSco...
2014-10-28 David BlaikieMinimize the scope of some variables, NFC.
2014-10-24 David BlaikieDebugInfo: Sink DwarfDebug::ScopeVariables down into...
2014-10-24 David BlaikieRemove DwarfDebug::FirstCU as it has no use
2014-10-24 David BlaikieDebugInfo: Remove DwarfDebug::addScopeVariable now...
2014-10-23 David BlaikieDebugInfo: Remove DwarfDebug::CurrentFnArguments since...
2014-10-23 David BlaikieDebugInfo: Sink DwarfDebug::addNonArgumentScopeVariable...
2014-10-23 David Blaikie[DebugInfo] Sink DwarfDebug::addCurrentFnArgument down...
2014-10-23 David Blaikie[DebugInfo] Add DwarfDebug& to DwarfFile.
2014-10-23 David Blaikie[DebugInfo] Remove LexicalScopes::isCurrentFunctionScop...
2014-10-14 David BlaikieRevert some parts of r196288 that were confusing and...
2014-10-13 Adrian PrantlAdd an assertion about the integrity of the iterator.
2014-10-10 David BlaikieSimplify a few uses of DwarfDebug::SPMap
2014-10-10 David BlaikieSink the per-CU part of DwarfDebug::finishSubprogramDef...
2014-10-10 David BlaikieSink most of DwarfDebug::constructAbstractSubprogramSco...
2014-10-10 David BlaikieAvoid unnecessary map lookup/insertion.
2014-10-09 David BlaikieRemove unused parameter
2014-10-09 David BlaikieSink DwarfDebug::createAndAddScopeChildren down into...
2014-10-09 David BlaikieSink DwarfDebug::constructSubprogramScopeDIE down into...
2014-10-09 David BlaikieSink DwarfDebug::createScopeChildrenDIE down into Dwarf...
2014-10-09 David BlaikieSink DwarfDebug.cpp::constructVariableDIE into DwarfCom...
2014-10-09 David BlaikieSink DwarfDebug::constructLexicalScopeDIE into DwarfCom...
2014-10-09 David BlaikieSink DwarfDebug::constructInlinedScopeDIE into DwarfCom...
2014-10-09 David BlaikiePush DwarfDebug::attachRangesOrLowHighPC down into...
2014-10-09 David BlaikieSink DwarfDebug::addScopeRangeList down into DwarfCompi...
2014-10-08 David BlaikieSink and coalesce DwarfDebug.cpp::addSectionLabel and...
2014-10-08 David BlaikieDebugInfo: The rest of pushing DwarfDebug::constructSco...
2014-10-06 David BlaikieDebugInfo: Sink constructImportedEntityDIE down into...
2014-10-05 David BlaikieRemove unused map
2014-10-04 David BlaikieSink DwarfDebug::updateSubprogramScopeDIE into DwarfCom...
2014-10-04 David BlaikieSink DwarfDebug::attachLowHighPC into DwarfCompileUnit
2014-10-04 David BlaikieMove DwarfCompileUnit from DwarfUnit.h to its own heade...
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-09-30 David BlaikieOmit DW_AT_inline under -gmlt to save a little more...
2014-09-30 David BlaikieDebugInfo: Sink the code emitting DW_AT_APPLE_omit_fram...
2014-09-30 David BlaikieDisable the -gmlt optimization implemented in r218129...
2014-09-19 David BlaikieOmit DW_TAG_subprograms for subprograms without inlined...
2014-09-19 Frederic RissChange DwarfCompileUnit::createGlobalVariable to getOrC...
2014-09-19 David BlaikieOmit DW_AT_frame_base under -gmlt for size
2014-09-11 David BlaikieRemove the unused string section symbol parameter from...
2014-09-09 David BlaikieSink PrevCU updating into DwarfUnit::addRange to ensure...
2014-09-09 David BlaikieRemove DwarfDebug::PrevSection, PrevCU is sufficient...
2014-08-31 David BlaikieDebugInfo: Elide lexical scopes which only contain...
2014-08-31 David BlaikieDebugInfo: Move argument creation up into the caller...
2014-08-31 David BlaikieDelay adding imported entity DIEs to the lexical scope...
2014-08-31 David BlaikieModify DwarfDebug::constructImportedEntityDIE to return...
2014-08-31 David BlaikieRefactor constructImportedEntityDIE(DwarfUnit, DIImport...
2014-08-31 David BlaikieSimplify expression using container's front() rather...
2014-08-29 David BlaikieRevert accidentally committed patches r216787-r216789
2014-08-29 David BlaikieOmit dwarf::DW_AT_frame_base under -gmlt
2014-08-29 David BlaikieStuff
2014-08-29 Frederic RissUse DwarfDebug::attachLowHighPC for the compilation...
2014-08-28 Frederic RissConstify MCSymbol* parameters to DwarfDebug::attachLowH...
2014-08-27 David BlaikieRemove type unit skeletons. GDB no longer needs them...
2014-08-21 David BlaikieUse DILexicalBlockFile, rather than DILexicalBlock...
2014-08-21 Craig TopperRepace SmallPtrSet with SmallPtrSetImpl in function...
2014-08-18 Craig TopperRevert "Repace SmallPtrSet with SmallPtrSetImpl in...
2014-08-17 Craig TopperRepace SmallPtrSet with SmallPtrSetImpl in function...
2014-08-12 Adrian PrantlRemove a condition that can never be true, as wittnesse...
2014-08-12 David BlaikieRevert "Partially revert r214761 that asserted that...
2014-08-11 Adrian PrantlAdd a couple of convenience accessors to DebugLocEntry...
2014-08-11 Adrian PrantlDebug info: Modify DebugLocEntry::addValue to take...
2014-08-11 Adrian PrantlDebug info: Further simplify the implementation of...
2014-08-11 Adrian PrantlDebug Info: Move the sorting and uniqueing of pieces...
2014-08-11 Adrian PrantlDebug info: Refactor DebugLocEntry's Merge function...
2014-08-08 David BlaikieDebugInfo: Recommit (reverted in r215217, originally...
2014-08-08 David BlaikieDebugInfo: Remove assertion (added in r215157) that...
next