Don't pre-populate the set of keys in the map with variable locations history.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.cpp
2014-05-27 Alexey SamsonovDon't pre-populate the set of keys in the map with...
2014-05-27 David BlaikieDebugInfo: Simplify solution to avoid DW_AT_artificial...
2014-05-27 David BlaikieDebugInfo: Create abstract function definitions even...
2014-05-27 David BlaikieDebugInfo: Avoid an extra map lookup when finding abstr...
2014-05-27 David BlaikieDebugInfo: Lazily construct subprogram definition DIEs.
2014-05-27 David BlaikieDebugInfo: Lazily attach definition attributes to defin...
2014-05-23 David BlaikieDebugInfo: Put concrete definitions referencing abstrac...
2014-05-23 David BlaikieAdd FIXME comment based on code review feedback by...
2014-05-23 David BlaikieRename a couple of variables to be more accurate.
2014-05-23 David BlaikieDebugInfo: Fix cross-CU references for scopes (and...
2014-05-22 David BlaikieDebugInfo: Simplify dead variable collection slightly.
2014-05-21 David BlaikieRevert "DebugInfo: Don't put fission type units in...
2014-05-21 David BlaikieDebugInfo: Use the SPMap to find the parent CU of inlin...
2014-05-21 David BlaikieDebugInfo: Ensure concrete out of line variables from...
2014-05-20 David BlaikieRevert "DebugInfo: Assume all subprogram DIEs have...
2014-05-20 Alexey SamsonovRewrite calculateDbgValueHistory to make it (hopefully...
2014-05-20 David BlaikieDebugInfo: Emit function definitions within their names...
2014-05-19 David BlaikieDebugInfo: Assume all subprogram DIEs have been created...
2014-05-19 David BlaikieDebugInfo: Don't include DW_AT_inline on each abstract...
2014-05-19 David BlaikieDebugInfo: Fix missing inlined_subroutines caused by...
2014-05-16 David BlaikieDebugInfo: Assert rather than conditionalizing when...
2014-05-16 David BlaikieDebugInfo: Add an assert regarding the subprogram in...
2014-05-16 David BlaikieDebugInfo: Assume the CU's Subprogram list only contain...
2014-05-16 David BlaikieDwarfDebug: Refactor AT_ranges/AT_high_pc+AT_low_pc...
2014-05-15 David BlaikieDebugInfo: Don't put fission type units in comdat sections.
2014-05-15 David BlaikieDebugInfo: Simplify retrieving filename/directory name...
2014-05-14 David BlaikieDwarfDebug: Don't set frame index locations on abstract...
2014-05-14 David BlaikieDebugInfo: Sure up subprogram variable list handling...
2014-05-14 David BlaikieDebugInfo: Assert that a CU's subprogram list contains...
2014-05-14 David BlaikieDebugInfo: Do not delay attaching DW_AT_inline attribut...
2014-05-14 David BlaikieRecommit r208506: DebugInfo: Include lexical scopes...
2014-05-12 David BlaikieRevert "DebugInfo: Include lexical scopes in inlined...
2014-05-12 David BlaikieDebugInfo: Attach DW_AT_inline to inlined subprograms...
2014-05-12 David BlaikieDwarfDebug: Avoid an extra map lookup while constructin...
2014-05-11 David BlaikieDebugInfo: Include lexical scopes in inlined subroutines.
2014-04-30 Alexey SamsonovUse a single data structure to store all user variables...
2014-04-30 David BlaikieRevert "Emit DW_AT_object_pointer once, on the declarat...
2014-04-30 David BlaikieDebugInfo: Omit DW_AT_artificial on DW_TAG_formal_param...
2014-04-30 Alexey SamsonovConvert more loops to range-based equivalents
2014-04-30 Alexey SamsonovSlightly simplify code in DwarfDebug::beginFunction
2014-04-30 Alexey SamsonovMove logic for calculating DBG_VALUE history map into...
2014-04-30 David BlaikieEmit DW_AT_object_pointer once, on the declaration...
2014-04-30 Reid KlecknerFix the clang-cl self-host build by defining ~DwarfDebu...
2014-04-29 David BlaikieFix some 80 cols violations committed in r207539
2014-04-29 David BlaikieDwarfDebug: Split the initialization of abstract and...
2014-04-28 David BlaikieRemove DwarfUnit::LabelRange since it's unused.
2014-04-28 David BlaikieSatisfy sub-optimal GCC warning.
2014-04-28 Eli BenderskyAdd (...) around && clause to appeace gcc 4.8's warning
2014-04-28 David BlaikieDebugInfo: Just store the DIE by value in the DwarfUnit
2014-04-28 David BlaikiePass DIEs to DwarfUnit constructors by unique_ptr.
2014-04-28 Eric ChristopherReformat, 80-col, tab characters, etc.
2014-04-28 David BlaikieImprove explicit memory ownership of DIEs
2014-04-28 David BlaikieDwarfDebug: Omit DW_AT_object_pointer on inlined_subrou...
2014-04-28 Craig Topper[C++] Use 'nullptr'.
2014-04-27 Adrian PrantlDebug Info: Prepare DebugLocEntry to handle more than...
2014-04-26 David BlaikieDwarfDebug: Roll argument into call.
2014-04-26 David BlaikieDebugInfo: Fix and test a regression caused by r207263...
2014-04-26 David BlaikieDWARF Type Units: Avoid emitting type units under fissi...
2014-04-26 David BlaikieDwarfDebug: Minor refactoring around type unit construction
2014-04-25 Eric ChristopherMake sure that rangelists are also relative to the...
2014-04-25 David BlaikieDwarfAccelTable: Store the string symbol in the acceler...
2014-04-25 David BlaikieEncapsulate the DWARF string pool in a separate type.
2014-04-25 David BlaikieDIE: Pass ownership of children via std::unique_ptr...
2014-04-25 David BlaikieDIEEntry: Refer to the specified DIE via reference...
2014-04-25 David BlaikieDwarfUnit: return by reference from createAndAddDIE
2014-04-25 David BlaikieReturn DIE by reference instead of pointer from DwarfUn...
2014-04-25 David BlaikieDwarfUnit: Suddently, DIE references, everywhere.
2014-04-24 Craig Topper[C++] Use 'nullptr'.
2014-04-24 David BlaikieRemove unused parameter
2014-04-24 David BlaikieRemove the intermediate AccelTypes maps in DWARF units.
2014-04-24 David BlaikieRemove the intermediate AccelNamespace maps in DWARF...
2014-04-24 David BlaikieRemove the intermediate AccelObjC maps in DWARF units
2014-04-23 David BlaikieAnd actually use the DwarfDebug::AccelNames to emit...
2014-04-23 David BlaikieMore formatting...
2014-04-23 David BlaikieRemove intermediate accelerator table for names.
2014-04-23 David BlaikieDwarfAccelTable: Remove trivial dtor and simplify const...
2014-04-23 David BlaikieMove the AddressPool from DwarfFile to DwarfDebug.
2014-04-23 David BlaikieSeparate out the DWARF address pool into its own type...
2014-04-23 David BlaikieSplit out DwarfFile from DwarfDebug into its own .h...
2014-04-22 David BlaikieRequisite reformatting for previous commit.
2014-04-22 David BlaikiePush memory ownership of DwarfUnits into clients of...
2014-04-22 David BlaikieUse std::unique_ptr to handle ownership of DwarfUnits...
2014-04-22 David BlaikieSimplify address pool index assignment.
2014-04-22 David BlaikieRevert "Use value semantics to manage DbgVariables...
2014-04-22 Chandler Carruth[Modules] Remove potential ODR violations by sinking...
2014-04-21 David BlaikieUse value semantics to manage DbgVariables rather than...
2014-04-17 Diego NovilloFix bug 19437 - Only add discriminators for DWARF 4...
2014-04-14 David BlaikieUse std::unique_ptr for DIE children
2014-04-12 David BlaikieUse dwarf::Tag rather than unsigned for DIE::Tag to...
2014-04-11 Adrian PrantlDebug info: Store the DIVariable in DebugLocEntry also...
2014-04-10 Adrian PrantlDebug info: Factor the retrieving of the DIVariable...
2014-04-02 David BlaikieAdjust comments regarding non-relocated abbrev offset...
2014-04-02 David BlaikieSplit debug_loc and debug_loc.dwo emission into two...
2014-04-02 David BlaikieDebugInfo: Introduce DebugLocList to encapsulate a...
2014-04-01 David BlaikieDebugInfo: Factor out common functionality for renderin...
2014-04-01 David BlaikieCleanup remaining use of removed variable to fix the...
2014-04-01 David BlaikieSimplify debug_loc.dwo handling slightly.
2014-04-01 Adrian PrantlLTO type uniquing: store the Decl field of a DIImported...
2014-03-25 David BlaikieDebugInfo: Add GNU_addr_base and GNU_ranges_base only...
2014-03-25 David BlaikieDebugInfo: Support debug_loc under fission
next