]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/CodeGen/AsmPrinter/DwarfDebug.cpp
Convert more loops to range-based equivalents
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.cpp
2014-04-30 Alexey SamsonovConvert more loops to range-based equivalents
2014-04-30 Alexey SamsonovSlightly simplify code in DwarfDebug::beginFunction
2014-04-30 Alexey SamsonovMove logic for calculating DBG_VALUE history map into...
2014-04-30 David BlaikieEmit DW_AT_object_pointer once, on the declaration...
2014-04-30 Reid KlecknerFix the clang-cl self-host build by defining ~DwarfDebu...
2014-04-29 David BlaikieFix some 80 cols violations committed in r207539
2014-04-29 David BlaikieDwarfDebug: Split the initialization of abstract and...
2014-04-28 David BlaikieRemove DwarfUnit::LabelRange since it's unused.
2014-04-28 David BlaikieSatisfy sub-optimal GCC warning.
2014-04-28 Eli BenderskyAdd (...) around && clause to appeace gcc 4.8's warning
2014-04-28 David BlaikieDebugInfo: Just store the DIE by value in the DwarfUnit
2014-04-28 David BlaikiePass DIEs to DwarfUnit constructors by unique_ptr.
2014-04-28 Eric ChristopherReformat, 80-col, tab characters, etc.
2014-04-28 David BlaikieImprove explicit memory ownership of DIEs
2014-04-28 David BlaikieDwarfDebug: Omit DW_AT_object_pointer on inlined_subrou...
2014-04-28 Craig Topper[C++] Use 'nullptr'.
2014-04-27 Adrian PrantlDebug Info: Prepare DebugLocEntry to handle more than...
2014-04-26 David BlaikieDwarfDebug: Roll argument into call.
2014-04-26 David BlaikieDebugInfo: Fix and test a regression caused by r207263...
2014-04-26 David BlaikieDWARF Type Units: Avoid emitting type units under fissi...
2014-04-26 David BlaikieDwarfDebug: Minor refactoring around type unit construction
2014-04-25 Eric ChristopherMake sure that rangelists are also relative to the...
2014-04-25 David BlaikieDwarfAccelTable: Store the string symbol in the acceler...
2014-04-25 David BlaikieEncapsulate the DWARF string pool in a separate type.
2014-04-25 David BlaikieDIE: Pass ownership of children via std::unique_ptr...
2014-04-25 David BlaikieDIEEntry: Refer to the specified DIE via reference...
2014-04-25 David BlaikieDwarfUnit: return by reference from createAndAddDIE
2014-04-25 David BlaikieReturn DIE by reference instead of pointer from DwarfUn...
2014-04-25 David BlaikieDwarfUnit: Suddently, DIE references, everywhere.
2014-04-24 Craig Topper[C++] Use 'nullptr'.
2014-04-24 David BlaikieRemove unused parameter
2014-04-24 David BlaikieRemove the intermediate AccelTypes maps in DWARF units.
2014-04-24 David BlaikieRemove the intermediate AccelNamespace maps in DWARF...
2014-04-24 David BlaikieRemove the intermediate AccelObjC maps in DWARF units
2014-04-23 David BlaikieAnd actually use the DwarfDebug::AccelNames to emit...
2014-04-23 David BlaikieMore formatting...
2014-04-23 David BlaikieRemove intermediate accelerator table for names.
2014-04-23 David BlaikieDwarfAccelTable: Remove trivial dtor and simplify const...
2014-04-23 David BlaikieMove the AddressPool from DwarfFile to DwarfDebug.
2014-04-23 David BlaikieSeparate out the DWARF address pool into its own type...
2014-04-23 David BlaikieSplit out DwarfFile from DwarfDebug into its own .h...
2014-04-22 David BlaikieRequisite reformatting for previous commit.
2014-04-22 David BlaikiePush memory ownership of DwarfUnits into clients of...
2014-04-22 David BlaikieUse std::unique_ptr to handle ownership of DwarfUnits...
2014-04-22 David BlaikieSimplify address pool index assignment.
2014-04-22 David BlaikieRevert "Use value semantics to manage DbgVariables...
2014-04-22 Chandler Carruth[Modules] Remove potential ODR violations by sinking...
2014-04-21 David BlaikieUse value semantics to manage DbgVariables rather than...
2014-04-17 Diego NovilloFix bug 19437 - Only add discriminators for DWARF 4...
2014-04-14 David BlaikieUse std::unique_ptr for DIE children
2014-04-12 David BlaikieUse dwarf::Tag rather than unsigned for DIE::Tag to...
2014-04-11 Adrian PrantlDebug info: Store the DIVariable in DebugLocEntry also...
2014-04-10 Adrian PrantlDebug info: Factor the retrieving of the DIVariable...
2014-04-02 David BlaikieAdjust comments regarding non-relocated abbrev offset...
2014-04-02 David BlaikieSplit debug_loc and debug_loc.dwo emission into two...
2014-04-02 David BlaikieDebugInfo: Introduce DebugLocList to encapsulate a...
2014-04-01 David BlaikieDebugInfo: Factor out common functionality for renderin...
2014-04-01 David BlaikieCleanup remaining use of removed variable to fix the...
2014-04-01 David BlaikieSimplify debug_loc.dwo handling slightly.
2014-04-01 Adrian PrantlLTO type uniquing: store the Decl field of a DIImported...
2014-03-25 David BlaikieDebugInfo: Add GNU_addr_base and GNU_ranges_base only...
2014-03-25 David BlaikieDebugInfo: Support debug_loc under fission
2014-03-25 David BlaikieDebugInfo: Remove unnecessary zero-size check
2014-03-24 David BlaikieDebugInfo: Simplify debug loc list handling by keeping...
2014-03-24 David BlaikieDwarfDebug: Simplify debug_loc merging
2014-03-24 David BlaikieDebugInfo: Add DW_AT_GNU_ranges_base to skeleton CUs
2014-03-24 David BlaikieDebugInfo: Implement relative addressing for DW_AT_rang...
2014-03-24 David BlaikieDebugInfo: Don't emit relocations to abbreviations...
2014-03-24 David BlaikieDwarfDebug: Remove an unused parameter
2014-03-24 David BlaikieRemove unused parameter
2014-03-21 Adrian PrantlDelete stale comment. Thanks, Eric!
2014-03-21 Adrian PrantlDwarf Debug: Remove some cargo-cult type uniquing....
2014-03-21 David BlaikieDebugInfo: Omit DW_AT_addr_base from skeletal type...
2014-03-20 Eric ChristopherReapply DW_AT_low/high_pc patch:
2014-03-20 David BlaikieAdd comments from Eric's review of r204094.
2014-03-20 Eric ChristopherRevert "Use the range machinery for DW_AT_ranges and...
2014-03-19 Eric ChristopherUse the range machinery for DW_AT_ranges and DW_AT_high...
2014-03-19 David BlaikieDebugInfo: Use the comp_dir of the referencing type...
2014-03-18 Adrian PrantlDebug info: Remove OdrMemberMap from DwarfDebug, it...
2014-03-18 Adrian PrantlDwarfDebug: Only unique retained types instead of all...
2014-03-18 Adrian PrantlSwitch the type field in DIVariable and DIGlobalVariabl...
2014-03-18 Eric ChristopherAdd explanatory comment.
2014-03-18 Eric ChristopherShorten DotDebugLocEntry to just DebugLocEntry and...
2014-03-18 David BlaikieDebugInfo: Avoid emitting standard opcode lengths in...
2014-03-18 David BlaikieDebugInfo: Implement debug_line.dwo for file names...
2014-03-18 David BlaikieDebugInfo: Do not rely on the compilation dir (index...
2014-03-17 David BlaikieDebugInfo: Move getOrCreateSourceID from DwarfDebug...
2014-03-17 David BlaikieDebugInfo: Move line table zero-directory-index (compil...
2014-03-17 David BlaikieDebugInfo: Use MC line table file entry uniquing for...
2014-03-14 Adrian PrantlDebug Info: Fix LTO type uniquing for C++ member declar...
2014-03-14 Eric ChristopherRemove command line option for CU hashing. This is...
2014-03-14 Eric ChristopherIf we see that we're emitting code for a function that...
2014-03-14 Eric ChristopherRemove the -generate-dwarf-cu-ranges flag.
2014-03-14 David BlaikieDwarfDebug: Remove some needless recursion.
2014-03-12 Eric ChristopherTurn on hashing by default for split dwarf compile...
2014-03-12 David BlaikieDebugInfo: Use common line/file attribute construction...
2014-03-11 David BlaikieDebugInfo: Do not emit pubnames/pubtypes sections if...
2014-03-11 David BlaikieDebugInfo: Avoid re-looking up the DwarfUnit when emitt...
2014-03-11 David BlaikieDebugInfo: Refactor emitDebugPubNames/Types into a...
2014-03-11 David BlaikieDebugInfo: Remove unused labels now that we just emit...
next