Replace unnecessary #include directive with forward declarations.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.h
2014-03-18 Adrian PrantlReplace unnecessary #include directive with forward...
2014-03-18 Eric ChristopherShorten DotDebugLocEntry to just DebugLocEntry and...
2014-03-18 David BlaikieDebugInfo: Avoid emitting standard opcode lengths in...
2014-03-18 David BlaikieDebugInfo: Implement debug_line.dwo for file names...
2014-03-18 David BlaikieDebugInfo: Do not rely on the compilation dir (index...
2014-03-17 David BlaikieDebugInfo: Move getOrCreateSourceID from DwarfDebug...
2014-03-17 David BlaikieDebugInfo: Use MC line table file entry uniquing for...
2014-03-14 Adrian PrantlDebug Info: Fix LTO type uniquing for C++ member declar...
2014-03-11 David BlaikieDebugInfo: Refactor emitDebugPubNames/Types into a...
2014-03-08 Craig Topper[C++11] Add 'override' keyword to virtual methods that...
2014-03-08 Eric ChristopherAdd support for hashing location information for CU...
2014-03-07 Eric ChristopherTwo part patch:
2014-03-07 David BlaikieDebugInfo: Refactor high_pc/low_pc construction into...
2014-03-06 Eric ChristopherConstify a few things with DotDebugLocEntry.
2014-03-06 Chandler Carruth[Layering] Move DebugInfo.h into the IR library where...
2014-03-06 Eric ChristopherRemove the last of the special case code for emitting...
2014-03-06 Eric Christopherconstify a few accessors.
2014-03-05 Eric ChristopherAdd a DIELocList class to handle pointers into the...
2014-03-05 Chandler Carruth[Layering] Move DebugLoc.h into the IR library. The...
2014-03-04 Chandler Carruth[cleanup] Re-sort all the includes with utils/sort_incl...
2014-02-16 Eric ChristopherAdd a DIELoc class to cover the DW_FORM_exprloc set...
2014-02-15 David BlaikieDebugInfo: Deduplicate entries in the fission address...
2014-02-12 David BlaikieDwarfUnit: Provide a reference to a defining DwarfCompi...
2014-01-29 Eric ChristopherMake the compile unit map a MapVector so that we can...
2014-01-28 Eric ChristopherRevert r199871 and replace it with a simple check in...
2014-01-24 Eric ChristopherRevert "Use DW_AT_high_pc and DW_AT_low_pc for the...
2014-01-24 Eric ChristopherUse DW_AT_high_pc and DW_AT_low_pc for the high and...
2014-01-15 Eric ChristopherMake sure we emit a relocation to the debug_ranges...
2014-01-10 David BlaikieRevert "Revert r198851, "Prototype of skeleton type...
2014-01-09 NAKAMURA TakumiRevert r198851, "Prototype of skeleton type units for...
2014-01-09 David BlaikiePrototype of skeleton type units for fission
2014-01-09 David BlaikieDwarfDebug: Refactor out common skeleton construction...
2014-01-09 David BlaikieDwarfUnit: Rename "Node" to "CUNode" and propagate...
2014-01-03 David BlaikieRevert "Revert "Debug Info: Type Units: Simplify type...
2014-01-03 David BlaikieRevert "Debug Info: Type Units: Simplify type hashing...
2014-01-03 David BlaikieDebug Info: Type Units: Simplify type hashing using...
2013-12-30 Eric ChristopherRevert r198208 and reapply:
2013-12-30 NAKAMURA TakumiRevert r198199 (and r198202). It broke 3 DebugInfo...
2013-12-30 Eric ChristopherFix aranges and split dwarf by ensuring that the symbol...
2013-12-17 David BlaikieDebugInfo: Introduce new DIValue, DIETypeSignature...
2013-12-10 Eric ChristopherWe never emit info into the macro info section, stop...
2013-12-09 Eric ChristopherRename CompileUnit->DwarfCompileUnit and TypeUnit-...
2013-12-09 Eric ChristopherRename Unit->DwarfUnit to match the file name and make...
2013-12-06 David BlaikieDebugInfo: Include the section and start-of-section...
2013-12-06 David BlaikieDebugInfo: Ensure unit IDs (for non-skeletal units...
2013-12-05 Eric ChristopherRename DwarfUnits to DwarfFile to help avoid some namin...
2013-12-05 David BlaikieDwarfDebug/DwarfUnit: Push abbreviation structures...
2013-12-05 David BlaikieDwarfDebug: Avoid unnecessary abbreviation lookup when...
2013-12-05 David BlaikieDwarfDebug: Remove trivial function wrapper
2013-12-04 David BlaikieDwarfDebug: Reduce code duplication for sec offset...
2013-12-03 Eric ChristopherUpdate comment grammar and contents.
2013-12-03 Timur IskhodzhanovReland 196270 "Generalize debug info / EH emission...
2013-12-03 NAKAMURA TakumiRevert r196270, "Generalize debug info / EH emission...
2013-12-03 Timur IskhodzhanovGeneralize debug info / EH emission in AsmPrinter
2013-12-03 Eric ChristopherRefactor the handling of lexical block and inline scope...
2013-12-03 Eric ChristopherUpdate doxygen tags.
2013-12-03 Eric ChristopherReorder member function declarations to match source...
2013-12-03 Eric ChristopherMake ranges and range lists be a discrete entity that...
2013-12-02 David BlaikieDebugInfo: Refactor CompileUnit into a Unit baseclass...
2013-12-02 David BlaikieDebugInfo: Type Units: Propagate the correct DW_AT_lang...
2013-11-26 Eric Christopher80-column fixups.
2013-11-26 David BlaikieDwarfDebug: Include type units in accelerator tables.
2013-11-23 David BlaikieDwarfDebug: Move ownership of CompileUnits into DwarfUnits
2013-11-21 Eric ChristopherMove member variable up to where the rest of non-DWARF5...
2013-11-20 David BlaikieCR feedback for r195166: Add comments regarding type...
2013-11-19 David BlaikieDebugInfo: Partial implementation of DWARF type units.
2013-11-15 David BlaikieDwarfCompileUnit: Add type safety by using DICompileUni...
2013-11-15 David BlaikieDwarfDebug: Push DISubprogram through updateSubprogramS...
2013-10-31 Manman RenDebug Info: remove duplication of DIEs when a DIE can...
2013-10-30 David BlaikieDwarfDebug: Change Abbreviations member from pointer...
2013-10-29 Manman RenDebug Info: support for DW_FORM_ref_addr.
2013-10-24 Eric ChristopherGrammar.
2013-10-15 Adrian PrantlRemove some dead code. (DarwinGDBCompat was retired...
2013-10-08 Manman RenAdd DbgVariable::resolve per Eric's suggestion.
2013-10-05 Manman RenDebug Info: In DIBuilder, the derived-from field of...
2013-10-05 Eric ChristopherFix one comment and update another. Slightly reformat.
2013-10-04 Eric ChristopherTemporarily revert r176882 as it needs to be implemente...
2013-10-04 Eric ChristopherTemporarily revert r191792 as it is causing some LTO...
2013-10-03 Alexey SamsonovRemove wild .debug_aranges entries generated from unimp...
2013-10-01 Manman RenDebug Info: In DIBuilder, the derived-from field of...
2013-10-01 Manman RenDebug Info: remove duplication of DIEs when a DIE is...
2013-09-30 Eric ChristopherThe DW_AT_GNU_pubnames/pubtypes attributes are actually...
2013-09-23 Richard MittonFixed debug_aranges handling for common symbols.
2013-09-19 Richard MittonAdded support for generate DWARF .debug_aranges section...
2013-09-13 Eric ChristopherAdd initial support for handling gnu style pubnames...
2013-09-11 Benjamin KramerRevert "Give internal classes hidden visibility."
2013-09-11 Benjamin KramerGive internal classes hidden visibility.
2013-09-10 Manman RenDebug Info: create scope children DIEs when the scope...
2013-09-10 Manman RenDebug Info: define a DIRef template.
2013-09-09 Manman RenDebug Info: move DIScope::getContext back from DwarfDebug.
2013-09-09 Eric ChristopherRename for consistency.
2013-09-09 Manman RenDebug Info: move DIScope::getContext to DwarfDebug.
2013-09-09 Manman RenDebug Info: Move isSubprogramContext from DebugInfo...
2013-09-09 Manman RenDebug Info: Rename DITypeRef to DIScopeRef.
2013-09-05 Manman RenDebug Info: Use identifier to reference DIType in base...
2013-08-28 Eric ChristopherRemove support for the .debug_inlined section. No known...
2013-08-26 Eric ChristopherHave the skeleton compile unit construction method...
2013-08-26 Eric ChristopherTreat the pubtypes section similarly to the pubnames...
2013-08-19 Eric ChristopherTurn on pubnames by default on linux.
2013-08-08 Eric ChristopherBe more rigorous about the sizes of forms and attributes.
next