]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/CodeGen/AsmPrinter/DwarfUnit.cpp
DI: Fold constant arguments into a single MDString
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfUnit.cpp
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 David BlaikieImplement DW_TAG_subrange_type with DW_AT_count rather...
2014-09-19 David BlaikieOmit DW_TAG_subprograms for subprograms without inlined...
2014-09-19 Frederic RissChange DwarfCompileUnit::createGlobalVariable to getOrC...
2014-09-19 David BlaikieDescribe the -gmlt optimization committed in the previo...
2014-09-19 David BlaikieOmit all the extra static attributes on subprograms...
2014-09-18 Frederic RissRevert part of r218041.
2014-09-18 Frederic RissAlways emit DW_AT_declaration attribute when the variab...
2014-09-15 David BlaikieDebugInfo: Add comment describing the need to disable...
2014-09-11 David BlaikieRemove the unused string section symbol parameter from...
2014-09-09 David BlaikieSink PrevCU updating into DwarfUnit::addRange to ensure...
2014-09-09 David BlaikieRemove DwarfDebug::PrevSection, PrevCU is sufficient...
2014-09-07 David BlaikieDebugInfo: Do not use DW_FORM_GNU_addr_index in skeleto...
2014-08-29 Adrian PrantlDebug info: Add a new explicit DIDescriptor flag for...
2014-08-29 David BlaikieRevert accidentally committed patches r216787-r216789
2014-08-29 David BlaikieOmit DW_AT_artificial, DW_AT_external, and similar...
2014-08-04 Eric ChristopherRemove the TargetMachine forwards for TargetSubtargetIn...
2014-08-01 Adrian PrantlDebug info: Infrastructure to support debug locations...
2014-07-29 Manman RenFeedback on r214189, no functionality change.
2014-07-29 Manman Ren[Debug Info] remove DITrivialType and use null to repre...
2014-07-28 Manman Ren[Debug Info] add DISubroutineType and its creation...
2014-07-28 Manman Ren[Debug Info] rename getTypeArray to getElements, setTyp...
2014-06-13 David BlaikieDebugInfo: Following up to r209677, refactor local...
2014-06-07 Alp TokerFix typos
2014-06-06 David BlaikieDebugInfo: Use the scope of the function declaration...
2014-06-06 David BlaikieDebugInfo: pubnames: include file-local (static or...
2014-06-05 David BlaikieRevert r210221 again, due to a crash Richard Smith...
2014-06-05 David BlaikieDebugInfo: Add comments/assert description to r209674...
2014-06-04 David BlaikieDebugInfo: Reapply r209984 (reverted in r210143), asser...
2014-06-04 David BlaikieDebugInfo: Partial revert r209984 due to more cases...
2014-06-01 David BlaikieDebugInfo: Assert that DbgVariables have associated...
2014-05-31 Alp TokerFix typos
2014-05-27 David BlaikieDebugInfo: partially revert cleanup committed in r209680
2014-05-27 David BlaikieDebugInfo: Simplify solution to avoid DW_AT_artificial...
2014-05-27 David BlaikieDebugInfo: Lazily attach definition attributes to defin...
2014-05-27 David BlaikieDebugInfo: Separate out the addition of subprogram...
2014-05-26 David BlaikieDwarfUnit: Remove some misleading no-op code introduced...
2014-05-21 David BlaikieDebugInfo: Simplify subprogram declaration creation...
2014-05-20 David BlaikieUnbreak the sanitizer buildbots after r209226 due to...
2014-05-20 David BlaikieFix test breakage introduced in r209223.
2014-05-20 David BlaikiePR19767: DebugInfo emission of pointer constants.
2014-05-16 David BlaikieDebugInfo: Handle emitting constants of C++ unicode...
2014-05-12 Saleem AbdulrasoolCodeGen: add parenthesis around complex expression
2014-05-11 David BlaikieDwarfUnit: Make explicit a limitation/bug in enumeratio...
2014-05-11 David BlaikieDwarfUnit: Pick a winner between isTypeSigned and isUns...
2014-05-11 David BlaikieDwarfUnit: Factor out calling isUnsignedDIType into...
2014-05-11 David BlaikieDwarfUnit: Share common constant value emission between...
2014-05-11 David BlaikieDebugInfo: Simplify constant value emission.
2014-04-30 David BlaikieRevert "Emit DW_AT_object_pointer once, on the declarat...
2014-04-30 David BlaikieDebugInfo: Omit DW_AT_artificial on DW_TAG_formal_param...
2014-04-30 David BlaikieEmit DW_AT_object_pointer once, on the declaration...
2014-04-28 David BlaikieRemove DwarfUnit::LabelRange since it's unused.
2014-04-28 David BlaikieDebugInfo: Just store the DIE by value in the DwarfUnit
2014-04-28 David BlaikiePass DIEs to DwarfUnit constructors by unique_ptr.
2014-04-26 David BlaikieDwarfDebug: Minor refactoring around type unit construction
2014-04-25 David BlaikieEncapsulate the DWARF string pool in a separate type.
2014-04-25 David BlaikieDIE: Pass ownership of children via std::unique_ptr...
2014-04-25 David BlaikieDIEEntry: Refer to the specified DIE via reference...
2014-04-25 David BlaikieDwarfUnit: return by reference from createAndAddDIE
2014-04-25 David BlaikieReturn DIE by reference instead of pointer from DwarfUn...
2014-04-25 David BlaikieDwarfUnit: Suddently, DIE references, everywhere.
2014-04-25 David BlaikieRefactor some common logic in DwarfUnit::constructVaria...
2014-04-24 Craig Topper[C++] Use 'nullptr'.
2014-04-24 David BlaikieRemove the intermediate AccelTypes maps in DWARF units.
2014-04-24 David BlaikieRemove the intermediate AccelNamespace maps in DWARF...
2014-04-24 David BlaikieRemove the intermediate AccelObjC maps in DWARF units
2014-04-23 David BlaikieRemove intermediate accelerator table for names.
2014-04-23 David BlaikieMove the AddressPool from DwarfFile to DwarfDebug.
2014-04-23 David BlaikieSeparate out the DWARF address pool into its own type...
2014-04-22 Chandler Carruth[Modules] Remove potential ODR violations by sinking...
2014-04-14 Adrian PrantlRe-apply r206096 after investigating the gdb buildbot...
2014-04-12 David BlaikiePR13337: Omit DW_TAG_restrict_type when compiling for...
2014-04-12 Adrian PrantlRevert "Debug info: (bugfix) C++ C/Dtors can be compile...
2014-04-12 David BlaikieUse dwarf::Tag rather than unsigned for DIE::Tag to...
2014-04-12 Adrian PrantlDebug info: (bugfix) C++ C/Dtors can be compiled to...
2014-04-03 David BlaikieDebugInfo: Use a 64 bit type for the subrange
2014-04-02 David BlaikieAdjust comments regarding non-relocated abbrev offset...
2014-04-01 David BlaikieDebugInfo: Avoid creating unnecessary/empty line tables...
2014-03-24 Adrian PrantlGet rid of an unnecessary use of the * and & operators.
2014-03-24 David BlaikieDebugInfo: Don't emit relocations to abbreviations...
2014-03-24 David BlaikieRemove unused parameter
2014-03-20 Eric ChristopherReapply DW_AT_low/high_pc patch:
2014-03-20 Eric ChristopherRevert "Use the range machinery for DW_AT_ranges and...
2014-03-19 Eric ChristopherUse the range machinery for DW_AT_ranges and DW_AT_high...
2014-03-18 Adrian PrantlDebug info: Remove OdrMemberMap from DwarfDebug, it...
2014-03-18 Adrian PrantlDwarfDebug: Only unique retained types instead of all...
2014-03-18 Adrian PrantlSwitch the type field in DIVariable and DIGlobalVariabl...
2014-03-18 David BlaikieDebugInfo: Avoid emitting standard opcode lengths in...
2014-03-18 David BlaikieDebugInfo: Implement debug_line.dwo for file names...
2014-03-17 David BlaikieDebugInfo: Move getOrCreateSourceID from DwarfDebug...
2014-03-14 Adrian PrantlDebug info: Unique types before emitting them to DWARF...
2014-03-14 Adrian PrantlDebug Info: Fix LTO type uniquing for C++ member declar...
2014-03-14 Adrian Prantltypo
2014-03-13 Eric ChristopherUse DW_AT_linkage_name when we're emitting DWARF4 or...
2014-03-12 Eric ChristopherWhen computing the size of a base type be conservative...
2014-03-12 Eric ChristopherUse values we've already computed, update comment.
2014-03-12 David BlaikieDebugInfo: Omit pubnames/pubtypes when compiling with...
next