Explain why LLVM is emitting a DW_AT_containing_type inside of a class.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfUnit.cpp
2014-12-19 Adrian PrantlExplain why LLVM is emitting a DW_AT_containing_type...
2014-12-17 David BlaikiePR21875: codegen for non-type template parameters of...
2014-12-09 Duncan P. N. Exon... IR: Split Metadata from Value
2014-12-05 Eric ChristopherThese two calls were grabbing the same register info...
2014-12-05 Adrian PrantlCleanup: Calls to getDwarfRegNum() may actually fail...
2014-11-04 David BlaikieProvide gmlt-like inline scope information in the skele...
2014-11-04 David BlaikieMove cross-unit DIE caching to the DwarfFile level...
2014-11-02 David BlaikieAdd DwarfUnit::isDwoUnit and use it to generalize strin...
2014-11-02 David BlaikieRemove the last mention of LineTablesOnly from DwarfUni...
2014-11-02 David BlaikieSink DwarfUnit::applySubprogramAttributesToDefinition...
2014-11-02 David BlaikieSink DwarfUnit::addExpr into DwarfCompileUnit
2014-11-02 David BlaikieSink DwarfUnit::applyVariableAttributes into DwarfCompi...
2014-11-02 David BlaikieSink DwarfUnit::addLocationList down into DwarfCompileUnit
2014-11-02 David BlaikieSink DwarfUnit::addComplexAddress down into DwarfCompil...
2014-11-02 David BlaikiePush DwarfUnit::addAddress down into DwarfCompileUnit
2014-11-02 David BlaikieSink DwarfUnit::addVariableAddress into DwarfCompileUni...
2014-11-02 David BlaikieDebugInfo: Sink accelerator table lists down (GlobalNam...
2014-11-02 David BlaikieAdd DwarfUnit::addGlobalType to match DwarfUnit::addGlo...
2014-11-02 David BlaikieDebugInfo: Refactor index type DIE initialization by...
2014-11-02 David BlaikieSink DwarfUnit::LabelBegin down into DwarfCompileUnit...
2014-11-01 David BlaikieSink dwarf unit length emission down into DwarfUnit...
2014-11-01 David BlaikieRemove DwarfUnit::LabelEnd in favor of computing the...
2014-11-01 David BlaikieSink DwarfUnit::SectionSym into DwarfCompileUnit as...
2014-11-01 David BlaikieSink DwarfUnit::Skeleton down into DwarfCompileUnit
2014-10-26 David BlaikieRemove some unnecessary casts.
2014-10-24 Frederic RissSink DwarfUnit::constructImportedEntityDIE into DwarfCo...
2014-10-09 David BlaikieMove DwarfUnit::constructVariableDIE down to DwarfCompi...
2014-10-08 David BlaikieSink DwarfUnit::addSectionDelta into DwarfCompileUnit...
2014-10-08 David BlaikieSink and coalesce DwarfDebug.cpp::addSectionLabel and...
2014-10-06 David BlaikieDebugInfo: Sink constructImportedEntityDIE down into...
2014-10-04 David BlaikieMove DwarfCompileUnit from DwarfUnit.h to its own heade...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 David BlaikieImplement DW_TAG_subrange_type with DW_AT_count rather...
2014-09-19 David BlaikieOmit DW_TAG_subprograms for subprograms without inlined...
2014-09-19 Frederic RissChange DwarfCompileUnit::createGlobalVariable to getOrC...
2014-09-19 David BlaikieDescribe the -gmlt optimization committed in the previo...
2014-09-19 David BlaikieOmit all the extra static attributes on subprograms...
2014-09-18 Frederic RissRevert part of r218041.
2014-09-18 Frederic RissAlways emit DW_AT_declaration attribute when the variab...
2014-09-15 David BlaikieDebugInfo: Add comment describing the need to disable...
2014-09-11 David BlaikieRemove the unused string section symbol parameter from...
2014-09-09 David BlaikieSink PrevCU updating into DwarfUnit::addRange to ensure...
2014-09-09 David BlaikieRemove DwarfDebug::PrevSection, PrevCU is sufficient...
2014-09-07 David BlaikieDebugInfo: Do not use DW_FORM_GNU_addr_index in skeleto...
2014-08-29 Adrian PrantlDebug info: Add a new explicit DIDescriptor flag for...
2014-08-29 David BlaikieRevert accidentally committed patches r216787-r216789
2014-08-29 David BlaikieOmit DW_AT_artificial, DW_AT_external, and similar...
2014-08-04 Eric ChristopherRemove the TargetMachine forwards for TargetSubtargetIn...
2014-08-01 Adrian PrantlDebug info: Infrastructure to support debug locations...
2014-07-29 Manman RenFeedback on r214189, no functionality change.
2014-07-29 Manman Ren[Debug Info] remove DITrivialType and use null to repre...
2014-07-28 Manman Ren[Debug Info] add DISubroutineType and its creation...
2014-07-28 Manman Ren[Debug Info] rename getTypeArray to getElements, setTyp...
2014-06-13 David BlaikieDebugInfo: Following up to r209677, refactor local...
2014-06-07 Alp TokerFix typos
2014-06-06 David BlaikieDebugInfo: Use the scope of the function declaration...
2014-06-06 David BlaikieDebugInfo: pubnames: include file-local (static or...
2014-06-05 David BlaikieRevert r210221 again, due to a crash Richard Smith...
2014-06-05 David BlaikieDebugInfo: Add comments/assert description to r209674...
2014-06-04 David BlaikieDebugInfo: Reapply r209984 (reverted in r210143), asser...
2014-06-04 David BlaikieDebugInfo: Partial revert r209984 due to more cases...
2014-06-01 David BlaikieDebugInfo: Assert that DbgVariables have associated...
2014-05-31 Alp TokerFix typos
2014-05-27 David BlaikieDebugInfo: partially revert cleanup committed in r209680
2014-05-27 David BlaikieDebugInfo: Simplify solution to avoid DW_AT_artificial...
2014-05-27 David BlaikieDebugInfo: Lazily attach definition attributes to defin...
2014-05-27 David BlaikieDebugInfo: Separate out the addition of subprogram...
2014-05-26 David BlaikieDwarfUnit: Remove some misleading no-op code introduced...
2014-05-21 David BlaikieDebugInfo: Simplify subprogram declaration creation...
2014-05-20 David BlaikieUnbreak the sanitizer buildbots after r209226 due to...
2014-05-20 David BlaikieFix test breakage introduced in r209223.
2014-05-20 David BlaikiePR19767: DebugInfo emission of pointer constants.
2014-05-16 David BlaikieDebugInfo: Handle emitting constants of C++ unicode...
2014-05-12 Saleem AbdulrasoolCodeGen: add parenthesis around complex expression
2014-05-11 David BlaikieDwarfUnit: Make explicit a limitation/bug in enumeratio...
2014-05-11 David BlaikieDwarfUnit: Pick a winner between isTypeSigned and isUns...
2014-05-11 David BlaikieDwarfUnit: Factor out calling isUnsignedDIType into...
2014-05-11 David BlaikieDwarfUnit: Share common constant value emission between...
2014-05-11 David BlaikieDebugInfo: Simplify constant value emission.
2014-04-30 David BlaikieRevert "Emit DW_AT_object_pointer once, on the declarat...
2014-04-30 David BlaikieDebugInfo: Omit DW_AT_artificial on DW_TAG_formal_param...
2014-04-30 David BlaikieEmit DW_AT_object_pointer once, on the declaration...
2014-04-28 David BlaikieRemove DwarfUnit::LabelRange since it's unused.
2014-04-28 David BlaikieDebugInfo: Just store the DIE by value in the DwarfUnit
2014-04-28 David BlaikiePass DIEs to DwarfUnit constructors by unique_ptr.
2014-04-26 David BlaikieDwarfDebug: Minor refactoring around type unit construction
2014-04-25 David BlaikieEncapsulate the DWARF string pool in a separate type.
2014-04-25 David BlaikieDIE: Pass ownership of children via std::unique_ptr...
2014-04-25 David BlaikieDIEEntry: Refer to the specified DIE via reference...
2014-04-25 David BlaikieDwarfUnit: return by reference from createAndAddDIE
2014-04-25 David BlaikieReturn DIE by reference instead of pointer from DwarfUn...
2014-04-25 David BlaikieDwarfUnit: Suddently, DIE references, everywhere.
2014-04-25 David BlaikieRefactor some common logic in DwarfUnit::constructVaria...
2014-04-24 Craig Topper[C++] Use 'nullptr'.
2014-04-24 David BlaikieRemove the intermediate AccelTypes maps in DWARF units.
next