typo
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfUnit.cpp
2014-03-14 Adrian Prantltypo
2014-03-13 Eric ChristopherUse DW_AT_linkage_name when we're emitting DWARF4 or...
2014-03-12 Eric ChristopherWhen computing the size of a base type be conservative...
2014-03-12 Eric ChristopherUse values we've already computed, update comment.
2014-03-12 David BlaikieDebugInfo: Omit pubnames/pubtypes when compiling with...
2014-03-07 David BlaikieDebugInfo: Emit DW_TAG_subprogram's DW_AT_high_pc as...
2014-03-06 David BlaikieDebugInfo: Shrink pubnames/pubtypes in the presence...
2014-03-06 Chandler Carruth[Layering] Move DIBuilder.h into the IR library where...
2014-03-05 Eric ChristopherAdd a DIELocList class to handle pointers into the...
2014-02-27 Eric ChristopherRevert r201751 and solve the const problem a different...
2014-02-26 Eric ChristopherRemove unnecessary llvm:: qualification.
2014-02-25 Adrian PrantlAddress review comments for r202188.
2014-02-25 Adrian PrantlDebug info: Support variadic functions.
2014-02-25 Adrian PrantlRevert "Debug info: Support variadic functions."
2014-02-25 Adrian PrantlDebug info: Support variadic functions.
2014-02-20 Eric ChristopherMake DIELoc/DIEBlock's ComputeSize method const. Add...
2014-02-20 Eric ChristopherRemove FIXME that had snuck in.
2014-02-16 Eric ChristopherAdd a DIELoc class to cover the DW_FORM_exprloc set...
2014-02-15 David BlaikieDebugInfo: Deduplicate entries in the fission address...
2014-02-14 David BlaikieDebugInfo: Implement DW_AT_stmt_list for type units
2014-02-14 David BlaikieDwarfUnit: Remove unnecessarily explicit/out of line...
2014-02-14 David BlaikieDwarfUnit: Remove unnecessary (void)t; that was previou...
2014-02-14 David BlaikieDwarfUnit: Refactor out DW_AT_stmt_list creation into...
2014-02-12 Eric ChristopherReformat a few lines with clang-format.
2014-02-12 Eric Christopher80-col.
2014-02-12 Adrian PrantlDebug info: Bugfix for r201190: DW_OP_piece takes bytes...
2014-02-12 David BlaikieDwarfUnit: Include type unit's file strings in the...
2014-02-12 David BlaikieDwarfUnit: Provide a reference to a defining DwarfCompi...
2014-02-12 David BlaikieDwarfUnit: Refactor DW_AT_file creation into a common...
2014-02-11 David BlaikieDwarfUnit: Replace unnecessary conditionals with asserts.
2014-02-11 Adrian PrantlReapply r201180 with an additional error path.
2014-02-11 Adrian PrantlRevert "Debug info: Emit values in subregisters that...
2014-02-11 Adrian PrantlDebug info: Emit values in subregisters that do not...
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2014-01-31 Paul RobinsonIf we're not producing DWARF accel tables, don't waste...
2014-01-28 Adrian Prantltypo
2014-01-24 Eric ChristopherRevert "Use DW_AT_high_pc and DW_AT_low_pc for the...
2014-01-24 Eric ChristopherUse DW_AT_high_pc and DW_AT_low_pc for the high and...
2014-01-23 Eric ChristopherAvoid emitting a DWARF type attribute for an ObjC prope...
2014-01-18 Adrian PrantlDebug info (LTO): Move the creation of accessibility...
2014-01-10 David BlaikieRevert "Revert r198851, "Prototype of skeleton type...
2014-01-09 NAKAMURA TakumiRevert r198851, "Prototype of skeleton type units for...
2014-01-09 David BlaikiePrototype of skeleton type units for fission
2014-01-09 David BlaikieDwarfUnit: Rename "Node" to "CUNode" and propagate...
2014-01-09 David BlaikieRevert "DwarfUnit: Move the DICompileUnit Node to the...
2014-01-09 David BlaikieDwarfUnit: Move the DICompileUnit Node to the DwarfComp...
2014-01-07 Rafael EspindolaMove the llvm mangler to lib/IR.
2014-01-07 Chandler CarruthRe-sort all of the includes with ./utils/sort_includes...
2014-01-03 David BlaikieRevert "Revert "Debug Info: Type Units: Simplify type...
2014-01-03 David BlaikieRevert "Debug Info: Type Units: Simplify type hashing...
2014-01-03 David BlaikieDebug Info: Type Units: Simplify type hashing using...
2014-01-03 David BlaikieRevert "Reverting r193835 due to weirdness with Go..."
2014-01-03 David BlaikieReverting r193835 due to weirdness with Go...
2014-01-02 Eric ChristopherSimplify conditional.
2014-01-02 Adrian PrantlRevert "Debug info: Add enumerators to the __apple_name...
2013-12-30 Eric ChristopherRefactor and reduce code duplication for non-split...
2013-12-30 Eric ChristopherRevert r198208 and reapply:
2013-12-30 NAKAMURA TakumiRevert r198199 (and r198202). It broke 3 DebugInfo...
2013-12-30 Eric ChristopherReapply r198196 with a fix to zero initialize the skele...
2013-12-30 Eric ChristopherTemporarily revert "Use a pointer to keep track of...
2013-12-30 Eric ChristopherUse a pointer to keep track of the skeleton unit for...
2013-12-28 Eric ChristopherRemove AsmPrinter::needsRelocationsForDwarfStringPool...
2013-12-23 Adrian PrantlDebug info: Add enumerators to the __apple_names accele...
2013-12-18 Adrian PrantlDebug info: Implement (rvalue) reference qualifiers...
2013-12-17 David BlaikieDebugInfo: Introduce new DIValue, DIETypeSignature...
2013-12-14 Juergen RibutzkaRemove weak vtables. No functional change.
2013-12-13 David BlaikieDebugInfo: Move type units into the debug_types section...
2013-12-13 David BlaikieRevert "DebugInfo: Move type units into the debug_types...
2013-12-13 David BlaikieDebugInfo: Move type units into the debug_types section...
2013-12-13 David BlaikieRevert "DebugInfo: Move type units into the debug_types...
2013-12-13 David BlaikieDebugInfo: Move type units into the debug_types section...
2013-12-11 David BlaikieRevert "DebugInfo: Move type units into the debug_types...
2013-12-11 David BlaikieDebugInfo: Move type units into the debug_types section...
2013-12-11 David BlaikieDwarfUnit: LLVM_OVERRIDE and constify some functions
2013-12-09 Eric ChristopherRename CompileUnit->DwarfCompileUnit and TypeUnit-...
2013-12-09 Eric ChristopherRename Unit->DwarfUnit to match the file name and make...
2013-12-06 David BlaikieDebugInfo: Include the section and start-of-section...
2013-12-05 Eric ChristopherRename DwarfUnits to DwarfFile to help avoid some namin...
2013-12-05 Eric ChristopherFix comment.
2013-12-04 David BlaikieDwarfUnit: Correct comment by generalizing over all...
2013-12-04 Eric ChristopherUse move and stack allocation for RangeSpanLists. As...
2013-12-04 David BlaikieDebugInfo: Remove unused start/end labels for the debug...
2013-12-03 Eric ChristopherMake ranges and range lists be a discrete entity that...
2013-12-02 David BlaikieDebugInfo: Rename generic unit references to "TheU...
2013-12-02 David BlaikieDebugInfo: Rename DwarfCompileUnit.* to DwarfUnit....