Revert "This reapplies r207130 with an additional testcase+and a missing check for"
[opencl/llvm.git] / lib / CodeGen / SelectionDAG / InstrEmitter.cpp
2014-04-25 Adrian PrantlRevert "This reapplies r207130 with an additional testc...
2014-04-25 Adrian PrantlThis reapplies r207130 with an additional testcase...
2014-04-25 Adrian PrantlRevert "Debug info for optimized code: Support variable...
2014-04-24 Adrian PrantlDebug info for optimized code: Support variables that...
2014-04-22 Chandler Carruth[Modules] Remove potential ODR violations by sinking...
2014-04-14 Craig Topper[C++11] More 'nullptr' conversion. In some cases just...
2014-04-11 Jim Grosbach[c++11] Range'ify use list loops in InstrEmitter.
2014-04-04 Craig TopperMake consistent use of MCPhysReg instead of uint16_t...
2014-03-05 Andrew TrickMake stackmap machineinstrs clobber the scratch regs...
2014-01-14 Jakob Stoklund OlesenAlways let value types influence register classes.
2013-11-19 Andrew TrickFix patchpoint comments.
2013-11-09 Juergen Ributzka[Stackmap] Materialize the jump address within the...
2013-11-08 Juergen Ributzka[Stackmap] Add AnyReg calling convention support for...
2013-07-09 Adrian PrantlReapply an improved version of r180816/180817.
2013-06-16 David BlaikieDebug Info: Simplify Frame Index handling in DBG_VALUE...
2013-04-30 Adrian PrantlTemporarily revert "Change the informal convention...
2013-04-30 Adrian PrantlChange the informal convention of DBG_VALUE so that...
2013-01-02 Chandler CarruthMove all of the header files which are involved in...
2012-12-20 Jakob Stoklund OlesenUse MachineInstrBuilder in InstrEmitter.
2012-12-13 Patrik HagglundChange TargetLowering::getRegClassFor to take an MVT...
2012-12-11 Patrik HagglundRevert EVT->MVT changes, r169836-169851, due to buildbo...
2012-12-11 Patrik HagglundChange TargetLowering::getRegClassFor to take an MVT...
2012-12-03 Chandler CarruthUse the new script to sort the includes of every file...
2012-10-30 Chad Rosier[inline asm] Get the mayLoad/mayStore directly from...
2012-10-30 Chad Rosier[inline asm] Implement mayLoad and mayStore for inline...
2012-10-08 Micah VillmowMove TargetData to DataLayout.
2012-09-12 Michael LiaoFix PR11985
2012-09-12 Owen AndersonRemove an overly-aggressive assertion. The code follow...
2012-09-06 Nadav RotemAdd a new optimization pass: Stack Coloring, that merge...
2012-08-31 Jakob Stoklund OlesenAdd MachineInstr::tieOperands, remove setIsTied().
2012-08-31 Jakob Stoklund OlesenDon't enforce ordered inline asm operands.
2012-08-29 Jakob Stoklund OlesenVerify the order of tied operands in inline asm.
2012-08-29 Jakob Stoklund OlesenSet the isTied flags when building INLINEASM MachineInstrs.
2012-08-24 Jakob Stoklund OlesenAvoid including explicit uses when counting SDNode...
2012-08-07 Jakob Stoklund OlesenAdd SelectionDAG::getTargetIndex.
2012-07-11 Evan ChengInstrEmitter::EmitSubregNode() optimize extract_subreg...
2012-07-04 Jakob Stoklund OlesenAllow trailing physreg RegisterSDNode operands on non...
2012-06-29 Jakob Stoklund OlesenClear kill flags in InstrEmitter::EmitSubregNode().
2012-05-07 Jakob Stoklund OlesenAdd an MF argument to TRI::getPointerRegClass() and...
2012-05-03 Andrew TrickAdded TargetRegisterInfo::getAllocatableClass.
2012-02-24 Hal FinkelDon't crash when a glue node contains an internal CopyToReg
2012-02-03 Jakob Stoklund OlesenHandle all live physreg defs in the same place.
2012-01-20 David BlaikieMore dead code removal (using -Wunreachable-code)
2012-01-18 Jakob Stoklund OlesenAdd a RegisterMaskSDNode class.
2012-01-18 Pete CooperFix ISD::REG_SEQUENCE to accept physical registers...
2011-12-07 Evan ChengAdd bundle aware API for querying instruction propertie...
2011-10-05 Jakob Stoklund OlesenSimplify EXTRACT_SUBREG emission.
2011-10-05 Jakob Stoklund OlesenSimplify INSERT_SUBREG emission.
2011-09-30 Jakob Stoklund OlesenMove getCommonSubClass() into TRI.
2011-09-22 Jakob Stoklund OlesenConstrain register classes instead of emitting copies.
2011-09-21 Andrew TrickLower ARM adds/subs to add/sub after adding optional...
2011-09-20 Andrew TrickRestore hasPostISelHook tblgen flag.
2011-09-20 Andrew TrickARM isel bug fix for adds/subs operands.
2011-09-20 Andrew Trickwhitespace
2011-08-30 Evan ChengFollow up to r138791.
2011-07-18 Chris Lattnerland David Blaikie's patch to de-constify Type, with...
2011-06-28 Evan Cheng- Rename TargetInstrDesc, TargetOperandInfo to MCInstrD...
2011-06-27 Evan ChengMore refactoring. Move getRegClass from TargetOperandIn...
2011-06-27 Jakob Stoklund OlesenDistinguish early clobber output operands from clobbere...
2011-06-24 Devang PatelHandle debug info for i128 constants.
2011-06-16 Jakob Stoklund OlesenDon't use register classes larger than TLI->getRegClass...
2011-06-16 Owen AndersonChange the REG_SEQUENCE SDNode to take an explict regis...
2011-06-02 Jakob Stoklund OlesenUse TRI::has{Sub,Super}ClassEq() where possible.
2011-01-10 Jakob Stoklund OlesenSimplify a bunch of isVirtualRegister() and isPhysicalR...
2011-01-07 Evan ChengDo not model all INLINEASM instructions as having unmod...
2011-01-05 Evan ChengOptimize:
2010-12-23 Chris Lattnerflags -> glue for selectiondag
2010-12-23 Jeffrey YasskinChange all self assignments X=X to (void)X, so that...
2010-12-21 Chris Lattnerrename MVT::Flag to MVT::Glue. "Flag" is a terrible...
2010-12-17 Bob WilsonFix crash compiling a QQQQ REG_SEQUENCE for a Neon...
2010-12-08 Eric ChristopherReword comment slightly.
2010-11-16 Dan GohmanSplit pseudo-instruction expansion into a separate...
2010-08-30 Bill WendlingRevert r112461. It was failing on PPC...
2010-08-30 Bill WendlingWhen adding a register, we should mark it as "def"...
2010-07-10 Jakob Stoklund OlesenEmit COPY instructions instead of using copyRegToReg...
2010-07-10 Dan GohmanInsert IMPLICIT_DEF instructions at the current insert...
2010-07-10 Dan GohmanReapply bottom-up fast-isel, with several fixes for...
2010-07-09 Bob Wilson--- Reverse-merging r107947 into '.':
2010-07-09 Dan GohmanRe-apply bottom-up fast-isel, with fixes. Be very caref...
2010-07-08 Jakob Stoklund OlesenConvert EXTRACT_SUBREG to COPY when emitting machine...
2010-07-08 Dan GohmanRevert 107840 107839 107813 107804 107800 107797 107791.
2010-07-07 Dan GohmanNot all custom inserters create new basic blocks. If...
2010-07-07 Devang PatelUpdate comment.
2010-07-06 Dan GohmanReapply r107655 with fixes; insert the pseudo instructi...
2010-07-02 Dale JohannesenPropagate the AlignStack bit in InlineAsm's to the
2010-06-29 Rafael EspindolaAdd a VT argument to getMinimalPhysRegClass and replace...
2010-06-18 Dan GohmanTeach regular and fast isel to set dead flags on unused...
2010-06-09 Jakob Stoklund OlesenMark physregs defined by inline asm as implicit.
2010-06-09 Jakob Stoklund OlesenAdd argument name comments.
2010-05-18 Evan ChengContinuously refine the register class of REG_SEQUENCE...
2010-05-18 Evan ChengFix PR7162: Use source register classes and sub-indices...
2010-05-14 Dan GohmanDon't set kill flags for instructions which the schedul...
2010-05-11 Dan GohmanDon't set kill flags on uses of CopyFromReg nodes....
2010-05-10 Evan ChengIndentation.
2010-05-07 Dan GohmanSDDbgValues are apparently not being legalized. Fix...
2010-05-06 Dan GohmanAdd a DebugLoc argument to TargetInstrInfo::copyRegToRe...
2010-05-04 Evan ChengTeach scheduler about REG_SEQUENCE.
2010-05-04 Dan GohmanRe-enable isel kill flags, now that the local allocator...
2010-05-01 Dan GohmanRe-disable kill flags, as there is more trouble.
2010-05-01 Dan GohmanRe-enable kill flags from SelectionDAGISel, with a...
next