]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/CodeGen/SelectionDAG/SelectionDAGISel.cpp
constify the getters in SDNodeDbgValue.
[opencl/llvm.git] / lib / CodeGen / SelectionDAG / SelectionDAGISel.cpp
2014-10-09 Eric ChristopherRemove uses of the TargetMachine from FunctionLoweringInfo
2014-10-08 Eric ChristopherGrab the TargetRegisterInfo off of the subtarget from the
2014-10-08 Eric ChristopherCache TargetLowering on SelectionDAGISel and update...
2014-10-08 Eric ChristopherCache SelectionDAGISel TargetInstrInfo lookups on the...
2014-10-08 Eric ChristopherReset the target options and optimization level as...
2014-10-08 Eric ChristopherHave the selection dag grab TargetLowering off of the...
2014-10-03 Adam Nemet[ISel] Keep matching state consistent when folding...
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-09-26 Eric ChristopherMove resetTargetOptions from taking a MachineFunction...
2014-09-03 Juergen Ributzka[FastISel] Rename public visible FastISel functions...
2014-09-03 Eric ChristopherRemove resetSubtargetFeatures as it is unused.
2014-08-21 Craig TopperRepace SmallPtrSet with SmallPtrSetImpl in function...
2014-08-18 Craig TopperRevert "Repace SmallPtrSet with SmallPtrSetImpl in...
2014-08-17 Craig TopperRepace SmallPtrSet with SmallPtrSetImpl in function...
2014-08-04 Eric ChristopherRemove the TargetMachine forwards for TargetSubtargetIn...
2014-08-02 Justin BognerCodeGen: Remove commented out code
2014-07-21 Duncan P. N. Exon... Revert "[C++11] Add predecessors(BasicBlock *) / succes...
2014-07-20 Manuel Jacob[C++11] Add predecessors(BasicBlock *) / successors...
2014-06-26 Alp TokerRevert "Introduce a string_ostream string builder facilty"
2014-06-26 Alp TokerIntroduce a string_ostream string builder facilty
2014-06-10 Juergen Ributzka[FastISel] Collect statistics about failing intrinsic...
2014-05-14 Jay FoadRename ComputeMaskedBits to computeKnownBits. "Masked...
2014-05-11 Hal FinkelPass the value type to TLI::getRegisterByName
2014-05-06 Renato GolinImplememting named register intrinsics
2014-04-30 Alexey SamsonovConvert more loops to range-based equivalents
2014-04-27 Craig TopperConvert SelectionDAGISel::MorphNode to use ArrayRef.
2014-04-27 Craig TopperConvert SelectionDAG::MorphNodeTo to use ArrayRef.
2014-04-26 Craig TopperConvert SelectionDAG::getNode methods to use ArrayRef...
2014-04-22 Chandler Carruth[Modules] Remove potential ODR violations by sinking...
2014-04-16 Craig TopperConvert SelectionDAG::getVTList to use ArrayRef
2014-04-14 Craig Topper[C++11] More 'nullptr' conversion. In some cases just...
2014-03-13 Owen AndersonPhase 1 of refactoring the MachineRegisterInfo iterator...
2014-03-08 Craig Topper[C++11] Add 'override' keyword to virtual methods that...
2014-03-06 Chandler Carruth[Layering] Move DebugInfo.h into the IR library where...
2014-03-05 Hans WennborgCheck for dynamic allocas and inline asm that clobbers...
2014-03-02 Benjamin Kramer[C++11] Replace llvm::next and llvm::prior with std...
2014-02-05 Craig TopperAdd CheckChildInteger to ISelMatcher operations. Remove...
2014-01-28 Juergen Ributzka[TLI] Add a new hook to TargetLowering to query the...
2014-01-13 Andrew TrickHide the pre-RA-sched= option.
2013-12-17 Jim GrosbachAdd a machine code print in DEBUG() following instructi...
2013-12-10 Reid KlecknerReland "Fix miscompile of MS inline assembly with stack...
2013-12-10 Reid KlecknerRevert "Fix miscompile of MS inline assembly with stack...
2013-12-10 Reid KlecknerFix miscompile of MS inline assembly with stack realignment
2013-11-25 Daniel SandersFixed tryFoldToZero() for vector types that need expansion.
2013-11-22 Paul RobinsonTeach ISel not to optimize 'optnone' functions (revised).
2013-11-21 NAKAMURA TakumiRevert r195317 (and r195333), "Teach ISel not to optimi...
2013-11-21 Paul RobinsonTeach ISel not to optimize 'optnone' functions.
2013-11-20 Jack Carterlong line correction
2013-11-19 Juergen Ributzka[DAG] Refactor vector splitting code in SelectionDAG...
2013-11-15 Daniel SandersFix illegal DAG produced by SelectionDAG::getConstant...
2013-10-06 Craig TopperFix some assert messages to say the correct opcode...
2013-10-05 Craig TopperAdd OPC_CheckChildSame0-3 to the DAG isel matcher....
2013-10-05 Adrian PrantlDebug info: Don't crash in SelectionDAGISel when a...
2013-10-04 Craig TopperRevert r191940 to see if it fixes the build bots.
2013-10-04 Craig TopperAdd OPC_CheckChildSame0-3 to the DAG isel matcher....
2013-10-01 Rafael EspindolaRemove several unused variables.
2013-09-26 Andrew TrickAdded temp flag -misched-bench for staging in default...
2013-09-26 Andrew Trickwhitespace
2013-09-24 Michael Gottesman[stackprotector] Allow for copies from vreg -> vreg...
2013-09-22 Tim NorthoverISelDAG: spot chain cycles involving MachineNodes
2013-09-16 Adrian PrantlDebug info: Fix PR16736 and rdar://problem/14990587.
2013-08-22 Michael Gottesman[stackprotector] When finding the split point to splice...
2013-08-20 Michael GottesmanRemove unused variables that crept in.
2013-08-20 Michael GottesmanTeach selectiondag how to handle the stackprotectorchec...
2013-08-16 Jim GrosbachARM: Fix more fast-isel verifier failures.
2013-08-15 Craig TopperReplace getValueType().getSimpleVT() with getSimpleValu...
2013-07-27 Nick LewyckyReimplement isPotentiallyReachable to make nocapture...
2013-07-09 Adrian PrantlReapply an improved version of r180816/180817.
2013-07-04 Jakob Stoklund OlesenSimplify landing pad lowering.
2013-07-04 Jakob Stoklund OlesenRevert r185595-185596 which broke buildbots.
2013-07-03 Jakob Stoklund OlesenSimplify landing pad lowering.
2013-07-03 Craig TopperUse SmallVectorImpl::const_iterator instead of SmallVec...
2013-06-19 Bill WendlingAccess the TargetLoweringInfo from the TargetMachine...
2013-06-16 David BlaikieDebug Info: Simplify Frame Index handling in DBG_VALUE...
2013-06-06 Bill WendlingCache the TargetLowering info object as a pointer.
2013-06-06 Bill WendlingDon't cache the TargetLoweringInfo object inside of...
2013-05-25 Andrew TrickTrack IR ordering of SelectionDAG nodes 3/4.
2013-05-25 Andrew TrickTrack IR ordering of SelectionDAG nodes 2/4.
2013-04-30 Adrian PrantlTemporarily revert "Change the informal convention...
2013-04-30 Adrian PrantlChange the informal convention of DBG_VALUE so that...
2013-04-19 Eli BenderskyMove TryToFoldFastISelLoad to FastISel, where it belong...
2013-04-19 Michael LiaoArrayRefize getMachineNode(). No functionality change.
2013-04-19 Eli BenderskyUse dbgs() consistently for -debug printouts
2013-04-19 Eli BenderskyAdd some more stats for fast isel vs. SelectionDAG...
2013-03-20 Justin HolewinskiMove SDNode order propagation to SDNodeOrdering, which...
2013-03-20 Justin HolewinskiPropagate DAG node ordering during type legalization...
2013-03-13 Bill WendlingReset some of the target options which affect code...
2013-03-08 Jan Wen VoungDisable statistics on Release builds and move tests...
2013-03-07 Benjamin KramerArrayRefize some code. No functionality change.
2013-03-07 Nadav RotemNo need to go through int64 and APInt when generating...
2013-03-01 Eli BenderskyRemove duplicate line and move another closer to its...
2013-02-28 Eli BenderskyA small refactoring + adding comments.
2013-02-27 Eric ChristopherRemove unnecessary cast to void.
2013-02-27 Nadav RotemSilence the unused variable warning.
2013-02-27 Nadav RotemThe FastISEL should be fast. But when we record statist...
2013-02-25 Chad RosierFix wording.
2013-02-25 Chad Rosier[fast-isel] Add X86FastIsel::FastLowerArguments to...
2013-02-18 Chad Rosier[ms-inline asm] Remove a redundant call to the setHasMS...
next