]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/LTO
Revert "Revert "Revert "PR20038: DebugInfo: Inlined call sites where the caller has...
[opencl/llvm.git] / lib / LTO /
2014-06-26 Alp TokerRevert "Introduce a string_ostream string builder facilty"
2014-06-26 Alp TokerIntroduce a string_ostream string builder facilty
2014-06-25 Rafael EspindolaMerge the used symbol scanning of MCObjectStreamer...
2014-06-25 Rafael EspindolaMove expression visitation logic up to MCStreamer.
2014-06-25 Rafael EspindolaMove some trivial methods up to MCStreamer.
2014-06-25 Rafael EspindolaSimplify the handling of .cfi_endproc.
2014-06-24 Rafael EspindolaSimplify EmitLabel.
2014-06-24 Rafael EspindolaPrint a=b as an assignment.
2014-06-19 Rafael EspindolaUse the assignment operator.
2014-06-19 Rafael EspindolaSet missing options in LTOCodeGenerator::setTargetOptions.
2014-06-13 Rafael EspindolaRemove 'using std::errro_code' from lib.
2014-06-12 Rafael EspindolaDon't use 'using std::error_code' in include/llvm.
2014-06-12 Rafael EspindolaRemove system_error.h.
2014-06-07 Alp TokerBuild fix: remove initializeJumpInstrTablesPass() call...
2014-06-05 Tom RoederAdd a new attribute called 'jumptable' that creates...
2014-06-03 Rafael EspindolaAllow alias to point to an arbitrary ConstantExpr.
2014-05-24 Tim NorthoverAArch64/ARM64: move ARM64 into AArch64's place
2014-05-23 Rafael EspindolaAliases are always definition, delete dead code.
2014-05-16 Rafael EspindolaDelete getAliasedGlobal.
2014-05-12 Rafael EspindolaMove EmitDwarfAdvanceLineAddr and EmitDwarfAdvanceFrame...
2014-05-07 Duncan P. N. Exon... LTO: Check local linkage first
2014-05-05 Rafael EspindolaUse a range loop.
2014-05-05 Rafael EspindolaTrivial simplification. No functionality change.
2014-05-03 Rafael EspindolaRename member variable to try to fix the bots.
2014-04-25 Tom RoederAdd an -mattr option to the gold plugin to support...
2014-04-23 Evgeniy StepanovCreate MCTargetOptions.
2014-04-22 Kevin EnderbyFix the assembler to print a better relocatable express...
2014-04-19 Alp TokerRemove some empty statements
2014-04-15 Duncan P. N. Exon... verify-di: Implement DebugInfoVerifier
2014-04-15 Craig Topper[C++11] More 'nullptr' conversion. In some cases just...
2014-04-14 James MolloyTeach llvm-lto to respect the given RelocModel.
2014-04-10 Reid KlecknerMove the segmented stack switch to a function attribute
2014-04-02 Duncan P. N. Exon... Revert "Reapply "LTO: add API to set strategy for ...
2014-03-31 Tom RoederThis patch fixes LTO's RecordStreamer so that it record...
2014-03-29 Tim NorthoverARM64: initial backend import
2014-03-13 Rafael EspindolaRemove the linker_private and linker_private_weak linkages.
2014-03-08 Craig Topper[C++11] Add 'override' keyword to virtual methods that...
2014-03-06 Ahmed CharlesReplace OwningPtr<T> with std::unique_ptr<T>.
2014-03-06 Chandler Carruth[Layering] Sink Linker.h into a Linker subdirectory...
2014-03-05 Ahmed Charles[C++11] Replace OwningPtr::take() with OwningPtr::relea...
2014-03-04 Chandler Carruth[cleanup] Re-sort all the includes with utils/sort_incl...
2014-02-28 Tobias GrosserAdd 'remark' diagnostic type in LLVM
2014-02-25 Rafael EspindolaUse DataLayout from the module when easily available.
2014-02-25 Rafael EspindolaMake DataLayout a plain object, not a pass.
2014-02-24 Rafael EspindolaReplace the F_Binary flag with a F_Text one.
2014-02-19 Rafael Espindolamove getNameWithPrefix and getSymbol to TargetMachine.
2014-02-19 Rafael EspindolaAdd back r201608, r201622, r201624 and r201625
2014-02-19 Daniel JasperRevert r201622 and r201608.
2014-02-18 Rafael EspindolaFix PR18743.
2014-02-10 Manman RenLTO API: add lto_module_create_from_memory_with_path.
2014-02-07 Rafael EspindolaDon't internalize linkonce_odr non constant variables.
2014-01-28 David WoodhouseChange MCStreamer EmitInstruction interface to take...
2014-01-26 Rafael EspindolaConstruct the MCStreamer before constructing the MCTarg...
2014-01-24 Rafael EspindolaMost streamers' InitSections just create a text section...
2014-01-24 Rafael EspindolaUse the actual .text section, it is less code than...
2014-01-23 Rafael EspindolaInitToTextSection is redundant with InitSections. Remov...
2014-01-23 Juergen RibutzkaAdd target analysis passes to the codegen pipeline...
2014-01-22 Rafael EspindolaProvide a dummy section to fix a crash with inline...
2014-01-21 Yunzhong GaoAdding new LTO APIs to parse metadata nodes and extract...
2014-01-15 Quentin Colombet[LTO] Add a hook to map LLVM diagnostics into the clien...
2014-01-14 Rafael EspindolaReturn an error_code from materializeAllPermanently.
2014-01-14 Duncan P. N. Exon... Reapply "LTO: add API to set strategy for -internalize"
2014-01-14 NAKAMURA TakumiRevert r199191, "LTO: add API to set strategy for ...
2014-01-14 Duncan P. N. Exon... LTO: add API to set strategy for -internalize
2014-01-13 Rafael EspindolaUpdate getLazyBitcodeModule to use ErrorOr for error...
2014-01-13 Chandler Carruth[cleanup] Move the Dominators.h and Verifier.h headers...
2014-01-10 Duncan P. N. Exon... LTO: whitespace changes
2014-01-07 Rafael EspindolaMove the llvm mangler to lib/IR.
2014-01-07 Chandler CarruthRe-sort all of the includes with ./utils/sort_includes...
2014-01-03 Rafael EspindolaMake the llvm mangler depend only on DataLayout.
2013-12-12 Yi JiangAdd TargetLibraryInfo in LTO passes builder
2013-12-11 NAKAMURA TakumiPrune redundant dependencies in LLVMBuild.txt.
2013-12-10 NAKAMURA TakumiAdd proper dependencies to LLVMBuild.txt in llvm/lib.
2013-12-10 NAKAMURA TakumiWhitespaces.
2013-12-09 Rafael EspindolaUse a more direct check for finding out the file type.
2013-12-05 Rafael EspindolaRemove the isImplicitlyPrivate argument of getNameWithP...
2013-11-16 Duncan P. N. Exon... Use array_pod_sort instead of std::sort
2013-11-12 Justin BognerProtect user-supplied runtime library functions in LTO
2013-11-01 Rafael EspindolaRemove linkonce_odr_auto_hide.
2013-10-31 Rafael EspindolaUse LTO_SYMBOL_SCOPE_DEFAULT_CAN_BE_HIDDEN instead...
2013-10-29 Rafael EspindolaMove getSymbol to TargetLoweringObjectFile.
2013-10-16 Bill WendlingAdd a 'deleteModule' method to the Linker class.
2013-10-08 Rafael EspindolaAdd a MCTargetStreamer interface.
2013-10-05 Rafael EspindolaRemove some really nasty uses of hasRawTextSupport.
2013-10-03 Rafael EspindolaOptimize linkonce_odr unnamed_addr functions during...
2013-10-03 Tom RoederTest commit. Fixed a copy-paste error in the Makefile...
2013-10-02 Rafael EspindolaFix option parsing in the gold plugin.
2013-09-30 Rafael EspindolaMove command line options to the users of libLTO. Fixes...
2013-09-24 Peter CollingbourneMove LTO support library to a component, allowing it...