]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib/Object
- Added some stub implementations for C6000 target transform info oracles
[opencl/llvm.git] / lib / Object /
2015-01-16 Kevin EnderbyFix the Archive::Child::getRawSize() method used by...
2015-01-16 Kevin EnderbyThis should fix the build bot clang-cmake-armv7-a15...
2015-01-15 Filipe CabecinhasFix edge case when Start overflowed in 32 bit mode
2015-01-15 Kevin EnderbyAdd the option, -archive-headers, used with -macho...
2015-01-15 Filipe CabecinhasReport fatal errors instead of segfaulting/asserting...
2015-01-15 Lang Hames[Object] Add SF_Exported flag. This flag will be set...
2015-01-14 Chandler Carruth[cleanup] Re-sort all the #include lines in LLVM using
2015-01-06 Filipe CabecinhasDon't loop endlessly for MachO files with 0 ncmds
2014-12-23 Kevin EnderbyAdd printing the LC_THREAD load commands with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_ROUTINES load commands with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_CLIENT load command with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_LIBRARY load command with llvm...
2014-12-19 Juergen Ributzka[Object] Don't crash on empty export lists.
2014-12-18 Kevin EnderbyAdd printing the LC_SUB_UMBRELLA load command with...
2014-12-18 Kevin EnderbyAdd printing the LC_SUB_FRAMEWORK load command with...
2014-12-18 Kevin EnderbyAdd printing the LC_LINKER_OPTION load command with...
2014-12-17 Kevin EnderbyAdd printing the LC_ENCRYPTION_INFO_64 load command...
2014-12-16 Kevin EnderbyAdd printing the LC_ENCRYPTION_INFO load command with...
2014-12-16 Rafael EspindolaStart adding thin archive support.
2014-12-15 Michael IlsemanSilence more static analyzer warnings.
2014-12-10 Rafael EspindolaMove three methods only used by MCJIT to MCJIT.
2014-12-09 Rafael EspindolaReturn ErrorOr<std::unique_ptr<Archive>> form getAsArchive.
2014-12-09 Rafael EspindolaRename createIRObjectFile to just create.
2014-12-09 Rafael EspindolaMove method out of line to make buildbot happy.
2014-12-09 Rafael EspindolaDon't lookup an object symbol name in the module.
2014-12-04 Jean-Daniel DupasAdd mach-o LC_RPATH support to llvm-objdump
2014-12-02 Will NewtonAdd ARM relocations to ELFYAML
2014-11-26 Rui UeyamaObject/COFF: Fix off-by-one error for object having...
2014-11-25 David MajnemerCOFF: Add back an assertion that is superseded by r222124
2014-11-21 Tim NorthoverRemove duplication of relocation names in lib/Object...
2014-11-21 Tim NorthoverRemove duplication of relocation names in lib/Object...
2014-11-19 Rui Ueyamallvm-readobj: fix off-by-one error in COFFDumper
2014-11-19 Rui Ueyamallvm-readobj: teach it how to dump COFF base relocation...
2014-11-18 Michael J. SpencerSupport ELF files of unknown type.
2014-11-17 David MajnemerObject, COFF: Tighten the object file parser
2014-11-14 David Majnemerobj2yaml, yaml2obj: Add support for COFF executables
2014-11-13 Rui UeyamaUn-break the big-endian buildbots
2014-11-13 David MajnemerObject, Mach-O: Refactor and clean code up
2014-11-13 David MajnemerObject, COFF: Refactor code to get relocation iterators
2014-11-13 David MajnemerObject, COFF: Increase code reuse
2014-11-13 David MajnemerObject, COFF: getRelocationSymbol shouldn't assert
2014-11-13 David MajnemerObject, COFF: Cleanup some code in getSectionName
2014-11-13 David MajnemerObject, COFF: Fix some theoretical bugs
2014-11-13 Rui Ueyamallvm-readobj: Print out address table when dumping...
2014-11-12 Nick KledzikObject, support both mach-o archive t.o.c file names
2014-11-10 Chad Rosier[yaml2obj] Support AArch64 relocations.
2014-11-06 Simon Atanasyan[ELF][yaml2obj] Handle additional MIPS specific st_othe...
2014-11-06 David MajnemerObject, COFF: Don't consider AuxFunctionDefinition...
2014-11-06 David MajnemerObject, COFF: Infer symbol sizes from adjacent symbols
2014-11-05 David Majnemerllvm-readobj: Add support for dumping the DOS header...
2014-11-04 Simon Atanasyan[yaml2obj] Allow yaml2obj tool to recognize EF_MIPS_NAN...
2014-11-04 Kevin EnderbyRemove the static version of getScatteredRelocationType...
2014-11-04 Kevin EnderbyAdd the code and test cases for 32-bit Intel to llvm...
2014-10-31 David MajnemerObject, COFF: Cleanup symbol type code, improve binutil...
2014-10-27 NAKAMURA TakumiFix unicode chars into ascii in comment lines.
2014-10-24 Rafael EspindolaDon't ever call materializeAllPermanently during LTO.
2014-10-24 Benjamin Kramer[Object] Fix MachO's getUuid to return a pointer into...
2014-10-23 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code for Object...
2014-10-21 Lang Hames[MCJIT] Temporarily revert r220245 - it broke several...
2014-10-20 Lang Hames[MCJIT] Make MCJIT honor symbol visibility settings...
2014-10-20 Alexey SamsonovBe more specific about return type of MachOUniversalBin...
2014-10-18 Nick Kledzik[llvm-objdump] Fix mach-o binding decompression error
2014-10-15 Alexander PotapenkoAdd MachOObjectFile::getUuid()
2014-10-09 David MajnemerObject, COFF: Move the VirtualSize/SizeOfRawData logic...
2014-10-09 David MajnemerObject, COFF: Cap the section contents to min(VirtualSi...
2014-10-09 Rui UeyamaObject: Add range iterators for COFF import/export...
2014-10-08 Rafael EspindolaCorrectly compute the size of common symbols in COFF.
2014-10-08 Rafael EspindolaRemove bogus std::error_code returns form SectionRef.
2014-10-07 Rafael EspindolaDon't check for null after calling COFFObjectFile:...
2014-10-07 Rafael EspindolaOptimize COFFObjectFile::sectionContainsSymbol a bit.
2014-10-03 Rui Ueyamallvm-readobj: print out the fields of the COFF delay...
2014-10-03 Rui Ueyamallvm-readobj: print COFF delay-load import table
2014-10-02 Rui Ueyamallvm-readobj: print COFF imported symbols
2014-10-02 Rui UeyamaThis patch adds a new flag "-coff-imports" to llvm...
2014-09-26 David MajnemerObject: BSS/virtual sections don't have contents
2014-09-19 Chris BienemanConverting object's error_category to a ManagedStatic...
2014-09-18 Peter CollingbourneLTO: introduce object file-based on-disk module format.
2014-09-17 Nick Kledzik[Object] keep trailing '\0' out of StringRef when parsi...
2014-09-17 Nick Kledzik[llvm-objdump] properly use c_str() with format("%s...
2014-09-16 Nick Kledzik[llvm-objdump] for mach-o add -bind, -lazy-bind, and...
2014-09-12 Nick Kledzik[llvm-objdump] support -rebase option for mach-o to...
2014-09-11 Rui UeyamaSupport: Delete {aligned_,}{u,}{little,big}8_t
2014-09-10 David MajnemerAttempt to pacify buildbots.
2014-09-10 David MajnemerObject: Add support for bigobj
2014-09-05 Bjorn SteinbrinkRestore the ability to check if LLVMCreateObjectFile...
2014-09-04 Kevin EnderbyAdds the next bit of support for llvm-objdump’s -privat...
2014-09-03 David Blaikieunique_ptrify IRObjectFile::createIRObjectFile
2014-09-03 David Blaikieunique_ptrify MachOUniversalBinary::create
2014-09-03 Rafael EspindolaPass a && to getLazyBitcodeModule.
2014-09-03 David BlaikieEnsure ErrorOr cannot implicitly invoke explicit ctors...
2014-09-02 Nick KledzikCode review tweaks
2014-08-30 Nick KledzikFix typo and formatting
2014-08-30 Nick KledzikObject/llvm-objdump: allow dumping of mach-o exports...
2014-08-27 Craig TopperSimplify creation of a bunch of ArrayRefs by using...
2014-08-26 Rafael EspindolaPass a std::unique_ptr<MemoryBuffer>& to getLazyBitcode...
2014-08-26 Rafael EspindolaPass a MemoryBufferRef when we can avoid taking ownership.
2014-08-21 David BlaikieExplicitly pass ownership of the MemoryBuffer to AddNew...
2014-08-19 Rafael EspindolaFix a pair of use after free. Should bring the bots...
2014-08-19 Rafael EspindolaDon't own the buffer in object::Binary.
2014-08-18 Kevin EnderbyMake llvm-objdump handle both arm and thumb disassembly...
next