[XCore] Support functions returning more than 4 words.
[opencl/llvm.git] / lib / Target / XCore / XCoreISelLowering.h
2014-02-27 Richard Osborne[XCore] Support functions returning more than 4 words.
2014-02-27 Richard Osborne[XCore] Make LowerCallResult a static function.
2014-02-27 Richard OsborneRevert r202396, r202397.
2014-02-27 Richard Osborne[XCore] Support functions returning more than 4 words.
2014-02-27 Richard Osborne[XCore] Make LowerCallResult a static function.
2014-02-11 Robert Lytton XCore target: Lower ATOMIC_LOAD & ATOMIC_STORE
2014-01-06 Robert LyttonXCore target: Lower EH_RETURN
2014-01-06 Robert LyttonXCore target: Lower FRAME_TO_ARGS_OFFSET
2014-01-06 Robert LyttonXCore target: Lower RETURNADDR
2013-11-12 Robert LyttonAdd XCore support for ATOMIC_FENCE.
2013-10-11 Robert LyttonXCore target: add XCoreTargetLowering::isZExtFree()
2013-06-22 Chad RosierThe getRegForInlineAsmConstraint function should only...
2013-05-25 Andrew TrickTrack IR ordering of SelectionDAG nodes 2/4.
2013-05-04 Richard Osborne[XCore] Make use of the target independent global addre...
2013-05-04 Richard Osborne[XCore] Simplify code that checks for an aligned base...
2013-05-04 Richard Osborne[XCore] Use static relocation model by default.
2013-03-01 Michael LiaoFix PR10475
2013-01-25 Richard OsborneFix order of operands for crc8_l4r
2012-07-19 Bill WendlingRemove tabs.
2012-05-25 Justin HolewinskiChange interface for TargetLowering::LowerCallTo and...
2012-04-04 Rafael EspindolaAlways compute all the bits in ComputeMaskedBits.
2012-03-17 Craig TopperReorder includes in Target backends to following coding...
2012-02-28 Evan ChengRe-commit r151623 with fix. Only issue special no-retur...
2012-02-28 Daniel DunbarRevert r151623 "Some ARM implementaions, e.g. A-series...
2012-02-28 Evan ChengSome ARM implementaions, e.g. A-series, does return...
2011-09-06 Duncan SandsSplit the init.trampoline intrinsic, which currently...
2011-07-18 Chris Lattnerland David Blaikie's patch to de-constify Type, with...
2011-06-29 Eric ChristopherMove XCore from getRegClassForInlineAsmConstraint to
2011-06-08 Eric ChristopherAdd a parameter to CCState so that it can access the...
2011-05-06 Eli FriedmanMake the logic for determining function alignment more...
2011-02-25 Owen AndersonAllow targets to specify a the type of the RHS of a...
2011-02-02 Richard OsborneAdd support for trampolines on the XCore.
2010-07-10 Dan GohmanReapply bottom-up fast-isel, with several fixes for...
2010-07-09 Bob Wilson--- Reverse-merging r107947 into '.':
2010-07-09 Dan GohmanRe-apply bottom-up fast-isel, with fixes. Be very caref...
2010-07-08 Dan GohmanRevert 107840 107839 107813 107804 107800 107797 107791.
2010-07-07 Dan GohmanAdd X86FastISel support for return statements. This...
2010-07-07 Dan GohmanSplit the SDValue out of OutputArg so that SelectionDAG...
2010-07-06 Dan GohmanCanLowerReturn doesn't need a SelectionDAG; it just...
2010-05-01 Dan GohmanGet rid of the EdgeMapping map. Instead, just check...
2010-04-17 Dan GohmanUse const qualifiers with TargetLowering. This eliminat...
2010-04-15 Dan GohmanAdd const qualifiers to CodeGen's use of LLVM IR constr...
2010-03-11 Richard OsborneSwitch XCore over to using inline jump table entries.
2010-03-10 Richard OsborneFix thinko.
2010-03-10 Richard OsbornePrefer LMUL to MACCU as LMUL has no tied operands.
2010-03-10 Richard OsborneCustom lower (S|U)MUL_LOHI -> MACC(S|U)
2010-03-10 Richard OsborneLower add (mul a, b), c into MACCU / MACCS nodes which...
2010-03-09 Richard OsborneAdd DAG combine for ladd / lsub.
2010-02-23 Richard OsborneRemove unused lowering function LowerJumpTable
2010-02-23 Richard OsborneLower BR_JT on the XCore to a jump into a series of...
2010-02-15 Chris Lattnerno need to add the instruction count anymore.
2010-02-02 Evan ChengRevert 95130.
2010-02-02 Evan ChengPass callsite return type to TargetLowering::LowerCall...
2010-01-27 Evan ChengEliminate target hook IsEligibleForTailCallOptimization.
2009-11-18 Richard OsborneAdd XCore support for indirectbr / blockaddress.
2009-11-14 Richard OsborneAdd XCore support for arbitrary-sized aggregate returns.
2009-09-18 Evan ChengEnhance EmitInstrWithCustomInserter() so target can...
2009-09-02 Sandeep PatelRetype from unsigned to CallingConv::ID accordingly...
2009-08-10 Owen AndersonRename MVT to EVT, in preparation for splitting SimpleV...
2009-08-05 Dan GohmanMajor calling convention code refactoring.
2009-07-16 Richard OsborneCombine an unaligned store of unaligned load into a...
2009-07-16 Richard OsborneCustom lower unaligned 32 bit stores and loads into...
2009-07-01 Bill WendlingUpdate comments to make it clear that the function...
2009-06-30 Bill WendlingAdd an "alignment" field to the MachineFunction object...
2009-02-07 Dan GohmanConstify TargetInstrInfo::EmitInstrWithCustomInserter...
2008-12-01 Duncan SandsChange the interface to the type legalization method
2008-11-14 Richard Osborne[XCore] Fix expansion of 64 bit add/sub. Don't custom...
2008-11-07 Richard OsborneAdd XCore backend.