2014-06-27 |
David Blaikie | ArgumentPromotion: Propagate debug locations on calls... |
blob | commitdiff | raw |
2014-04-25 |
Craig Topper | [C++] Use 'nullptr'. Transforms edition. |
blob | commitdiff | raw | diff to current |
2014-04-22 |
Chandler Carruth | [Modules] Fix potential ODR violations by sinking the... |
blob | commitdiff | raw | diff to current |
2014-03-09 |
Chandler Carruth | [C++11] Add range based accessors for the Use-Def chain... |
blob | commitdiff | raw | diff to current |
2014-03-05 |
Craig Topper | [C++11] Add 'override' keyword to virtual methods that... |
blob | commitdiff | raw | diff to current |
2014-03-04 |
Chandler Carruth | [Modules] Move CFG.h to the IR library as it defines... |
blob | commitdiff | raw | diff to current |
2014-03-04 |
Chandler Carruth | [Modules] Move CallSite into the IR library where it... |
blob | commitdiff | raw | diff to current |
2014-01-28 |
Reid Kleckner | Update optimization passes to handle inalloca arguments |
blob | commitdiff | raw | diff to current |
2014-01-23 |
Rafael Espindola | Remove tail marker when changing an argument to an... |
blob | commitdiff | raw | diff to current |
2013-11-26 |
Chandler Carruth | [PM] Split the CallGraph out from the ModulePass which... |
blob | commitdiff | raw | diff to current |
2013-11-15 |
Manman Ren | ArgumentPromotion: correctly transfer TBAA tags and... |
blob | commitdiff | raw | diff to current |
2013-10-31 |
Rafael Espindola | Merge CallGraph and BasicCallGraph. |
blob | commitdiff | raw | diff to current |
2013-07-18 |
Nick Lewycky | Clean up some of this code a tiny bit, no functionality... |
blob | commitdiff | raw | diff to current |
2013-01-27 |
Bill Wendling | Use the AttributeSet instead of AttributeWithIndex. |
blob | commitdiff | raw | diff to current |
2013-01-23 |
Bill Wendling | Remove the last of uses that use the Attribute object... |
blob | commitdiff | raw | diff to current |
2013-01-21 |
Bill Wendling | Have AttributeSet::getRetAttributes() return an Attribu... |
blob | commitdiff | raw | diff to current |
2013-01-21 |
Bill Wendling | Make AttributeSet::getFnAttributes() return an Attribut... |
blob | commitdiff | raw | diff to current |
2013-01-18 |
Bill Wendling | Use AttributeSet accessor methods instead of Attribute... |
blob | commitdiff | raw | diff to current |
2013-01-18 |
Bill Wendling | Push some more methods down to hide the use of the... |
blob | commitdiff | raw | diff to current |
2013-01-07 |
Chandler Carruth | Move CallGraphSCCPass.h into the Analysis tree; that... |
blob | commitdiff | raw | diff to current |
2013-01-02 |
Chandler Carruth | Move all of the header files which are involved in... |
blob | commitdiff | raw | diff to current |
2012-12-30 |
Bill Wendling | Remove Function::getParamAttributes and use the Attribu... |
blob | commitdiff | raw | diff to current |
2012-12-19 |
Bill Wendling | Rename the 'Attributes' class to 'Attribute'. It's... |
blob | commitdiff | raw | diff to current |
2012-12-07 |
Bill Wendling | s/AttrListPtr/AttributeSet/g to better label what this... |
blob | commitdiff | raw | diff to current |
2012-12-03 |
Chandler Carruth | Use the new script to sort the includes of every file... |
blob | commitdiff | raw | diff to current |
2012-11-20 |
Bill Wendling | Make the AttrListPtr object a part of the LLVMContext. |
blob | commitdiff | raw | diff to current |
2012-10-15 |
Bill Wendling | Add an enum for the return and function indexes into... |
blob | commitdiff | raw | diff to current |
2012-10-14 |
Bill Wendling | Remove operator cast method in favor of querying with... |
blob | commitdiff | raw | diff to current |
2012-10-09 |
Bill Wendling | Create enums for the different attributes. |
blob | commitdiff | raw | diff to current |
2012-10-04 |
Bill Wendling | Use method to query for attributes. |
blob | commitdiff | raw | diff to current |
2012-09-30 |
Benjamin Kramer | ArgumentPromotion: Remove ancient workaround for a... |
blob | commitdiff | raw | diff to current |
2012-07-19 |
Benjamin Kramer | Replace some explicit compare loops with std::equal. |
blob | commitdiff | raw | diff to current |
2012-05-28 |
Chris Lattner | switch AttrListPtr::get to take an ArrayRef, simplifyin... |
blob | commitdiff | raw | diff to current |
2011-08-15 |
Eli Friedman | Update inter-procedural optimizations for atomic load... |
blob | commitdiff | raw | diff to current |
2011-07-25 |
Jay Foad | Convert GetElementPtrInst to use ArrayRef. |
blob | commitdiff | raw | diff to current |
2011-07-18 |
Chris Lattner | land David Blaikie's patch to de-constify Type, with... |
blob | commitdiff | raw | diff to current |
2011-07-15 |
Jay Foad | Convert CallInst and InvokeInst APIs to use ArrayRef. |
blob | commitdiff | raw | diff to current |
2011-07-12 |
Jay Foad | Second attempt at de-constifying LLVM Types in Function... |
blob | commitdiff | raw | diff to current |
2011-07-12 |
Bill Wendling | Revert r134893 and r134888 (and related patches in... |
blob | commitdiff | raw | diff to current |
2011-07-11 |
Jay Foad | De-constify Types in FunctionType::get(). |
blob | commitdiff | raw | diff to current |
2011-04-15 |
Chris Lattner | Fix a ton of comment typos found by codespell. Patch by |
blob | commitdiff | raw | diff to current |
2011-01-16 |
Chris Lattner | fix PR8932, a case where arg promotion could infinitely... |
blob | commitdiff | raw | diff to current |
2010-11-11 |
Dan Gohman | Add helper functions for computing the Location of... |
blob | commitdiff | raw | diff to current |
2010-11-11 |
Dan Gohman | Factor out Instruction::isSafeToSpeculativelyExecute... |
blob | commitdiff | raw | diff to current |
2010-11-11 |
Dan Gohman | TBAA-enable ArgumentPromotion. |
blob | commitdiff | raw | diff to current |
2010-10-19 |
Dan Gohman | Reapply r116831 and r116839, converting AliasAnalysis... |
blob | commitdiff | raw | diff to current |
2010-10-19 |
Owen Anderson | Get rid of static constructors for pass registration... |
blob | commitdiff | raw | diff to current |
2010-10-13 |
Owen Anderson | CallGraphSCC passes implicity require CallGraph analysis. |
blob | commitdiff | raw | diff to current |
2010-10-12 |
Owen Anderson | Begin adding static dependence information to passes... |
blob | commitdiff | raw | diff to current |
2010-10-07 |
Owen Anderson | Now with fewer extraneous semicolons! |
blob | commitdiff | raw | diff to current |
2010-08-06 |
Owen Anderson | Reapply r110396, with fixes to appease the Linux buildb... |
blob | commitdiff | raw | diff to current |
2010-08-06 |
Owen Anderson | Revert r110396 to fix buildbots. |
blob | commitdiff | raw | diff to current |
2010-08-05 |
Owen Anderson | Don't use PassInfo* as a type identifier for passes... |
blob | commitdiff | raw | diff to current |
2010-07-28 |
Gabor Greif | simplify by using CallSite constructors; virtually... |
blob | commitdiff | raw | diff to current |
2010-07-21 |
Owen Anderson | Fix batch of converting RegisterPass<> to INTIALIZE_PASS(). |
blob | commitdiff | raw | diff to current |
2010-07-12 |
Gabor Greif | cache result of operator* |
blob | commitdiff | raw | diff to current |
2010-04-20 |
Chris Lattner | Fix rdar://7879828 - crash in CallGraph, a self host... |
blob | commitdiff | raw | diff to current |
2010-04-16 |
Chris Lattner | introduce a new CallGraphSCC class, and pass it around |
blob | commitdiff | raw | diff to current |
2010-03-27 |
Eric Christopher | When we promote a load of an argument make sure to... |
blob | commitdiff | raw | diff to current |
2010-03-23 |
Gabor Greif | add assert in argpromotion, which cannot trigger |
blob | commitdiff | raw | diff to current |
2010-02-25 |
Nick Lewycky | Correct whitespace. |
blob | commitdiff | raw | diff to current |
2010-02-16 |
Duncan Sands | There are two ways of checking for a given type, for... |
blob | commitdiff | raw | diff to current |
2010-02-10 |
Dan Gohman | Fix "the the" and similar typos. |
blob | commitdiff | raw | diff to current |
2010-01-05 |
David Greene | Change errs() to dbgs(). |
blob | commitdiff | raw | diff to current |
2009-10-25 |
Nick Lewycky | Remove includes of Support/Compiler.h that are no longe... |
blob | commitdiff | raw | diff to current |
2009-10-25 |
Nick Lewycky | Remove VISIBILITY_HIDDEN from class/struct found inside... |
blob | commitdiff | raw | diff to current |
2009-09-15 |
Chris Lattner | add a new CallGraphNode::replaceCallEdge method and... |
blob | commitdiff | raw | diff to current |
2009-09-01 |
Chris Lattner | remove CallGraphNode::replaceCallSite, it is redundant... |
blob | commitdiff | raw | diff to current |
2009-08-31 |
Chris Lattner | add -debug output |
blob | commitdiff | raw | diff to current |
2009-08-31 |
Chris Lattner | Fix some nasty callgraph dangling pointer problems in |
blob | commitdiff | raw | diff to current |
2009-08-24 |
Chris Lattner | prune the #includes in raw_ostream.h by moving a |
blob | commitdiff | raw | diff to current |
2009-08-14 |
Dan Gohman | Make TargetData optional in GlobalOpt and ArgumentPromo... |
blob | commitdiff | raw | diff to current |
2009-08-13 |
Owen Anderson | Push LLVMContexts through the IntegerType APIs. |
blob | commitdiff | raw | diff to current |
2009-07-31 |
Owen Anderson | Move a few more APIs back to 2.5 forms. The only remai... |
blob | commitdiff | raw | diff to current |
2009-07-30 |
Daniel Dunbar | Twines: Don't allow implicit conversion from integers... |
blob | commitdiff | raw | diff to current |
2009-07-30 |
Daniel Dunbar | Switch obvious clients to Twine instead of utostr ... |
blob | commitdiff | raw | diff to current |
2009-07-29 |
Owen Anderson | Move types back to the 2.5 API. |
blob | commitdiff | raw | diff to current |
2009-07-25 |
Daniel Dunbar | More migration to raw_ostream, the water has dried... |
blob | commitdiff | raw | diff to current |
2009-07-24 |
Owen Anderson | Revert the ConstantInt constructors back to their 2... |
blob | commitdiff | raw | diff to current |
2009-07-22 |
Daniel Dunbar | Remove unnecessary store to temporary std::string. |
blob | commitdiff | raw | diff to current |
2009-07-22 |
Owen Anderson | Get rid of the Pass+Context magic. |
blob | commitdiff | raw | diff to current |
2009-07-15 |
Owen Anderson | Revert yesterday's change by removing the LLVMContext... |
blob | commitdiff | raw | diff to current |
2009-07-14 |
Owen Anderson | Move EVER MORE stuff over to LLVMContext. |
blob | commitdiff | raw | diff to current |
2009-07-06 |
Owen Anderson | More LLVMContext-ification. |
blob | commitdiff | raw | diff to current |
2009-06-10 |
Jay Foad | Implement and use new method Function::hasAddressTaken(). |
blob | commitdiff | raw | diff to current |
2009-04-17 |
David Greene | Use a safer iterator interface and get rid of std C... |
blob | commitdiff | raw | diff to current |
2009-02-18 |
Dan Gohman | Add explicit keywords. |
blob | commitdiff | raw | diff to current |
2009-01-22 |
Gabor Greif | introduce a useful abstraction to find out if a Use... |
blob | commitdiff | raw | diff to current |
2009-01-15 |
Rafael Espindola | Add the private linkage. |
blob | commitdiff | raw | diff to current |
2008-11-16 |
Torok Edwin | If SI->size() is 0, we are not allowed to dereference... |
blob | commitdiff | raw | diff to current |
2008-09-26 |
Devang Patel | Now Attributes are divided in three groups |
blob | commitdiff | raw | diff to current |
2008-09-25 |
Devang Patel | Large mechanical patch. |
blob | commitdiff | raw | diff to current |
2008-09-24 |
Devang Patel | s/ParamAttrsWithIndex/FnAttributeWithIndex/g |
blob | commitdiff | raw | diff to current |
2008-09-23 |
Devang Patel | s/ParameterAttributes/Attributes/g |
blob | commitdiff | raw | diff to current |
2008-09-08 |
Duncan Sands | Update the callgraph correctly in ArgumentPromotion. |
blob | commitdiff | raw | diff to current |
2008-09-07 |
Duncan Sands | Correct a comment and strip trailing whitespace. |
blob | commitdiff | raw | diff to current |
2008-09-04 |
Dan Gohman | Tidy up several unbeseeming casts from pointer to intptr_t. |
blob | commitdiff | raw | diff to current |
2008-07-29 |
Matthijs Kooijman | Restructure ArgumentPromotion a bit. Instead of just... |
blob | commitdiff | raw | diff to current |
2008-05-29 |
Gabor Greif | convert more operand loops to iterator formulation |
blob | commitdiff | raw | diff to current |
2008-05-27 |
Duncan Sands | Fix some constructs that gcc-4.4 warns about. |
blob | commitdiff | raw | diff to current |
next |