]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - lib
Replace the dangling context hotfix with an assertion.
[opencl/llvm.git] / lib /
2013-11-15 Adrian PrantlReplace the dangling context hotfix with an assertion.
2013-11-15 Lang HamesRemove unused arguments.
2013-11-15 Lang HamesDuring folding for patchpoint/stackmap instructions...
2013-11-15 David BlaikieDwarfDebug: Push DISubprogram through updateSubprogramS...
2013-11-15 Arnold SchwaighoferLoopVectorizer: Use abi alignment for accesses with...
2013-11-15 David BlaikieDwarfCompileUnit: Push DIDescriptors through a getDIE...
2013-11-15 David BlaikieDwarfCompileUnit: Push DIDescriptor usage out from...
2013-11-15 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-15 Matt ArsenaultFix confusing machine verifier error.
2013-11-15 Andrew KaylorFix a problem in MCJIT identifying the module containin...
2013-11-15 Matt ArsenaultMake method static
2013-11-15 Chandler Carruth[PM] Fix an iterator problem spotted by the MSVC debug...
2013-11-15 Chandler Carruth[PM] Run clang-format on a few lines that I missed...
2013-11-15 Chad Rosier[AArch64] Fix the scalar NEON ACLE functions so that...
2013-11-15 Rui UeyamaPath: Recognize COFF import library file magic.
2013-11-15 Adrian PrantlReimplement r194843 in a slightly less broken way.
2013-11-15 Manman RenArgumentPromotion: correctly transfer TBAA tags and...
2013-11-15 Rui UeyamaReadobj: If NumbersOfSections is 0xffff, it's an COFF...
2013-11-15 Adrian PrantlRestore the behaviour from before r194728.
2013-11-15 Bob WilsonAvoid illegal integer promotion in fastisel
2013-11-15 Tom StellardR600/SI: Add VReg_96 register class to SIRegisterInfo...
2013-11-15 Andrew KaylorResolve JIT runtime linking problems on Android.
2013-11-15 Andrew KaylorDon't try to initialize memory for a global if the...
2013-11-15 Cameron McInallyAdd AVX512 unmasked FMA intrinsics and support.
2013-11-15 Daniel Sanders[mips][msa] lowerMSABitClear() should use SelectionDAG...
2013-11-15 Alexey SamsonovHopefully fix uninitialized memory read in AArch64AsmPa...
2013-11-15 Daniel SandersFix illegal DAG produced by SelectionDAG::getConstant...
2013-11-15 Justin Holewinski[NVPTX] Fix handling of indirect calls
2013-11-15 Yaron KerenCorrect spelling.
2013-11-15 Kostya Serebryany[asan] use GlobalValue::PrivateLinkage for coverage...
2013-11-15 Benjamin Kramerllvm-cov: Clean up memory leaks.
2013-11-15 Zoran JovanovicUse instr mapping for microMIPS in llvm-mc.
2013-11-15 Bob WilsonReapply "[asan] Poor man's coverage that works with...
2013-11-15 Matt ArsenaultAdd instcombine visitor for addrspacecast
2013-11-15 Matt ArsenaultAdd target hook to prevent folding some bitcasted loads.
2013-11-15 Bob WilsonRevert "[asan] Poor man's coverage that works with...
2013-11-15 Peter Zotov[llvm-c] Make LLVMGetTargetFromName actually work
2013-11-15 Peter Zotov[llvm-c] Add missing const qualifiers to LLVMCreateTarg...
2013-11-15 Peter Zotov[llvm-c] Simplify signature of LLVMGetTargetFromName
2013-11-15 Reed KotlerMake all the conditional Mips 16 branches get initially...
2013-11-15 Eric ChristopherUse a reference rather than a pointer as we don't expec...
2013-11-15 Matt ArsenaultAdd addrspacecast instruction.
2013-11-15 Tom StellardR600: Fix scheduling of instructions that use the LDS...
2013-11-14 Tom StellardR600/SI: Add processor type for Hawaii
2013-11-14 Andrew TrickWhen folding memory operands, preserve existing Machine...
2013-11-14 Matt ArsenaultR600/SI: Remove redundant legalizeOperands call
2013-11-14 Hans WennborgAdd #include raw_ostream.h in lib/Target/R600/SIFixSGPR...
2013-11-14 Matt ArsenaultR600/SI: Specify S_ADDK/S_MULK set SCC and are commutable
2013-11-14 David BlaikieDebugInfo: Simplify/narrow null-check for getOrCreateType
2013-11-14 Rui UeyamaRecognize 0x0000 as a COFF file magic.
2013-11-14 Chad Rosier[AArch64] Remove redundant Neon_immAllOnes/Neon_immAllZ...
2013-11-14 David BlaikieDwarfCompileUnit::getOrCreateContext: Return the compil...
2013-11-14 David BlaikieRemove unnecessary 'else' after return.
2013-11-14 Tim NorthoverARM: produce friendly error for invalid inline asm
2013-11-14 Rafael EspindolaError if we see an alias to a declaration.
2013-11-14 Kostya Serebryany[asan] Poor man's coverage that works with ASan
2013-11-14 Evgeniy Stepanov[msan] Fast path optimization for wrap-indirect-calls...
2013-11-14 NAKAMURA TakumiIR/GCOV.cpp: Use PRIu64 as format string with uint64_t.
2013-11-14 NAKAMURA TakumiWhitespace.
2013-11-14 Elena DemikhovskyAVX-512: Handled extractelement from mask vector;
2013-11-14 Matt ArsenaultIndentation fixes
2013-11-14 Matt ArsenaultAdd a comment
2013-11-14 Matt ArsenaultFix trailing whitespace in debug printing
2013-11-14 NAKAMURA Takumiyaml::Input::mapTag(): Don't use StringRef to hold...
2013-11-14 NAKAMURA TakumiWhitespace.
2013-11-14 NAKAMURA TakumiAArch64DAGToDAGISel::SelectVTBL(): Fix a warning. ...
2013-11-14 Andrew TrickMinor extension to llvm.experimental.patchpoint: don...
2013-11-14 Rafael EspindolaDon't mangle \n and "
2013-11-14 NAKAMURA TakumiR600/SIFixSGPRCopies.cpp: Fix \param to \return. [...
2013-11-14 NAKAMURA TakumiWhitespace.
2013-11-14 Kevin Qin[AArch64 neon] support poly64 and relevant intrinsic...
2013-11-14 Kevin QinImplement aarch64 neon instruction class SIMD misc.
2013-11-14 Nick KledzikAdd dyn_cast<> support to YAML I/O's IO class
2013-11-14 Michael GottesmanAdded BlockFrequencyInfo::view for displaying the block...
2013-11-14 Jiangning LiuImplement AArch64 NEON instruction set AdvSIMD (table).
2013-11-14 Yunzhong GaoFixing a heisenbug where the memory dependence analysis...
2013-11-14 Nick KledzikAdd simple support for tags in YAML I/O
2013-11-14 Yuchen Wullvm-cov: Slightly improved error checking.
2013-11-14 Yuchen Wullvm-cov: Removed StringMap holding GCOVLines.
2013-11-14 Yuchen Wullvm-cov: Replaced asserts with proper error handling.
2013-11-14 Michael GottesmanFixed 80+ violations.
2013-11-13 Tom StellardR600: Fix uninitialized variable usage
2013-11-13 Reed KotlerTake care of long short branch immediate instructions...
2013-11-13 Tom StellardR600/SI: Add support for private address space load...
2013-11-13 Tom StellardR600/SI: Prefer SALU instructions for bit shift operations
2013-11-13 Sebastian Popadd more comments around the delinearization of arrays
2013-11-13 Jakub StaszakSimplify code. No functionality change.
2013-11-13 Jakub StaszakUse StringRef instead of std::string
2013-11-13 Chad Rosier[AArch64] Add support for legacy AArch32 NEON scalar...
2013-11-13 Weiming ZhaoEnable generating legacy IT block for AArch32
2013-11-13 David BlaikieDIEHash: Move header include to be first in the impleme...
2013-11-13 Richard Sandiford[SystemZ] Add the general form of BCR
2013-11-13 Benjamin KramerMove Delinearization pass into an anonymous namespace.
2013-11-13 Benjamin KramerMake sure LLVMLoadLibraryPermanently gets an extern...
2013-11-13 Rafael EspindolaRemove AllowQuotesInName and friends from MCAsmInfo.
2013-11-13 Rafael EspindolaDon't call doFinalization from verifyFunction.
2013-11-13 Vladimir MedicFix bug in .gpword directive parsing.
2013-11-13 Zoran JovanovicSupport for microMIPS trap instruction with immediate...
2013-11-13 Alexey SamsonovFix -Wdelete-non-virtual-dtor warnings by making Sample...
2013-11-13 Diego NovilloSampleProfileLoader pass. Initial setup.
next